CC32xx SimpleLink Core SDK 7.10.01.03 Release Notes
Table of Contents
Introduction
This is a GA release of the Core SDK 7.10.01.03 for CC32xx devices.
Documentation
Open the Documentation Overview file in the docs/ folder for a full list of documentation.
What’s New
- A summary of changes made in the current release of this product can be found in the product Change Log.
Upgrade and Compatibility Information
- Removed support for TI-RTOS6.
- Generate FreeRTOS configuration with SysConfig
Host Support
See the SDK release notes for a description of which host operating systems are supported in this release.
Dependencies
See the SDK release notes for a description of which components and tools are required to work with this product.
Device Support
See the SDK release notes for a list of TI devices that are supported in this product.
Validation Information
The Core SDK was validated with the following components:
- Code Composer Studio 12.2.0
- GNU Code Generation Tools
- ARM GCC 9.2019.q4.major-0
- IAR Code Generation Tools
- ARM 9.32.1
- TI Clang Code Generation Tools
- ARM ti-cgt-armllvm_2.1.2.LTS-0
- FreeRTOS 202104.00-0
- SysConfig 1.10.0
- XDCTools 3.62.01.15
- Python 3.8.10
New Features
ID | Summary |
---|---|
TIRTOS-2171 | Update Core SDK User Guide |
TIDRIVERS-5777 | Update to APIs to use inclusive technical terminology |
TIDRIVERS-5210 | GPIO-owning drivers should call GPIO_init() and GPIO_setConfig() to set direction |
Bugs Resolved
ID | Summary |
---|---|
TIDRIVERS-5750 | Race condition in SemaphoreP_nortos pend |
TIDRIVERS-5507 | Core SDK libraries cannot be rebuilt in-field |
Known Issues
ID | Summary |
---|---|
TIRTOS-2164 | Simultaneous TI-RTOS 6 and TI-RTOS 7 support causes CCS XDS include path warning for TI-RTOS 6 |
TIDRIVERS-5149 | CC32 I2C driver should ensure transferCallback != NULL before enabling HWI |
TIDRIVERS-4232 | [I2SCC32XX] Skipping samples in MONO DMA mode |
TIDRIVERS-4187 | CC32XX SD Driver does not properly initialize after LPDS |
TIDRIVERS-1642 | NVSSPI25x driver does not work when using internal SPI CS |
Customer Support
- Use the E2E support forums for customer support.
- Use the External Bug and Enhancement System to track issues.
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
Prior Release Changes
A summary of changes made in previous releases of this product can be found in the product Change Log