110 #ifndef ti_drivers_watchdog_WatchdogCC32XX__include 111 #define ti_drivers_watchdog_WatchdogCC32XX__include 153 #define WatchdogCC32XX_CMD_IS_TIMER_ENABLE (Watchdog_CMD_RESERVED + 0) 162 #define WatchdogCC32XX_CMD_GET_TIMER_VALUE (Watchdog_CMD_RESERVED + 1) 172 #define WatchdogCC32XX_CMD_IS_TIMER_LOCKED (Watchdog_CMD_RESERVED + 2) 182 #define WatchdogCC32XX_CMD_GET_TIMER_RELOAD_VALUE (Watchdog_CMD_RESERVED + 3) Watchdog_DebugMode debugMode
Definition: WatchdogCC32XX.h:223
unsigned int intPriority
Definition: WatchdogCC32XX.h:206
uint32_t reloadValue
Definition: WatchdogCC32XX.h:207
Watchdog driver interface.
Watchdog Object for CC32XX.
Definition: WatchdogCC32XX.h:215
Watchdog hardware attributes for CC32XX.
Definition: WatchdogCC32XX.h:202
Power_NotifyObj notifyObj
Definition: WatchdogCC32XX.h:217
Watchdog_DebugMode
Watchdog debug stall settings.
Definition: Watchdog.h:264
uint32_t reloadValue
Definition: WatchdogCC32XX.h:222
unsigned int baseAddr
Definition: WatchdogCC32XX.h:204
Power notify object structure.
Definition: Power.h:442
const Watchdog_FxnTable WatchdogCC32XX_fxnTable
Watchdog function table for CC32XX.
unsigned int intNum
Definition: WatchdogCC32XX.h:205
The definition of a Watchdog function table that contains the required set of functions to control a ...
Definition: Watchdog.h:360
bool isOpen
Definition: WatchdogCC32XX.h:224