I2CCC32XX.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015-2020, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 /*!****************************************************************************
33  * @file I2CCC32XX.h
34  *
35  * @brief I2C driver implementation for a CC32XX I2C controller.
36  *
37  * The I2C header file should be included in an application as follows:
38  * @code
39  * #include <ti/drivers/I2C.h>
40  * #include <ti/drivers/i2c/I2CCC32XX.h>
41  * @endcode
42  *
43  * Refer to @ref I2C.h for a complete description of APIs and usage.
44  *
45  * ## Supported Bit Rates ##
46  * - #I2C_100kHz
47  * - #I2C_400kHz
48  *
49  ******************************************************************************
50  */
51 
52 #ifndef ti_drivers_i2c_I2CCC32XX__include
53 #define ti_drivers_i2c_I2CCC32XX__include
54 
55 #include <stdint.h>
56 #include <stdbool.h>
57 
58 #include <ti/drivers/I2C.h>
59 #include <ti/drivers/Power.h>
60 
61 #ifdef __cplusplus
62 extern "C" {
63 #endif
64 
65 /*
66  * Macros defining possible I2C signal pin mux options
67  *
68  * The bits in the pin mode macros are as follows:
69  * The lower 8 bits of the macro refer to the pin, offset by 1, to match
70  * driverlib pin defines. For example, I2CCC32XX_PIN_01_I2C_SCL & 0xff = 0,
71  * which equals PIN_01 in driverlib pin.h. By matching the PIN_xx defines in
72  * driverlib pin.h, we can pass the pin directly to the driverlib functions.
73  * The upper 8 bits of the macro correspond to the pin mux confg mode
74  * value for the pin to operate in the I2C mode. For example, pin 1 is
75  * configured with mode 1 to operate as I2C_SCL.
76  */
77 #define I2CCC32XX_PIN_01_I2C_SCL 0x100
78 #define I2CCC32XX_PIN_02_I2C_SDA 0x101
79 #define I2CCC32XX_PIN_03_I2C_SCL 0x502
80 #define I2CCC32XX_PIN_04_I2C_SDA 0x503
81 #define I2CCC32XX_PIN_05_I2C_SCL 0x504
82 #define I2CCC32XX_PIN_06_I2C_SDA 0x505
83 #define I2CCC32XX_PIN_16_I2C_SCL 0x90F
84 #define I2CCC32XX_PIN_17_I2C_SDA 0x910
96 /* Add I2CCC32XX_STATUS_* macros here */
97 
110 /* Add I2CCC32XX_CMD_* macros here */
111 
150 typedef struct {
151  I2C_BASE_HWATTRS
152 
154  uint32_t sclTimeout;
155  /* I2C clock pin configuration */
156  uint16_t clkPin;
157  /* I2C data pin configuration */
158  uint16_t dataPin;
160 
166 typedef struct {
167  I2C_BASE_OBJECT
168 
169  /* Burst counters */
170  uint16_t burstCount;
172 
173  /* Enumerated bit rate */
175 
176  /* For notification of wake from LPDS */
179 
180 #ifdef __cplusplus
181 }
182 #endif
183 
184 #endif /* ti_drivers_i2c_I2CCC32XX__include */
I2CCC32XX Object.
Definition: I2CCC32XX.h:166
I2C_BitRate
Bit rate for an I2C driver instance specified in the I2C_Params.
Definition: I2C.h:574
uint16_t dataPin
Definition: I2CCC32XX.h:158
Power Manager.
I2C_BASE_OBJECT uint16_t burstCount
Definition: I2CCC32XX.h:170
bool burstStarted
Definition: I2CCC32XX.h:171
I2C_BASE_HWATTRS uint32_t sclTimeout
Definition: I2CCC32XX.h:154
Power notify object structure.
Definition: Power.h:443
I2CCC32XX Hardware attributes.
Definition: I2CCC32XX.h:150
Power_NotifyObj notifyObj
Definition: I2CCC32XX.h:177
uint16_t clkPin
Definition: I2CCC32XX.h:156
I2C_BitRate bitRate
Definition: I2CCC32XX.h:174
Inter-Integrated Circuit (I2C) Driver.
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale