SimpleLink Gen1 to Gen2 SDK Migration Guide
Table of Contents
Appendicies
- Appendix I. Reference porting code
- Appendix I-1. Simplelink API porting code (sl_compat.h)
- Appendix I-2. OS API porting code
- Appendix I-2.1 OS adaption header (osi.h)
- Appendix I-2.2 OS adaption source (os_posix.c)
List of Figures
- Fig. 1: Top level SDK structure
- Fig. 2: Top level folder structure
- Fig. 3: Examples folder structure
List of Tables
- Table 1: Host driver API changes
1. Introduction
CC31xx SimpleLink Wi-Fi Network Processor and CC32xx SimpleLink Wi-Fi Wireless MCU are the second generation devices in the SimpleLink Wi-Fi and Internet-of-Things family. These devices introduce some new features and capabilities that further simplify the connectivity of things to the internet.
Among the new capabilities are:
- AP supporting up to 4 stations
- Improved provisioning
- Improved power consumption
- Increased number of secure sockets with a new ability to upgrade TCP socket to secure during connection
- IPv6 addressing scheme
- Return to factory defaults or Factory image
- Bundle protection to allow keeping the system integrity during OTA
- Security aspects:
- Secure file system
- Cloning protection
- Software tamper detection
- Trusted root certificate catalog for authentication
- Access control using tokens
- Other utilities such as secure content delivery
This document intends to guide users who already have experience with the CC3100/CC3200 devices and need to port their software to the new CC31xx/CC32xx family of devices. The document describes the new SDK structure and highlights the software components that require attention including host driver, OS layers, board drivers, and external libraries.
2. SDK Structure
2.1 Overview
The new SDK structure for CC31xx/CC32xx intends to create a common software development platform across all TI chipsets. Its main target is to emphasize the ease of use and specifically highlight:
- New folder structure which is easy to access and follow through
- Same look and feel for all documents and modules
- Simple migration between TI MCUs
- Simple migration between operating systems
2.2 High level view of SDK
Figure 1 illustrates the top level SDK structure. The SDK software abstracts the specific hardware (in this case, CC31xx/CC32xx) to the application.
The main target of the hardware abstraction layer is to simplify access to device modules. Each device or family of devices implements its device-specific implementation. In the previous SDK, this was also known as the driverlib module.
The RTOS layer implements the operating system. The SDK includes implementations for SYS/BIOS (TI-RTOS) and FreeRTOS. In case a different OS is desired, its implementation goes under the RTOS block. POSIX layer is used for OS abstraction. If a new OS is implemented, it needs to fit the POSIX layer. DPL (Driver Porting Layer) is used by the Drivers layer whenever OS services are required. The DPL abstracts the drivers similarly to how the POSIX layer abstracts the RTOS kernel functionality used by the application.
The Drivers layer is platform-independent. This layer bridges between the platform-dependent HAL layer and the application layer. This layer is common to all TI family of devices. In case OS services are required, the Drivers layer uses the DPL block.
The Middleware layer implements common libraries that may be used by the application. These components add additional functionality on top of the hardware-specific drivers. Examples of such common libraries include the graphic grlib, file system fatfs, and so forth.
Fig. 1: Top level SDK structure
2.3 Top level folder structure
Figure 2 illustrates the top level folder structure. The OS directory includes SYS/BIOS (TIRTOS) implementation as well as FreeRTOS implementation. The source
directory includes the third_party
directory for middleware implementation and ti
directory mainly for Drivers (/source/ti/drivers
directory) and HAL layers (/source/ti/devices/cc32xx/driverlib
directory). It also includes the net
directory for external libraries. Additional libraries may be added in future releases. For reference, the Wi-Fi host driver is located as one of the many drivers under /source/ti/drivers/net/wifi
directory. The examples
directory is detailed in section 2.4.
Fig. 2: Top level folder structure
2.4 Examples folder structure
Figure 3 illustrates the examples
folder structure. Every board flavor has a corresponding directory. As illustrated, CC32xxS and CC32xxSF implementations for the CC32xx secured and CC32xx secured flash devices are included. Each board has a sysbios
directory for TI-RTOS examples, drivers
directory for drivers examples, and demos
directory for a few full demos examples.
Fig. 3: Examples folder structure
3. Host Driver
3.1 Overview
The new host driver adds support for the new features and capabilities. Most of the APIs remain similar but not all of them are identical to those used in the CC3100/CC3200 host driver. The changes include modifications to function parameters (type, meaning or values), return codes and types, and new naming conventions.
Additionally, there are a few changes in device behavior or defaults that also require attention when moving to CC31xx/CC32xx devices.
3.2 SimpleLink device behavior and defaults changes
The following list outlines key changes to CC31xx/CC32xx SimpleLink devices that require attention. CC3100/CC3200 devices are marked as R1 denoting 1st generation devices while CC31xx/CC32xx devices are marked as R2 denoting 2nd generation devices:
- Device Default
- Wi-Fi Mode
- R1: STA
- R2: AP
- Regulatory Domain
- R1: US (channels 1-11)
- R2: EU (channels 1-13)
- Wi-Fi Mode
- Security related
- Behavior while the SFLASH is empty:
- R1: Start to run with some default settings
- R2: Device enters into a “lock” state and waits to be programmed. In this state, all APIs are blocked excluding those APIs intended for programming the device or return to factory image or default
- SFLASH Corruption
- R1: No clear indication, system behavior is not predicted
- R2: System is locked. The host gets an event that allows it to be able only to reprogram the system or try to return to factory image
- Certificate files
- R1: Certificates were located under /sys/cert/. Only der format supported
- R2: Certificates could be stored anywhere. Both der and pem formats supported. Enterprise certificates still need to be stored under predefined locations:
/sys/cert/ca.pem
/sys/cert/client.pem
/sys/cert/private.key
- Behavior while the SFLASH is empty:
- HTTP Web Server
- R1: HTML format
- R2: Improved web pages based on rest APIs
- IPv6
- R1: Not supported
- R2: IPv6 supported, disabled by default
- Supported only in STA mode
- **In host driver under
user.h
header file, ensure to#define SL_SUPPORT_IPV6**
Enable at least local address (global is optional). See netcfg.h header file for more details
IfBitmap = SL_NETCFG_IF_IPV6_STA_LOCAL | SL_NETCFG_IF_IPV6_STA_GLOBAL; sl_NetCfgSet(SL_NETCFG_IF,SL_NEFCFG_IF_STATE,sizeof(IfBitmap),&IfBitmap);
- File System
- R1: Support up to 100 user files
- R2: Support up to 180 user files
- CC3100 ForceAP GPIO (GPIO13):
- R1: Force the system to wake-up in AP mode regardless other settings
- R2: Removed
- Trusted root-certificate catalog:
- R1: NA
- R2: All certificate authorities should reside in the list of valid CAs as part of the certificate catalog file. Some of the file system security options require the CA to be part of the list otherwise it might be interpreted as a security alert. Secure sockets could be used without it but consequently, a warning might be sent to the Host. The Image Creator installs the certificate catalog by default.
- IPv4 Addressing
- LLA
- R1: When DHCP client is enabled and there is no DHCP server available, the device does not have a valid IPv4 address so it is not able to use the network
- R2: On timeout of trying to acquire an IPv4 address from a DHCP server, the system self-acquires an IP address using LLA protocol. This IP is limited to be used in a local network only. The host should be aware of this possibility.
- Default IP settings in AP mode:
- R1: 192.168.1.1
- R2: 10.123.45.1
- LLA
- API Errors codes
- R1: Each function implements its own error codes. Same error codes could repeat in different functions
- R2: Unique errors per function. All error definition available in a new header file
3.3 API changes
API modifications are required when porting a working application from CC3100/CC3200 to CC31xx/CC32xx. The type of change is either an API addition, API removal, API change, parameters extension or return value change. It can also be a combination of changes. New naming conventions for functions and variables are also used in order to align with unified coding conventions across all product families. Table 1 lists all API changes.
API name | Silo | Change type | Change description |
---|---|---|---|
sl_Start |
device | Return code | Extended return codes in case of error. For example, error of calibration, corrupted FS, device get locked, and so forth |
sl_DeviceSet |
device | API change Return code |
API was named sl_Devset SL_DEVICE_GENERAL_PERSISTENT option addedpersistent system configuration option saves configuration in the FS (valid after reset) SlDateTime_t members renamedConfigLen value was changed from _i8 to _i16 Return value was changed from _i32 to _i16 |
sl_DeviceGet |
device | API change Return code |
API was named sl_DevGet SlDateTime_t members renamedpConfigLen value was changed from _u8* to _u16* Return value was changed from _i32 to _i16 |
sl_DeviceEventMaskGet |
device | API change | API was named sl_EventMaskGet Event class removed: SL_EVENT_CLASS_GLOBAL Event class added: SL_DEVICE_EVENT_CLASS_NETUTIL Event mask bitmap changed for WLAN and NETAPP classes |
sl_DeviceEventMaskSet |
device | API change | API was named sl_EventMaskSet Event class removed: SL_EVENT_CLASS_GLOBAL Event class added: SL_DEVICE_EVENT_CLASS_NETUTIL Event mask bitmap changed for WLAN and NETAPP classes |
sl_DeviceUartSetMode |
device | API change | API was named sl_UartSetMode pUartParams type changes from SlDeviceUartIfParams_t* to SlUartIfParams_t* |
sl_FsClose |
fs | API change | Parameters: pCeritificateFileName , pSignature and SignatureLen are supported |
sl_FsOpen |
fs | API change Return code |
pFileHandle parameter removedFile handle returns as part of return code (together with error codes in case of failure) pToken parameter is supported |
sl_FsGetInfo |
fs | API change | Token parameter is supported |
sl_FsDel |
fs | API change | Token parameter is supported |
sl_FsGetFileList |
fs | New API | New API for file system listing |
sl_FsProgram |
fs | New API | New API for device programming |
sl_FsCtl |
fs | New API | New API to control various file system operations. For example, commit or rollback a file or a bundle, return to factory image or default, get storage info, and so forth |
sl_NetAppDnsGetHostByService |
netapp | Return code | Return value was changed from _i32 to _i16 |
sl_NetAppGetServiceList |
netapp | Parameters extended | IPv6 options added: SL_NET_APP_FULL_SERVICE_WITH_TEXT_IPV6_TYPE SL_NET_APP_FULL_SERVICE_IPV6_TYPE SL_NET_APP_SHORT_SERVICE_IPV6_TYPE |
sl_NetAppMDNSUnRegisterService |
netapp | API change | Parameter options added to the API |
sl_NetAppMDNSRegisterService |
netapp | Parameters extended | Parameter options extended: SL_NETAPP_MDNS_IPV6_IPV4_SERVICE SL_NETAPP_MDNS_IPV6_ONLY_SERVICE SL_NETAPP_MDNS_OPTION_UPDATE_TEXT SL_NETAPP_MDNS_OPTIONS_IS_NOT_PERSISTENT |
sl_NetAppPing |
netapp | API change | API was named sl_NetAppPingStart Structures renamed to SlNetAppPingReport_t and SlNetAppPingCommand_t |
sl_NetAppGet |
netapp | Parameters extended Return code |
Return value was changed from _i32 to _i16 Option names have been changed DNS option added: SL_NETAPP_DNS_CLIENT_TIME HTTP options added: SL_NETAPP_HTTP_SECONDARY_PORT_NUMBER SL_NETAPP_HTTP_SECONDARY_PORT_ENABLE SL_NETAPP_HTTP_PRIMARY_PORT_SECURITY_MODE |
sl_NetAppSet |
netapp | Parameters extended Return code |
Return value was changed from _i32 to _i16 Option names have been changed DNS Option added: SL_NETAPP_DNS_CLIENT_TIME Http options added: SL_NETAPP_HTTP_SECONDARY_PORT_NUMBER SL_NETAPP_HTTP_SECONDARY_PORT_ENABLE SL_NETAPP_HTTP_PRIMARY_PORT_SECURITY_MODE SL_NETAPP_HTTP_PRIVATE_KEY_FILENAME SL_NETAPP_HTTP_DEVICE_CERTIFICATE_FILE_NAME SL_NETAPP_HTTP_CA_CERTIFICATE_FILENAME |
sl_NetAppRecv |
netapp | New API | New API for retrieving data from the network processor following a Netapp request event |
sl_NetAppSend |
netapp | New API | New API for sending Netapp response or data following a Netapp request event |
sl_NetAppGet |
netapp | API change | Return value was changed from _i32 to _i16 |
sl_NetCfgGet |
netcfg | API change Parameters extended Return code |
Parameter ConfigId changed from _u8 to _u16 Parameter pConfigOpt changed from _u8* to _u16* Parameter pConfigLen changed from _u8* to _u16* Return value was changed from _i32 to _i16 |
sl_NetCfgSet |
netcfg | API change Parameters extended Return code |
Parameter ConfigId changed from _u8 to _u16 Parameter ConfigOpt changed from _u8 to _u16 Parameter ConfigLen changed from _u8 to _u16 Return value was changed from _i32 to _i16 ConfigId and ConfigOpt have been extended |
sl_SetSockOpt |
socket | Parameters extended | Socket options added:SL_SO_KEEPALIVETIME SL_SO_RX_NO_IP_BOUNDARY SL_SO_SECURE_ALPN SL_SO_PHY_TX_INHIBIT_THRESHOLD SL_SO_PHY_TX_TIMEOUT SL_SO_PHY_ALLOW_ACKS SL_SO_LINGER SL_SO_SECURE_EXT_CLIENT_CHLNG_RESP SL_SO_SECURE_DOMAIN_NAME_VERIFICATION Socket options changed: SL_SO_SECURE_MASK |
sl_NetUtilCmd |
netutil | New API | New API for performing utilities-related commands |
sl_NetUtilGet |
netutil | New API | New API for getting configurations of utilities |
sl_NetUtilSet |
netutil | New API | New API for setting configurations of utilities |
sl_WlanConnect |
wlan | Parameters extended | pSecParams changed to SlWlanSecParams_t type, its members changed and SL_WLAN_SEC_TYPE_WEP_SHARED addedpSecExtParams changed to SlWlanSecParamsExt_t |
sl_WlanProfileAdd |
wlan | Parameters extended | pSecParams changed to SlWlanSecParams_t type, its members changed and SL_WLAN_SEC_TYPE_WEP_SHARED addedpSecExtParams changed to SlWlanSecParamsExt_t |
sl_WlanProfileGet |
wlan | Parameters extended | pSecParams changed to SlWlanSecParams_t type, its members changed and SL_WLAN_SEC_TYPE_WEP_SHARED addedpSecExtParams changed to SlWlanSecParamsExt_t |
sl_WlanPolicySet |
wlan | Parameters extended | Policy types renamed For connection policy, open policy removed and autoSmartConfig renamed to autoProvisioning |
sl_WlanPolicyGet |
wlan | Parameters extended API change |
Policy types renamed For connection policy, open policy removed and autoSmartConfig renamed to autoProvisioning Policy argument has changed to pointer type from _u8 |
sl_WlanGetNetworkList |
wlan | Parameters extended | Sl_WlanNetworkEntry_t instead of SlWlanNetworkEntry_t Sl_WlanNetworkEntry_t members renamed and channel member added |
sl_WlanProvisioning |
wlan | New API | New API added in R2 to replace sl_WlanSmartConfigStart and sl_WlanSmartConfigStop |
sl_WlanSmartConfigStart |
wlan | API replaced | Replaced by sl_WlanProvisioning |
sl_WlanSmartConfigStop |
wlan | API replaced | Replaced by sl_WlanProvisioning |
sl_WlanGet |
wlan | Parameters extended | SL_WLAN_RX_FILTERS_ID addedSL_WLAN_CFG_AP_ACCESS_LIST_ID addedSL_WLAN_CFG_AP_ID options added:SL_WLAN_AP_OPT_MAX_STATIONS SL_WLAN_AP_OPT_MAX_STA_AGING SL_WLAN_AP_ACCESS_LIST_NUM_ENTRIES SL_WLAN_CFG_AP_ACCESS_LIST_ID |
sl_WlanSet |
wlan | Parameters extended | SL_WLAN_RX_FILTERS_ID addedSL_WLAN_CFG_AP_ID options added:SL_WLAN_AP_OPT_MAX_STATIONS SL_WLAN_AP_OPT_MAX_STA_AGING SL_WLAN_AP_ACCESS_LIST_MODE SL_WLAN_AP_ACCESS_LIST_ADD_MAC SL_WLAN_AP_ACCESS_LIST_DEL_MAC SL_WLAN_AP_ACCESS_LIST_DEL_IDX SL_WLAN_CFG_GENERAL_PARAM_ID options added:SL_WLAN_GENERAL_PARAM_OPT_SUSPEND_PROFILES SL_WLAN_GENERAL_PARAM_DISABLE_ENT_SERVER_AUTH |
NOTE: To reduce the initial porting effort, you may refer to the sample code provided below (see Appendix I-1. Simplelink API porting code) that converts the old CC3x00 API to the updated CC3x20 interface (it mostly includes the updates as defined by the table above).
For future compatibility, it is recommended to update the original application code so it directly uses the latest Simplelink API. Although the provided code can be used as is, it should be referred as an example for the required code adaptation.
Note also that the code covers most of the API changes, but not all of them. Some of the changes would still cause compilation errors and would need to be handled manually. The sample code only covers backward compatibility. There are new features and parameter values in the new release that must be handled specifically by the application (examples of usage can be found in the CC3x20 SDK demo code).
3.4 Miscellaneous
In additional to the changes above, the following additional changes were made to the new host driver:
netutil.c
: new module providing network utilities such as secure content delivery.errors.h
: new header file added to concentrate all errors types in the driver.user.h
: the following optional async event user’s callbacks were added:slcb_GetTimestamp
: enables the host driver to detect timeouts and errors during its communication with the network processor.slcb_NetAppRequestHdlr
: enables the application to respond to resource requests by the network processor during HTTP requests.slcb_NetAppRequestMemFree
: enables the host driver to free resources which were dynamically allocated by the application. If not implemented, static allocation is assumed.slcb_DeviceFatalErrorEvtHdlr
: enables the application to receive fatal error events which occur in the network processor or host driver, and require device restart. In previous version, these kinds of events have been notified by theslcb_DeviceGeneralEvtHdlr
callback.
4. Operating system
4.1 Overview
The SDK for CC3100/C3200 included an osi.h
header file which declared all the supported OS-related utilities as well as osi_tirtos.c
and osi_freertos.c
for specific SYS/BIOS (TIRTOS) and FreeRTOS implementations.
The SDK for CC31xx/CC32xx includes a POSIX layer which implements the operating system. The SDK includes implementations for SYS/BIOS (TI-RTOS) and FreeRTOS. In case a different OS is desired, it must be implemented such that its API matches the POSIX layer for OS abstraction.
POSIX implementation for FreeRTOS is located under: /os/freertos/posix
POSIX implementation for SYS/BIOS (TI-RTOS) is located under: /os/tirtos/packages/ti/sysbios/posix
NOTE: To reduce the initial porting effort, you may refer to the abstraction code provided here (see Appendix I-2. OS API porting code) that converts the obsolete OSI interface to POSIX calls. For future compatibility (and to eliminate redundant code), it is recommended to update the original application code so it directly uses the POSIX API. Although the provided code can be used as is, it should be referred as an example for the required code adaptation.
The following paragraphs describe the typical configuration of all OS-related elements using the POSIX APIs. Browse the POSIX documentation in case a special OS configuration is desired.
4.2 Threads
Thread creation is composed of a two-step procedure: setting the thread attributes and creating the thread. Thread attributes are configured using the pthread_attr
APIs. Thread creation is configured using the pthread
APIs.
int pthread_attr_init(pthread_attr_t *attr);
int pthread_attr_destroy(pthread_attr_t *attr);
pthread_attr_init()
initializes the pthread_attr_t
object pointed to by attr
with default values. The stack size is initialized to Task_defaultStackSize
and the priority to 1
. The other pthread_attr_
functions can be used to change the defaults.
pthread_attr_destroy()
destroys the pthread_attr_t
object pointed to by attr
.
To modify the stack size, pthread_attr_setstack()
needs to be used.
int pthread_attr_setstacksize(pthread_attr_t *attr, size_t stacksize);
To modify the thread priority, pthread_attr_setstack()
needs to be used.
int pthread_attr_setschedparam(pthread_attr_t *attr, const struct sched_param *schedparam);
To create a thread, pthread_create()
needs to be used.
int pthread_create(pthread_t *newthread, const pthread_attr_t *attr, void * (*startroutine)(void *), void *arg);
This function starts a new thread running the startroutine
function, with the parameter arg passed to startroutine
. If attr is NULL
, the thread is created with default pthread
attributes.
4.3 Semaphores
The following semaphore APIs are supported:
int sem_destroy(sem_t *sem);
int sem_getvalue(sem_t *sem, int *value);
int sem_init(sem_t *sem, int pshared, unsigned value);
int sem_post(sem_t *sem);
int sem_timedwait(sem_t *sem, const struct timespec *abstime);
int sem_trywait(sem_t *sem);
int sem_wait(sem_t *sem);
sem_wait()
waits forever on a semaphore where as sem_timedwait()
waits for a specific timeout. sem_timedwait()
API blocks only until the specified time has been reached or the semaphore becomes available, whichever happens first. Note that the time passed to the API is an absolute time, not a relative timeout. The timespec structure is defined in types.h
:
struct timespec {
time_t tv_sec; /* Seconds */
long tv_nsec; /* Nanoseconds */
};
To fill in the timespec
object, clock_gettime()
API needs to be used first.
clock_gettime(0, &abstime);
Add the relative timeout value to abstime
. For example:
abstime.tv_sec++; /* A one second timeout */
- or -
abstime.tv_nsec = 1000000; /* A one msec timeout */
4.4 Mutex
A mutex (or “mutual exclusion”) is a data structure used to allow multiple threads to share a resource without accessing it simultaneously. Upon mutex creation, its attributes can be created. The pthread_mutexattr_
APIs are used for setting and getting the attributes to be used when a mutex is created. They do not modify the attributes of a mutex that has already been created.
The default attributes, if not set, indicate that subsequent calls to lock the mutex will block, until the owner releases it. If the owner holds the mutex and tries to lock it again without first releasing it, a deadlock situation will occur.
To initialize or de-initialize a mutex:
int pthread_mutex_destroy(pthread_mutex_t *mutex);
int pthread_mutex_init(pthread_mutex_t *mutex, const pthread_mutexattr_t *attr);
attr
can be NULL
for default attributes.
To lock a mutex:
int pthread_mutex_lock(pthread_mutex_t *mutex);
int pthread_mutex_timedlock(pthread_mutex_t *mutex, const struct timespec *abstime);
int pthread_mutex_trylock(pthread_mutex_t *mutex);
The function pthread_mutex_lock()
blocks until the mutex is acquired by the calling thread. The non-blocking function, pthread_mutex_trylock()
, returns immediately, and if the mutex is available, the calling thread will now own it.
The pthread_mutex_timedlock()
API blocks only until the specified time has been reached or the mutex becomes available, whichever happens first. Note that the time passed to pthread_mutex_timedlock()
is an absolute time, not a relative timeout. The timespec structure is defined in types.h
:
struct timespec {
time_t tv_sec; /* Seconds */
long tv_nsec; /* Nanoseconds */
};
To fill in the timespec object, clock_gettime()
API needs to be used first.
clock_gettime(0, &abstime);
Add the relative timeout value to abstime
. For example:
abstime.tv_sec++; /* A one second timeout */
- or -
abstime.tv_nsec = 1000000; /* A one msec timeout */
To unlock a mutex:
int pthread_mutex_unlock(pthread_mutex_t *mutex);
4.5 Message queues
To create or open an existing message queue:
mqd_t mq_open(const char *name, int oflag, mode_t mode, struct mq_attr *attr);
mq_attr
structure includes flags (as for non-blocking mode), message size, and maximum number of messages in the queue.
To close an existing message queue:
int mq_close(mqd_t mqdes);
To send an element to or receive an element from the message queue:
long mq_timedreceive(mqd_t mqdes, char *msg_ptr, size_t msg_len, unsigned int *msg_prio);
int mq_timedsend(mqd_t mqdes, const char *msg_ptr, size_t msg_len, unsigned int msg_prio);
To send an element to or receive an element from the message queue and wait on timeout:
long mq_timedreceive(mqd_t mqdes, char *msg_ptr, size_t msg_len, unsigned int *msg_prio, const struct timespec *abstime);
int mq_timedsend(mqd_t mqdes, const char *msg_ptr, size_t msg_len, unsigned int msg_prio, const struct timespec *abstime);
These APIs block only until the specified time has been reached or a queue element becomes available, whichever happens first. Note that the time passed to pthread_mutex_timedlock()
is an absolute time, not a relative timeout. The timespec
structure is defined in types.h
:
struct timespec {
time_t tv_sec; /* Seconds */
long tv_nsec; /* Nanoseconds */
};
To fill in the timespec object, clock_gettime()
API needs to be used first.
clock_gettime(0, &abstime);
Add the relative timeout value to abstime
. For example:
abstime.tv_sec++; /* A one second timeout */
- or -
abstime.tv_nsec = 1000000; /* A one msec timeout */
4.6 Timers
The following timer APIs are supported:
int timer_create(clockid_t clockid, struct sigevent *evp, timer_t *timerid);
int timer_delete(timer_t timerid);
int timer_gettime(timer_t timerid, struct itimerspec *its);
int timer_settime(timer_t timerid, int flags, const struct itimerspec *value, struct itimerspec *ovalue);
The timer_create()
function creates a new timer
object. A handle to the newly created timer is stored in the timerid
parameter. clockid
parameter can be set to CLOCK_MONOTONIC
.
typedef struct sigevent {
int sigev_notify;
int sigev_signo;
sigval sigev_value;
void (*sigev_notify_function)(sigval val);
pthread_attr_t *sigev_notify_attributes;
} sigevent;
The evp
parameter points to a sigevent
structure, and must not be NULL
, since it contains the notification function that is called when the timer expires. For SYS/BIOS only, since it does not have support for signals, the sigev_signo
parameter in the structure is not used. However, the SYS/BIOS implementation of timer allows the application to specify whether the notification function is called from Swi context or from Task context. If the sigev_notify
field is set to SIGEV_SIGNAL
, the notification will be called from a Swi. In this case, the notification function must not make any blocking calls.
The following APIs get and set a timer’s expiration.
int timer_gettime(timer_t timerid, struct itimerspec *its);
int timer_settime(timer_t timerid, int flags, const struct itimerspec *value, struct itimerspec *ovalue);
Itimerspec
is as follows:
struct itimerspec {
struct timespec it_interval; /* Timer interval */
struct timespec it_value; /* Timer expiration */
};
The timer_settime()
API can be passed either a relative time or an absolute time when the timer expires. When this API is called, the timer will be armed if the it_value
parameter specifies a non-zero time. If it_value
specifies a time of 0
, the timer will be dis-armed. A non-zero it_interval
will cause the timer to fire periodically at the specified interval.
4.7 Memory management
Implementation for malloc()
or free()
for memory management is taken from the OS flavor used. For SYS/BIOS, it is taken from TI-RTOS package. For FreeRTOS, the package needs to be installed separately. The package includes the type of the heap used. For example, heap_4.c
can be used and all memory implementations should reside in this file.
5. Board Drivers
5.1 Overview
CC3200 SDK included driverlib
as the hardware abstraction layer. Calling to drivers was applied directly to one of the driverlib
APIs. This design requires the developer to know the details of every peripheral, its registers, the flow and procedures of how to configure it, and so forth.
CC32xx SDK is designed differently. As described in Figure 1, the original driverlib
still exists and is located under /ti/devices/cc32xx/driverlib
. On top of the driverlib
, there is a new abstraction layer that is referred to TI Drivers and is located under /ti/drivers
. This layer is common to all TI family of devices. The application layer should call the TI Drivers layer instead of directly calling Driverlib.
In case OS services are required, the TI Drivers layer uses the DPL block (Driver Porting Layer). The DPL block for SYS/BIOS is located under /os/tirtos/packages/ti/dpl
. The DPL block for FreeRTOS is located under /os/freertos/dpl
. In case a different RTOS is desired, its corresponding DPL block needs to be implemented.
5.2 Programming model
The next few sections describe a set of discrepancies between drivers’ implementation and usage on CC3200 SDK and CC32xx SDK.
5.2.1 Driver configuration and initialization
5.2.1.1 CC3200 SDK
Driver configuration is implemented in dedicated APIs according to the peripheral and is located in interface files under /example/common
directory. The name convention is <peripheral>_if.c/h
; usually it is part of the initialization function.
5.2.1.2 CC32xx SDK
Driver configuration is implemented in a board-specific file according to the board flavor. For the CC3220S device, it is CC3220S_LAUNCHXL.c/h
and board.h
, and can be found under /source/ti/boards/CC3220S_LAUNCHXL
directory. For the CC3220SF device, it is CC3220SF_LAUNCHXL.c/h
and board.h
, and can be found under /source/ti/boards/CC3220SF_LAUNCHXL
directory. For the CC3235S device, it is CC3235S_LAUNCHXL.c/h
and board.h
, and can be found under /source/ti/boards/CC3235S_LAUNCHXL
directory. For the CC3235SF device, it is CC3235SF_LAUNCHXL.c/h
and board.h
, and can be found under /source/ti/boards/CC3235SF_LAUNCHXL
directory.
These files include configuration and setup for all peripherals. Each peripheral includes structures which include an object for TI drivers internal usage (application layer should not alter it), HW attributes configuration and functions table initialized to peripheral specific operations.
For example:
/*
* =============================== Watchdog ===============================
*/
#include <ti/drivers/Watchdog.h>
#include <ti/drivers/watchdog/WatchdogCC3200.h>
WatchdogCC3200_Object watchdogCC3220SObjects[CC3220S_LAUNCHXL_WATCHDOGCOUNT];
const WatchdogCC3200_HWAttrs watchdogCC3220SHWAttrs[CC3220S_LAUNCHXL_WATCHDOGCOUNT] =
{
{
.baseAddr = WDT_BASE,
.intNum = INT_WDT,
.intPriority = (~0),
.reloadValue = 80000000 // 1 second period at default CPU clock freq
}
};
const Watchdog_Config Watchdog_config[CC3220S_LAUNCHXL_WATCHDOGCOUNT] =
{
{
.fxnTablePtr = &WatchdogCC3200_fxnTable,
.object = &watchdogCC3220SObjects[CC3220S_LAUNCHXL_WATCHDOG0],
.hwAttrs = &watchdogCC3220SHWAttrs[CC3220S_LAUNCHXL_WATCHDOG0]
}
};
const uint8_t Watchdog_count = CC3220S_LAUNCHXL_WATCHDOGCOUNT;
Functions for peripherals initialization is located in the board.h
header file and should be invoked from application layer.
5.2.2 Set of APIs
5.2.2.1 CC3200 SDK
The set of drivers APIs pointing to the driversLib is located under the /driverlib
directory. Another layer is implemented according to the peripheral and is located in interface files under /example/common
directory. The name convention is <peripheral>_if.c
or <peripheral>_if.h
. The application layer may directly call the driverLib
APIs or use the interface files.
5.2.2.2 CC32xx SDK
The set of drivers APIs pointing to TI drivers is located under /source/ti/drivers
directory. Each peripheral has a C function following its name which implements the supported operations. Using this model, some less typical device-specific features are not available. The motivation is that TI Drivers abstract the common features rather than providing feature-completeness.
In a different programming model, it is possible to directly interact with the driverLib
layer. The goal of this model is to provide most (if not all) of the features of the device or peripheral at an abstracted API level. Since APIs and features are closely tied to the hardware, it may not be easy to migrate the application code from one MCU to another.
The TI Drivers include files per peripheral in its root directory as well as directory per peripheral. All APIs used by the application layer can be found in the root directory files. These APIs further call similar APIs that are implemented under the directory per peripheral. For example, watchdog
includes the following APIs in watchdog.c
:
void Watchdog_clear(Watchdog_Handle handle)
void Watchdog_close(Watchdog_Handle handle)
int Watchdog_control(Watchdog_Handle handle, unsigned int cmd, void *arg)
void Watchdog_init(void)
Watchdog_Handle Watchdog_open(unsigned int index, Watchdog_Params *params)
void Watchdog_Params_init(Watchdog_Params *params)
void Watchdog_setReload(Watchdog_Handle handle, uint32_t ticks)
uint32_t Watchdog_convertMsToTicks(Watchdog_Handle handle, uint32_t milliseconds)
6. External libraries
External libraries refer to pre-compiled libraries (with sources) implementing functionalities that are required by the application.
The CC3200 SDK included the following libraries:
- Under
/simplelink_extlib
- OTA and FLC for Over-the-Air update
- Under
/netapps
- HTTP client and server
- JSON parser
- SMTP client
- TFTP client
- XMPP client
- MQTT client and server
The CC32xx SDK currently includes the following libraries:
- Under
/source/ti/net/
- OTA for Over-the-Air update
- HTTP client
- MQTT client and server
- AT Command
- SNTP - Simple Network Time Protocol
- Under
/source/ti/utils/
- JSON parser
Further libraries are planned in future releases.
6.1 OTA library
OTA design is different in CC3220/CC3235 compared to CC3200, so it is not possible to port to SimpleLink Gen2 devices. The main reasons for redesigning OTA include the new secured file system and the new boot loader.
In SimpleLink Gen2 devices, the file system enables bundle support and rollback/commit options in case a new image found to be non-valid. SimpleLink Gen1 devices do not have this feature, and this is why a new entity called Secondary boot loader was introduced. Additionally, the SimpleLink Gen2 devices boot loader has full support for OTA procedure including a watchdog.
Although Gen1 OTA implementation can be used as-is on Gen2 devices, it is highly recommended to move to the new OTA design and take advantage of the new features supported by the boot loader and the file system.
Appendix I. Reference porting code
This chapter contains a reference C code (header and source files) that can be used to reduce the porting effort. The reference code provided below handles both the Simplelink driver’s API changes (see Appendix I-1. Simplelink API porting code) and OS API changes (see Appendix I-2. OS API porting code).
IMPORTANT: This code is provided to ease the initial migration efforts. It is recommended that a customer will update the original code (based on the given reference) so it directly uses the new API.
NOTE: As driverlib (board specific peripheral drivers) still part of the new CC32xx SDK (see Board Drivers), the direct calls to driverlib API would work as is. For future compatibility, it is also recommended to replace these calls with the equivalent TI drivers’ ones.
Appendix I-1. Simplelink API porting code (sl_compat.h)
The following header file contains most of the definitions required for the Simplelink driver API migration. Few other updates must be fixed manually to resolve specific compilation error (see API changes for details on required fix).
This header should be included by any source file that uses the R1 drivers’ API (include sl_compat.h
just before the simplelink.h
is included).
/*
* Copyright (C) 2016 Texas Instruments Incorporated
*
* All rights reserved. Property of Texas Instruments Incorporated.
* Restricted rights to use, duplicate or disclose this code are
* granted through contract.
*
* The program may not be used without the written permission of
* Texas Instruments Incorporated or against the terms and conditions
* stipulated in the agreement under which this program has been supplied,
* and under no circumstances can it be used with non-TI connectivity device.
*
*/
/*****************************************************************************/
/* Include files */
/*****************************************************************************/
#ifndef __SL_COMPAT_H__
#define __SL_COMPAT_H__
#ifdef __cplusplus
extern "C" {
#endif
#ifdef SUPPORT_SL_R1_API
/* Updated Macro Definitions */
#define SL_DEVICE_GENERAL_CONFIGURATION SL_DEVICE_GENERAL
#define SL_DEVICE_GENERAL_CONFIGURATION_DATE_TIME \
SL_DEVICE_GENERAL_DATE_TIME
#define SL_SCAN_SEC_TYPE_OPEN SL_WLAN_SEC_TYPE_OPEN
#define SL_SCAN_SEC_TYPE_WEP SL_WLAN_SEC_TYPE_WEP
#define SL_SCAN_SEC_TYPE_WPA SL_WLAN_SEC_TYPE_WPA
#define SL_SCAN_SEC_TYPE_WPA2 SL_WLAN_SEC_TYPE_WPA_WPA2
#define FS_MODE_OPEN_WRITE SL_FS_WRITE
#define FS_MODE_OPEN_READ SL_FS_READ
#define SL_POLICY_CONNECTION SL_WLAN_POLICY_CONNECTION
#define SL_POLICY_SCAN SL_WLAN_POLICY_SCAN
#define SL_POLICY_PM SL_WLAN_POLICY_PM
#define SL_POLICY_P2P SL_WLAN_POLICY_P2P
#define SL_NORMAL_POLICY SL_WLAN_NORMAL_POLICY
#define SL_BSSID_LENGTH SL_WLAN_BSSID_LENGTH
#define SL_WLAN_CONNECT_EVENT SL_WLAN_EVENT_CONNECT
#define SL_WLAN_DISCONNECT_EVENT SL_WLAN_EVENT_DISCONNECT
#define SL_WLAN_SMART_CONFIG_COMPLETE_EVENT SL_WLAN_EVENT_PROVISIONING_STATUS
#define SL_WLAN_STA_CONNECTED_EVENT SL_WLAN_EVENT_P2P_CLIENT_ADDED
#define SL_WLAN_STA_DISCONNECTED_EVENT SL_WLAN_EVENT_P2P_CLIENT_REMOVED
#define SL_USER_INITIATED_DISCONNECTION SL_WLAN_DISCONNECT_USER_INITIATED
#define WLAN_AP_OPT_SSID SL_WLAN_AP_OPT_SSID
#define WLAN_AP_OPT_CHANNEL SL_WLAN_AP_OPT_CHANNEL
#define WLAN_AP_OPT_HIDDEN_SSID SL_WLAN_AP_OPT_HIDDEN_SSID
#define WLAN_AP_OPT_SECURITY_TYPE SL_WLAN_AP_OPT_SECURITY_TYPE
#define WLAN_AP_OPT_PASSWORD SL_WLAN_AP_OPT_PASSWORD
#define WLAN_AP_OPT_MAX_STATIONS SL_WLAN_AP_OPT_MAX_STATIONS
#define SL_SEC_TYPE_OPEN SL_WLAN_SEC_TYPE_OPEN
#define SL_SEC_TYPE_WEP SL_WLAN_SEC_TYPE_WEP
#define SL_SEC_TYPE_WPA SL_WLAN_SEC_TYPE_WPA
#define SL_SEC_TYPE_WPA_WPA2 SL_WLAN_SEC_TYPE_WPA_WPA2
#define WLAN_GENERAL_PARAM_OPT_STA_TX_POWER SL_WLAN_GENERAL_PARAM_OPT_STA_TX_POWER
#define WLAN_GENERAL_PARAM_OPT_AP_TX_POWER SL_WLAN_GENERAL_PARAM_OPT_AP_TX_POWER
#define SL_REMOVE_RX_FILTER SL_WLAN_RX_FILTER_REMOVE
#define SL_NETAPP_IP_LEASED_EVENT SL_NETAPP_EVENT_DHCPV4_LEASED
#define SL_NETAPP_IP_RELEASED_EVENT SL_NETAPP_EVENT_DHCPV4_RELEASED
#define SL_NETAPP_IPV4_IPACQUIRED_EVENT SL_NETAPP_EVENT_IPV4_ACQUIRED
#define SL_NETAPP_HTTPGETTOKENVALUE_EVENT SL_NETAPP_EVENT_HTTP_TOKEN_GET
#define SL_NETAPP_HTTPPOSTTOKENVALUE_EVENT SL_NETAPP_EVENT_HTTP_TOKEN_POST
#define SL_NET_APP_HTTP_SERVER_ID SL_NETAPP_HTTP_SERVER_ID
#define SL_IPV4_DNS_CLIENT SL_NETCFG_IPV4_DNS_CLIENT
#define SL_MAC_ADDRESS_GET SL_NETCFG_MAC_ADDRESS_GET
#define SL_MAC_ADDRESS_SET SL_NETCFG_MAC_ADDRESS_SET
#define SL_IPV4_STA_P2P_CL_DHCP_ENABLE SL_NETCFG_IPV4_DHCP_CLIENT
#define SL_SO_SECURE_FILES_DH_KEY_FILE_NAME SL_SO_SECURE_FILES_PEER_CERT_OR_DH_KEY_FILE_NAME
#define SO_SECURE_DOMAIN_NAME_VERIFICATION SL_SO_SECURE_DOMAIN_NAME_VERIFICATION
/*** Updatetd Structure Names ***/
#define Sl_WlanNetworkEntry_t SlWlanNetworkEntry_t
#define SlHttpServerEvent_t SlNetAppHttpServerEvent_t
#define SlHttpServerResponse_t SlNetAppHttpServerResponse_t
#define APModeStaConnected P2PClientAdded
#define APModestaDisconnected P2PClientRemoved
#define STAandP2PModeWlanConnected Connect
#define STAandP2PModeDisconnected Disconnect
#define SlSecParams_t SlWlanSecParams_t
#define SlSecParamsExt_t SlWlanSecParamsExt_t
#define SlGetSecParamsExt_t SlWlanGetSecParamsExt_t
#define SlWlanProtocolInfoElement_t SlWlanInfoElement_t
#define SlWlanProtocolSetInfoElement_t SlWlanSetInfoElement_t
#define slWlanConnectAsyncResponse_t SlWlanEventDisconnect_t /* ??? */
#define _WlanRxFilterOperationCommandBuff_t SlWlanRxFilterOperationCommandBuff_t
#define slPeerInfoAsyncResponse_t SlWlanEventP2PClientAdded_t
#define SlVersionFull SlDeviceVersion_t
#define SlSockSecureMethod SlSockSecureMethod_t
#define SlSockSecureMask SlSockSecureMask_t
/*** Updatetd Structure Members Names ***/
#define AllocatedLen StorageSize
#define FileLen Len
#define NonblockingEnabled NonBlockingEnabled
#define reason Reason
#define reason_code ReasonCode
#define sd Sd
#define type Type
#define val Val
#define mac Mac
#define secureMask SecureMask
#define secureMethod SecureMethod
#define sl_tm_year tm_year
#define sl_tm_mon tm_mon
#define sl_tm_day tm_day
#define sl_tm_hour tm_hour
#define sl_tm_min tm_min
#define sl_tm_sec tm_sec
#define socketAsyncEvent SocketAsyncEvent
#define deviceDriverReport DeviceDriverReport
#define deviceEvent DeviceEvent
#define deviceReport DeviceReport
#define ipAcquiredV4 IpAcquiredV4
#define ipLeased IpLeased
#define ipReleased IpReleased
#define status Status
#define rssi Rssi
#define bssid Bssid
#define ssid Ssid
#define ssid_len SsidLen
#define sec_type SecurityInfo
#define ssid_name SsidName
#define FilterIdMask FilterBitmap
/*** Updatetd Error Names ***/
#define SL_FS_ERR_FILE_NOT_EXISTS SL_ERROR_FS_FILE_NOT_EXISTS
#define SL_EAGAIN SL_ERROR_BSD_EAGAIN
#define SL_ENSOCK SL_ERROR_BSD_ENSOCK
#define SL_INEXE SL_ERROR_BSD_INEXE
#define SL_ESECCLOSED SL_ERROR_BSD_ESECCLOSED
#define SL_ECLOSE SL_ERROR_BSD_ECLOSE
#define SL_ESECT00MANYSSLOPENED SL_ERROR_BSD_ESECT00MANYSSLOPENED
#define SL_FS_FILE_HAS_NOT_BEEN_CLOSE_CORRECTLY \
SL_ERROR_FS_FILE_HAS_NOT_BEEN_CLOSE_CORRECTLY
#define SL_ESEC_RSA_WRONG_TYPE_E
#define SL_ESEC_ASN_SIG_CONFIRM_E SL_ERROR_BSD_ESEC_ASN_SIG_CONFIRM_E
#define ROLE_STA_ERR SL_ERROR_ROLE_STA_ERR
#define ROLE_AP_ERR SL_ERROR_ROLE_AP_ERR
#define ROLE_P2P_ERR SL_ERROR_ROLE_P2P_ERR
/*** Update Macro Functions ***/
#define SL_CONNECTION_POLICY(Auto,Fast,Open,anyP2P,autoSmartConfig) \
SL_WLAN_CONNECTION_POLICY(Auto,Fast,anyP2P,autoSmartConfig)
#define SL_SCAN_POLICY(enable) \
SL_WLAN_SCAN_POLICY(enable, 0)
#define FS_MODE_OPEN_CREATE(_maxSize_, _flag_) \
(SL_FS_CREATE | SL_FS_CREATE_MAX_SIZE( _maxSize_ ))
/*** Updatetd Function ***/
#define sl_WlanRxFilterSet(opcode, maskeSize, mask) \
sl_WlanSet(SL_WLAN_RX_FILTERS_ID, opcode, mask, maskeSize)
#define sl_DevSet sl_DeviceSet
#define sl_DevGet sl_DeviceGet
#endif // SUPPORT_SL_R1_API
#ifdef __cplusplus
}
#endif /* __cplusplus */
#endif /* __SL_COMPAT_H__ */
Appendix I-2. OS API porting code
The following code (header and source file) contains implementation of POSIX . Most of the porting is achieved by using direct (MACRO) calls to POSIX API (within the osi.h
), but some updates required specific handling in a source file (osi_posix
) mainly due to the following:
- OSI API requires maintaining a context (e.g. for storing the Message queue element’s size)
- To avoid long/complicated macros (e.g. for Task creation which prepares the thread attributes through several
pthread
system calls).
Appendix I-2.1 OS adaption header (osi.h)
This header should replace the osi.h
used in CC3200 SDK. This supposed to be included by any source that uses OS resources.
//*****************************************************************************
// osi.h
//
// MACRO and Function prototypes for TI-RTOS and Free-RTOS API calls
//
// Copyright (C) 2014 Texas Instruments Incorporated - https://www.ti.com/
//
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list zof conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
//
//*****************************************************************************
#ifndef __OSI_H__
#define __OSI_H__
#include <pthread.h>
#include <time.h>
#include <unistd.h>
#include <ti/sysbios/BIOS.h>
#ifdef __cplusplus
extern "C" {
#endif
#define OSI_WAIT_FOREVER (0xFFFFFFFF)
#define OSI_NO_WAIT (0)
#ifndef SPAWN_TASK_STACK
#define STACK_LEN (2048) /*Stack Size*/
#else
#define STACK_LEN (SPAWN_TASK_STACK)
#endif
#define OSI_OK 0
#define OSI_FAILURE SL_ERROR_BSD_SOC_ERROR
#define OSI_OPERATION_FAILED SL_ERROR_BSD_SOC_ERROR
#define OSI_ABORTED SL_ERROR_BSD_SOC_ERROR
#define OSI_INVALID_PARAMS SL_ERROR_BSD_EINVAL
#define OSI_MEMORY_ALLOCATION_FAILURE SL_ERROR_BSD_ENOMEM
#define OSI_TIMEOUT SL_ERROR_BSD_ETIMEDOUT
#define OSI_EVENTS_IN_USE -16 //SL_ERROR_BSD_EBUSY
#define OSI_EVENT_OPEARTION_FAILURE SL_ERROR_BSD_SOC_ERROR
typedef int OsiReturnVal_e;
//#define ENTER_CRITICAL_SECTION osi_EnterCritical()
//#define EXIT_CRITICAL_SECTION osi_ExitCritical()
typedef void* OsiMsgQ_t;
/*!
\brief type definition for a time value
\note On each porting or platform the type could be whatever is needed - integer, pointer to structure etc.
*/
//typedef unsigned int OsiTime_t;
typedef unsigned int OsiTime_t;
/*!
\brief type definition for a sync object container
Sync object is object used to synchronize between two threads or thread and interrupt handler.
One thread is waiting on the object and the other thread send a signal, which then
release the waiting thread.
The signal must be able to be sent from interrupt context.
This object is generally implemented by binary semaphore or events.
\note On each porting or platform the type could be whatever is needed - integer, structure etc.
*/
//typedef unsigned int OsiSyncObj_t;
typedef sem_t OsiSyncObj_t;
/*!
\brief type definition for a locking object container
Locking object are used to protect a resource from mutual accesses of two or more threads.
The locking object should support re-entrant locks by a signal thread.
This object is generally implemented by mutex semaphore
\note On each porting or platform the type could be whatever is needed - integer, structure etc.
*/
//typedef unsigned int OsiLockObj_t;
typedef pthread_mutex_t OsiLockObj_t;
/*!
\brief type definition for a spawn entry callback
the spawn mechanism enable to run a function on different context.
This mechanism allow to transfer the execution context from interrupt context to thread context
or changing the context from an unknown user thread to general context.
The implementation of the spawn mechanism depends on the user's system requirements and could varies
from implementation of serialized execution using single thread to creating thread per call
\note The stack size of the execution thread must be at least of TBD bytes!
*/
typedef short (*P_OSI_SPAWN_ENTRY)(void* pValue);
typedef void (*P_OSI_EVENT_HANDLER)(void* pValue);
typedef void* (*P_OSI_TASK_ENTRY)(void* pValue);
typedef void (*P_OSI_INTR_ENTRY)(void);
typedef pthread_t OsiTaskHandle;
int osi_ThreadCreate(void *(*pEntry)(void *),unsigned short stackDepth,void *pvParameters,unsigned long uxPriority,pthread_t *pThread);
/*!
\brief This function registers an interrupt in NVIC table
The sync object is used for synchronization between different thread or ISR and
a thread.
\param iIntrNum - Interrupt number to register
\param pEntry - Pointer to the interrupt handler
\return upon successful creation the function should return 0
Otherwise, a negative value indicating the error code shall be returned
\note
\warning
*/
OsiReturnVal_e osi_InterruptRegister(int iIntrNum,P_OSI_INTR_ENTRY pEntry,unsigned char ucPriority);
/*!
\brief This function De-registers an interrupt in NVIC table
\param iIntrNum - Interrupt number to register
\param pEntry - Pointer to the interrupt handler
\return upon successful creation the function should return Positive number
Otherwise, a negative value indicating the error code shall be returned
\note
\warning
*/
void osi_InterruptDeRegister(int iIntrNum);
/*!
\brief This function creates a sync object
The sync object is used for synchronization between different thread or ISR and
a thread.
\param pSyncObj - pointer to the sync object control block
\return upon successful creation the function should return 0
Otherwise, a negative value indicating the error code shall be returned
\note
\warning
*/
//OsiReturnVal_e osi_SyncObjCreate(OsiSyncObj_t* pSyncObj);
#define osi_SyncObjCreate(pSyncObj) sem_init(pSyncObj, 0 , 0)
/*!
\brief This function deletes a sync object
\param pSyncObj - pointer to the sync object control block
\return upon successful deletion the function should return 0
Otherwise, a negative value indicating the error code shall be returned
\note
\warning
*/
//OsiReturnVal_e osi_SyncObjDelete(OsiSyncObj_t* pSyncObj);
#define osi_SyncObjDelete(pSyncObj) sem_destroy(pSyncObj)
/*!
\brief This function generates a sync signal for the object.
All suspended threads waiting on this sync object are resumed
\param pSyncObj - pointer to the sync object control block
\return upon successful signalling the function should return 0
Otherwise, a negative value indicating the error code shall be returned
\note the function could be called from ISR context
\warning
*/
//OsiReturnVal_e osi_SyncObjSignal(OsiSyncObj_t* pSyncObj);
#define osi_SyncObjSignal(pSyncObj) sem_post(pSyncObj)
/*!
\brief This function generates a sync signal for the object.
from ISR context.
All suspended threads waiting on this sync object are resumed
\param pSyncObj - pointer to the sync object control block
\return upon successful signalling the function should return 0
Otherwise, a negative value indicating the error code shall be returned
\note the function is called from ISR context
\warning
*/
//OsiReturnVal_e osi_SyncObjSignalFromISR(OsiSyncObj_t* pSyncObj);
#define osi_SyncObjSignalFromISR(pSyncObj) sem_post(pSyncObj)
/*!
\brief This function waits for a sync signal of the specific sync object
\param pSyncObj - pointer to the sync object control block
\param Timeout - numeric value specifies the maximum number of mSec to
stay suspended while waiting for the sync signal
Currently, the simple link driver uses only two values:
- OSI_WAIT_FOREVER
- OSI_NO_WAIT
\return upon successful reception of the signal within the timeout window return 0
Otherwise, a negative value indicating the error code shall be returned
\note
\warning
*/
//OsiReturnVal_e osi_SyncObjWait(OsiSyncObj_t* pSyncObj , OsiTime_t Timeout);
#define osi_SyncObjWait(pSyncObj, Timeout) sem_wait_timed(pSyncObj, Timeout)
/*!
\brief This function clears a sync object
\param pSyncObj - pointer to the sync object control block
\return upon successful clearing the function should return 0
Otherwise, a negative value indicating the error code shall be returned
\note
\warning
*/
//OsiReturnVal_e osi_SyncObjClear(OsiSyncObj_t* pSyncObj);
#define osi_SyncObjClear(pSyncObj) sem_wait_timed(pSyncObj, 0)
/*!
\brief This function creates a locking object.
The locking object is used for protecting a shared resources between different
threads.
\param pLockObj - pointer to the locking object control block
\return upon successful creation the function should return 0
Otherwise, a negative value indicating the error code shall be returned
\note
\warning
*/
//OsiReturnVal_e osi_LockObjCreate(OsiLockObj_t* pLockObj);
#define osi_LockObjCreate(pLockObj) pthread_mutex_init(pLockObj, NULL)
/*!
\brief This function deletes a locking object.
\param pLockObj - pointer to the locking object control block
\return upon successful deletion the function should return 0
Otherwise, a negative value indicating the error code shall be returned
\note
\warning
*/
//OsiReturnVal_e osi_LockObjDelete(OsiLockObj_t* pLockObj);
#define osi_LockObjDelete(pLockObj) pthread_mutex_destroy(pLockObj, NULL)
/*!
\brief This function locks a locking object.
All other threads that call this function before this thread calls
the osi_LockObjUnlock would be suspended
\param pLockObj - pointer to the locking object control block
\param Timeout - numeric value specifies the maximum number of mSec to
stay suspended while waiting for the locking object
Currently, the simple link driver uses only two values:
- OSI_WAIT_FOREVER
- OSI_NO_WAIT
\return upon successful reception of the locking object the function should return 0
Otherwise, a negative value indicating the error code shall be returned
\note
\warning
*/
//OsiReturnVal_e osi_LockObjLock(OsiLockObj_t* pLockObj , OsiTime_t Timeout);
#define osi_LockObjLock(pLockObj, Timeout) mutex_lock_timed(pLockObj, Timeout)
/*!
\brief This function unlock a locking object.
\param pLockObj - pointer to the locking object control block
\return upon successful unlocking the function should return 0
Otherwise, a negative value indicating the error code shall be returned
\note
\warning
*/
//OsiReturnVal_e osi_LockObjUnlock(OsiLockObj_t* pLockObj);
#define osi_LockObjUnlock(pLockObj) pthread_mutex_unlock(pLockObj)
/*!
\brief This function call the pEntry callback from a different context
\param pEntry - pointer to the entry callback function
\param pValue - pointer to any type of memory structure that would be
passed to pEntry callback from the execution thread.
\param flags - execution flags - reserved for future usage
\return upon successful registration of the spawn the function should return 0
(the function is not blocked till the end of the execution of the function
and could be returned before the execution is actually completed)
Otherwise, a negative value indicating the error code shall be returned
\note
\warning
*/
/*!
\brief This function creates a Task.
Creates a new Task and add it to the last of tasks that are ready to run
\param pEntry - pointer to the Task Function
\param pcName - Task Name String
\param usStackDepth - Stack Size Stack Size in 32-bit long words
\param pvParameters - pointer to structure to be passed to the Task Function
\param uxPriority - Task Priority
\return upon successful unlocking the function should return 0
Otherwise, a negative value indicating the error code shall be returned
\note
\warning
*/
//int osi_TaskCreate(P_OSI_TASK_ENTRY pEntry,const signed char * const pcName,unsigned short usStackDepth,void *pvParameters,unsigned long uxPriority,OsiTaskHandle *pTaskHandle);
#define osi_TaskCreate(pEntry, pcName, usStackDepth, pvParameters, uxPriority, pTaskHandle) \
osi_ThreadCreate(pEntry, usStackDepth, pvParameters, uxPriority, pTaskHandle)
/*!
\brief This function Deletes a Task.
Deletes a Task and remove it from list of running task
\param pTaskHandle - Task Handle
\note
\warning
*/
//void osi_TaskDelete(OsiTaskHandle* pTaskHandle);
#define osi_TaskDelete(pTaskHandle) pthread_detach(pTaskHandle)
/*!
\brief This function used to disable the tasks
\param - void
\return - Key with the suspended tasks
\note
\warning
*/
//unsigned long osi_TaskDisable(void);
#define osi_TaskDisable() SL_ERROR_BSD_EOPNOTSUPP // NOT SUPPORTED
/*!
\brief This function used to enable all tasks
\param unsigned long
\return - void
\note
\warning
*/
//void osi_TaskEnable(unsigned long);
#define osi_TaskEnable() SL_ERROR_BSD_EOPNOTSUPP // NOT SUPPORTED
/*!
\brief This function call the pEntry callback from a different context
\param pEntry - pointer to the entry callback function
\param pValue - pointer to any type of memory structure that would be
passed to pEntry callback from the execution thread.
\param flags - execution flags - reserved for future usage
\return upon successful registration of the spawn the function should return 0
(the function is not blocked till the end of the execution of the function
and could be returned before the execution is actually completed)
Otherwise, a negative value indicating the error code shall be returned
\note
\warning
*/
//OsiReturnVal_e osi_Spawn(P_OSI_SPAWN_ENTRY pEntry , void* pValue , unsigned long flags);
#define osi_Spawn(pEntry, pValue, flags)
/*******************************************************************************
This function creates a message queue that is typically used for inter thread
communication.
Parameters:
pMsgQ - pointer to the message queue control block
pMsgQName - pointer to the name of the message queue
MsgSize - the size of the message.
NOTICE: THE MESSGAE SIZE MUST BE SMALLER THAN 16
MaxMsgs - maximum number of messages.
Please note that this function allocates the entire memory required
for the maximum number of messages (MsgSize * MaxMsgs).
********************************************************************************/
OsiReturnVal_e osi_MsgQCreate(OsiMsgQ_t* pMsgQ ,
char* pMsgQName,
unsigned long MsgSize,
unsigned long MaxMsgs);
/*******************************************************************************
This function deletes a specific message queue.
All threads suspended waiting for a message from this queue are resumed with
an error return value.
Parameters:
pMsgQ - pointer to the message queue control block
********************************************************************************/
OsiReturnVal_e osi_MsgQDelete(OsiMsgQ_t* pMsgQ);
/*******************************************************************************
This function writes a message to a specific message queue.
Notice that the message is copied to the queue from the memory area specified
by pMsg pointer.
--------------------------------------------------------------------------------
THIS FUNCTION COULD BE CALLED FROM ISR AS LONG AS THE TIMEOUT PARAMETER IS
SET TO "OSI_NO_WAIT"
--------------------------------------------------------------------------------
Parameters:
pMsgQ - pointer to the message queue control block
pMsg - pointer to the message
Timeout - numeric value specifies the maximum number of mSec to stay
suspended while waiting for available space for the message
********************************************************************************/
OsiReturnVal_e osi_MsgQWrite(OsiMsgQ_t* pMsgQ, void* pMsg , OsiTime_t Timeout);
/*******************************************************************************
This function retrieves a message from the specified message queue. The
retrieved message is copied from the queue into the memory area specified by
the pMsg pointer
Parameters:
pMsgQ - pointer to the message queue control block
pMsg - pointer that specify the location where to copy the message
Timeout - numeric value specifies the maximum number of mSec to stay
suspended while waiting for a message to be available
********************************************************************************/
OsiReturnVal_e osi_MsgQRead(OsiMsgQ_t* pMsgQ, void* pMsg , OsiTime_t Timeout);
/*!
\brief This function starts the OS Scheduler
\param - void
\return - void
\note
\warning
*/
//void osi_start();
#ifdef USE_FREERTOS
/* Start the FreeRTOS scheduler */
#define osi_start() vTaskStartScheduler();
#else
#define osi_start() BIOS_start()
#endif
/*!
\brief Allocates Memory on Heap
\param Size - Size of the Buffer to be allocated
\sa
\note
\warning
*/
//void * mem_Malloc(unsigned long Size);
#define mem_Malloc(Size) malloc(Size)
/*!
\brief Deallocates Memory
\param pMem - Pointer to the Buffer to be freed
\return void
\sa
\note
\warning
*/
//void mem_Free(void *pMem);
#define mem_Free(pMem) free(pMem)
/*!
\brief Set Memory
\param pBuf - Pointer to the Buffer
\param Val - Value to be set
\param Size - Size of the memory to be set
\sa
\note
\warning
*/
//void mem_set(void *pBuf,int Val, int Size);
#define mem_set(pBuf, Val, Size) memset(pBuf, Val, Size)
/*!
\brief Copy Memory
\param pDst - Pointer to the Destination Buffer
\param pSrc - Pointer to the Source Buffer
\param Size - Size of the memory to be copied
\return void
\note
\warning
*/
//void mem_copy(void *pDst, void *pSrc, int Size);
#define mem_copy(pDst, pSrc, Size) memcpy(pDst, pSrc, Size)
/*!
\brief Enter Critical Section
\sa
\note
\warning
*/
//unsigned long osi_EnterCritical(void);
#define osi_EnterCritical() HwiP_disable()
/*!
\brief Exit Critical Section
\sa
\note
\warning
*/
//void osi_ExitCritical(unsigned long ulKey);
#define osi_ExitCritical(ulKey) HwiP_restore(ulKey)
/*!
\brief This function used to save the os context before sleep
\param void
\return void
\note
\warning
*/
//void osi_ContextSave();
#define osi_ContextSave() SL_ERROR_BSD_EOPNOTSUPP // NOT SUPPORTED
/*!
\brief This function used to retrieve the context after sleep
\param void
\return void
\note
\warning
*/
//void osi_ContextRestore();
#define osi_ContextRestore() SL_ERROR_BSD_EOPNOTSUPP // NOT SUPPORTED
/*!
\brief This function used to suspend the task for the specified number of milli secs
\param MilliSecs - Time in millisecs to suspend the task
\return void
\note
\warning
*/
//void osi_Sleep(unsigned int MilliSecs);
#define osi_Sleep(MilliSecs) {if(MilliSecs >= 1000) { sleep((MilliSecs+500)/1000); } else { usleep(MilliSecs * 1000); } }
/* API for SL Task*/
//OsiReturnVal_e VStartSimpleLinkSpawnTask(unsigned long uxPriority);
extern pthread_t slSpawnThread;
#define SPAWN_TASK_STACK_SIZE 2048
#define VStartSimpleLinkSpawnTask(priority) osi_ThreadCreate(sl_Task, SPAWN_TASK_STACK_SIZE, NULL, priority, &slSpawnThread)
//void VDeleteSimpleLinkSpawnTask( void );
#define VDeleteSimpleLinkSpawnTask() pthread_detach(&slSpawnThread)
#ifdef __cplusplus
}
#endif // __cplusplus
#endif
Appendix I-2.2 OS adaption source (os_posix.c)
The following C source file should be compiled and linked with the application code. It includes implementation of specific OS system calls that could not be ported through MACROs.
//*****************************************************************************
// osi_posix.c
//
// OS Adaptation implementation converting the obsolete CC3x00 OSI interface
// CC3X20 (MCPI) POSIX implemtation (supporting both TI-RTOS and FreeRTOS).
//
// Copyright (C) 2014 Texas Instruments Incorporated - https://www.ti.com/
//
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
//
//*****************************************************************************
#include <stdio.h>
#include <stdbool.h>
#include <stdint.h>
#include <stdlib.h>
#include <string.h>
#include <signal.h>
#include <unistd.h>
#include <semaphore.h>
#include <mqueue.h>
#include "osi.h"
#include "uart_term.h"
#include <ti/drivers/net/wifi/simplelink.h> /* sl_Task */
/* RTOS header files */
#ifdef USE_FREERTOS
#else
#define SPAWN_TASK_PRIORITY 9
#endif
pthread_t slSpawnThread;
static void st_GetAbsoluteTime(OsiTime_t msecToAdd, struct timespec *pOutTM)
{
clock_gettime(0, pOutTM);
pOutTM->tv_sec += msecToAdd / 1000 ;
pOutTM->tv_nsec += (msecToAdd % 1000)*1000000;
pOutTM->tv_sec += (pOutTM->tv_nsec / 1000000000);
pOutTM->tv_nsec = pOutTM->tv_nsec % 1000000000;
}
unsigned long GetAbsoluteTimeMS()
{
struct timespec tm;
clock_gettime(0, &tm);
return (tm.tv_sec * 1000) + (tm.tv_nsec / 1000000);
}
/*!
\brief This function registers an interrupt in NVIC table
The sync object is used for synchronization between different thread or ISR and
a thread.
\param iIntrNum - Interrupt number to register
\param pEntry - Pointer to the interrupt handler e.g. INT_PRIORITY_LVL_1
\param ucPriority - Priority of the interrupt
\return upon successful creation the function should return 0
Otherwise, a negative value indicating the error code shall be returned
\note
\warning
*/
typedef struct _osiIntContext_t
{
int intNum;
HwiP_Handle intHandle;
struct _osiIntContext_t *pNext;
} osiIntContext_t;
osiIntContext_t *g_osiInterrupts = NULL;
OsiReturnVal_e osi_InterruptRegister(int iIntrNum, P_OSI_INTR_ENTRY fInterruptHdl, unsigned char ucPriority)
{
#ifdef SL_PLATFORM_MULTI_THREADED
HwiP_Params intParams;
HwiP_Handle intHandle;
OsiReturnVal_e ret = OSI_FAILURE;
//OSI_HEADER_NL();
HwiP_clearInterrupt(iIntrNum);
if(!fInterruptHdl)
{
ret = OSI_INVALID_PARAMS;
}
else
{
intParams.priority = ucPriority; //
intHandle = HwiP_create(iIntrNum , (HwiP_Fxn)(fInterruptHdl) , &intParams);
if(intHandle)
{
osiIntContext_t *pIntContext = (osiIntContext_t*)malloc(sizeof(osiIntContext_t));
if(pIntContext)
{
pIntContext->intNum = iIntrNum;
pIntContext->intHandle = intHandle;
pIntContext->pNext = g_osiInterrupts;
g_osiInterrupts = pIntContext;
ret = OSI_OK;
}
}
}
return ret;
#else
if(!InterruptHdl)
{
MAP_IntDisable(INT_NWPIC);
MAP_IntUnregister(INT_NWPIC);
MAP_IntPendClear(INT_NWPIC);
}
else
{
MAP_IntRegister(INT_NWPIC, InterruptHdl);
MAP_IntPrioritySet(INT_NWPIC, INT_PRIORITY_LVL_1);
MAP_IntPendClear(INT_NWPIC);
MAP_IntEnable(INT_NWPIC);
}
return 0 ;
#endif //SL_PLATFORM_MULTI_THREADED
}
/*!
\brief This function De registers an interrupt in NVIC table
\param iIntrNum - Interrupt number to register
\return none
\note
\warning
*/
void osi_InterruptDeRegister(int iIntrNum)
{
osiIntContext_t *pIntContext, *pPrev;
//OSI_HEADER_NL();
for(pIntContext=g_osiInterrupts;
pIntContext && pIntContext->intNum!=iIntrNum;
pIntContext=pIntContext->pNext)
pPrev = pIntContext;
if(pIntContext)
{
HwiP_delete(pIntContext->intHandle);
if(pPrev)
pPrev->pNext = pIntContext->pNext;
else if(pIntContext == g_osiInterrupts)
g_osiInterrupts = NULL;
free(pIntContext);
}
}
int osi_ThreadCreate(void *(*pEntry)(void *),unsigned short stackDepth,void *pvParameters,unsigned long uxPriority,pthread_t *pThread)
{
int ret;
pthread_attr_t attr;
struct sched_param priParam;
int detachState;
ret = pthread_attr_init(&attr);
priParam.sched_priority = uxPriority;
ret |= pthread_attr_setschedparam(&attr, &priParam);
detachState = PTHREAD_CREATE_DETACHED;
ret |= pthread_attr_setdetachstate(&attr, detachState);
ret |= pthread_attr_setstacksize(&attr, stackDepth);
if (ret == 0)
ret = pthread_create(pThread, &attr, pEntry, pvParameters);
return ret;
}
typedef struct
{
mqd_t mq;
unsigned long MsgSize;
} osiMSGQContext_t;
/*!
\brief This function used to create a message queue
\param pMsgQ - pointer to the message queue
\param pMsgQName - Name of the Message queue
\param MsgSize - Size of msg on the message queue
\param MaxMsgs - Max number of msgs on the queue
\return - OsiReturnVal_e
\note
\warning
*/
OsiReturnVal_e osi_MsgQCreate(OsiMsgQ_t *pMsgQ,
char *pMsgQName,
unsigned long MsgSize,
unsigned long MaxMsgs)
{
int ret = OSI_FAILURE;
mq_attr attr;
osiMSGQContext_t *pMqContext;
attr.mq_maxmsg = MaxMsgs; // queue size
attr.mq_msgsize = MsgSize; // Size of message
pMqContext = (osiMSGQContext_t*) malloc (sizeof (osiMSGQContext_t));
if(pMqContext)
{
pMqContext->mq = mq_open(pMsgQName, O_CREAT, 0, &attr);
//OSI_PRINT(("%p->%p %d %d\r\n", pMqContext, pMqContext->mq, MsgSize, MaxMsgs));
if(pMqContext->mq == 0)
{
free (pMqContext);
}
else
{
pMqContext->MsgSize = MsgSize;
*pMsgQ = (void *)pMqContext;
ret = OSI_OK;
}
}
return (OsiReturnVal_e)ret;
}
/*!
\brief This function used to delete a message queue
\param pMsgQ - pointer to the msg queue
\return - OsiReturnVal_e
\note
\warning
*/
OsiReturnVal_e osi_MsgQDelete(OsiMsgQ_t *pMsgQ)
{
osiMSGQContext_t *pMqContext = (osiMSGQContext_t*)*pMsgQ;
//OSI_HEADER_NL();
mq_close(pMqContext->mq);
free(pMqContext);
return OSI_OK;
}
/*!
\brief This function is used to write data to the MsgQ
\param pMsgQ - pointer to the message queue
\param pMsg - pointer to the Msg strut to read into
\param Timeout - timeout to wait for the Msg to be available
\return - OsiReturnVal_e
\note
\warning
*/
OsiReturnVal_e osi_MsgQWrite(OsiMsgQ_t *pMsgQ, void *pMsg, OsiTime_t Timeout)
{
osiMSGQContext_t *pMqContext = (osiMSGQContext_t*)*pMsgQ;
int ret;
//OSI_PRINT(("%p\r\n", pMqContext));
//
//signal provisioning task about SL Event
//
if(Timeout == OSI_WAIT_FOREVER)
{
ret = mq_send(pMqContext->mq, (char *)pMsg, pMqContext->MsgSize, 0);
}
else
{
struct timespec tm;
st_GetAbsoluteTime(Timeout, &tm);
ret = mq_timedsend(pMqContext->mq, (char *)pMsg, pMqContext->MsgSize, 0, &tm);
}
if(ret < 0)
ret = OSI_FAILURE;
else
ret = OSI_OK;
return (OsiReturnVal_e)ret;
}
/*!
\brief This function is used to read data from the MsgQ
\param pMsgQ - pointer to the message queue
\param pMsg - pointer to the Msg strut to read into
\param Timeout - timeout to wait for the Msg to be available
\return - OsiReturnVal_e
\note
\warning
*/
OsiReturnVal_e osi_MsgQRead(OsiMsgQ_t* pMsgQ, void* pMsg , OsiTime_t Timeout)
{
osiMSGQContext_t *pMqContext = (osiMSGQContext_t*)*pMsgQ;
int ret;
unsigned int prio;
//OSI_PRINT(("%p\r\n", pMqContext));
//
//signal provisioning task about SL Event
//
if(Timeout == OSI_WAIT_FOREVER)
{
ret = mq_receive(pMqContext->mq, (char *)pMsg, pMqContext->MsgSize, &prio);
}
else
{
struct timespec tm;
st_GetAbsoluteTime(Timeout, &tm);
ret = mq_timedreceive(pMqContext->mq, (char *)pMsg, pMqContext->MsgSize, &prio, &tm);
}
if(ret == ETIMEDOUT)
ret = OSI_TIMEOUT;
else if (ret < 0)
ret = OSI_FAILURE;
else
ret = OSI_OK;
return (OsiReturnVal_e)ret;
}
Important Notice
Texas Instruments and its subsidiaries (TI) reserve the right to make changes to their products or to discontinue any product or service without notice, and advise customers to obtain the latest version of relevant information to verify, before placing orders, that information being relied on is current and complete. All products are sold subject to the terms and conditions of sale supplied at the time of order acknowledgement, including those pertaining to warranty, patent infringement, and limitation of liability.
TI warrants performance of its semiconductor products to the specifications applicable at the time of sale in accordance with TI’s standard warranty. Testing and other quality control techniques are utilized to the extent TI deems necessary to support this warranty. Specific testing of all parameters of each device is not necessarily performed, except those mandated by government requirements.
CERTAIN APPLICATIONS USING SEMICONDUCTOR PRODUCTS MAY INVOLVE POTENTIAL RISKS OF DEATH, PERSONAL INJURY, OR SEVERE PROPERTY OR ENVIRONMENTAL DAMAGE (“CRITICAL APPLICATIONS”). TI SEMICONDUCTOR PRODUCTS ARE NOT DESIGNED, AUTHORIZED, OR WARRANTED TO BE SUITABLE FOR USE IN LIFE–SUPPORT DEVICES OR SYSTEMS OR OTHER CRITICAL APPLICATIONS. INCLUSION OF TI PRODUCTS IN SUCH APPLICATIONS IS UNDERSTOOD TO BE FULLY AT THE CUSTOMER’S RISK.
In order to minimize risks associated with the customer’s applications, the customer to minimize inherent or procedural hazards must provide adequate design and operating safeguards.
TI assumes no liability for applications assistance or customer product design. TI does not warrant or represent that any license, either express or implied, is granted under any patent right, copyright, mask work right, or other intellectual property right of TI covering or relating to any combination, machine, or process in which such semiconductor products or services might be or are used. TI’s publication of information regarding any third party’s products or services does not constitute TI’s approval, warranty or endorsement thereof.