ADCCC32XX.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2016-2019, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 /*!****************************************************************************
33  * @file ADCCC32XX.h
34  * @brief ADC driver implementation for the ADC peripheral on CC32XX
35  *
36  * This ADC driver implementation is designed to operate on a CC32XX ADC
37  * peripheral.
38  *
39  * Refer to @ref ADC.h for a complete description of APIs & example of use.
40  *
41  ******************************************************************************
42  */
43 #ifndef ti_drivers_adc_ADCMSP432__include
44 #define ti_drivers_adc_ADCMSP432__include
45 
46 #include <stdint.h>
47 #include <stdbool.h>
48 
49 #include <ti/drivers/ADC.h>
50 
51 #ifdef __cplusplus
52 extern "C" {
53 #endif
54 
55 /*
56  * The bits in the pin mode macros are as follows:
57  * The lower 8 bits of the macro refer to the pin, offset by 1, to match
58  * driverlib pin defines.
59  * The upper 16 bits is the value that can be passed to APIs as the
60  * ulChannel parameter.
61  */
62 
64 #define ADCCC32XX_PIN_57_CH_0 (ADC_CH_0 << 8) | 0x38
65 
66 #define ADCCC32XX_PIN_58_CH_1 (ADC_CH_1 << 8) | 0x39
67 
68 #define ADCCC32XX_PIN_59_CH_2 (ADC_CH_2 << 8) | 0x3a
69 
70 #define ADCCC32XX_PIN_60_CH_3 (ADC_CH_3 << 8) | 0x3b
71 
72 /* ADC function table pointer */
73 extern const ADC_FxnTable ADCCC32XX_fxnTable;
74 
91 typedef struct {
92  uint_fast16_t adcPin;
94 
100 typedef struct {
101  uint_fast32_t baseAddr;
102  uint_least8_t numOpenChannels;
104 
110 typedef struct {
111  bool isOpen;
113 
114 #ifdef __cplusplus
115 }
116 #endif
117 
118 #endif /* ti_drivers_adc_ADCMSP432__include */
uint_least8_t numOpenChannels
Definition: ADCCC32XX.h:102
const ADC_FxnTable ADCCC32XX_fxnTable
ADCCC32XX Hardware attributes.
Definition: ADCCC32XX.h:91
ADCCC32XX Object.
Definition: ADCCC32XX.h:110
Analog to Digital Conversion (ADC) Input Driver.
The definition of an ADC function table that contains the required set of functions to control a spec...
Definition: ADC.h:319
uint_fast32_t baseAddr
Definition: ADCCC32XX.h:101
ADCCC32XX_Status.
Definition: ADCCC32XX.h:100
uint_fast16_t adcPin
Definition: ADCCC32XX.h:92
bool isOpen
Definition: ADCCC32XX.h:111
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale