110 #ifndef ti_drivers_watchdog_WatchdogCC32XX__include 111 #define ti_drivers_watchdog_WatchdogCC32XX__include 153 #define WatchdogCC32XX_CMD_IS_TIMER_ENABLE (Watchdog_CMD_RESERVED + 0) 163 #define WatchdogCC32XX_CMD_GET_TIMER_VALUE (Watchdog_CMD_RESERVED + 1) 174 #define WatchdogCC32XX_CMD_IS_TIMER_LOCKED (Watchdog_CMD_RESERVED + 2) 185 #define WatchdogCC32XX_CMD_GET_TIMER_RELOAD_VALUE (Watchdog_CMD_RESERVED + 3) Watchdog_DebugMode debugMode
Definition: WatchdogCC32XX.h:225
unsigned int intPriority
Definition: WatchdogCC32XX.h:209
uint32_t reloadValue
Definition: WatchdogCC32XX.h:210
Watchdog driver interface.
Watchdog Object for CC32XX.
Definition: WatchdogCC32XX.h:218
Watchdog hardware attributes for CC32XX.
Definition: WatchdogCC32XX.h:206
Power_NotifyObj notifyObj
Definition: WatchdogCC32XX.h:219
Watchdog_DebugMode
Watchdog debug stall settings.
Definition: Watchdog.h:264
uint32_t reloadValue
Definition: WatchdogCC32XX.h:224
unsigned int baseAddr
Definition: WatchdogCC32XX.h:207
Power notify object structure.
Definition: Power.h:443
const Watchdog_FxnTable WatchdogCC32XX_fxnTable
Watchdog function table for CC32XX.
unsigned int intNum
Definition: WatchdogCC32XX.h:208
The definition of a Watchdog function table that contains the required set of functions to control a ...
Definition: Watchdog.h:362
bool isOpen
Definition: WatchdogCC32XX.h:226