52 #ifndef ti_drivers_dma_UDMACC32XX__include 53 #define ti_drivers_dma_UDMACC32XX__include 61 #include <ti/drivers/dpl/HwiP.h> uint8_t intNum
Definition: UDMACC32XX.h:112
UDMACC32XX_Handle UDMACC32XX_open()
Function to initialize the CC32XX DMA peripheral.
UDMACC32XX_ErrorFxn dmaErrorFxn
Definition: UDMACC32XX.h:111
HwiP_Handle hwiHandle
Definition: UDMACC32XX.h:142
void(* UDMACC32XX_ErrorFxn)(uintptr_t arg)
UDMA error function pointer.
Definition: UDMACC32XX.h:66
struct UDMACC32XX_Config * UDMACC32XX_Handle
A handle that is returned from a UDMACC32XX_open() call.
Definition: UDMACC32XX.h:133
uint8_t intPriority
Definition: UDMACC32XX.h:113
struct UDMACC32XX_Object UDMACC32XX_Object
UDMACC32XX object.
void const * hwAttrs
Definition: UDMACC32XX.h:127
UDMACC32XX Global configuration.
Definition: UDMACC32XX.h:125
struct UDMACC32XX_HWAttrs UDMACC32XX_HWAttrs
UDMACC32XX Hardware attributes.
struct UDMACC32XX_Config UDMACC32XX_Config
UDMACC32XX Global configuration.
UDMACC32XX object.
Definition: UDMACC32XX.h:140
bool isOpen
Definition: UDMACC32XX.h:141
void * controlBaseAddr
Definition: UDMACC32XX.h:110
void UDMACC32XX_close(UDMACC32XX_Handle handle)
Function to close the DMA driver.
UDMACC32XX Hardware attributes.
Definition: UDMACC32XX.h:109
void * object
Definition: UDMACC32XX.h:126
void UDMACC32XX_init()
Function to initialize the CC32XX DMA driver.