124#define SL_ERROR_BSD_ESECT00MANYSSLOPENED (-460L) /* MAX SSL Sockets are opened */
125#define SL_ERROR_BSD_ESECDATEERROR (-461L) /* connected with certificate date verification error */
126#define SL_ERROR_BSD_ESECHANDSHAKETIMEDOUT (-462L) /* connection timed out due to handshake time */
127#define SL_ERROR_BSD_ESECTXBUFFERNOTEMPTY (-463L) /* cannot start ssl connection while send buffer is full */
128#define SL_ERROR_BSD_ESECRXBUFFERNOTEMPTY (-464L) /* cannot start ssl connection while recv buffer is full */
129#define SL_ERROR_BSD_ESECSSLDURINGHANDSHAKE (-465L) /* cannot use while in hanshaking */
130#define SL_ERROR_BSD_ESECNOTALLOWEDWHENLISTENING (-466L) /* the operation is not allowed when listening, do before listen*/
131#define SL_ERROR_BSD_ESECCERTIFICATEREVOKED (-467L) /* connected but on of the certificates in the chain is revoked */
132#define SL_ERROR_BSD_ESECUNKNOWNROOTCA (-468L) /* connected but the root CA used to validate the peer is unknown */
133#define SL_ERROR_BSD_ESECWRONGPEERCERT (-469L) /* wrong peer cert (server cert) was received while trying to connect to server */
134#define SL_ERROR_BSD_ESECTCPDISCONNECTEDUNCOMPLETERECORD (-470L) /* the other side disconnected the TCP layer and didn't send the whole ssl record */
135
136#define SL_ERROR_BSD_ESEC_BUFFER_E (-632L) /* output buffer too small or input too large */
137#define SL_ERROR_BSD_ESEC_ALGO_ID_E (-633L) /* setting algo id error */
138#define SL_ERROR_BSD_ESEC_PUBLIC_KEY_E (-634L) /* setting public key error */
139#define SL_ERROR_BSD_ESEC_DATE_E (-635L) /* setting date validity error */
140#define SL_ERROR_BSD_ESEC_SUBJECT_E (-636L) /* setting subject name error */
141#define SL_ERROR_BSD_ESEC_ISSUER_E (-637L) /* setting issuer name error */
302#define SL_ERROR_RXFL_NUMBER_OF_CONNECTION_POINTS_EXCEEDED (-2112L) /* Number of connection points exceeded */
303#define SL_ERROR_RXFL_DEPENDENT_FILTER_DEPENDENCY_ACTION_IS_DROP (-2113L) /* The dependent filter has Drop action, thus the filter can't be created */
304#define SL_ERROR_RXFL_FILTER_DO_NOT_EXISTS (-2114L) /* The filter doesn't exists */
305#define SL_ERROR_RXFL_DEPEDENCY_NOT_ON_THE_SAME_LAYER (-2115L) /* The filter and its dependency must be on the same layer */
306#define SL_ERROR_RXFL_NUMBER_OF_ARGS_EXCEEDED (-2116L) /* Number of arguments excceded */
307#define SL_ERROR_RXFL_ACTION_NO_REG_NUMBER (-2117L) /* Action require counter number */
308#define SL_ERROR_RXFL_DEPENDENT_FILTER_LAYER_DO_NOT_FIT (-2118L) /* the filter and its dependency should be from the same layer */
309#define SL_ERROR_RXFL_DEPENDENT_FILTER_SYSTEM_STATE_DO_NOT_FIT (-2119L) /* The filter and its dependency system state don't fit */
310#define SL_ERROR_RXFL_DEPENDENT_FILTER_DO_NOT_EXIST_2 (-2120L) /* The parent filter don't exist */
311#define SL_ERROR_RXFL_DEPENDENT_FILTER_DO_NOT_EXIST_1 (-2121L) /* The parent filter is null */
312#define SL_ERROR_RXFL_RULE_HEADER_ACTION_TYPE_NOT_SUPPORTED (-2122L) /* The action type is not supported */
313#define SL_ERROR_RXFL_RULE_HEADER_TRIGGER_COMPARE_FUNC_OUT_OF_RANGE (-2123L) /* The Trigger comparision function is out of range */
314#define SL_ERROR_RXFL_RULE_HEADER_TRIGGER_OUT_OF_RANGE (-2124L) /* The Trigger is out of range */
315#define SL_ERROR_RXFL_RULE_HEADER_COMPARE_FUNC_OUT_OF_RANGE (-2125L) /* The rule compare function is out of range */
316#define SL_ERROR_RXFL_FRAME_TYPE_NOT_SUPPORTED (-2126L) /* ASCII frame type string is illegal */
317#define SL_ERROR_RXFL_RULE_FIELD_ID_NOT_SUPPORTED (-2127L) /* Rule field ID is out of range */
318#define SL_ERROR_RXFL_RULE_HEADER_FIELD_ID_ASCII_NOT_SUPPORTED (-2128L) /* This ASCII field ID is not supported */
319#define SL_ERROR_RXFL_RULE_HEADER_NOT_SUPPORTED (-2129L) /* The header rule is not supported on current release */
320#define SL_ERROR_RXFL_RULE_HEADER_OUT_OF_RANGE (-2130L) /* The header rule is out of range */
321#define SL_ERROR_RXFL_RULE_HEADER_COMBINATION_OPERATOR_OUT_OF_RANGE (-2131L) /* Combination function Id is out of ramge */
322#define SL_ERROR_RXFL_RULE_HEADER_FIELD_ID_OUT_OF_RANGE (-2132L) /* rule field Id is out of range */
323#define SL_ERROR_RXFL_UPDATE_NOT_SUPPORTED (-2133L) /* Update not supported */
384#define SL_ERROR_ROLE_STA_ERR (-4107L) /* Failure to load MAC/PHY in STA role */
385#define SL_ERROR_ROLE_AP_ERR (-4108L) /* Failure to load MAC/PHY in AP role */
386#define SL_ERROR_ROLE_P2P_ERR (-4109L) /* Failure to load MAC/PHY in P2P role */
387#define SL_ERROR_CALIB_FAIL (-4110L) /* Failure of calibration */
388#define SL_ERROR_FS_CORRUPTED_ERR (-4111L) /* FS is corrupted, Return to Factory Image or Program new image should be invoked (see sl_FsCtl, sl_FsProgram) */
389#define SL_ERROR_FS_ALERT_ERR (-4112L) /* Device is locked, Return to Factory Image or Program new image should be invoked (see sl_FsCtl, sl_FsProgram) */
638#define SL_ERROR_NOT_ALLOWED_NWP_LOCKED (-14343L) /* Device is locked, Return to Factory Image or Program new image should be invoked (see sl_FsCtl, sl_FsProgram) */