Table of Contents
Overview
SSL is the universally accepted means by which communication is authenticated and encrypted on the World Wide Web. SSL certificates are designed to provide two principles, privacy and authentication. Privacy is achieved by encryption/decryption and authentication is achieved by signature/verification. This wiki will introduce a user to SSL/TLS and its implementation on the CC3200 devices.
Application details
Protocol and Ciphers
The SSL Protocol supports the use of a variety of different encryption/decryption algorithms - also known as ciphers - for use in operations such as authenticating the connection between a server and client, transmitting certificates, and establishing session keys. Depending on the version of SSL supported, clients and servers may support different sets of ciphers. The following methods and ciphers are supported by CC3200.
| Method | Cipher |
|---|---|
| SSLv3 | RSA_WITH_RC4_128_SHA |
| SSLv3 | RSA_WITH_RC4_128_MD5 |
| TLSv1 | RSA_WITH_RC4_128_SHA |
| TLSv1 | RSA_WITH_RC4_128_MD5 |
| TLSv1 | RSA_WITH_AES_256_CBC_SHA |
| TLSv1 | DHE_RSA_WITH_AES_256_CBC_SHA |
| TLSv1 | ECDHE_RSA_WITH_AES_256_CBC_SHA |
| TLSv1 | ECDHE_RSA_WITH_RC4_128_SHA |
API for SSL
The CC3200 has extended the BSD Socket API in order to support the SSL layer. At the application level, the basic socket flow when using a secured socket is kept the same; operations such as connect(), accept(), send(), recv() or select() are supported.
When a client application ‘connects’ to a secure socket, the function will only return successfully if a secure session was established with the server successfully. An error is returned if the secure session is not established. After the connection is established, the data path is secure.
When a server application ‘accepts’ a connection over a secure opened socket, the function will only return successfully if a secure session was established with the client successfully. If the client is rejected by the secure session, the CC3200 will automatically prepare itself to accept a new connection from another client without application interference. In other words, if a secure client connection is not successful, there is no need to recall the accept() function via the user application. After the connection is established, the data path is secure.
If the remote side decides to downgrade the connection to an unsecured socket, recv() will return with the ESECCLOSED error. How the socket is handled (whether to close the socket or continue unsecured) will need to be decided by the application.
The CC3200 cannot initiate a downgrade to an unsecured socket, nor can it dynamically upgrade from an insecure to secure socket.
Set Current Time
To ensure a secure connection, the current time must be set in the device. This time is used to validate the certificate. If the time is beyond the validity period of the certificate, sl_connect() will return an error.
g_time.tm_day = DATE;
g_time.tm_mon = MONTH;
g_time.tm_year = YEAR;
g_time.tm_sec = SECOND;
g_time.tm_hour = HOUR;
g_time.tm_min = MINUTE;
retVal = sl_DeviceSet(SL_DEVICE_GENERAL_CONFIGURATION,
SL_DEVICE_GENERAL_CONFIGURATION_DATE_TIME,
sizeof(SlDateTime), (unsigned char *)(&g_time));Open a Secure Socket
A secure socket must be opened by the CC3200 device. The sl_Socket() function may be used with the protocol parameter set to SL\_SEC\_SOCKET.
SockID = sl_Socket(SL_AF_INET, SL_SOCK_STREAM, SL_SEC_SOCKET);Force specific method (optional)
The CC3200 supports the SSL 3.0, TLS 1.0, TLS 1.1, and TLS 1.2 protocols/methods. By default, SSL 3.0 and TLS 1.2 are enabled. A specific method can be forced by using the sl_SetSockOpt() function.
char method = SL_SO_SEC_METHOD_SSLV3;
Status = sl_SetSockOpt(SockID, SL_SOL_SOCKET, SL_SO_SEC_METHOD, &method, sizeof(method));The full list of supported methods is available in the CC3100/CC3200 Network Processor User’s Guide.
Force specific cipher (optional)
By default, the CC3200 will pick the most secure cipher suite that both sides of the connection can support. A specific cipher can be forced by using the sl_SetSockOpt() function.
long cipher = SL_SEC_MASK_SSL_RSA_WITH_RC4_128_SHA;
Status = sl_SetSockOpt(SockID, SL_SOL_SOCKET, SL_SO_SEC_MASK, &cipher, sizeof(cipher));The full list of supported ciphers is available in the CC3100/CC3200 Network Processor User’s Guide.
TLS/SSL Basics
The CC3200 uses files specific to TLS/SSL that may be defined by the user at the application level. The files needed are listed below based on the connection type and must be expressed in the DER format.
Client Files
- Private Key - used when server verifies the client. If file mapped to 0, the connection may be refused by the server if the server wishes to verify client.
- Certificate - used when server verifies the client. If file mapped to 0, the connection may be refused by the server if the server wishes to verify client.
- CA, Certificate Authority - used when verifying the certificate provided by the server. There is the option to disable server verification by mapping file to id 0. In that case, if the secure session established successfully, connect will return with a specific error (ESECSNOVERIFY). It`s application decision to close socket, or to ignore it and continue with secured data.
- DH, Diffie-Hellman key - this file is not needed in the client case, map to id 0.
Server Files
- Private Key - this file is always needed by a server.
- Certificate - the file is always needed by a server.
- CA, Certificate Authority - used when server verifies the client. By mapping file to id 0, server will not try to verify the certificate of the client.
- DH, Diffie-Hellman key - This key is only needed for the following cipher suites: DHE_RSA_WITH_AES_256_CBC_SHA, ECDHE_RSA_WITH_AES_256_CBC_SHA, or ECDHE_RSA_WITH_RC4_128_SHA.
Defining secure files
The TLS/SSL files and variables can be defined and mapped to a socket using the following code.
typedef struct
{
unsigned char PrivateKey;
unsigned char Certificate;
unsigned char CA;
unsigned char DH;
} SlSockSecureFiles_t;
SlSockSecureFiles_t SecureFiles;
sockSecureFiles.secureFiles[0] = 0; // mapping private key, 0 file not exist
sockSecureFiles.secureFiles[1] = 0; // mapping certificate, 0 file not exist
sockSecureFiles.secureFiles[2] = SL_SSL_CA_CERT/*129*/; // mapping CA, 0 file not exist
sockSecureFiles.secureFiles[3] = 0; // mapping certificate, 0 file not exist
Status = sl_SetSockOpt(SockID, SL_SOL_SOCKET, SL_SO_SEC_FILES, &SecureFiles, sizeof(SlSockSecureFiles));Source Files briefly explained
- main.c - The main file that explains how certificate can be used with SSL.
- pinmux.c - Generated by the PinMUX utility.
- startup_*.c - Initialize vector table and IDE related functions
- gpio_if.c - GPIO interface APIs
Usage
- Preload valid CA Certificate in DER format into serial flash using UniFlash. In UniFlash, click Add File and name the file “/cert/129.der”.
- For details on finding your CA certificate, see the CA Certificate section below.
Edit common.h and modify the values of the below macros for the device to connect to the AP:
#define SSID_NAME "<ap_name>" /* AP SSID */ #define SECURITY_TYPE SL_SEC_TYPE_OPEN /* Security type (OPEN or WEP or WPA*/ #define SECURITY_KEY "" /* Password of the secured AP */- Run the reference application.
- Open the project in CCS/IAR. Build the application and debug to load to the device, or flash the binary using UniFlash. 3. The application will connect to the configured AP and attempt to connect to “www.google.com” securely using the provided CA certificate.
sl\_Connectshould return with a non-negative value indicating successful connection with the server, and this will be printed to the serial terminal. - If an error occurs, the red LED will turn on. If the connection is successful, the green LED will turn on.
- Open the project in CCS/IAR. Build the application and debug to load to the device, or flash the binary using UniFlash. 3. The application will connect to the configured AP and attempt to connect to “www.google.com” securely using the provided CA certificate.
CA Certificate
CA Certificates can be downloaded using various methods. For example, the following shows how to find and download the CA Certificate for www.google.com using the Chrome browser:
- Open Google Chrome and navigate to www.google.com
- Click on the lock icon in the browser URL bar. It should tell you about your connection to www.google.com.
- Select Certificate. In the Certificate Path, you should see the root CA certificate is “Google Trust Services - GlobalSign Root CA-R2”. Select View Certificate.
- In the Details tab, select Copy to File and export the certificate as a DER format.
For Firefox, the procedure is:
- Open FireFox. Go to Tools->Options
- Click the Advanced tab
- In the Advanced, click the Certificates tab
- Click View Certificates
- Find “Google Trust Services - GlobalSign Root CA-R2” and export it as DER format.
Limitations/Known Issues
- SSL certificates are not encrypted on the CC3200.