Table of Contents
Overview
The Secure Digital Host (SD Host)controller on CC3200 provides an interface to standard SD memory cards in 1-bit transfer mode and handles the SD protocol and data packing at transmission level with minimum CPU intervention.
Application details
This application uses the FatFS to provide the block level read/write access to SD card, using the SD Host controller on CC3200. The application initializes the FatFs and lists the files and/or directories that are present on the SD card at the root followed by contents of a predefined file on the terminal. The application also writes a predefined pattern to a predefine file. The user can change the predefine(s) by changing following macros
#define USERFILE "userfile.txt" // Application reads out this file
#define SYSFILE "sysfile.txt" // Application write to this file
#define SYSTEXT "The quick brown fox jumps over the lazy dog" // Pattern to be written to SYSFILEShown is the BOOSTXL-SHARP128 display and micro SD card reader connected to the CC3200 Launchpad.
Source Files briefly explained
- main.c - Implements the main function.
- diskio.c - Implements low-level function for FatFS using DriverLib API(s)
- pinmux.c - Generated by Pinmux utility to mux out the SD Host controller signal to chip boundary.
- uart_if.c - Implements the UART terminal.
- startup_*.c - Initialize vector table and IDE related functions
Connect the boards
The BOOSTXL-SHARP128 is recommended for use with the CC3200 in this demo. THe BOOSTXL-SHARP128 is a boosterpack with a micro SD card interface in addition to the Sharp LCD. More information on the BOOSTXL-SHARP128 can be found here: https://www.ti.com/tool/boostxl-sharp128
However, the BOOSTXL-SHARP128 cannot be mounted directly onto the CC3200 through the Launchpad connectors. Instead, the needed signals from the SD card need to be wired directly to the appropriate pins on the CC3200.
Required wiring
| CC3220 Pin | BOOSTXL-SHARP128 Pin |
|---|---|
| 3V3 | 3V3 |
| GND | GND |
| 5V | 5V |
| P07 | SPI_CLK |
| P08 | SPI_MOSI |
| P06 | SPI_MISO |
Ensure that wire lengths are kept to a minimum, especially for the SPI_CLK signal.
Usage
- Setup a serial communication application. Open a serial terminal on a PC with the following settings:
- Port: Enumerated COM port
- Baud rate: 115200
- Data: 8 bit
- Parity: None
- Stop: 1 bit
- Flow control: None
- Run the reference application.
- Open the project in CCS/IAR. Build the application and debug to load to the device, or flash the binary using UniFlash.
Limitations/Known Issues
- For many SD cards pull up resistors are required on the bidirectional signal lines, DAT0 and CMD.