Table of Contents
Overview
This example demonstrates how to connect the CC3200 to a P2P device. The application starts a TCP server on port 5001 and waits for a P2P device to connect to send data.
Supported P2P roles:
SL_P2P_ROLE_GROUP_OWNER: CC3200 will be configured in ‘Group-Owner’ modeSL_P2P_ROLE_CLIENT: CC3200 will be configured in ‘Client’ modeSL_P2P_ROLE_NEGOTIATE: CC3200 will negotiate with remote device for client/GO role.
The CC3200 can be configured in the following modes to initiate negotiation:
SL_P2P_NEG_INITIATOR_ACTIVE: CC3200 will perform discovery - Once the remote device is found, it sends the negotiation request immediatelySL_P2P_NEG_INITIATOR_PASSIVE: CC3200 will perform discovery - Once the remote device is found, CC3200 waits for it to start negotiationSL_P2P_NEG_INITIATOR_RAND_BACKOFF: CC3200 will perform discovery - Once the remote device is found, it triggers a random timer (1-7 seconds) and waits for the remote device to negotiate. On timer expiry, CC3200 starts negotiation itself
Supported security types for P2P negotiation:
SL_SEC_TYPE_P2P_PBCSL_SEC_TYPE_P2P_PIN_DISPLAYSL_SEC_TYPE_P2P_PIN_KEYPAD
The CC3200 can be configured in any_p2p mode as well. When configured, the CC3200 will perform discovery and connect to the first found device using security type SL_SEC_TYPE_P2P_PBC.
Application details
This example configures the device with following settings:
- P2P role negotiate (
SL_P2P_ROLE_NEGOTIATE) - P2P negotiation initiation active (
SL_P2P_NEG_INITIATOR_ACTIVE) - P2P device listens on channel 11 and P2P device’s operation channel is set to 6
- P2P connect security type
PBC
Usage
- Setup a serial communication application. Open a serial terminal on a PC with the following settings:
- Port: Enumerated COM port
- Baud rate: 115200
- Data: 8 bit
- Parity: None
- Stop: 1 bit
- Flow control: None
- Run the reference application.
- Open the project in CCS/IAR. Build the application and debug to load to the device, or flash the binary using UniFlash.
- Start a remote P2P device. The CC3200 will be visible cc3200-p2p-device by default, set by
P2P\_DEVICE\_NAME.
- Connect to the CC3200. On successful connection, the acquired IP address will be printed to the serial terminal.
Additionally, you can open an Iperf client on the remote P2P device and connect on
PORT_NUMIperf.exe -c-p-i 1