Table of Contents
Overview
MQTT (Message Queue Telemetry Transport) protocol is an extremely light weight machine to machine connectivity protocol. It is based on publish/subscribe messaging model and is designed to be used on the top of TCP/IP protocol. Key point of this protocol includes small code footprint and low network bandwidth requirement. Other features include faster response time, low power requirement, ease of scalability. All these advantages makes it an ideal candidate for communication protocol in embedded devices intended to implement IOT(internet of things) applications. More information regarding MQTT protocol can be obtained from the latest MQTT Protocol specification.
MQTT Network
A simple MQTT network contains a server / broker (like a central hub) that can handle connections from multiple clients. Each of the connected client can publish data for any topic (token). Whereas, the server / broker is responsible for forwarding the data published for a topic by a client to all the other clients who have subscribed for that particular topic. This is a very simplistic description of a MQTT network to set the tone for the sample application provided in SDK.
MQTT Library
MQTT library abstracts out the underlying intricacies of MQTT network and provide you with an intuitive and easy to use APIs to implement the MQTT protocol on CC3200 device.
Application details
This application make use of the APIs from MQTT client library to communicate with a MQTT client through a broker. Three LEDs on the CC3200 device can be controlled from a web client by publishing msg on appropriate topics. Similarly, messages can be published on pre-configured topics defined in the code by pressing the switch buttons on the CC3200 device.
Configurations
Most the parameters user will need to modify are specified as MACROs which will eventually get populated in following structures containing connection configurations and library configurations respectively.
/*Operate Lib in MQTT 3.1 mode.*/
#define MQTT_3_1_1 false /*MQTT 3.1.1 */
#define MQTT_3_1 true /*MQTT 3.1*/
/*Defining Broker IP address and port Number*/
#define SERVER_ADDRESS "m2m.eclipse.org"
#define SERVER_IP_ADDRESS "192.168.178.67"
#define PORT_NUMBER 1883
#define SECURED_PORT_NUMBER 8883
#define LOOPBACK_PORT 1882
#define MAX_BROKER_CONN 1
#define SERVER_MODE MQTT_3_1
/*Specifying Receive time out for the Receive task*/
#define RCV_TIMEOUT 30
/*Background receive task priority*/
#define TASK_PRIORITY 3
/* Keep Alive Timer value*/
#define KEEP_ALIVE_TIMER 25
/*Clean session flag*/
#define CLEAN_SESSION true
/*Retain Flag. Used in publish message. */
#define RETAIN 1
/*Defining Publish Topic*/
#define PUB_TOPIC_FOR_SW3 "/cc3200/ButtonPressEvtSw3"
#define PUB_TOPIC_FOR_SW2 "/cc3200/ButtonPressEvtSw2"
/*Defining Number of topics*/
#define TOPIC_COUNT 3
/*Defining Subscription Topic Values*/
#define TOPIC1 "/cc3200/ToggleLEDCmdL1"
#define TOPIC2 "/cc3200/ToggleLEDCmdL2"
#define TOPIC3 "/cc3200/ToggleLEDCmdL3"Note: CC3200 MQTT library has the capability of connecting to up to four brokers simultaneously. The configuration for the new connection can be added as new element(on next index) in connect_config.
/* connection configuration */
connect_config usr_connect_config[] =
{
{
{
{
SL_MQTT_NETCONN_URL,
SERVER_ADDRESS,
PORT_NUMBER,
0,
0,
0,
NULL
},
SERVER_MODE,
true,
},
NULL,
"user1",
NULL,
NULL,
true,
KEEP_ALIVE_TIMER,
{Mqtt_Recv, sl_MqttEvt, sl_MqttDisconnect},
TOPIC_COUNT,
{TOPIC1, TOPIC2, TOPIC3},
{QOS2, QOS2, QOS2},
{WILL_TOPIC,WILL_MSG,WILL_QOS,WILL_RETAIN},
false
}
};
/* library configuration */
SlMqttClientLibCfg_t Mqtt_Client={
1882,
TASK_PRIORITY,
30,
true,
UART_PRINT
};Source Files briefly explained
- main.c - The main file implementing the mqtt client.
- pinmux.c - Generated by the PinMUX utility.
- button_if.c - Interface file to handle button click events
- gpio_if.c - Basic GPIO interface APIs. Used to control the LEDs.
- network_if.c - Common functions to handle connection to AP and FreeRTOS hook functions.
- startup_*.c - Initialize vector table and IDE related functions
- timer_if.c - Wrapper functions for timer module driver
- uart_if.c - To display status information over the UART
Usage
This example can use TI-RTOS or FreeRTOS.
- On a host PC, open a serial terminal with the following parameters:
- Port: Enumerated COM port
- Baud rate: 115200
- Data: 8 bit
- Parity: None
- Stop: 1 bit
- Flow control: None
- Run the reference application.
- Open the project in CCS/IAR. Build the application and debug to load to the device, or flash the binary using UniFlash.
- This example requires the AP to have internet connectivity. In case the connection to the default AP fails, the user will see a prompt on the serial terminal.
- The green LED denotes that the network processor has turned on successfully, and the red LED continuously blinks as long as a connection with AP is not established.
- Once established, the red LED stays continuously ON for one second and then all the LEDs will be turned off.
- From a host PC or mobile device, open any MQTT client application. Connect to the m2m.eclipse.org broker we are using for this example.
- Subscribe to topics
/cc3200/ButtonPressEvtSw3and/cc3200/ButtonPressEvtSw2. - Publish on
/cc3200/ToggleLEDCmdL1,/cc3200/ToggleLEDCmdL2, or/cc3200/ToggleLEDCmdL3to control LED9, LED10 and LED11 respectively. - Press the SW2 or SW3 switch on CC3200 LaunchPad to publish message on
/cc3200/ButtonPressEvtSw2or/cc3200/ButtonPressEvtSw3respectively.
Note: The client ID should be unique for every client. We recommended changing the client ID for the CC3200 device to avoid interference with other users. In this example, this is defined in struct usr_connect_config as "user1".
Debug
Note: To print packet-level details on the serial terminal for debugging, add DEBUG_NET_DEV as a predefined symbol in the MQTT client library.
Limitations/Known Issues
- Client can connect to up to 4 brokers simultaneously