Table of Contents
Overview
The Get Weather application connects to “openweathermap.org” server, requests for weather details of the specified city, process data and displays it on the Hyperterminal.
Application details
This application connects to the default AP credentials set in common.h. In case the connection to this default AP is unsuccessful, the user is prompted to enter the AP details on the hyperterminal.
The AP details have to be entered in the format as specified below:
<ap_ssid>:<security_type>:<password>:<wep_key_id>
- ap_ssid - ssid of the AP to be connected
- security_type - values 1 (Open), 2 (WEP), or 3(WPA)
- password - network password in case of options 2 (WEP) or 3 (WPA)
- wep_key_id - key ID in case of option 2 (WEP)
The red LED continuously blinks until a connection is established with the AP. Once established, the red LED stays continuously on.
The user is prompted to enter a city name to obtain the weather information.
The weather information is then requested from “openweathermap.org” server for the specified city. This is done by opening a TCP socket with
server and sending a HTTP Get request. The response is parsed and the weather information displayed.
Source Files briefly explained
- network_if.c - Common functions to handle connection to AP and FreeRTOS hook functions.
- gpio_if.c - Basic GPIO interface APIs. Used to control the RED LED.
- main.c - Initializes the device, connects to a AP, performs a DNS lookup, open a TCP socket, send a HTTP Get request and displays weather information
- pinmux.c - Assigns a personality to the pins at the device boundary
- uart_if.c - To display status information over the UART
- udma_if.c - Wrapper functions for uDMA module driver
- timer_if.c - Wrapper functions for timer module driver
- startup_*.c - Initialize vector table and IDE related functions
Usage
- Setup a serial communication application. Open a serial terminal on a PC with the following settings:
- Port: Enumerated COM port
- Baud rate: 115200
- Data: 8 bit
- Parity: None
- Stop: 1 bit
- Flow control: None
- From openweathermap.org, create an API Key and modify the ‘API Key’ value in the POST_BUFFER macro in main.c found below:
#define POST_BUFFER "&mode=xml&units=imperial&APPID=<API KEY> HTTP/1.1\r\nHost:api.openweathermap.org\r\nAccept: */" Edit common.h and modify the values of the below macros for the device to connect to the AP:
#define SSID_NAME "<ap_name>" /* AP SSID */ #define SECURITY_TYPE SL_SEC_TYPE_OPEN /* Security type (OPEN or WEP or WPA*/ #define SECURITY_KEY "" /* Password of the secured AP */- Run the reference application.
- Open the project in CCS/IAR. Build the application and debug to load to the device, or flash the binary using UniFlash.
- If the connection to the default AP is unsuccessful, the user will be prompted on the terminal to enter AP details.
- The red LED will continuously blinks while a connection with the AP is not established. Once established, the red LED will stay continuously on.
The user is prompted to enter the city name in the serial terminal.
Limitations/Known Issues
- WEP connectivity is not tested with this application.