The following significant changes have been made since 5.00
5.10 (This Release)
Introduction of xDM 1.00 Beta.
The Reference Guide has been updated to include these Beta
APIs.
Added "What's New in xDM 1.00" documentation,
describing the high-level changes in the
xDM 1.00 Beta specification.
This xDM 1.00 Beta spec addresses the following items:
SDSCM00004685 - xDM speech enc and dec OutArgs should
have extendedError field for consistency
SDSCM00005009 - IIMGDEC_OutArgs bytesconsumed should be
camelCase
SDSCM00005245 - Video enc interface needs to reconsider
reconBufs conventions for RPCs
Addition of example "copy" codecs, conforming with xDM 1.00 Beta
interfaces.
Addition of example G.711 algorithm, conforming with xDM 0.90
speech encoder interface. This example shows how to wrap an xDM
interface around an existing algorithm.
Addition of example "extended" video encoder copy codec. This
example shows how an algorithm can extend the xDM interface to
implement codec-specific features.
SDSCM00005726 - Add doxygen comments to ialg.h
SDSCM00005728 - IDMA3 channel object documentation needs to
include scratch environment support
SDSCM00010925 - xDM User's manual uses XMI in places
SDSCM00011274 - xDAIS header files for c55 need to include fully
qualified package files