![]() |
![]() |
Describes the interface to the contiguous memory allocator.
The cmem user interface library wraps file system calls to an associated kernel dll (cmemk.dll), which needs to be loaded in order for calls to this library to succeed.
#include <windows.h>
Go to the source code of this file.
Data Structures | |
struct | CMEM_AllocParams |
Parameters for CMEM_alloc(), CMEM_alloc2(), CMEM_allocPool(), CMEM_allocPool2(), CMEM_free(). More... | |
struct | CMEM_BlockAttrs |
Defines | |
#define | CMEM_VERSION 0x02200000U |
#define | CMEM_WB 0x0100 |
#define | CMEM_INV 0x0200 |
#define | CMEM_HEAP 0x0400 |
#define | CMEM_POOL 0x0000 |
#define | CMEM_CACHED 0x0800 |
#define | CMEM_NONCACHED 0x0000 |
#define | CMEM_PHYS 0x1000 |
#define | CMEM_IOCALLOC 1 |
#define | CMEM_IOCALLOCHEAP 2 |
#define | CMEM_IOCFREE 3 |
#define | CMEM_IOCGETPHYS 4 |
#define | CMEM_IOCGETSIZE 5 |
#define | CMEM_IOCGETPOOL 6 |
#define | CMEM_IOCCACHE 7 |
#define | CMEM_IOCGETVERSION 8 |
#define | CMEM_IOCGETBLOCK 9 |
#define | CMEM_IOCREGUSER 10 |
#define | CMEM_IOCGETNUMBLOCKS 11 |
#define | CMEM_IOCMAPADDRESS 12 |
#define | CMEM_IOCUNMAPADDRESS 13 |
#define | CMEM_IOCCACHEWBINV CMEM_IOCCACHE | CMEM_WB | CMEM_INV |
#define | CMEM_IOCCACHEWB CMEM_IOCCACHE | CMEM_WB |
#define | CMEM_IOCCACHEINV CMEM_IOCCACHE | CMEM_INV |
#define | CMEM_IOCALLOCCACHED CMEM_IOCALLOC | CMEM_CACHED |
#define | CMEM_IOCALLOCHEAPCACHED CMEM_IOCALLOCHEAP | CMEM_CACHED |
#define | CMEM_IOCFREEHEAP CMEM_IOCFREE | CMEM_HEAP |
#define | CMEM_IOCFREEPHYS CMEM_IOCFREE | CMEM_PHYS |
#define | CMEM_IOCFREEHEAPPHYS CMEM_IOCFREE | CMEM_HEAP | CMEM_PHYS |
#define | CMEM_IOCCMDMASK 0x000000ff |
Functions | |
int | CMEM_init (void) |
Initialize the CMEM module. Must be called before other API calls. | |
int | CMEM_getPool (size_t size) |
Find the pool that best fits a given buffer size and has a buffer available. | |
int | CMEM_getPool2 (int blockid, size_t size) |
Find the pool in memory block blockid that best fits a given buffer size and has a buffer available. | |
void * | CMEM_allocPool (int poolid, CMEM_AllocParams *params) |
Allocate memory from a specified pool. | |
void * | CMEM_allocPool2 (int blockid, int poolid, CMEM_AllocParams *params) |
Allocate memory from a specified pool in a specified memory block. | |
void * | CMEM_alloc (size_t size, CMEM_AllocParams *params) |
Allocate memory of a specified size. | |
void * | CMEM_alloc2 (int blockid, size_t size, CMEM_AllocParams *params) |
Allocate memory of a specified size from a specified memory block. | |
int | CMEM_free (void *ptr, CMEM_AllocParams *params) |
Free a buffer previously allocated with CMEM_alloc()/ CMEM_allocPool(). | |
unsigned long | CMEM_getPhys (void *ptr) |
Get the physical address of a contiguous buffer. | |
int | CMEM_cacheWb (void *ptr, size_t size) |
Do a cache writeback of the block pointed to by ptr/ | |
int | CMEM_cacheInv (void *ptr, size_t size) |
Do a cache invalidate of the block pointed to by ptr/ | |
int | CMEM_cacheWbInv (void *ptr, size_t size) |
Do a cache writeback/invalidate of the block pointed to by ptr/ | |
int | CMEM_getVersion (void) |
Retrieve version from CMEM driver. | |
int | CMEM_getBlock (unsigned long *pphys_base, size_t *psize) |
Retrieve memory block bounds from CMEM driver. | |
int | CMEM_getBlockAttrs (int blockid, CMEM_BlockAttrs *pattrs) |
Retrieve extended memory block attributes from CMEM driver. | |
int | CMEM_getNumBlocks (int *pnblocks) |
Retrieve number of blocks configured into CMEM driver. | |
int | CMEM_exit (void) |
Finalize the CMEM module. | |
int | CMEM_mapAddress (unsigned long physAddr, unsigned long length, unsigned int flags, unsigned long *pVirtAddr) |
Map a physical address to the calling process's virtual address space. | |
int | CMEM_unmapAddress (unsigned long virtAddr, unsigned long length) |
Unmap a virtual address that was previously mapped to the calling process's virtual address space with CMEM_mapAddress(). | |
Variables | |
CMEM_AllocParams | CMEM_DEFAULTPARAMS |