UIA needs to provide makefile.defs file for each
example to better support clean for custom build
SDOCM00085472
LoggerSM's sharedBuffer should be in Module_state, not
a config parameter
SDOCM00085285
docs links in UIA 1.00.02.22 GA Release Notes are
broken (UG and GSG have bad links)
For information on enhancements and defect fixes in earlier releases,
please refer to the release notes from previous releases that are
available in the relnotes_archive
directory.
UIA ships with with many examples that interact with System Analyzer
Single-core The
following examples can be built for all the supported targets. The
actual application is the same for all examples. The difference is the
way the data is moved up to System Analyzer. Stairstep varies the Task,
Swi and
Hwi load every 5 seconds. When viewed on the CPU Load Analysis Feature,
it looks like a staircase.
Stairstep
JTAG Stopmode: The Log data is obtained
when the target is halted
Stairstep
JTAG RunMode: The Log data is obtained by
reading the running target (only works on C64X+ and C66 CPUs).
Stairstep
Ethernet:
The Log data is obtained by UDP packets. This example, as is, only
works for the EVM6472 board. Refer to the bottom of the .cfg file on
how to use on a different board.
Stairstep
Simulator: The Log data is obtained by
temporarily stopping the target when the
Log call is made. To build this example, the XDC version must be 3.22
(or later) or the RTSC Build-Profile must be "release"
or "debug"
(not "whole_program").
Stairstep
ProbePoint:
The Log data is obtained by temporarily stopping the target when the
Log call is made. To build this example, the XDC version must be 3.22
(or later) or the RTSC Build-Profile must be "release"
or "debug"
(not "whole_program").
Multi-core
Message:
The message example shows how to use MessageQ on EVM6472 and UIA. It is
a single-image example that must be loaded on all cores. A message is
sent from core 0 to core 1 to core 2...back to core 0. The
UIABenchmark_start and stop is used on core 0 to determine the duration
of a round trip. The Log data is obtained via Ethernet.
SimpleTask:
This example flips bits on an array. The example can be built for the
DSP and M3 targets on the EVMTI816X. There are two examples. One uses
LoggerCircBuf and one that uses LoggerSM. Refer to the readme.txt in
packages\ti\uia\examples\evmti816x directory and the System Analyzer
User Guide
for more details.
Tutorials
System
Analyzer and UIA
Tutorial 1: Logging events, benchmarking, controlling
events (C64X+ or C66X simulator).
System
Analyzer and UIA
Tutorial 2: Graphing events, using JTAG Run-Mode (C64X+ or
C66X emulation target)
All releases have 4 digits (M.mm.pp.bb).
This includes GA and pre-releases (engineering, EA, beta, etc.).
Pre-releases are denoted with a suffix (e.g. 1.01.00.16_eng or
1.01.00.21-beta).
This product's version follows a version format, M.mm.pp.bb,
where M is a single digit Major number, mm
is 2 digit minor number, pp is a 2 digit patch
number, and b is an unrestricted set of digits used
as an incrementing build counter.
To support multiple side-by-side installations of the product,
the product version is encoded in the top level directory, ex. uia_1_00_00_38.
Subsequent releases of patch upgrades will be identified by
the patch number, ex. UIA 1.00.00.26 with directory uia_1_00_00_38.
Typically, these patches only include critical bug fixes.
Please note that version numbers and compatibility keys are
NOT the same. For an explanation of compatibility keys, please refer to
the 'Upgrade and Compatibility Information' section.