Instance: CPU_FPB
Component: CPU_FPB
Base address: 0xE0002000
Cortex-M's Flash Patch and Breakpoint (FPB)
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
RW |
32 |
0x0000 0260 |
0x0000 0000 |
0xE000 2000 |
|
RW |
32 |
0b001X XXXX XXXX XXXX XXXX XXXX XXX0 0000 |
0x0000 0004 |
0xE000 2004 |
|
RW |
32 |
0x0000 0000 |
0x0000 0008 |
0xE000 2008 |
|
RW |
32 |
0x0000 0000 |
0x0000 000C |
0xE000 200C |
|
RW |
32 |
0x0000 0000 |
0x0000 0010 |
0xE000 2010 |
|
RW |
32 |
0x0000 0000 |
0x0000 0014 |
0xE000 2014 |
|
RW |
32 |
0x0000 0000 |
0x0000 0018 |
0xE000 2018 |
|
RW |
32 |
0x0000 0000 |
0x0000 001C |
0xE000 201C |
|
RW |
32 |
0x0000 0000 |
0x0000 0020 |
0xE000 2020 |
|
RW |
32 |
0x0000 0000 |
0x0000 0024 |
0xE000 2024 |
Address Offset | 0x0000 0000 | ||
Physical Address | 0xE000 2000 | Instance | 0xE000 2000 |
Description | Control This register is used to enable the flash patch block. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:14 | RESERVED14 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 | ||
13:12 | NUM_CODE2 | Number of full banks of code comparators, sixteen comparators per bank. Where less than sixteen code comparators are provided, the bank count is zero, and the number present indicated by NUM_CODE1. This read only field contains 3'b000 to indicate 0 banks for Cortex-M processor. | RO | 0b00 | ||
11:8 | NUM_LIT | Number of literal slots field. 0x0: No literal slots 0x2: Two literal slots |
RO | 0x2 | ||
7:4 | NUM_CODE1 | Number of code slots field. 0x0: No code slots 0x2: Two code slots 0x6: Six code slots |
RO | 0x6 | ||
3:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 | ||
1 | KEY | Key field. In order to write to this register, this bit-field must be written to '1'. This bit always reads 0. | WO | 0 | ||
0 | ENABLE | Flash patch unit enable bit 0x0: Flash patch unit disabled 0x1: Flash patch unit enabled |
RW | 0 |
Address Offset | 0x0000 0004 | ||
Physical Address | 0xE000 2004 | Instance | 0xE000 2004 |
Description | Remap This register provides the remap base address location where a matched addresses are remapped. The three most significant bits and the five least significant bits of the remap base address are hard-coded to 3'b001 and 5'b00000 respectively. The remap base address must be in system space and is it required to be 8-word aligned, with one word allocated to each of the eight FPB comparators. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:29 | RESERVED29 | This field always reads 3'b001. Writing to this field is ignored. | RO | 0b001 | ||
28:5 | REMAP | Remap base address field. | RW | 0xXX XXXX | ||
4:0 | RESERVED0 | This field always reads 0. Writing to this field is ignored. | RO | 0b0 0000 |
Address Offset | 0x0000 0008 | ||
Physical Address | 0xE000 2008 | Instance | 0xE000 2008 |
Description | Comparator 0 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:30 | REPLACE | This selects what happens when the COMP address is matched. Address remapping only takes place for the 0x0 setting. 0x0: Remap to remap address. See REMAP.REMAP 0x1: Set BKPT on lower halfword, upper is unaffected 0x2: Set BKPT on upper halfword, lower is unaffected 0x3: Set BKPT on both lower and upper halfwords. |
RW | 0b00 | ||
29 | RESERVED29 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
28:2 | COMP | Comparison address. | RW | 0b000 0000 0000 0000 0000 0000 0000 | ||
1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
0 | ENABLE | Compare and remap enable comparator 0. CTRL.ENABLE must also be set to enable comparisons. 0x0: Compare and remap for comparator 0 disabled 0x1: Compare and remap for comparator 0 enabled |
RW | 0 |
Address Offset | 0x0000 000C | ||
Physical Address | 0xE000 200C | Instance | 0xE000 200C |
Description | Comparator 1 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:30 | REPLACE | This selects what happens when the COMP address is matched. Address remapping only takes place for the 0x0 setting. 0x0: Remap to remap address. See REMAP.REMAP 0x1: Set BKPT on lower halfword, upper is unaffected 0x2: Set BKPT on upper halfword, lower is unaffected 0x3: Set BKPT on both lower and upper halfwords. |
RW | 0b00 | ||
29 | RESERVED29 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
28:2 | COMP | Comparison address. | RW | 0b000 0000 0000 0000 0000 0000 0000 | ||
1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
0 | ENABLE | Compare and remap enable comparator 1. CTRL.ENABLE must also be set to enable comparisons. 0x0: Compare and remap for comparator 1 disabled 0x1: Compare and remap for comparator 1 enabled |
RW | 0 |
Address Offset | 0x0000 0010 | ||
Physical Address | 0xE000 2010 | Instance | 0xE000 2010 |
Description | Comparator 2 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:30 | REPLACE | This selects what happens when the COMP address is matched. Address remapping only takes place for the 0x0 setting. 0x0: Remap to remap address. See REMAP.REMAP 0x1: Set BKPT on lower halfword, upper is unaffected 0x2: Set BKPT on upper halfword, lower is unaffected 0x3: Set BKPT on both lower and upper halfwords. |
RW | 0b00 | ||
29 | RESERVED29 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
28:2 | COMP | Comparison address. | RW | 0b000 0000 0000 0000 0000 0000 0000 | ||
1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
0 | ENABLE | Compare and remap enable comparator 2. CTRL.ENABLE must also be set to enable comparisons. 0x0: Compare and remap for comparator 2 disabled 0x1: Compare and remap for comparator 2 enabled |
RW | 0 |
Address Offset | 0x0000 0014 | ||
Physical Address | 0xE000 2014 | Instance | 0xE000 2014 |
Description | Comparator 3 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:30 | REPLACE | This selects what happens when the COMP address is matched. Address remapping only takes place for the 0x0 setting. 0x0: Remap to remap address. See REMAP.REMAP 0x1: Set BKPT on lower halfword, upper is unaffected 0x2: Set BKPT on upper halfword, lower is unaffected 0x3: Set BKPT on both lower and upper halfwords. |
RW | 0b00 | ||
29 | RESERVED29 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
28:2 | COMP | Comparison address. | RW | 0b000 0000 0000 0000 0000 0000 0000 | ||
1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
0 | ENABLE | Compare and remap enable comparator 3. CTRL.ENABLE must also be set to enable comparisons. 0x0: Compare and remap for comparator 3 disabled 0x1: Compare and remap for comparator 3 enabled |
RW | 0 |
Address Offset | 0x0000 0018 | ||
Physical Address | 0xE000 2018 | Instance | 0xE000 2018 |
Description | Comparator 4 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:30 | REPLACE | This selects what happens when the COMP address is matched. Address remapping only takes place for the 0x0 setting. 0x0: Remap to remap address. See REMAP.REMAP 0x1: Set BKPT on lower halfword, upper is unaffected 0x2: Set BKPT on upper halfword, lower is unaffected 0x3: Set BKPT on both lower and upper halfwords. |
RW | 0b00 | ||
29 | RESERVED29 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
28:2 | COMP | Comparison address. | RW | 0b000 0000 0000 0000 0000 0000 0000 | ||
1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
0 | ENABLE | Compare and remap enable comparator 4. CTRL.ENABLE must also be set to enable comparisons. 0x0: Compare and remap for comparator 4 disabled 0x1: Compare and remap for comparator 4 enabled |
RW | 0 |
Address Offset | 0x0000 001C | ||
Physical Address | 0xE000 201C | Instance | 0xE000 201C |
Description | Comparator 5 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:30 | REPLACE | This selects what happens when the COMP address is matched. Address remapping only takes place for the 0x0 setting. 0x0: Remap to remap address. See REMAP.REMAP 0x1: Set BKPT on lower halfword, upper is unaffected 0x2: Set BKPT on upper halfword, lower is unaffected 0x3: Set BKPT on both lower and upper halfwords. |
RW | 0b00 | ||
29 | RESERVED29 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
28:2 | COMP | Comparison address. | RW | 0b000 0000 0000 0000 0000 0000 0000 | ||
1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
0 | ENABLE | Compare and remap enable comparator 5. CTRL.ENABLE must also be set to enable comparisons. 0x0: Compare and remap for comparator 5 disabled 0x1: Compare and remap for comparator 5 enabled |
RW | 0 |
Address Offset | 0x0000 0020 | ||
Physical Address | 0xE000 2020 | Instance | 0xE000 2020 |
Description | Comparator 6 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:30 | REPLACE | This selects what happens when the COMP address is matched. Comparator 6 is a literal comparator and the only supported setting is 0x0. Other settings will be ignored. 0x0: Remap to remap address. See REMAP.REMAP 0x1: Set BKPT on lower halfword, upper is unaffected 0x2: Set BKPT on upper halfword, lower is unaffected 0x3: Set BKPT on both lower and upper halfwords. |
RW | 0b00 | ||
29 | RESERVED29 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
28:2 | COMP | Comparison address. | RW | 0b000 0000 0000 0000 0000 0000 0000 | ||
1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
0 | ENABLE | Compare and remap enable comparator 6. CTRL.ENABLE must also be set to enable comparisons. 0x0: Compare and remap for comparator 6 disabled 0x1: Compare and remap for comparator 6 enabled |
RW | 0 |
Address Offset | 0x0000 0024 | ||
Physical Address | 0xE000 2024 | Instance | 0xE000 2024 |
Description | Comparator 7 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:30 | REPLACE | This selects what happens when the COMP address is matched. Comparator 7 is a literal comparator and the only supported setting is 0x0. Other settings will be ignored. 0x0: Remap to remap address. See REMAP.REMAP 0x1: Set BKPT on lower halfword, upper is unaffected 0x2: Set BKPT on upper halfword, lower is unaffected 0x3: Set BKPT on both lower and upper halfwords. |
RW | 0b00 | ||
29 | RESERVED29 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
28:2 | COMP | Comparison address. | RW | 0b000 0000 0000 0000 0000 0000 0000 | ||
1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
0 | ENABLE | Compare and remap enable comparator 7. CTRL.ENABLE must also be set to enable comparisons. 0x0: Compare and remap for comparator 7 disabled 0x1: Compare and remap for comparator 7 enabled |
RW | 0 |
© 2015 - 2016. Texas Instruments | All Rights Reserved |