1    /*
     2     * Copyright (c) 2015-2016, Texas Instruments Incorporated
     3     * All rights reserved.
     4     *
     5     * Redistribution and use in source and binary forms, with or without
     6     * modification, are permitted provided that the following conditions
     7     * are met:
     8     *
     9     * *  Redistributions of source code must retain the above copyright
    10     *    notice, this list of conditions and the following disclaimer.
    11     *
    12     * *  Redistributions in binary form must reproduce the above copyright
    13     *    notice, this list of conditions and the following disclaimer in the
    14     *    documentation and/or other materials provided with the distribution.
    15     *
    16     * *  Neither the name of Texas Instruments Incorporated nor the names of
    17     *    its contributors may be used to endorse or promote products derived
    18     *    from this software without specific prior written permission.
    19     *
    20     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
    21     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
    22     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
    23     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
    24     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
    25     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
    26     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
    27     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
    28     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
    29     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
    30     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    31     */
    32    
    33    /*
    34     *  ======== Hwi.xdc ========
    35     *
    36     */
    37    package ti.sysbios.family.arm.m3;
    38    
    39    import xdc.rov.ViewInfo;
    40    import xdc.runtime.Diags;
    41    import xdc.runtime.Log;
    42    import xdc.runtime.Assert;
    43    import xdc.runtime.Error;
    44    
    45    import ti.sysbios.BIOS;
    46    import ti.sysbios.interfaces.IHwi;
    47    
    48    /*!
    49     *  ======== Hwi ========
    50     *  Cortex M3 Hardware Interrupt Manager
    51     *
    52     *  The Cortex M3's Nested Vectored Interrupt Controller (NVIC)
    53     *  supports up to 256 interrupts/exceptions. In practice, most
    54     *  devices support much fewer (ie the Stellaris family of devices
    55     *  have only 80 total interrupts defined).
    56     *
    57     *  SYS/BIOS Interrupt IDs or interrupt numbers correspond
    58     *  to an interrupt's position in the interrupt vector table.
    59     *
    60     *  ID 0 corresponds to vector 0 which is used by the NVIC
    61     *  to hold the initial (reset) stack pointer value.
    62     *
    63     *  ID 1 corresponds to vector 1 which is the reset vector (ie _c_int00)
    64     *
    65     *  IDs 2-14 are hardwired to exceptions.
    66     *
    67     *  ID 15 is the SysTick timer interrupt.
    68     *
    69     *  ID's 16-255 are mapped to the NVIC's user interrupts 0-239
    70     *  which are tied to platform specific interrupt sources.
    71     *
    72     *  @a(Zero Latency Interrupts)
    73     *  The M3 Hwi module supports "zero latency" interrupts.
    74     *  Interrupts configured with priority greater (in actual
    75     *  hardware priority, but lower in number) than
    76     *  {@link #disablePriority Hwi.disablePriority} are NOT
    77     *  disabled by Hwi_disable().
    78     *
    79     *  Zero latency interrupts are distinguished from regular dispatched
    80     *  interrupts at create time by their priority being greater
    81     *  than Hwi.disablePriority.
    82     *
    83     *  Note that since zero latency interrupts don't use the dispatcher,
    84     *  the {@link ti.sysbios.interfaces.IHwi#arg arg} parameter is not
    85     *  functional. Also note that due to the M3's native automatic
    86     *  stacking of saved-by-caller C context on the way to an ISR, zero
    87     *  latency interrupt handlers are implemented using regular C functions
    88     *  (ie no 'interrupt' keyword is required).
    89     *
    90     *  @a(WARNING)
    91     *  Zero latency interrupts are NOT HANDLED by the SYS/BIOS
    92     *  interrupt dispatcher! Instead, they are vectored to directly.
    93     *  As such, and because they are NOT DISABLED BY Hwi_disable(),
    94     *  these interrupt handlers are SEVERELY RESTRICTED in terms of the
    95     *  SYS/BIOS APIs they can invoke and THREAD SAFETY MUST BE CAREFULLY
    96     *  CONSIDERED! See the descriptions of {@link #disable Hwi_disable()} and
    97     *  and {@link #disablePriority Hwi.disablePriority} for more details.
    98     *
    99     *  @a(Interrupt Masking Options)
   100     *
   101     *  The NVIC interrupt controller is designed for priority based
   102     *  interrupts.
   103     *
   104     *  In this Hwi module, the {@link #maskSetting} instance configuration
   105     *  parameter is ignored.
   106     *  Effectively, only the {@link #MaskingOption_LOWER} is supported.
   107     *
   108     *  @a(Interrupt Priorities)
   109     *
   110     *  In general, the NVIC supports priority values of 0 thru 255.
   111     *
   112     *  In practice, the number of priorities and their values are device
   113     *  dependent, and their nesting behaviors depend on the
   114     *  {@link #priGroup Hwi.priGroup} setting.
   115     *
   116     *  For most TI MCU devices, 8 priorities are supported. A peculiarity
   117     *  of ARM's NVIC is that, although the priority field is an 8 bit value,
   118     *  the range of supported priority values are left-justified within this
   119     *  8 bit field. Consequently, the 8 priority values are not 0 thru 7 as
   120     *  one might expect, but rather:
   121     *
   122     *  @p(code)
   123     *      0x00    // highest priority, non dispatched, Zero Latency priority
   124     *      0x20    // highest dispatched interrupt priority
   125     *      0x40
   126     *      0x60
   127     *      0x80
   128     *      0xa0
   129     *      0xc0
   130     *      0xe0    // lowest dispatched interrupt priority, (default)
   131     *  @p
   132     *
   133     *  Priority 0 is the highest priority and by default is
   134     *  reserved for zero latency interrupts
   135     *  (see {@link #disablePriority Hwi.disablePriority}).
   136     *
   137     *  See the Cortex M3 architecture reference manual for details
   138     *  on the behavior of interrupt priorities and their relationship
   139     *  to the {@link #priGroup Hwi.priGroup} setting.
   140     *
   141     *  @a(Interrupt Vector Tables)
   142     *  Tiva devices:
   143     *
   144     *  By default, two vector tables are created for Tiva devices:
   145     *
   146     *  A 16 entry boot vector table is placed at address 0x00000000 in
   147     *  FLASH.
   148     *
   149     *  An 80 entry vector table is placed at address 0x20000000 in RAM.
   150     *
   151     *  The FLASH boot vector table contains the reset vector and exception
   152     *  handler vectors used until the RAM based vector table is initialized.
   153     *
   154     *  The RAM vector table contains the 16 exception vectors as well as all
   155     *  the 64 user interrupt vectors.
   156     *
   157     *  During system startup, the NVIC Vector Table Offset Registor is
   158     *  intialized to point to this vector table after the table has been
   159     *  initialized.
   160     *
   161     *  @a( )
   162     *  Dual M3 Core ('Ducati') devices:
   163     *
   164     *  By default, Ducati core 0 places its runtime vector table at address
   165     *  0x00000400 and core 1 places its runtime vector table at address
   166     *  0x00000800.
   167     *
   168     *  Additionally, a boot vector table is placed at address
   169     *  0x00000000 which is shared by both cores.
   170     *
   171     *  The boot reset vector function determines which core it is being
   172     *  executed on and jumps to the reset vector contained in its corresponding
   173     *  runtime vector table.
   174     *
   175     *  The generation and placement of these vector tables is made
   176     *  automatically when the
   177     *  {@link ti.sysbios.family.arm.ducati.Core} module is used.
   178     *
   179     *  Although STRONGLY discouraged, this default behavior can be overridden
   180     *  by explicitly setting the
   181     *  {@link #resetVectorAddress Hwi.resetVectorAddress} and
   182     *  {@link #vectorTableAddress Hwi.vectorTableAddress} config parameters.
   183     *
   184     *  @a(Restrictions)
   185     *  When used within a dual M3 core (Ducati) arrangement, care must be
   186     *  taken when initializing this shared resource.
   187     *  The "Shared Resources" note provided
   188     *  in the {@link ti.sysbios.family.arm.ducati ducati} package discusses
   189     *  the management of the various hardware and software resources
   190     *  shared by the two M3 cores.
   191     *  @a
   192     *
   193     *  @p(html)
   194     *  <h3> Calling Context </h3>
   195     *  <table border="1" cellpadding="3">
   196     *    <colgroup span="1"></colgroup> <colgroup span="5" align="center"></colgroup>
   197     *
   198     *    <tr><th> Function                 </th><th>  Hwi   </th><th>  Swi   </th><th>  Task  </th><th>  Main  </th><th>  Startup  </th></tr>
   199     *    <!--                                                                                                                 -->
   200     *    <tr><td> {@link #clearInterrupt}   </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   Y    </td></tr>
   201     *    <tr><td> {@link #create}           </td><td>   N    </td><td>   N    </td><td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   202     *    <tr><td> {@link #disable}          </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   Y    </td></tr>
   203     *    <tr><td> {@link #disableInterrupt} </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   204     *    <tr><td> {@link #enable}           </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   N    </td><td>   N    </td></tr>
   205     *    <tr><td> {@link #enableInterrupt}  </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   206     *    <tr><td> {@link #Params_init}      </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   Y    </td></tr>
   207     *    <tr><td> {@link #restore}          </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   Y    </td></tr>
   208     *    <tr><td> {@link #restoreInterrupt} </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   Y    </td></tr>
   209     *    <tr><td> {@link #construct}        </td><td>   N    </td><td>   N    </td><td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   210     *    <tr><td> {@link #delete}           </td><td>   N    </td><td>   N    </td><td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   211     *    <tr><td> {@link #destruct}         </td><td>   N    </td><td>   N    </td><td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   212     *    <tr><td> {@link #getHookContext}   </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   213     *    <tr><td> {@link #setFunc}          </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   214     *    <tr><td> {@link #setHookContext}   </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   215     *    <tr><td colspan="6"> Definitions: <br />
   216     *       <ul>
   217     *         <li> <b>Hwi</b>: API is callable from a Hwi thread. </li>
   218     *         <li> <b>Swi</b>: API is callable from a Swi thread. </li>
   219     *         <li> <b>Task</b>: API is callable from a Task thread. </li>
   220     *         <li> <b>Main</b>: API is callable during any of these phases: </li>
   221     *           <ul>
   222     *             <li> In your module startup after this module is started (e.g. Hwi_Module_startupDone() returns TRUE). </li>
   223     *             <li> During xdc.runtime.Startup.lastFxns. </li>
   224     *             <li> During main().</li>
   225     *             <li> During BIOS.startupFxns.</li>
   226     *           </ul>
   227     *         <li> <b>Startup</b>: API is callable during any of these phases:</li>
   228     *           <ul>
   229     *             <li> During xdc.runtime.Startup.firstFxns.</li>
   230     *             <li> In your module startup before this module is started (e.g. Hwi_Module_startupDone() returns FALSE).</li>
   231     *           </ul>
   232     *       </ul>
   233     *    </td></tr>
   234     *
   235     *  </table>
   236     *  @p
   237     */
   238    
   239    
   240    @Template("./Hwi.xdt")  /* generates the vector table and the dispatcher */
   241    @ModuleStartup      /* generate a call to startup function */
   242    @InstanceInitStatic /* allow constructs in static only systems */
   243    
   244    module Hwi inherits ti.sysbios.interfaces.IHwi
   245    {
   246        // -------- Module Constants --------
   247    
   248        /*!
   249         *  The Cortex M3 NVIC supports up to 256 interrupts/exceptions.
   250         *
   251         *  The actual number supported is device specific and provided by
   252         *  the catalog device specification.
   253         */
   254        config Int NUM_INTERRUPTS;
   255    
   256        /*!
   257         *  The Cortex M3 NVIC supports up to 256 interrupt priorities.
   258         *
   259         *  The actual number supported is device specific and provided by
   260         *  the catalog device specification.
   261         */
   262        config Int NUM_PRIORITIES;
   263    
   264        // -------- Module Types --------
   265    
   266        /*! Hwi vector function type definition. */
   267        typedef Void (*VectorFuncPtr)(void);
   268    
   269        /*! Exception hook function type definition. */
   270        typedef Void (*ExceptionHookFuncPtr)(ExcContext *);
   271    
   272        /*! NVIC Configuration Control Register (CCR). */
   273        struct CCR {
   274            Bits8 STKALIGN;         /*! Auto stack alignment in exception */
   275            Bits8 BFHFNMIGN;        /*! All faults ignore BUS Faults */
   276            Bits8 DIV_0_TRP;        /*! Trap on divide by zero */
   277            Bits8 UNALIGN_TRP;      /*! Trap on all unaligned accesses */
   278            Bits8 USERSETMPEND;     /*! Allow user to trigger interrupts */
   279            Bits8 NONEBASETHRDENA;  /*! Allow entering thread mode anytime */
   280        };
   281    
   282        /*! @_nodoc
   283         * Nested Vectored Interrupt Controller.
   284         */
   285        struct NVIC {
   286            UInt32 RES_00;       /*! 0xE000E000 reserved */
   287            UInt32 ICTR;         /*! 0xE000E004 Interrupt Control Type */
   288            UInt32 RES_08;       /*! 0xE000E008 reserved */
   289            UInt32 RES_0C;       /*! 0xE000E00C reserved */
   290            UInt32 STCSR;        /*! 0xE000E010 SysTick Control & Status Register */
   291            UInt32 STRVR;        /*! 0xE000E014 SysTick Reload Value Register */
   292            UInt32 STCVR;        /*! 0xE000E018 SysTick Current Value Register */
   293            UInt32 STCALIB;      /*! 0xE000E01C SysTick Calibration Value Register */
   294            UInt32 RES_20 [56];  /*! 0xE000E020-0xE000E0FC reserved */
   295            UInt32 ISER [8];     /*! 0xE000E100-0xE000E11C Interrupt Set Enable Registers */
   296            UInt32 RES_120 [24]; /*! 0xE000E120-0xE000E17C reserved */
   297            UInt32 ICER [8];     /*! 0xE000E180-0xE000E19C Interrupt Clear Enable Registers */
   298            UInt32 RES_1A0 [24]; /*! 0xE000E1A0-0xE000E1FC reserved */
   299            UInt32 ISPR [8];     /*! 0xE000E200-0xE000E21C Interrupt Set Pending Registers */
   300            UInt32 RES_220 [24]; /*! 0xE000E220-0xE000E7C reserved */
   301            UInt32 ICPR [8];     /*! 0xE000E280-0xE000E29C Interrupt Clear Pending Registers */
   302            UInt32 RES_2A0 [24]; /*! 0xE000E2A0-0xE000E2FC reserved */
   303            UInt32 IABR [8];     /*! 0xE000E300-0xE000E31C Interrupt Active Bit Registers */
   304            UInt32 RES_320 [56]; /*! 0xE000E320-0xE000E3FC reserved */
   305            UInt8  IPR [240];    /*! 0xE000E400-0xE000E4EF Interrupt Priority Registers */
   306            UInt32 RES_4F0 [516];/*! 0xE000E4F0-0xE000ECFC reserved */
   307            UInt32 CPUIDBR;      /*! 0xE000ED00 CPUID Base Register */
   308            UInt32 ICSR;         /*! 0xE000ED04 Interrupt Control State Register */
   309            UInt32 VTOR;         /*! 0xE000ED08 Vector Table Offset Register */
   310            UInt32 AIRCR;        /*! 0xE000ED0C Application Interrupt/Reset Control Register */
   311            UInt32 SCR;          /*! 0xE000ED10 System Control Register */
   312            UInt32 CCR;          /*! 0xE000ED14 Configuration Control Register */
   313            UInt8  SHPR[12];     /*! 0xE000ED18 System Handlers 4-15 Priority Registers */
   314            UInt32 SHCSR;        /*! 0xE000ED24 System Handler Control & State Register */
   315            UInt8  MMFSR;        /*! 0xE000ED28 Memory Manage Fault Status Register */
   316            UInt8  BFSR;         /*! 0xE000ED29 Bus Fault Status Register */
   317            UInt16 UFSR;         /*! 0xE000ED2A Usage Fault Status Register */
   318            UInt32 HFSR;         /*! 0xE000ED2C Hard Fault Status Register */
   319            UInt32 DFSR;         /*! 0xE000ED30 Debug Fault Status Register */
   320            UInt32 MMAR;         /*! 0xE000ED34 Memory Manager Address Register */
   321            UInt32 BFAR;         /*! 0xE000ED38 Bus Fault Address Register */
   322            UInt32 AFSR;         /*! 0xE000ED3C Auxiliary Fault Status Register */
   323            UInt32 PFR0;         /*! 0xE000ED40 Processor Feature Register */
   324            UInt32 PFR1;         /*! 0xE000ED44 Processor Feature Register */
   325            UInt32 DFR0;         /*! 0xE000ED48 Debug Feature Register */
   326            UInt32 AFR0;         /*! 0xE000ED4C Auxiliary Feature Register */
   327            UInt32 MMFR0;        /*! 0xE000ED50 Memory Model Fault Register0 */
   328            UInt32 MMFR1;        /*! 0xE000ED54 Memory Model Fault Register1 */
   329            UInt32 MMFR2;        /*! 0xE000ED58 Memory Model Fault Register2 */
   330            UInt32 MMFR3;        /*! 0xE000ED5C Memory Model Fault Register3 */
   331            UInt32 ISAR0;        /*! 0xE000ED60 ISA Feature Register0 */
   332            UInt32 ISAR1;        /*! 0xE000ED64 ISA Feature Register1 */
   333            UInt32 ISAR2;        /*! 0xE000ED68 ISA Feature Register2 */
   334            UInt32 ISAR3;        /*! 0xE000ED6C ISA Feature Register3 */
   335            UInt32 ISAR4;        /*! 0xE000ED70 ISA Feature Register4 */
   336            UInt32 RES_D74[5];   /*! 0xE000ED74-0xE000ED84 reserved */
   337            UInt32 CPACR;        /*! 0xE000ED88 Coprocessor Access Control Register */
   338            UInt32 RES_D8C[93];  /*! 0xE000ED8C-0xE000EEFC reserved */
   339            UInt32 STI;          /*! 0xE000EF00 Software Trigger Interrupt Register */
   340            UInt32 RES_F04[12];  /*! 0xE000EF04-0xE000EF30 reserved */
   341            UInt32 FPCCR;        /*! 0xE000EF34 FP Context Control Register */
   342            UInt32 FPCAR;        /*! 0xE000EF38 FP Context Address Register */
   343            UInt32 FPDSCR;       /*! 0xE000EF3C FP Default Status Control Register */
   344            UInt32 MVFR0;        /*! 0xE000EF40 Media & FP Feature Register0 */
   345            UInt32 MVFR1;        /*! 0xE000EF44 Media & FP Feature Register1 */
   346            UInt32 RES_F48[34];  /*! 0xE000EF48-0xE000EFCC reserved */
   347            UInt32 PID4;         /*! 0xE000EFD0 Peripheral ID Register4 */
   348            UInt32 PID5;         /*! 0xE000EFD4 Peripheral ID Register5 */
   349            UInt32 PID6;         /*! 0xE000EFD8 Peripheral ID Register6 */
   350            UInt32 PID7;         /*! 0xE000EFDC Peripheral ID Register7 */
   351            UInt32 PID0;         /*! 0xE000EFE0 Peripheral ID Register0 */
   352            UInt32 PID1;         /*! 0xE000EFE4 Peripheral ID Register1 */
   353            UInt32 PID2;         /*! 0xE000EFE8 Peripheral ID Register2 */
   354            UInt32 PID3;         /*! 0xE000EFEC Peripheral ID Register3 */
   355            UInt32 CID0;         /*! 0xE000EFF0 Component ID Register0 */
   356            UInt32 CID1;         /*! 0xE000EFF4 Component ID Register1 */
   357            UInt32 CID2;         /*! 0xE000EFF8 Component ID Register2 */
   358            UInt32 CID3;         /*! 0xE000EFFC Component ID Register3 */
   359        }
   360    
   361        /*!
   362         * Physical Nested Vectored Interrupt Controller Device.
   363         * Short name is "Hwi_nvic"
   364         * Long name is "ti_sysbios_family_arm_m3_Hwi_nvic"
   365         */
   366        extern volatile NVIC nvic;
   367    
   368        /*!
   369         * Virtual Nested Vectored Interrupt Controller structure
   370         * written to by both cores for SMP.
   371         * Short name is "Hwi_vnvic"
   372         * Long name is "ti_sysbios_family_arm_m3_Hwi_vnvic"
   373         */
   374        extern volatile NVIC vnvic;
   375    
   376        /*!
   377         *  Exception Context - Register contents at the time of an exception.
   378         */
   379        struct ExcContext {
   380            /* Thread Context */
   381            BIOS.ThreadType threadType; /* Type of thread executing at */
   382                                        /* the time the exception occurred */
   383            Ptr     threadHandle;       /* Handle to thread executing at */
   384                                        /* the time the exception occurred */
   385            Ptr     threadStack;        /* Address of stack contents of thread */
   386                                        /* executing at the time the exception */
   387                                        /* occurred */
   388            SizeT   threadStackSize;    /* size of thread stack */
   389    
   390            /* Internal Registers */
   391            Ptr     r0;
   392            Ptr     r1;
   393            Ptr     r2;
   394            Ptr     r3;
   395            Ptr     r4;
   396            Ptr     r5;
   397            Ptr     r6;
   398            Ptr     r7;
   399            Ptr     r8;
   400            Ptr     r9;
   401            Ptr     r10;
   402            Ptr     r11;
   403            Ptr     r12;
   404            Ptr     sp;
   405            Ptr     lr;
   406            Ptr     pc;
   407            Ptr     psr;
   408    
   409            /* NVIC registers */
   410            Ptr     ICSR;
   411            Ptr     MMFSR;
   412            Ptr     BFSR;
   413            Ptr     UFSR;
   414            Ptr     HFSR;
   415            Ptr     DFSR;
   416            Ptr     MMAR;
   417            Ptr     BFAR;
   418            Ptr     AFSR;
   419        }
   420    
   421        /*! @_nodoc */
   422        metaonly struct BasicView {
   423            Ptr         halHwiHandle;
   424            String      label;
   425            String      type;
   426            Int         intNum;
   427            Int         priority;
   428            Int         group;
   429            Int         subPriority;
   430            String      fxn;
   431            UArg        arg;
   432        };
   433    
   434        /*! @_nodoc */
   435        metaonly struct DetailedView {
   436            Ptr         halHwiHandle;
   437            String      label;
   438            String      type;
   439            Int         intNum;
   440            Int         priority;
   441            Int         group;
   442            Int         subPriority;
   443            String      fxn;
   444            UArg        arg;
   445            Ptr         irp;
   446            String      status;
   447            Int         coreId;
   448        };
   449    
   450        /*! @_nodoc */
   451        metaonly struct ModuleView {
   452            String      options[4];
   453            String      activeInterrupt;
   454            String      pendingInterrupt;
   455            String      exception;
   456            String      hwiStackPeak;
   457            SizeT       hwiStackSize;
   458            Ptr         hwiStackBase;
   459        };
   460    
   461        /*! @_nodoc */
   462        @Facet
   463        metaonly config ViewInfo.Instance rovViewInfo =
   464            ViewInfo.create({
   465                viewMap: [
   466                    ['Basic',
   467                        {
   468                            type: ViewInfo.INSTANCE,
   469                            viewInitFxn: 'viewInitBasic',
   470                            structName: 'BasicView'
   471                        }
   472                    ],
   473                    ['Detailed',
   474                        {
   475                            type: ViewInfo.INSTANCE,
   476                            viewInitFxn: 'viewInitDetailed',
   477                            structName: 'DetailedView'
   478                        }
   479                    ],
   480                    ['Module',
   481                        {
   482                            type: ViewInfo.MODULE,
   483                            viewInitFxn: 'viewInitModule',
   484                            structName: 'ModuleView'
   485                        }
   486                    ],
   487                    ['Exception',
   488                        {
   489                            type: ViewInfo.TREE,
   490                            viewInitFxn: 'viewInitException',
   491                            structName: 'ExcContext'
   492                        }
   493                    ]
   494                ]
   495            });
   496    
   497        // -------- Module Parameters --------
   498    
   499        // Logs
   500    
   501        /*!
   502         *  Issued just prior to Hwi function invocation (with interrupts disabled)
   503         */
   504        config Log.Event LM_begin = {
   505            mask: Diags.USER1 | Diags.USER2,
   506            msg: "LM_begin: hwi: 0x%x, func: 0x%x, preThread: %d, intNum: %d, irp: 0x%x"
   507        };
   508    
   509        /*!
   510         *  Issued just after return from Hwi function (with interrupts disabled)
   511         */
   512        config Log.Event LD_end = {
   513            mask: Diags.USER2,
   514            msg: "LD_end: hwi: 0x%x"
   515        };
   516    
   517        // Asserts
   518    
   519        /*! Assert when bad maskSetting parameter provided */
   520        config Assert.Id A_unsupportedMaskingOption = {
   521            msg: "A_unsupportedMaskingOption: unsupported maskSetting."
   522        };
   523    
   524        // Errors
   525    
   526        /*!
   527         *  Error raised when Hwi is already defined
   528         */
   529        config Error.Id E_alreadyDefined = {
   530            msg: "E_alreadyDefined: Hwi already defined: intr# %d"
   531        };
   532    
   533        /*!
   534         *  Error raised when the number of interrupts being created
   535         *  exceeds the number supported.
   536         */
   537        config Error.Id E_hwiLimitExceeded = {
   538            msg: "E_hwiLimitExceeded: Too many interrupts defined"
   539        };
   540    
   541        /*!
   542         *  Error raised when an exception occurs
   543         */
   544        config Error.Id E_exception = {
   545            msg: "E_exception: id = %d, pc = %08x.\nTo see more exception detail, set ti.sysbios.family.arm.m3.Hwi.enableException = true or,\nexamine the Exception view for the ti.sysbios.family.arm.m3.Hwi module using ROV."
   546        };
   547    
   548        /*!
   549         *  Error raised when an uninitialized interrupt occurs
   550         */
   551        config Error.Id E_noIsr = {
   552            msg: "E_noIsr: id = %d, pc = %08x"
   553        };
   554    
   555        /*!
   556         *  Error raised when NMI exception occurs
   557         */
   558        config Error.Id E_NMI = {
   559            msg: "E_NMI: %s"
   560        };
   561    
   562        /*!
   563         *  Error raised when hard fault exception occurs
   564         */
   565        config Error.Id E_hardFault = {
   566            msg: "E_hardFault: %s"
   567        };
   568    
   569        /*!
   570         *  Error raised when memory fault exception occurs
   571         */
   572        config Error.Id E_memFault = {
   573            msg: "E_memFault: %s, address: %08x"
   574        };
   575    
   576        /*!
   577         *  Error raised when bus fault exception occurs
   578         */
   579        config Error.Id E_busFault = {
   580            msg: "E_busFault: %s, address: %08x"
   581        };
   582    
   583        /*!
   584         *  Error raised when usage fault exception occurs
   585         */
   586        config Error.Id E_usageFault = {
   587            msg: "E_usageFault: %s"
   588        };
   589    
   590        /*!
   591         *  Error raised when svCall exception occurs
   592         */
   593        config Error.Id E_svCall = {
   594            msg: "E_svCall: svNum = %d"
   595        };
   596    
   597        /*!
   598         *  Error raised when debugMon exception occurs
   599         */
   600        config Error.Id E_debugMon = {
   601            msg: "E_debugMon: %s"
   602        };
   603    
   604        /*!
   605         *  Error raised when reserved exception occurs
   606         */
   607        config Error.Id E_reserved = {
   608            msg: "E_reserved: %s %d"
   609        };
   610    
   611        // configs
   612    
   613        /*!
   614         *  Size (in number of interrupts) of the table used by the interrupt
   615         *  dispatcher to locate the corresponding Hwi object. By default,
   616         *  Hwi.dispatchTableSize will be internally set
   617         *  to the number of interrupts supported by the device.
   618         *
   619         *  When the Hwi dispatch table size is equal to the number of interrupts
   620         *  supported {@link #NUM_INTERRUPTS} by the device, a linear-indexed
   621         *  dispatch table mechanism is used that will consume 4 bytes of RAM
   622         *  for each interrupt supported.
   623         *
   624         *  If the dispatch table size is set to a number less than the number
   625         *  of interrupts supported by the device, then a non linear-indexed
   626         *  dispatch table mechanism is employed that uses 12 bytes of RAM for
   627         *  each interrupt supported.
   628         *
   629         *  Consequently, for applications that use less than 1/3 of the total
   630         *  number of interrupts supported by the device, setting this parameter
   631         *  to the number of interrupts ACTUALLY USED will result in less RAM
   632         *  memory being used than otherwise.
   633         *
   634         *  For applications that use very few interrupts, this can be a significant RAM memory savings.</p>
   635         */
   636        metaonly config UInt dispatchTableSize;
   637    
   638        /*!
   639         *  Location of the Runtime Interrupt Vector Table.
   640         *  Default is device dependent.
   641         *
   642         *  This parameter allows the user to override the default placement
   643         *  of the runtime interrupt vector table.
   644         *  The NVIC's Vector Table Offset
   645         *  Register (VTOR) is also programmed to this value.
   646         *
   647         *  Some systems require the runtime vector table to be placed at
   648         *  an address
   649         *  other than 0 but still need a copy of the two M3 boot vectors
   650         *  (SP and reset PC), located there. To achieve this, a separate
   651         *  parameter {@link #resetVectorAdress} is provided. If the
   652         *  resetVectorAddress has a different value then the vectorTableAddress
   653         *  then a separate vector table is generated and placed at that
   654         *  address.
   655         *
   656         *  The vector table must be placed at an address at or lower than
   657         *  0x3FFFFC00 and must be aligned on an even 64 word boundary.
   658         */
   659        metaonly config Ptr vectorTableAddress = 0x00000000;
   660    
   661        /*!
   662         *  Reset vector table address. Default is 0x00000000.
   663         *
   664         *  This parameter is the address of the vector table used
   665         *  at system reset time. Typically this is placed at 0x00000000.
   666         *
   667         *  If the Hwi.resetVectorAddress has a different value than
   668         *  the {@link #vectorTableAddress Hwi.vectorTableAddress}
   669         *  then two vector tables are generated, one at the Hwi.resetVectorAddress
   670         *  and another at the {@link #vectorTableAddress Hwi.vectorTableAddress}.
   671         *
   672         *  After the initial boot code has been executed at startup, the NVIC's
   673         *  Vector Table Offset Register will be programmed to point to the
   674         *  vector table at the {@link #vectorTableAddress Hwi.vectorTableAddress}.
   675         *
   676         *  is created and placed in the ".resetVecs" section.
   677         */
   678        metaonly config Ptr resetVectorAddress = 0x00000000;
   679    
   680        /*! Reset Handler. Default is c_int00 */
   681        metaonly config VectorFuncPtr resetFunc;
   682    
   683        /*! NMI Handler. Default is set to an internal exception handler */
   684        metaonly config VectorFuncPtr nmiFunc;
   685    
   686        /*! Hard Fault Handler. Default is set to an internal exception handler */
   687        metaonly config VectorFuncPtr hardFaultFunc;
   688    
   689        /*! Hard Mem Handler. Default is set to an internal exception handler */
   690        metaonly config VectorFuncPtr memFaultFunc;
   691    
   692        /*! Bus Fault Handler. Default is set to an internal exception handler */
   693        metaonly config VectorFuncPtr busFaultFunc;
   694    
   695        /*! Usage Fault Handler. Default is set to an internal exception handler */
   696        metaonly config VectorFuncPtr usageFaultFunc;
   697    
   698        /*! SVCall Handler. Default is set to an internal exception handler */
   699        metaonly config VectorFuncPtr svCallFunc;
   700    
   701        /*! Debug Mon Handler. Default is set to an internal exception handler */
   702        metaonly config VectorFuncPtr debugMonFunc;
   703    
   704        /*! Reserved Exception Handler. Default is set to an internal exception handler */
   705        metaonly config VectorFuncPtr reservedFunc;
   706    
   707        /*! Uninitialized ISR Handler. Default is set to an internal exception handler */
   708        config VectorFuncPtr nullIsrFunc;
   709    
   710        /*! Hwi exception handler function type definition. */
   711        typedef Void (*ExcHandlerFuncPtr)(UInt *, UInt);
   712    
   713        /*!
   714         *  Exception handler function pointer.
   715         *
   716         *  The default is determined by the value of Hwi.enableException.
   717         *
   718         *  If the user does NOT set this parameter, then the following default
   719         *  behavior is followed:
   720         *
   721         *  If Hwi.enableException is true, then the internal 'Hwi_excHandlerMax'
   722         *  function is used. This exception handler saves the exception context
   723         *  then does a complete exception decode and dump to the console, then
   724         *  raises an Error. The exception context can be viewed within CCS
   725         *  in the ROV Hwi module's Exception view.
   726         *
   727         *  If Hwi.enableException is false, then the internal 'Hwi_excHandlerMin'
   728         *  function is used. This exception handler saves the exception context
   729         *  then raises an Error. The exception context can be viewed within CCS
   730         *  in the ROV Hwi module's Exception view.
   731         *
   732         *  If the user sets this parameter to their own function, then the user's
   733         *  function will be invoked with the following arguments:
   734         *
   735         *      Void myExceptionHandler(UInt *excStack, UInt lr);
   736         *
   737         *  Where 'excStack' is the address of the stack containing the
   738         *  register context at the time of the exception, and 'lr' is the
   739         *  link register value when the low-level-assembly-coded exception
   740         *  handler was vectored to.
   741         *
   742         *  If this parameter is set to 'null', then an infinite while loop is
   743         *  entered when an exception occurs. This setting minimizes code and
   744         *  data footprint but provides no automatic exception decoding.
   745         */
   746        config ExcHandlerFuncPtr excHandlerFunc = excHandlerMax;
   747    
   748        /*
   749         *  SMP Interrupt affinity mappings
   750         *
   751         *  In SMP mode, this array maps an interrupt number to the
   752         *  coreId it is to be tied to. By default, all ints are mapped to
   753         *  core 0.
   754         *
   755         *  For example, to make Timer 1 from the
   756         *  ti.sysbios.family.arm.ducati.Timer
   757         *  module interrupt on core 1 rather than core 0, add the following to
   758         *  your config file:
   759         *
   760         *  @p(code)
   761         *     var m3Hwi = xdc.useModule('ti.sysbios.family.arm.m3.Hwi');
   762         *     m3Hwi.intAffinity[22] = 1;
   763         *  @p
   764         *
   765         *  @a(constraints)
   766         *  Valid core Ids are 0 and 1 for Ducati/Benelli SMP applications.
   767         *
   768         *  Interrupt numbers below 16 are ignored.
   769         *  Only interrupt numbers greater than or equal to #16 can be routed to
   770         *  either Ducati/Benelli core.
   771         *
   772         *  Interrupt #19, the Ducati inter-core interrupt, is reserved for
   773         *  exclusive use within the SMP kernel.
   774         */
   775        metaonly config UInt8 intAffinity[];
   776    
   777        /*!
   778         *  Enable full exception decoding
   779         *
   780         *  When this is enabled, the exception handler will fully
   781         *  decode an exception and dump the registers to the
   782         *  system console.
   783         */
   784        metaonly config Bool enableException = true;
   785    
   786        /*!
   787         *  User Exception Context Buffer Address
   788         *
   789         *  By default, when an exception occurs, an {@link #ExcContext}
   790         *  structure is allocated on the ISR stack and filled in within the
   791         *  exception handler.
   792         *
   793         *  If {@link #excContextBuffer} is initialized by the user, the
   794         *  {@link #ExcContext} structure will be placed at that address instead.
   795         *
   796         *  The buffer must be large enough to contain an {@link #ExcContext}
   797         *  structure.
   798         */
   799        metaonly config Ptr excContextBuffer;
   800        metaonly config Ptr excContextBuffers[];
   801    
   802        /*!
   803         *  User Exception Stack Buffer Address
   804         *
   805         *  By default, when an exception occurs, a pointer to the base address
   806         *  of the stack being used by the thread causing the exception is placed
   807         *
   808         *  If {@link #excStackBuffer} is initialized by the user, the
   809         *  stack contents of the thread causing the exception will be
   810         *  copied to that address instead.
   811         *
   812         *  The buffer must be large enough to contain the largest task stack
   813         *  or ISR stack defined in the application.
   814         */
   815        metaonly config Ptr excStackBuffer;
   816        metaonly config Ptr excStackBuffers[];
   817    
   818    
   819        /*!
   820         *  User Exception hook function.
   821         *
   822         *  Called just after the exception context has been initialized.
   823         *
   824         *  This function will be run on the ISR stack.
   825         *
   826         *  This function must run to completion.
   827         *
   828         *  It is called without any Task or Swi scheduling protection
   829         *  and therefore can not call any functions that may cause a Swi or Task
   830         *  scheduling operation (Swi_post(), Semaphore_post(), Event_post(), etc).
   831         */
   832        config ExceptionHookFuncPtr excHookFunc = null;
   833        config ExceptionHookFuncPtr excHookFuncs[];
   834    
   835        /*!
   836         *  NVIC CCR register settings
   837         *
   838         *  These setting are written to Hwi_nvic.CCR at startup time.
   839         *
   840         *  See the Cortex M3 architecture reference manual for details
   841         *  on the meanings of these parameters.
   842         */
   843        metaonly config CCR nvicCCR = {
   844            STKALIGN: 1,
   845            BFHFNMIGN: 0,
   846            DIV_0_TRP: 0,
   847            UNALIGN_TRP: 0,
   848            USERSETMPEND: 0,
   849            NONEBASETHRDENA: 0
   850        };
   851    
   852        /*!
   853         *  The priority that BASEPRI is set to by Hwi_disable().
   854         *
   855         *  All interrupts configured with equal or less priority (equal or
   856         *  higher number) than disablePriority are disabled by
   857         *  {@link #disable Hwi_disable}.
   858         *  Interrupts configured with higher priority (smaller number) than
   859         *  Hwi.disablePriority are non-maskable (ie zero-latency).
   860         *
   861         *  The default setting is the second highest interrupt priority
   862         *  defined for the device (typically '0x20' for devices
   863         *  which support 8 priority values).
   864         *  This results in priority 0 (and all
   865         *  other values in the same priority group, ie 0x00 thru 0x1f)
   866         *  being the zero-latency, non-maskable interrupt priority.
   867         *  All other priorities are disabled with Hwi_disable().
   868         */
   869        config UInt disablePriority;
   870    
   871        /*!
   872         *  The PRIGROUP setting. Default is 0.
   873         *
   874         *  This value will be written to the PRIGROUP field
   875         *  within the NVIC's Application Interrupt and Reset Control
   876         *  Register (Hwi_nvic.AIRCR). It defines how the 8 bit priority
   877         *  values are interpreted by the hardware.
   878         *
   879         *  Valid settings are 0-7.
   880         *
   881         *  The default setting of 0 causes bits 7-1 of an interrupt's
   882         *  priority value to be used as pre-emption priority, while bit 0
   883         *  is used to determine which of two simultaneous interrupts with
   884         *  the same pre-emption priority will be serviced first.
   885         *
   886         *  For most TI MCU devices, this means that each of the 8 supported
   887         *  priority values are unique pre-emption priorities and are not
   888         *  subdivided into priority groups.
   889         */
   890        config UInt priGroup = 0;
   891    
   892        // -------- Module Functions --------
   893    
   894        /*!
   895         *  ======== disable ========
   896         *  Disable all non zero-latency interrupts
   897         *
   898         *  Hwi_disable disables all non zero-latency hardware interrupts and
   899         *  returns an
   900         *  opaque key indicating whether interrupts were globally enabled or
   901         *  disabled on entry to Hwi_disable().
   902         *  The actual value of the key is target/device specific and is meant
   903         *  to be passed to Hwi_restore().
   904         *
   905         *  Call Hwi_disable before a portion of a function that needs
   906         *  to run without interruption. When critical processing is complete, call
   907         *  Hwi_restore or Hwi_enable to reenable hardware interrupts.
   908         *
   909         *  Servicing of interrupts that occur while interrupts are disabled is
   910         *  postponed until interrupts are reenabled. However, if the same type
   911         *  of interrupt occurs several times while interrupts are disabled,
   912         *  the interrupt's function is executed only once when interrupts are
   913         *  reenabled.
   914         *
   915         *  A context switch can occur when calling Hwi_enable or Hwi_restore if
   916         *  an enabled interrupt occurred while interrupts are disabled.
   917         *
   918         *  Hwi_disable may be called from main(). However, since Hwi interrupts
   919         *  are already disabled in main(), such a call has no effect.
   920         *
   921         *  @a(Implementation Note)
   922         *  In order to support zero latency interrupts, rather
   923         *  than setting PRIMASK (which would globally disable all NVIC
   924         *  interrupts), Hwi_disable() instead writes the value of
   925         *  {@link #disablePriority Hwi.disablePriority}
   926         *  to the BASEPRI register. In doing so, all interrupts of equal or
   927         *  lower priority than Hwi.disablePriority are disabled.
   928         *
   929         *  @a(constraints)
   930         *  If a Task switching API such as
   931         *  {@link ti.sysbios.knl.Semaphore#pend Semaphore_pend()},
   932         *  {@link ti.sysbios.knl.Semaphore#post Semaphore_post()},
   933         *  {@link ti.sysbios.knl.Task#sleep Task_sleep()}, or
   934         *  {@link ti.sysbios.knl.Task#yield Task_yield()}
   935         *  is invoked which results in a context switch while
   936         *  interrupts are disabled, an embedded call to
   937         *  {@link #enable Hwi_enable} occurs
   938         *  on the way to the new thread context which unconditionally re-enables
   939         *  interrupts. Interrupts will remain enabled until a subsequent
   940         *  {@link #disable Hwi_disable}
   941         *  invocation.
   942         *
   943         *  Swis always run with interrupts enabled.
   944         *  See {@link ti.sysbios.knl.Swi#post Swi_post()} for a discussion Swis and
   945         *  interrupts.
   946         *
   947         *  @b(returns)     opaque key for use by Hwi_restore()
   948         */
   949        @Macro
   950        override UInt disable();
   951    
   952        /*!
   953         *  ======== enable ========
   954         */
   955        @Macro
   956        override UInt enable();
   957    
   958        /*!
   959         *  ======== restore ========
   960         */
   961        @Macro
   962        override Void restore(UInt key);
   963    
   964        /*!
   965         *  @_nodoc
   966         *  ======== disableFxn ========
   967         *  function call implementation
   968         */
   969        UInt disableFxn();
   970    
   971        /*!
   972         *  @_nodoc
   973         *  ======== enableFxn ========
   974         *  function call implementation
   975         */
   976        UInt enableFxn();
   977    
   978        /*!
   979         *  @_nodoc
   980         *  ======== restoreFxn ========
   981         *  function call implementation
   982         */
   983        Void restoreFxn(UInt key);
   984    
   985        /*!
   986         *  ======== inUseMeta ========
   987         *  @_nodoc
   988         *  Check for Hwi already in use.
   989         *  For internal SYS/BIOS use only.
   990         *  Should be called prior to any internal Hwi.create().
   991         *
   992         *  @param(intNum)  interrupt number
   993         */
   994        metaonly Bool inUseMeta(UInt intNum);
   995    
   996        /*!
   997         *  @_nodoc
   998         *  ======== plug ========
   999         *  Plug a non dispatched interrupt vector with an ISR address.
  1000         *
  1001         *  @param(intNum)  interrupt number
  1002         *  @param(fxn)     pointer to ISR function
  1003         */
  1004        Void plug(UInt intNum, Void *fxn);
  1005    
  1006        /*!
  1007         *  ======== getHandle ========
  1008         *  Returns Hwi_handle associated with intNum
  1009         *
  1010         *  @param(intNum)  interrupt number
  1011         */
  1012        Handle getHandle(UInt intNum);
  1013    
  1014        /*!
  1015         *  ======== setPriority ========
  1016         *  Set an interrupt's relative priority.
  1017         *
  1018         *  Valid priorities are 0 - 255. 0 is highest priority.
  1019         *
  1020         *  @a(WARNING)
  1021         *  Setting the priority of a dispatched Hwi to a value higher
  1022         *  than {@link #disablePriority Hwi.disablePriority} will make
  1023         *  it become non-maskable by {@link #disable Hwi_disable()}.
  1024         *  The behavior of your application after that will be
  1025         *  unpredictable and will likely yield catastrophic results!
  1026         *
  1027         *  @param(intNum)      ID of interrupt
  1028         *  @param(priority)    priority
  1029         */
  1030        Void setPriority(UInt intNum, UInt priority);
  1031    
  1032        /*!
  1033         *  ======== excSetBuffers ========
  1034         *  Set the exception context and stack buffer pointers
  1035         *
  1036         *  @param(excContextBuffer)        Address to place ExcContext
  1037         *  @param(excStackBuffer)          Address to place ExcStack
  1038         */
  1039        Void excSetBuffers(Ptr excContextBuffer, Ptr excStackBuffer);
  1040    
  1041        /*!
  1042         *  @_nodoc
  1043         *  ======== initNVIC ========
  1044         *  initialize everything but leave ints disabled
  1045         */
  1046        Void initNVIC();
  1047    
  1048        /*!
  1049         *  @_nodoc
  1050         *  ======== initStacks ========
  1051         * set up M3 split stacks
  1052         */
  1053        Void initStacks(Ptr hwiStack);
  1054    
  1055        /*!
  1056         *  @_nodoc
  1057         *  ======== flushVnvic ========
  1058         *  Reconfigure a dispatched interrupt.
  1059         *
  1060         *  Called by the internal function "Hwi_updateNvic()".
  1061         *
  1062         *  This is a public API because it is also called by "Core_hwiFunc()".
  1063         */
  1064        Void flushVnvic();
  1065    
  1066    instance:
  1067    
  1068        /*!
  1069         *  Interrupt priority.
  1070         *  The default is 255 which is the lowest priority.
  1071         *
  1072         *  Priority 0 is the highest priority and by default is
  1073         *  reserved for zero latency interrupts
  1074         *  (see {@link #disablePriority}).
  1075         *
  1076         *  Valid priorities values are device dependent and their
  1077         *  nesting behaviors depend on the {@link #priGroup} setting.
  1078         *
  1079         *  See the Cortex M3 architecture reference manual for details
  1080         *  on the meanings of these parameters.
  1081         */
  1082        override config Int priority = 255;
  1083    
  1084        /*!
  1085         * Interrupt Masking Option. Only MaskingOption_LOWER is supported.
  1086         *
  1087         * The NVIC interrupt controller is designed for priority based
  1088         * interrupts. No support is provided for anything but
  1089         * Hwi.MaskingOption_LOWER.
  1090         */
  1091        override config IHwi.MaskingOption maskSetting = IHwi.MaskingOption_LOWER;
  1092    
  1093        /*!
  1094         *  Use the interrupt dispatcher with this interrupt. Default is true.
  1095         *
  1096         *  If set to false, the interrupt dispatcher is NOT used. Instead,
  1097         *  the configured Hwi function address is placed directly in the
  1098         *  vector table, which results in the dispatcher being bypassed.
  1099         *
  1100         *  @a(Warning)
  1101         *  Interrupts configured to bupass the dispatcher are not allowed
  1102         *  to call ANY SYS/BIOS APIs that effect thread scheduling. Examples
  1103         *  of API that should no be invoked are:
  1104         *
  1105         *  @p(dlist)
  1106         *    - Swi_post(),
  1107         *    - Semaphore_post(),
  1108         *    - Event_post(),
  1109         *    - Task_yield()
  1110         *  @p
  1111         *
  1112         *  Additionally, although the signature for a non-dispatched interrupt
  1113         *  function is the same as that for a dispatched interrupt
  1114         *  (see {@link #FuncPtr}), no argument is actually passed
  1115         *  to the non-dispatched ISR handler.
  1116         */
  1117        config Bool useDispatcher = true;
  1118    
  1119        /*!
  1120         *  ======== reconfig ========
  1121         *  Reconfigure a dispatched interrupt.
  1122         */
  1123        Void reconfig(FuncPtr fxn, const Params *params);
  1124    
  1125    internal:   /* not for client use */
  1126    
  1127        /*!
  1128         *  If Hwi.dispatchTableSize is initialized by the user then
  1129         *  Hwi.numSparseInterrupts is set to the value of Hwi.dispatchTableSize
  1130         *
  1131         *  If Hwi.dispatchTableSize is NOT set by the user, the normal
  1132         *  intNum-indexed Hwi dispatchTable mechanism is used by
  1133         *  the dispatcher to find the corresponding Hwi object.
  1134         *
  1135         *  If Hwi.dispatchTableSize is set by the user, then a
  1136         *  RAM-based fixed sized interrupt jump table is generated
  1137         *  that contains a repeating pattern of the following 3 word
  1138         *  assembly code snippets:
  1139         *
  1140         *   hwiX:        ldr r3, hwiObjectX
  1141         *                ldr pc, ti_sysbios_family_arm_m3_Hwi_dispatch__I
  1142         *   hwiObjectX: .word 0
  1143         *   hwiY:        ldr r3, hwiObjectY
  1144         *                ldr pc, ti_sysbios_family_arm_m3_Hwi_dispatch__I
  1145         *   hwiObjectY: .word 0
  1146         *               ...
  1147         *
  1148         *  Each dispatched interrupt vector is then initialized to point
  1149         *  to one of these tuples, and the address of the corresponding Hwi
  1150         *  object is written into the hwiObjectX field.
  1151         *
  1152         *  The low level assembly code in Hwi_dispatch__I preserves the
  1153         *  value of r3 when it calls Hwi_dispatchC(), which results in
  1154         *  the Hwi object being passed as the arg3.
  1155         *
  1156         *  Depending on the boolean value of Hwi_numSparseInterrupts, the
  1157         *  dispatcher either uses the value passed in arg3 as the
  1158         *  Hwi object, or uses intNum to index into the standard
  1159         *  dispatchTable to fetch the Hwi object.
  1160         */
  1161        config UInt numSparseInterrupts = 0;
  1162    
  1163        /*
  1164         *  Boolean to indicate whether the current target is being
  1165         *  built using tiva platform.
  1166         */
  1167        metaonly config Bool isTiva = false;
  1168    
  1169        /*
  1170         *  The omap4430 ES1 devices have a nasty bug in the unicache
  1171         *  that locks the bus up when an interrupt occurs at a specific
  1172         *  time during an internal cache operation.
  1173         *  The flag below, when set to true, activates special
  1174         *  code in the Hwi module to work around this bug.
  1175         *  "WA1_1" comes from "WorkAround 1.1" from a list of potential
  1176         *  solutions to the problem developed by the design team.
  1177         */
  1178        metaonly config Bool enableWA1_1 = false;
  1179    
  1180        /*
  1181         * Swi and Task module function pointers.
  1182         * Used to decouple Hwi from Swi and Task when
  1183         * dispatcherSwiSupport or
  1184         * dispatcherTaskSupport is false.
  1185         */
  1186        config UInt (*swiDisable)();
  1187        config Void (*swiRestoreHwi)(UInt);
  1188        config UInt (*taskDisable)();
  1189        config Void (*taskRestoreHwi)(UInt);
  1190    
  1191        /* initial Hwi_nvic.CCR value */
  1192        config UInt32 ccr;
  1193    
  1194        /*!
  1195         *  const array to hold all HookSet objects.
  1196         */
  1197        config HookSet hooks[length] = [];
  1198    
  1199        /*
  1200         *  ======== postInit ========
  1201         *  finish initializing static and dynamic Hwis
  1202         */
  1203        Int postInit(Object *hwi, Error.Block *eb);
  1204    
  1205        /*!
  1206         *  ======== updateNvic ========
  1207         *  Internal SMP function to cause the virtual NVIC to be flushed to the
  1208         *  actual NVIC.
  1209         *
  1210         *  This function is called by the various user APIs that manipulate
  1211         *  individual NVIC register bits
  1212         *  (ie Hwi_enable/disable/restore/clearInterrupt())
  1213         *
  1214         *  If the current core is the owner of "intNum", flushVnvic() is called
  1215         *  immediately.
  1216         *
  1217         *  Otherwise an intercore interrupt is generated to force the other core
  1218         *  to perform the flushVnvic().
  1219         *
  1220         */
  1221        Void updateNvic(UInt intNum);
  1222    
  1223        /*!
  1224         *  ======== excHandlerAsm ========
  1225         *  asm code exception handler
  1226         */
  1227        Void excHandlerAsm();
  1228    
  1229        /*!
  1230         *  ======== excHandler ========
  1231         *  exception Handler routes to
  1232         *  either min, max, or spin exception handler
  1233         */
  1234        Void excHandler(UInt *excStack, UInt lr);
  1235    
  1236        /*!
  1237         *  ======== excHandlerMin ========
  1238         *  Minimal Exception Handler
  1239         */
  1240        Void excHandlerMin(UInt *excStack, UInt lr);
  1241    
  1242        /*!
  1243         *  ======== excHandlerMax ========
  1244         *  Full Featured Exception Handler
  1245         */
  1246        Void excHandlerMax(UInt *excStack, UInt lr);
  1247    
  1248        /*!
  1249         *  ======== excFillContext ========
  1250         */
  1251        Void excFillContext(UInt *excStack);
  1252    
  1253        /*!
  1254         *  ======== excNmi ========
  1255         */
  1256        Void excNmi(UInt *excStack);
  1257    
  1258        /*!
  1259         *  ======== excHardFault ========
  1260         */
  1261        Void excHardFault(UInt *excStack);
  1262    
  1263        /*!
  1264         *  ======== excMemFault ========
  1265         */
  1266        Void excMemFault(UInt *excStack);
  1267    
  1268        /*!
  1269         *  ======== excBusFault ========
  1270         */
  1271        Void excBusFault(UInt *excStack);
  1272    
  1273        /*!
  1274         *  ======== excUsageFault ========
  1275         */
  1276        Void excUsageFault(UInt *excStack);
  1277    
  1278        /*!
  1279         *  ======== excSvCall ========
  1280         */
  1281        Void excSvCall(UInt *excStack);
  1282    
  1283        /*!
  1284         *  ======== excDebugMon ========
  1285         */
  1286        Void excDebugMon(UInt *excStack);
  1287    
  1288        /*!
  1289         *  ======== excReserved ========
  1290         */
  1291        Void excReserved(UInt *excStack, UInt excNum);
  1292    
  1293        /*!
  1294         *  ======== excNoIsr ========
  1295         */
  1296        Void excNoIsr(UInt *excStack, UInt excNum);
  1297    
  1298        /*!
  1299         *  ======== excDumpRegs ========
  1300         */
  1301        Void excDumpRegs(UInt lr);
  1302    
  1303        /*!
  1304         *  ======== pendSV ========
  1305         * Used by dispatcher
  1306         */
  1307        Void pendSV();
  1308    
  1309        /*! Hwi vector function type definition. */
  1310        typedef Void (*HandlerFuncPtr)(Handle, UInt);
  1311    
  1312        /* Low Level Interrupt Dispatcher Wrapper */
  1313        Void dispatch();
  1314    
  1315        /*
  1316         *  ======== cc26xxRomInitNVIC ========
  1317         *  Fix for SDOCM00114681: broken Hwi_initNVIC() function.
  1318         *  Installed rather than Hwi.initNVIC for CC26xx ROM build
  1319         *  when Hwi.resetVectorAddress is not 0x00000000.
  1320         */
  1321        Void cc26xxRomInitNVIC();
  1322    
  1323        /*
  1324         * "Top Half" of Interrupt Dispatcher
  1325         *  Does not include Swi_restore() and Task_restore()
  1326         */
  1327        UInt dispatchC(Irp irp, UInt32 dummy1, UInt32 dummy2, Object *hwi);
  1328    
  1329        /* "Bottom half", run swi scheduler */
  1330        Void doSwiRestore(UInt tskKey);
  1331    
  1332        /* "Bottom half", run task scheduler */
  1333        Void doTaskRestore(UInt tskKey);
  1334    
  1335        /*! Meta World Only Hwi Configuration Object. */
  1336        metaonly struct InterruptObj {
  1337            String name;            /* symbol used for vector table entry */
  1338            Bool used;              /* Interrupt already defined? */
  1339            Bool useDispatcher;     /* Should dispatcher handle this Int? */
  1340            UInt priority;          /* priority */
  1341            FuncPtr fxn;            /* Dispatched ISR function */
  1342            Handle  hwi;            /* Hwi object address */
  1343        };
  1344    
  1345        /*!
  1346         * Meta-only array of interrupt objects.
  1347         * This meta-only array of Hwi config objects is initialized
  1348         * in Hwi.xs:module$meta$init().
  1349         */
  1350        metaonly config InterruptObj interrupt[];
  1351    
  1352        struct Instance_State {
  1353            UArg            arg;            // Argument to Hwi function.
  1354            FuncPtr         fxn;            // Hwi function.
  1355            Irp             irp;            // current IRP/enabled flag
  1356                                            // for static Hwis
  1357            UInt8           priority;       // Interrupt priorty
  1358            Int16           intNum;         // Interrupt number. 16 bits used to
  1359                                            // encode non-dispatched interrupt
  1360                                            // as negative intNum
  1361            Ptr             hookEnv[];
  1362        };
  1363    
  1364        struct Module_State {
  1365            Char            *taskSP;            // Temporary storage of interrupted
  1366                                                // Task's SP during ISR execution
  1367            Bool            excActive[];        // TRUE if an exception has occurred
  1368            ExcContext      *excContext[];      // Exception context
  1369            Ptr             excStack[];         // Exception thread stack
  1370            Ptr             isrStack;           // Points to isrStack address
  1371            Ptr             isrStackBase;       // = __TI_STACK_BASE
  1372            Ptr             isrStackSize;       // = Program.stack
  1373            Ptr             vectorTableBase;    // Points to base of vector table
  1374            UInt            swiTaskKeys;        // dispatcher Swi and Task key storage
  1375            Ptr             dispatchTable;      // Ptr to dispatchTable or sparseInterruptTable
  1376            volatile Bool   vnvicFlushRequired; // if TRUE, Hwi_vnvicFlush will copy
  1377                                                // changed vnvic regs to nvic
  1378            UInt8           intAffinity[];      // smp int-to-coreId mappings
  1379            UInt32          intAffinityMasks[][]; // smp per-core NVIC register masks
  1380        };
  1381    }