Instance: DDI_0_OSC
Component: DDI_0_OSC
Base address: 0x400CA000
This is the DDI for the digital block that controls all the analog clock oscillators (OSC_DIG) and performs qualification of the clocks generated.
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
RW |
32 |
0x0000 0000 |
0x0000 0000 |
0x400C A000 |
|
RW |
32 |
0x0000 0000 |
0x0000 0004 |
0x400C A004 |
|
RW |
32 |
0x0000 0000 |
0x0000 0008 |
0x400C A008 |
|
RW |
32 |
0x0000 0000 |
0x0000 000C |
0x400C A00C |
|
RW |
32 |
0x0000 0000 |
0x0000 0010 |
0x400C A010 |
|
RW |
32 |
0x0000 0000 |
0x0000 0014 |
0x400C A014 |
|
RW |
32 |
0x0000 0000 |
0x0000 0018 |
0x400C A018 |
|
RW |
32 |
0x0000 0000 |
0x0000 001C |
0x400C A01C |
|
RW |
32 |
0x0000 0000 |
0x0000 0020 |
0x400C A020 |
|
RW |
32 |
0x0000 0000 |
0x0000 0024 |
0x400C A024 |
|
RW |
32 |
0x0000 0000 |
0x0000 0028 |
0x400C A028 |
|
RW |
32 |
0x0000 0000 |
0x0000 002C |
0x400C A02C |
|
RW |
32 |
0x0000 0000 |
0x0000 0030 |
0x400C A030 |
|
RO |
32 |
0x0000 0000 |
0x0000 0034 |
0x400C A034 |
|
RO |
32 |
0x0000 0000 |
0x0000 0038 |
0x400C A038 |
|
RO |
32 |
0x0000 0000 |
0x0000 003C |
0x400C A03C |
Address Offset | 0x0000 0000 | ||
Physical Address | 0x400C A000 | Instance | 0x400C A000 |
Description | Control 0 Controls various clock source selects |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||||||||
31 | XTAL_IS_24M | Set based on the accurate high frequency XTAL.
|
RW | 0 | |||||||||||||||||
30 | RESERVED30 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | |||||||||||||||||
29 | BYPASS_XOSC_LF_CLK_QUAL | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||
28 | BYPASS_RCOSC_LF_CLK_QUAL | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||
27:26 | DOUBLER_START_DURATION | Internal. Only to be used through TI provided API. | RW | 0b00 | |||||||||||||||||
25 | DOUBLER_RESET_DURATION | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||
24:23 | RESERVED23 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 | |||||||||||||||||
22 | FORCE_KICKSTART_EN | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||
21:17 | RESERVED17 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b0 0000 | |||||||||||||||||
16 | ALLOW_SCLK_HF_SWITCHING | 0: Default - Switching of HF clock source is disabled . 1: Allows swtiching of sclk_hf source. Provided to prevent switching of the SCLK_HF source when running from flash (a long period during switching could corrupt flash). When sclk_hf switching is disabled, a new source can be started when SCLK_HF_SRC_SEL is changed, but the switch will not occur until this bit is set. This bit should be set to enable clock switching after STAT0.PENDINGSCLKHFSWITCHING indicates the new HF clock is ready. When switching completes (also indicated by STAT0.PENDINGSCLKHFSWITCHING) sclk_hf switching should be disabled to prevent flash corruption. Switching should not be enabled when running from flash. |
RW | 0 | |||||||||||||||||
15 | RESERVED15 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | |||||||||||||||||
14 | HPOSC_MODE_EN | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||
13 | RESERVED13 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | |||||||||||||||||
12 | RCOSC_LF_TRIMMED | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||
11 | XOSC_HF_POWER_MODE | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||
10 | XOSC_LF_DIG_BYPASS | Bypass XOSC_LF and use the digital input clock from AON for the xosc_lf clock.. 0: Use 32kHz XOSC as xosc_lf clock source 1: Use digital input (from AON) as xosc_lf clock source. This bit will only have effect when SCLK_LF_SRC_SEL is selecting the xosc_lf as the sclk_lf source. The muxing performed by this bit is not glitch free. The following procedure should be followed when changing this field to avoid glitches on sclk_lf.. 1) Set SCLK_LF_SRC_SEL to select any source other than the xosc_lf clock source. 2) Set or clear this bit to bypass or not bypass the xosc_lf. 3) Set SCLK_LF_SRC_SEL to use xosc_lf. It is recommended that either the rcosc_hf or xosc_hf (whichever is currently active) be selected as the source in step 1 above. This provides a faster clock change. |
RW | 0 | |||||||||||||||||
9 | CLK_LOSS_EN | Enable clock loss circuit and hence the indicators to system controller. Checks both SCLK_HF and SCLK_LF clock loss indicators. 0: Disable 1: Enable Clock loss detection should be disabled when changing the sclk_lf source. STAT0.SCLK_LF_SRC can be polled to determine when a change to a new sclk_lf source has completed. |
RW | 0 | |||||||||||||||||
8:7 | ACLK_TDC_SRC_SEL | Source select for aclk_tdc. 00: RCOSC_HF (48MHz) 01: RCOSC_HF (24MHz) 10: XOSC_HF (24MHz) 11: Not used |
RW | 0b00 | |||||||||||||||||
6:5 | ACLK_REF_SRC_SEL | Source select for aclk_ref 00: RCOSC_HF desirved (31.25kHz) 01: XOSC_HF derived (31.25kHz) 10: RCOSC_LF (32kHz) 11: XOSC_LF (32.768kHz) |
RW | 0b00 | |||||||||||||||||
4 | SPARE4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | |||||||||||||||||
3:2 | SCLK_LF_SRC_SEL | Source select for sclk_lf
|
RW | 0b00 | |||||||||||||||||
1 | SCLK_MF_SRC_SEL | Internal. Only to be used through TI provided API.
|
RW | 0 | |||||||||||||||||
0 | SCLK_HF_SRC_SEL | Source select for sclk_hf
|
RW | 0 |
Address Offset | 0x0000 0004 | ||
Physical Address | 0x400C A004 | Instance | 0x400C A004 |
Description | Control 1 This register contains various OSC_DIG configuration |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:23 | RESERVED23 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b0 0000 0000 | ||
22:18 | RCOSCHFCTRIMFRACT | Internal. Only to be used through TI provided API. | RW | 0b0 0000 | ||
17 | RCOSCHFCTRIMFRACT_EN | Internal. Only to be used through TI provided API. | RW | 0 | ||
16:2 | SPARE2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b000 0000 0000 0000 | ||
1:0 | XOSC_HF_FAST_START | Internal. Only to be used through TI provided API. | RW | 0b00 |
Address Offset | 0x0000 0008 | ||
Physical Address | 0x400C A008 | Instance | 0x400C A008 |
Description | RADC External Configuration | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:22 | HPM_IBIAS_WAIT_CNT | Internal. Only to be used through TI provided API. | RW | 0b00 0000 0000 | ||
21:16 | LPM_IBIAS_WAIT_CNT | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
15:12 | IDAC_STEP | Internal. Only to be used through TI provided API. | RW | 0x0 | ||
11:6 | RADC_DAC_TH | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
5 | RADC_MODE_IS_SAR | Internal. Only to be used through TI provided API. | RW | 0 | ||
4:0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b0 0000 |
Address Offset | 0x0000 000C | ||
Physical Address | 0x400C A00C | Instance | 0x400C A00C |
Description | Amplitude Compensation Control | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||||||||
31 | SPARE31 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | |||||||||||||||||
30 | AMPCOMP_REQ_MODE | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||
29:28 | AMPCOMP_FSM_UPDATE_RATE | Internal. Only to be used through TI provided API.
|
RW | 0b00 | |||||||||||||||||
27 | AMPCOMP_SW_CTRL | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||
26 | AMPCOMP_SW_EN | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||
25:24 | RESERVED24 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 | |||||||||||||||||
23:20 | IBIAS_OFFSET | Internal. Only to be used through TI provided API. | RW | 0x0 | |||||||||||||||||
19:16 | IBIAS_INIT | Internal. Only to be used through TI provided API. | RW | 0x0 | |||||||||||||||||
15:8 | LPM_IBIAS_WAIT_CNT_FINAL | Internal. Only to be used through TI provided API. | RW | 0x00 | |||||||||||||||||
7:4 | CAP_STEP | Internal. Only to be used through TI provided API. | RW | 0x0 | |||||||||||||||||
3:0 | IBIASCAP_HPTOLP_OL_CNT | Internal. Only to be used through TI provided API. | RW | 0x0 |
Address Offset | 0x0000 0010 | ||
Physical Address | 0x400C A010 | Instance | 0x400C A010 |
Description | Amplitude Compensation Threashold 1 This register contains various threshhold values for amplitude compensation algorithm |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:24 | SPARE24 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0x00 | ||
23:18 | HPMRAMP3_LTH | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
17:16 | SPARE16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 | ||
15:10 | HPMRAMP3_HTH | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
9:6 | IBIASCAP_LPTOHP_OL_CNT | Internal. Only to be used through TI provided API. | RW | 0x0 | ||
5:0 | HPMRAMP1_TH | Internal. Only to be used through TI provided API. | RW | 0b00 0000 |
Address Offset | 0x0000 0014 | ||
Physical Address | 0x400C A014 | Instance | 0x400C A014 |
Description | Amplitude Compensation Threashold 2 This register contains various threshhold values for amplitude compensation algorithm. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:26 | LPMUPDATE_LTH | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
25:24 | SPARE24 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 | ||
23:18 | LPMUPDATE_HTH | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
17:16 | SPARE16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 | ||
15:10 | ADC_COMP_AMPTH_LPM | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
9:8 | SPARE8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 | ||
7:2 | ADC_COMP_AMPTH_HPM | Internal. Only to be used through TI provided API. | RW | 0b00 0000 | ||
1:0 | SPARE0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 |
Address Offset | 0x0000 0018 | ||
Physical Address | 0x400C A018 | Instance | 0x400C A018 |
Description | Analog Bypass Values 1 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:20 | RESERVED20 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0x000 | ||
19:16 | XOSC_HF_ROW_Q12 | Internal. Only to be used through TI provided API. | RW | 0x0 | ||
15:0 | XOSC_HF_COLUMN_Q12 | Internal. Only to be used through TI provided API. | RW | 0x0000 |
Address Offset | 0x0000 001C | ||
Physical Address | 0x400C A01C | Instance | 0x400C A01C |
Description | Internal. Only to be used through TI provided API. | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:14 | RESERVED14 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 0000 0000 0000 0000 | ||
13:0 | XOSC_HF_IBIASTHERM | Internal. Only to be used through TI provided API. | RW | 0b00 0000 0000 0000 |
Address Offset | 0x0000 0020 | ||
Physical Address | 0x400C A020 | Instance | 0x400C A020 |
Description | Analog Test Control | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:30 | SPARE30 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 | ||
29 | SCLK_LF_AUX_EN | Enable 32 kHz clock to AUX_COMPB. | RW | 0 | ||
28:0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b0 0000 0000 0000 0000 0000 0000 0000 |
Address Offset | 0x0000 0024 | ||
Physical Address | 0x400C A024 | Instance | 0x400C A024 |
Description | ADC Doubler Nanoamp Control | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:25 | RESERVED25 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b000 0000 | ||
24 | NANOAMP_BIAS_ENABLE | Internal. Only to be used through TI provided API. | RW | 0 | ||
23 | SPARE23 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior | RW | 0 | ||
22:6 | RESERVED6 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b0 0000 0000 0000 0000 | ||
5 | ADC_SH_MODE_EN | Internal. Only to be used through TI provided API. | RW | 0 | ||
4 | ADC_SH_VBUF_EN | Internal. Only to be used through TI provided API. | RW | 0 | ||
3:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 | ||
1:0 | ADC_IREF_CTRL | Internal. Only to be used through TI provided API. | RW | 0b00 |
Address Offset | 0x0000 0028 | ||
Physical Address | 0x400C A028 | Instance | 0x400C A028 |
Description | XOSCHF Control | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:10 | RESERVED10 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 0000 0000 0000 0000 0000 | ||
9:8 | PEAK_DET_ITRIM | Internal. Only to be used through TI provided API. | RW | 0b00 | ||
7 | RESERVED7 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
6 | BYPASS | Internal. Only to be used through TI provided API. | RW | 0 | ||
5 | RESERVED5 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | ||
4:2 | HP_BUF_ITRIM | Internal. Only to be used through TI provided API. | RW | 0b000 | ||
1:0 | LP_BUF_ITRIM | Internal. Only to be used through TI provided API. | RW | 0b00 |
Address Offset | 0x0000 002C | ||
Physical Address | 0x400C A02C | Instance | 0x400C A02C |
Description | Low Frequency Oscillator Control | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||||||||
31:24 | RESERVED24 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0x00 | |||||||||||||||||
23:22 | XOSCLF_REGULATOR_TRIM | Internal. Only to be used through TI provided API. | RW | 0b00 | |||||||||||||||||
21:18 | XOSCLF_CMIRRWR_RATIO | Internal. Only to be used through TI provided API. | RW | 0x0 | |||||||||||||||||
17:10 | RESERVED10 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0x00 | |||||||||||||||||
9:8 | RCOSCLF_RTUNE_TRIM | Internal. Only to be used through TI provided API.
|
RW | 0b00 | |||||||||||||||||
7:0 | RCOSCLF_CTUNE_TRIM | Internal. Only to be used through TI provided API. | RW | 0x00 |
Address Offset | 0x0000 0030 | ||
Physical Address | 0x400C A030 | Instance | 0x400C A030 |
Description | RCOSCHF Control | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0x0000 | ||
15:8 | RCOSCHF_CTRIM | Internal. Only to be used through TI provided API. | RW | 0x00 | ||
7:0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0x00 |
Address Offset | 0x0000 0034 | ||
Physical Address | 0x400C A034 | Instance | 0x400C A034 |
Description | Status 0 This register contains status signals from OSC_DIG |
||
Type | RO |
Bits | Field Name | Description | Type | Reset | |||||||||||||||||
31 | SPARE31 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 | |||||||||||||||||
30:29 | SCLK_LF_SRC | Indicates source for the sclk_lf
|
RO | 0b00 | |||||||||||||||||
28 | SCLK_HF_SRC | Indicates source for the sclk_hf
|
RO | 0 | |||||||||||||||||
27:23 | RESERVED23 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b0 0000 | |||||||||||||||||
22 | RCOSC_HF_EN | RCOSC_HF_EN | RO | 0 | |||||||||||||||||
21 | RCOSC_LF_EN | RCOSC_LF_EN | RO | 0 | |||||||||||||||||
20 | XOSC_LF_EN | XOSC_LF_EN | RO | 0 | |||||||||||||||||
19 | CLK_DCDC_RDY | CLK_DCDC_RDY | RO | 0 | |||||||||||||||||
18 | CLK_DCDC_RDY_ACK | CLK_DCDC_RDY_ACK | RO | 0 | |||||||||||||||||
17 | SCLK_HF_LOSS | Indicates sclk_hf is lost | RO | 0 | |||||||||||||||||
16 | SCLK_LF_LOSS | Indicates sclk_lf is lost | RO | 0 | |||||||||||||||||
15 | XOSC_HF_EN | Indicates that XOSC_HF is enabled. | RO | 0 | |||||||||||||||||
14 | RESERVED14 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 | |||||||||||||||||
13 | XB_48M_CLK_EN | Indicates that the 48MHz clock from the DOUBLER is enabled. It will be enabled if 24 or 48 MHz chrystal is used (enabled in doulbler bypass for the 48MHz chrystal). |
RO | 0 | |||||||||||||||||
12 | RESERVED12 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 | |||||||||||||||||
11 | XOSC_HF_LP_BUF_EN | XOSC_HF_LP_BUF_EN | RO | 0 | |||||||||||||||||
10 | XOSC_HF_HP_BUF_EN | XOSC_HF_HP_BUF_EN | RO | 0 | |||||||||||||||||
9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 | |||||||||||||||||
8 | ADC_THMET | ADC_THMET | RO | 0 | |||||||||||||||||
7 | ADC_DATA_READY | indicates when adc_data is ready. | RO | 0 | |||||||||||||||||
6:1 | ADC_DATA | adc_data | RO | 0b00 0000 | |||||||||||||||||
0 | PENDINGSCLKHFSWITCHING | Indicates when sclk_hf is ready to be swtiched | RO | 0 |
Address Offset | 0x0000 0038 | ||
Physical Address | 0x400C A038 | Instance | 0x400C A038 |
Description | Status 1 This register contains status signals from OSC_DIG |
||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||||||||||||||||||||||||||||||||||||||||||||||||||
31:28 | RAMPSTATE | AMPCOMP FSM State
|
RO | 0x0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
27:22 | HPM_UPDATE_AMP | OSC amplitude during HPM_UPDATE state. When amplitude compensation of XOSC_HF is enabled in high performance mode, this value is the amplitude of the crystal oscillations measured by the on-chip oscillator ADC, divided by 15 mV. For example, a value of 0x20 would indicate that the crystal's amplitude is approximately 480 mV. To enable amplitude compensation, AON_WUC OSCCFG must be set to a non-zero value. |
RO | 0b00 0000 | ||||||||||||||||||||||||||||||||||||||||||||||||||
21:16 | LPM_UPDATE_AMP | OSC amplitude during LPM_UPDATE state When amplitude compensation of XOSC_HF is enabled in low power mode, this value is the amplitude of the crystal oscillations measured by the on-chip oscillator ADC, divided by 15 mV. For example, a value of 0x20 would indicate that the crystal's amplitude is approximately 480 mV. To enable amplitude compensation, AON_WUC OSCCFG must be set to a non-zero value. |
RO | 0b00 0000 | ||||||||||||||||||||||||||||||||||||||||||||||||||
15 | FORCE_RCOSC_HF | force_rcosc_hf | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
14 | SCLK_HF_EN | SCLK_HF_EN | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
13 | SCLK_MF_EN | SCLK_MF_EN | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
12 | ACLK_ADC_EN | ACLK_ADC_EN | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
11 | ACLK_TDC_EN | ACLK_TDC_EN | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
10 | ACLK_REF_EN | ACLK_REF_EN | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
9 | CLK_CHP_EN | CLK_CHP_EN | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
8 | CLK_DCDC_EN | CLK_DCDC_EN | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
7 | SCLK_HF_GOOD | SCLK_HF_GOOD | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
6 | SCLK_MF_GOOD | SCLK_MF_GOOD | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
5 | SCLK_LF_GOOD | SCLK_LF_GOOD | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
4 | ACLK_ADC_GOOD | ACLK_ADC_GOOD | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
3 | ACLK_TDC_GOOD | ACLK_TDC_GOOD | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
2 | ACLK_REF_GOOD | ACLK_REF_GOOD | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
1 | CLK_CHP_GOOD | CLK_CHP_GOOD | RO | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||
0 | CLK_DCDC_GOOD | CLK_DCDC_GOOD | RO | 0 |
Address Offset | 0x0000 003C | ||
Physical Address | 0x400C A03C | Instance | 0x400C A03C |
Description | Status 2 This register contains status signals from AMPCOMP FSM |
||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:26 | ADC_DCBIAS | DC Bias read by RADC during SAR mode The vaue is an unsigned interger. It is used for debug only. |
RO | 0b00 0000 | ||
25 | HPM_RAMP1_THMET | Indication of threshhold is met for hpm_ramp1 | RO | 0 | ||
24 | HPM_RAMP2_THMET | Indication of threshhold is met for hpm_ramp2 | RO | 0 | ||
23 | HPM_RAMP3_THMET | Indication of threshhold is met for hpm_ramp3 | RO | 0 | ||
22:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
15:12 | RAMPSTATE | xosc_hf amplitude compensation FSM This is identical to STAT1.RAMPSTATE. See that description for encoding. |
RO | 0x0 | ||
11:4 | RESERVED4 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 | ||
3 | AMPCOMP_REQ | ampcomp_req | RO | 0 | ||
2 | XOSC_HF_AMPGOOD | amplitude of xosc_hf is within the required threshold (set by DDI). Not used for anything just for debug/status | RO | 0 | ||
1 | XOSC_HF_FREQGOOD | frequency of xosc_hf is good to use for the digital clocks | RO | 0 | ||
0 | XOSC_HF_RF_FREQGOOD | frequency of xosc_hf is within +/- 20 ppm and xosc_hf is good for radio operations. Used for SW to start synthesizer. | RO | 0 |
© 2015 - 2016. Texas Instruments | All Rights Reserved |