1 /*
2 * Copyright (c) 2015, Texas Instruments Incorporated
3 * All rights reserved.
4 *
5 * Redistribution and use in source and binary forms, with or without
6 * modification, are permitted provided that the following conditions
7 * are met:
8 *
9 * * Redistributions of source code must retain the above copyright
10 * notice, this list of conditions and the following disclaimer.
11 *
12 * * Redistributions in binary form must reproduce the above copyright
13 * notice, this list of conditions and the following disclaimer in the
14 * documentation and/or other materials provided with the distribution.
15 *
16 * * Neither the name of Texas Instruments Incorporated nor the names of
17 * its contributors may be used to endorse or promote products derived
18 * from this software without specific prior written permission.
19 *
20 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31 */
32
33 /*
34 * ======== Hwi.xdc ========
35 *
36 */
37 package ti.sysbios.family.arm.m3;
38
39 import xdc.rov.ViewInfo;
40 import xdc.runtime.Diags;
41 import xdc.runtime.Log;
42 import xdc.runtime.Assert;
43 import xdc.runtime.Error;
44
45 import ti.sysbios.BIOS;
46 import ti.sysbios.interfaces.IHwi;
47
48 /*!
49 * ======== Hwi ========
50 * Cortex M3 Hardware Interrupt Manager
51 *
52 * The Cortex M3's Nested Vectored Interrupt Controller (NVIC)
53 * supports up to 256 interrupts/exceptions. In practice, most
54 * devices support much fewer (ie the Stellaris family of devices
55 * have only 80 total interrupts defined).
56 *
57 * SYS/BIOS Interrupt IDs or interrupt numbers correspond
58 * to an interrupt's position in the interrupt vector table.
59 *
60 * ID 0 corresponds to vector 0 which is used by the NVIC
61 * to hold the initial (reset) stack pointer value.
62 *
63 * ID 1 corresponds to vector 1 which is the reset vector (ie _c_int00)
64 *
65 * IDs 2-14 are hardwired to exceptions.
66 *
67 * ID 15 is the SysTick timer interrupt.
68 *
69 * ID's 16-255 are mapped to the NVIC's user interrupts 0-239
70 * which are tied to platform specific interrupt sources.
71 *
72 * @a(Zero Latency Interrupts) 73 * The M3 Hwi module supports "zero latency" interrupts.
74 * Interrupts configured with priority greater (in actual
75 * hardware priority, but lower in number) than
76 * {@link #disablePriority Hwi.disablePriority} are NOT
77 * disabled by Hwi_disable().
78 *
79 * Zero latency interrupts are distinguished from regular dispatched
80 * interrupts at create time by their priority being greater
81 * than Hwi.disablePriority.
82 *
83 * Note that since zero latency interrupts don't use the dispatcher,
84 * the {@link ti.sysbios.interfaces.IHwi#arg arg} parameter is not
85 * functional. Also note that due to the M3's native automatic
86 * stacking of saved-by-caller C context on the way to an ISR, zero
87 * latency interrupt handlers are implemented using regular C functions
88 * (ie no 'interrupt' keyword is required).
89 *
90 * @a(WARNING) 91 * Zero latency interrupts are NOT HANDLED by the SYS/BIOS
92 * interrupt dispatcher! Instead, they are vectored to directly.
93 * As such, and because they are NOT DISABLED BY Hwi_disable(),
94 * these interrupt handlers are SEVERELY RESTRICTED in terms of the
95 * SYS/BIOS APIs they can invoke and THREAD SAFETY MUST BE CAREFULLY
96 * CONSIDERED! See the descriptions of {@link #disable Hwi_disable()} and
97 * and {@link #disablePriority Hwi.disablePriority} for more details.
98 *
99 * @a(Interrupt Masking Options) 100 *
101 * The NVIC interrupt controller is designed for priority based
102 * interrupts.
103 *
104 * In this Hwi module, the {@link #maskSetting} instance configuration
105 * parameter is ignored.
106 * Effectively, only the {@link #MaskingOption_LOWER} is supported.
107 *
108 * @a(Interrupt Priorities) 109 *
110 * In general, the NVIC supports priority values of 0 thru 255.
111 *
112 * In practice, the number of priorities and their values are device
113 * dependent, and their nesting behaviors depend on the
114 * {@link #priGroup Hwi.priGroup} setting.
115 *
116 * For most TI MCU devices, 8 priorities are supported. A peculiarity
117 * of ARM's NVIC is that, although the priority field is an 8 bit value,
118 * the range of supported priority values are left-justified within this
119 * 8 bit field. Consequently, the 8 priority values are not 0 thru 7 as
120 * one might expect, but rather:
121 *
122 * @p(code) 123 * 0x00 // highest priority, non dispatched, Zero Latency priority
124 * 0x20 // highest dispatched interrupt priority
125 * 0x40
126 * 0x60
127 * 0x80
128 * 0xa0
129 * 0xc0
130 * 0xe0 // lowest dispatched interrupt priority, (default)
131 * @p 132 *
133 * Priority 0 is the highest priority and by default is
134 * reserved for zero latency interrupts
135 * (see {@link #disablePriority Hwi.disablePriority}).
136 *
137 * See the Cortex M3 architecture reference manual for details
138 * on the behavior of interrupt priorities and their relationship
139 * to the {@link #priGroup Hwi.priGroup} setting.
140 *
141 * @a(Interrupt Vector Tables) 142 * Tiva devices:
143 *
144 * By default, two vector tables are created for Tiva devices:
145 *
146 * A 16 entry boot vector table is placed at address 0x00000000 in
147 * FLASH.
148 *
149 * An 80 entry vector table is placed at address 0x20000000 in RAM.
150 *
151 * The FLASH boot vector table contains the reset vector and exception
152 * handler vectors used until the RAM based vector table is initialized.
153 *
154 * The RAM vector table contains the 16 exception vectors as well as all
155 * the 64 user interrupt vectors.
156 *
157 * During system startup, the NVIC Vector Table Offset Registor is
158 * intialized to point to this vector table after the table has been
159 * initialized.
160 *
161 * @a( ) 162 * Dual M3 Core ('Ducati') devices:
163 *
164 * By default, Ducati core 0 places its runtime vector table at address
165 * 0x00000400 and core 1 places its runtime vector table at address
166 * 0x00000800.
167 *
168 * Additionally, a boot vector table is placed at address
169 * 0x00000000 which is shared by both cores.
170 *
171 * The boot reset vector function determines which core it is being
172 * executed on and jumps to the reset vector contained in its corresponding
173 * runtime vector table.
174 *
175 * The generation and placement of these vector tables is made
176 * automatically when the
177 * {@link ti.sysbios.family.arm.ducati.Core} module is used.
178 *
179 * Although STRONGLY discouraged, this default behavior can be overridden
180 * by explicitly setting the
181 * {@link #resetVectorAddress Hwi.resetVectorAddress} and
182 * {@link #vectorTableAddress Hwi.vectorTableAddress} config parameters.
183 *
184 * @a(Restrictions) 185 * When used within a dual M3 core (Ducati) arrangement, care must be
186 * taken when initializing this shared resource.
187 * The "Shared Resources" note provided
188 * in the {@link ti.sysbios.family.arm.ducati ducati} package discusses
189 * the management of the various hardware and software resources
190 * shared by the two M3 cores.
191 * @a 192 *
193 * @p(html) 194 * <h3> Calling Context </h3>
195 * <table border="1" cellpadding="3">
196 * <colgroup span="1"></colgroup> <colgroup span="5" align="center"></colgroup>
197 *
198 * <tr><th> Function </th><th> Hwi </th><th> Swi </th><th> Task </th><th> Main </th><th> Startup </th></tr>
199 * <!-- -->
200 * <tr><td> {@link #clearInterrupt} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td></tr>
201 * <tr><td> {@link #create} </td><td> N </td><td> N </td><td> Y </td><td> Y </td><td> N </td></tr>
202 * <tr><td> {@link #disable} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td></tr>
203 * <tr><td> {@link #disableInterrupt} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
204 * <tr><td> {@link #enable} </td><td> Y </td><td> Y </td><td> Y </td><td> N </td><td> N </td></tr>
205 * <tr><td> {@link #enableInterrupt} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
206 * <tr><td> {@link #Params_init} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td></tr>
207 * <tr><td> {@link #restore} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td></tr>
208 * <tr><td> {@link #restoreInterrupt} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td></tr>
209 * <tr><td> {@link #construct} </td><td> N </td><td> N </td><td> Y </td><td> Y </td><td> N </td></tr>
210 * <tr><td> {@link #delete} </td><td> N </td><td> N </td><td> Y </td><td> Y </td><td> N </td></tr>
211 * <tr><td> {@link #destruct} </td><td> N </td><td> N </td><td> Y </td><td> Y </td><td> N </td></tr>
212 * <tr><td> {@link #getHookContext} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
213 * <tr><td> {@link #setFunc} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
214 * <tr><td> {@link #setHookContext} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
215 * <tr><td colspan="6"> Definitions: <br />
216 * <ul>
217 * <li> <b>Hwi</b>: API is callable from a Hwi thread. </li>
218 * <li> <b>Swi</b>: API is callable from a Swi thread. </li>
219 * <li> <b>Task</b>: API is callable from a Task thread. </li>
220 * <li> <b>Main</b>: API is callable during any of these phases: </li>
221 * <ul>
222 * <li> In your module startup after this module is started (e.g. Hwi_Module_startupDone() returns TRUE). </li>
223 * <li> During xdc.runtime.Startup.lastFxns. </li>
224 * <li> During main().</li>
225 * <li> During BIOS.startupFxns.</li>
226 * </ul>
227 * <li> <b>Startup</b>: API is callable during any of these phases:</li>
228 * <ul>
229 * <li> During xdc.runtime.Startup.firstFxns.</li>
230 * <li> In your module startup before this module is started (e.g. Hwi_Module_startupDone() returns FALSE).</li>
231 * </ul>
232 * </ul>
233 * </td></tr>
234 *
235 * </table>
236 * @p 237 */
238
239
240 @Template("./Hwi.xdt") /* generates the vector table and the dispatcher */
241 @ModuleStartup /* generate a call to startup function */
242 @InstanceInitStatic /* allow constructs in static only systems */
243
244 module Hwi inherits ti.sysbios.interfaces.IHwi
245 {
246 // -------- Module Constants --------
247
248 /*!
249 * The Cortex M3 NVIC supports up to 256 interrupts/exceptions.
250 *
251 * The actual number supported is device specific and provided by
252 * the catalog device specification.
253 */
254 config Int NUM_INTERRUPTS;
255
256 /*!
257 * The Cortex M3 NVIC supports up to 256 interrupt priorities.
258 *
259 * The actual number supported is device specific and provided by
260 * the catalog device specification.
261 */
262 config Int NUM_PRIORITIES;
263
264 // -------- Module Types --------
265
266 /*! Hwi vector function type definition. */
267 typedef Void (*VectorFuncPtr)(void);
268
269 /*! Exception hook function type definition. */
270 typedef Void (*ExceptionHookFuncPtr)(ExcContext *);
271
272 /*! NVIC Configuration Control Register (CCR). */
273 struct CCR {
274 Bits8 STKALIGN; /*! Auto stack alignment in exception */
275 Bits8 BFHFNMIGN; /*! All faults ignore BUS Faults */
276 Bits8 DIV_0_TRP; /*! Trap on divide by zero */
277 Bits8 UNALIGN_TRP; /*! Trap on all unaligned accesses */
278 Bits8 USERSETMPEND; /*! Allow user to trigger interrupts */
279 Bits8 NONEBASETHRDENA; /*! Allow entering thread mode anytime */
280 };
281
282 /*! @_nodoc 283 * Nested Vectored Interrupt Controller.
284 */
285 struct NVIC {
286 UInt32 RES_00; /*! 0xE000E000 reserved */
287 UInt32 ICTR; /*! 0xE000E004 Interrupt Control Type */
288 UInt32 RES_08; /*! 0xE000E008 reserved */
289 UInt32 RES_0C; /*! 0xE000E00C reserved */
290 UInt32 STCSR; /*! 0xE000E010 SysTick Control & Status Register */
291 UInt32 STRVR; /*! 0xE000E014 SysTick Reload Value Register */
292 UInt32 STCVR; /*! 0xE000E018 SysTick Current Value Register */
293 UInt32 STCALIB; /*! 0xE000E01C SysTick Calibration Value Register */
294 UInt32 RES_20 [56]; /*! 0xE000E020-0xE000E0FC reserved */
295 UInt32 ISER [8]; /*! 0xE000E100-0xE000E11C Interrupt Set Enable Registers */
296 UInt32 RES_120 [24]; /*! 0xE000E120-0xE000E17C reserved */
297 UInt32 ICER [8]; /*! 0xE000E180-0xE000E19C Interrupt Clear Enable Registers */
298 UInt32 RES_1A0 [24]; /*! 0xE000E1A0-0xE000E1FC reserved */
299 UInt32 ISPR [8]; /*! 0xE000E200-0xE000E21C Interrupt Set Pending Registers */
300 UInt32 RES_220 [24]; /*! 0xE000E220-0xE000E7C reserved */
301 UInt32 ICPR [8]; /*! 0xE000E280-0xE000E29C Interrupt Clear Pending Registers */
302 UInt32 RES_2A0 [24]; /*! 0xE000E2A0-0xE000E2FC reserved */
303 UInt32 IABR [8]; /*! 0xE000E300-0xE000E31C Interrupt Active Bit Registers */
304 UInt32 RES_320 [56]; /*! 0xE000E320-0xE000E3FC reserved */
305 UInt8 IPR [240]; /*! 0xE000E400-0xE000E4EF Interrupt Priority Registers */
306 UInt32 RES_4F0 [516];/*! 0xE000E4F0-0xE000ECFC reserved */
307 UInt32 CPUIDBR; /*! 0xE000ED00 CPUID Base Register */
308 UInt32 ICSR; /*! 0xE000ED04 Interrupt Control State Register */
309 UInt32 VTOR; /*! 0xE000ED08 Vector Table Offset Register */
310 UInt32 AIRCR; /*! 0xE000ED0C Application Interrupt/Reset Control Register */
311 UInt32 SCR; /*! 0xE000ED10 System Control Register */
312 UInt32 CCR; /*! 0xE000ED14 Configuration Control Register */
313 UInt8 SHPR[12]; /*! 0xE000ED18 System Handlers 4-15 Priority Registers */
314 UInt32 SHCSR; /*! 0xE000ED24 System Handler Control & State Register */
315 UInt8 MMFSR; /*! 0xE000ED28 Memory Manage Fault Status Register */
316 UInt8 BFSR; /*! 0xE000ED29 Bus Fault Status Register */
317 UInt16 UFSR; /*! 0xE000ED2A Usage Fault Status Register */
318 UInt32 HFSR; /*! 0xE000ED2C Hard Fault Status Register */
319 UInt32 DFSR; /*! 0xE000ED30 Debug Fault Status Register */
320 UInt32 MMAR; /*! 0xE000ED34 Memory Manager Address Register */
321 UInt32 BFAR; /*! 0xE000ED38 Bus Fault Address Register */
322 UInt32 AFSR; /*! 0xE000ED3C Auxiliary Fault Status Register */
323 UInt32 PFR0; /*! 0xE000ED40 Processor Feature Register */
324 UInt32 PFR1; /*! 0xE000ED44 Processor Feature Register */
325 UInt32 DFR0; /*! 0xE000ED48 Debug Feature Register */
326 UInt32 AFR0; /*! 0xE000ED4C Auxiliary Feature Register */
327 UInt32 MMFR0; /*! 0xE000ED50 Memory Model Fault Register0 */
328 UInt32 MMFR1; /*! 0xE000ED54 Memory Model Fault Register1 */
329 UInt32 MMFR2; /*! 0xE000ED58 Memory Model Fault Register2 */
330 UInt32 MMFR3; /*! 0xE000ED5C Memory Model Fault Register3 */
331 UInt32 ISAR0; /*! 0xE000ED60 ISA Feature Register0 */
332 UInt32 ISAR1; /*! 0xE000ED64 ISA Feature Register1 */
333 UInt32 ISAR2; /*! 0xE000ED68 ISA Feature Register2 */
334 UInt32 ISAR3; /*! 0xE000ED6C ISA Feature Register3 */
335 UInt32 ISAR4; /*! 0xE000ED70 ISA Feature Register4 */
336 UInt32 RES_D74[5]; /*! 0xE000ED74-0xE000ED84 reserved */
337 UInt32 CPACR; /*! 0xE000ED88 Coprocessor Access Control Register */
338 UInt32 RES_D8C[93]; /*! 0xE000ED8C-0xE000EEFC reserved */
339 UInt32 STI; /*! 0xE000EF00 Software Trigger Interrupt Register */
340 UInt32 RES_F04[12]; /*! 0xE000EF04-0xE000EF30 reserved */
341 UInt32 FPCCR; /*! 0xE000EF34 FP Context Control Register */
342 UInt32 FPCAR; /*! 0xE000EF38 FP Context Address Register */
343 UInt32 FPDSCR; /*! 0xE000EF3C FP Default Status Control Register */
344 UInt32 MVFR0; /*! 0xE000EF40 Media & FP Feature Register0 */
345 UInt32 MVFR1; /*! 0xE000EF44 Media & FP Feature Register1 */
346 UInt32 RES_F48[34]; /*! 0xE000EF48-0xE000EFCC reserved */
347 UInt32 PID4; /*! 0xE000EFD0 Peripheral ID Register4 */
348 UInt32 PID5; /*! 0xE000EFD4 Peripheral ID Register5 */
349 UInt32 PID6; /*! 0xE000EFD8 Peripheral ID Register6 */
350 UInt32 PID7; /*! 0xE000EFDC Peripheral ID Register7 */
351 UInt32 PID0; /*! 0xE000EFE0 Peripheral ID Register0 */
352 UInt32 PID1; /*! 0xE000EFE4 Peripheral ID Register1 */
353 UInt32 PID2; /*! 0xE000EFE8 Peripheral ID Register2 */
354 UInt32 PID3; /*! 0xE000EFEC Peripheral ID Register3 */
355 UInt32 CID0; /*! 0xE000EFF0 Component ID Register0 */
356 UInt32 CID1; /*! 0xE000EFF4 Component ID Register1 */
357 UInt32 CID2; /*! 0xE000EFF8 Component ID Register2 */
358 UInt32 CID3; /*! 0xE000EFFC Component ID Register3 */
359 }
360
361 /*!
362 * Physical Nested Vectored Interrupt Controller Device.
363 * Short name is "Hwi_nvic"
364 * Long name is "ti_sysbios_family_arm_m3_Hwi_nvic"
365 */
366 extern volatile NVIC nvic;
367
368 /*!
369 * Virtual Nested Vectored Interrupt Controller structure
370 * written to by both cores for SMP.
371 * Short name is "Hwi_vnvic"
372 * Long name is "ti_sysbios_family_arm_m3_Hwi_vnvic"
373 */
374 extern volatile NVIC vnvic;
375
376 /*!
377 * Exception Context - Register contents at the time of an exception.
378 */
379 struct ExcContext {
380 /* Thread Context */
381 BIOS.ThreadType threadType; /* Type of thread executing at */
382 /* the time the exception occurred */
383 Ptr threadHandle; /* Handle to thread executing at */
384 /* the time the exception occurred */
385 Ptr threadStack; /* Address of stack contents of thread */
386 /* executing at the time the exception */
387 /* occurred */
388 SizeT threadStackSize; /* size of thread stack */
389
390 /* Internal Registers */
391 Ptr r0;
392 Ptr r1;
393 Ptr r2;
394 Ptr r3;
395 Ptr r4;
396 Ptr r5;
397 Ptr r6;
398 Ptr r7;
399 Ptr r8;
400 Ptr r9;
401 Ptr r10;
402 Ptr r11;
403 Ptr r12;
404 Ptr sp;
405 Ptr lr;
406 Ptr pc;
407 Ptr psr;
408
409 /* NVIC registers */
410 Ptr ICSR;
411 Ptr MMFSR;
412 Ptr BFSR;
413 Ptr UFSR;
414 Ptr HFSR;
415 Ptr DFSR;
416 Ptr MMAR;
417 Ptr BFAR;
418 Ptr AFSR;
419 }
420
421 /*! @_nodoc */
422 metaonlystruct BasicView {
423 Ptr halHwiHandle;
424 String label;
425 String type;
426 Int intNum;
427 Int priority;
428 Int group;
429 Int subPriority;
430 String fxn;
431 UArg arg;
432 };
433
434 /*! @_nodoc */
435 metaonlystruct DetailedView {
436 Ptr halHwiHandle;
437 String label;
438 String type;
439 Int intNum;
440 Int priority;
441 Int group;
442 Int subPriority;
443 String fxn;
444 UArg arg;
445 Ptr irp;
446 String status;
447 Int coreId;
448 };
449
450 /*! @_nodoc */
451 metaonlystruct ModuleView {
452 String options[4];
453 String activeInterrupt;
454 String pendingInterrupt;
455 String exception;
456 String hwiStackPeak;
457 SizeT hwiStackSize;
458 Ptr hwiStackBase;
459 };
460
461 /*! @_nodoc */
462 @Facet
463 metaonlyconfig ViewInfo.Instance rovViewInfo =
464 ViewInfo.create({
465 viewMap: [
466 ['Basic',
467 {
468 type: ViewInfo.INSTANCE,
469 viewInitFxn: 'viewInitBasic',
470 structName: 'BasicView'
471 }
472 ],
473 ['Detailed',
474 {
475 type: ViewInfo.INSTANCE,
476 viewInitFxn: 'viewInitDetailed',
477 structName: 'DetailedView'
478 }
479 ],
480 ['Module',
481 {
482 type: ViewInfo.MODULE,
483 viewInitFxn: 'viewInitModule',
484 structName: 'ModuleView'
485 }
486 ],
487 ['Exception',
488 {
489 type: ViewInfo.TREE,
490 viewInitFxn: 'viewInitException',
491 structName: 'ExcContext'
492 }
493 ]
494 ]
495 });
496
497 // -------- Module Parameters --------
498
499 // Logs
500
501 /*!
502 * Issued just prior to Hwi function invocation (with interrupts disabled)
503 */
504 config Log.Event LM_begin = {
505 mask: Diags.USER1 | Diags.USER2,
506 msg: "LM_begin: hwi: 0x%x, func: 0x%x, preThread: %d, intNum: %d, irp: 0x%x"
507 };
508
509 /*!
510 * Issued just after return from Hwi function (with interrupts disabled)
511 */
512 config Log.Event LD_end = {
513 mask: Diags.USER2,
514 msg: "LD_end: hwi: 0x%x"
515 };
516
517 // Asserts
518
519 /*! Assert when bad maskSetting parameter provided */
520 config Assert.Id A_unsupportedMaskingOption = {
521 msg: "A_unsupportedMaskingOption: unsupported maskSetting."
522 };
523
524 // Errors
525
526 /*!
527 * Error raised when Hwi is already defined
528 */
529 config Error.Id E_alreadyDefined = {
530 msg: "E_alreadyDefined: Hwi already defined: intr# %d"
531 };
532
533 /*!
534 * Error raised when the number of interrupts being created
535 * exceeds the number supported.
536 */
537 config Error.Id E_hwiLimitExceeded = {
538 msg: "E_hwiLimitExceeded: Too many interrupts defined"
539 };
540
541 /*!
542 * Error raised when an exception occurs
543 */
544 config Error.Id E_exception = {
545 msg: "E_exception: id = %d, pc = %08x.\nTo see more exception detail, set ti.sysbios.family.arm.m3.Hwi.enableException = true or,\nexamine the Exception view for the ti.sysbios.family.arm.m3.Hwi module using ROV."
546 };
547
548 /*!
549 * Error raised when an uninitialized interrupt occurs
550 */
551 config Error.Id E_noIsr = {
552 msg: "E_noIsr: id = %d, pc = %08x"
553 };
554
555 /*!
556 * Error raised when NMI exception occurs
557 */
558 config Error.Id E_NMI = {
559 msg: "E_NMI: %s"
560 };
561
562 /*!
563 * Error raised when hard fault exception occurs
564 */
565 config Error.Id E_hardFault = {
566 msg: "E_hardFault: %s"
567 };
568
569 /*!
570 * Error raised when memory fault exception occurs
571 */
572 config Error.Id E_memFault = {
573 msg: "E_memFault: %s, address: %08x"
574 };
575
576 /*!
577 * Error raised when bus fault exception occurs
578 */
579 config Error.Id E_busFault = {
580 msg: "E_busFault: %s, address: %08x"
581 };
582
583 /*!
584 * Error raised when usage fault exception occurs
585 */
586 config Error.Id E_usageFault = {
587 msg: "E_usageFault: %s"
588 };
589
590 /*!
591 * Error raised when svCall exception occurs
592 */
593 config Error.Id E_svCall = {
594 msg: "E_svCall: svNum = %d"
595 };
596
597 /*!
598 * Error raised when debugMon exception occurs
599 */
600 config Error.Id E_debugMon = {
601 msg: "E_debugMon: %s"
602 };
603
604 /*!
605 * Error raised when reserved exception occurs
606 */
607 config Error.Id E_reserved = {
608 msg: "E_reserved: %s %d"
609 };
610
611 // configs
612
613 /*!
614 * Size (in number of interrupts) of the table used by the interrupt
615 * dispatcher to locate the corresponding Hwi object. By default,
616 * Hwi.dispatchTableSize will be internally set
617 * to the number of interrupts supported by the device.
618 *
619 * When the Hwi dispatch table size is equal to the number of interrupts
620 * supported {@link #NUM_INTERRUPTS} by the device, a linear-indexed
621 * dispatch table mechanism is used that will consume 4 bytes of RAM
622 * for each interrupt supported.
623 *
624 * If the dispatch table size is set to a number less than the number
625 * of interrupts supported by the device, then a non linear-indexed
626 * dispatch table mechanism is employed that uses 12 bytes of RAM for
627 * each interrupt supported.
628 *
629 * Consequently, for applications that use less than 1/3 of the total
630 * number of interrupts supported by the device, setting this parameter
631 * to the number of interrupts ACTUALLY USED will result in less RAM
632 * memory being used than otherwise.
633 *
634 * For applications that use very few interrupts, this can be a significant RAM memory savings.</p>
635 */
636 metaonlyconfig UInt dispatchTableSize;
637
638 /*!
639 * Location of the Runtime Interrupt Vector Table.
640 * Default is device dependent.
641 *
642 * This parameter allows the user to override the default placement
643 * of the runtime interrupt vector table.
644 * The NVIC's Vector Table Offset
645 * Register (VTOR) is also programmed to this value.
646 *
647 * Some systems require the runtime vector table to be placed at
648 * an address
649 * other than 0 but still need a copy of the two M3 boot vectors
650 * (SP and reset PC), located there. To achieve this, a separate
651 * parameter {@link #resetVectorAdress} is provided. If the
652 * resetVectorAddress has a different value then the vectorTableAddress
653 * then a separate vector table is generated and placed at that
654 * address.
655 *
656 * The vector table must be placed at an address at or lower than
657 * 0x3FFFFC00 and must be aligned on an even 64 word boundary.
658 */
659 metaonlyconfig Ptr vectorTableAddress = 0x00000000;
660
661 /*!
662 * Reset vector table address. Default is 0x00000000.
663 *
664 * This parameter is the address of the vector table used
665 * at system reset time. Typically this is placed at 0x00000000.
666 *
667 * If the Hwi.resetVectorAddress has a different value than
668 * the {@link #vectorTableAddress Hwi.vectorTableAddress}
669 * then two vector tables are generated, one at the Hwi.resetVectorAddress
670 * and another at the {@link #vectorTableAddress Hwi.vectorTableAddress}.
671 *
672 * After the initial boot code has been executed at startup, the NVIC's
673 * Vector Table Offset Register will be programmed to point to the
674 * vector table at the {@link #vectorTableAddress Hwi.vectorTableAddress}.
675 *
676 * is created and placed in the ".resetVecs" section.
677 */
678 metaonlyconfig Ptr resetVectorAddress = 0x00000000;
679
680 /*! Reset Handler. Default is c_int00 */
681 metaonlyconfig VectorFuncPtr resetFunc;
682
683 /*! NMI Handler. Default is set to an internal exception handler */
684 metaonlyconfig VectorFuncPtr nmiFunc;
685
686 /*! Hard Fault Handler. Default is set to an internal exception handler */
687 metaonlyconfig VectorFuncPtr hardFaultFunc;
688
689 /*! Hard Mem Handler. Default is set to an internal exception handler */
690 metaonlyconfig VectorFuncPtr memFaultFunc;
691
692 /*! Bus Fault Handler. Default is set to an internal exception handler */
693 metaonlyconfig VectorFuncPtr busFaultFunc;
694
695 /*! Usage Fault Handler. Default is set to an internal exception handler */
696 metaonlyconfig VectorFuncPtr usageFaultFunc;
697
698 /*! SVCall Handler. Default is set to an internal exception handler */
699 metaonlyconfig VectorFuncPtr svCallFunc;
700
701 /*! Debug Mon Handler. Default is set to an internal exception handler */
702 metaonlyconfig VectorFuncPtr debugMonFunc;
703
704 /*! Reserved Exception Handler. Default is set to an internal exception handler */
705 metaonlyconfig VectorFuncPtr reservedFunc;
706
707 /*! Uninitialized ISR Handler. Default is set to an internal exception handler */
708 config VectorFuncPtr nullIsrFunc;
709
710 /*! Hwi exception handler function type definition. */
711 typedef Void (*ExcHandlerFuncPtr)(UInt *, UInt);
712
713 /*!
714 * Exception handler function pointer.
715 *
716 * The default is determined by the value of Hwi.enableException.
717 *
718 * If the user does NOT set this parameter, then the following default
719 * behavior is followed:
720 *
721 * If Hwi.enableException is true, then the internal 'Hwi_excHandlerMax'
722 * function is used. This exception handler saves the exception context
723 * then does a complete exception decode and dump to the console, then
724 * raises an Error. The exception context can be viewed within CCS
725 * in the ROV Hwi module's Exception view.
726 *
727 * If Hwi.enableException is false, then the internal 'Hwi_excHandlerMin'
728 * function is used. This exception handler saves the exception context
729 * then raises an Error. The exception context can be viewed within CCS
730 * in the ROV Hwi module's Exception view.
731 *
732 * If the user sets this parameter to their own function, then the user's
733 * function will be invoked with the following arguments:
734 *
735 * Void myExceptionHandler(UInt *excStack, UInt lr);
736 *
737 * Where 'excStack' is the address of the stack containing the
738 * register context at the time of the exception, and 'lr' is the
739 * link register value when the low-level-assembly-coded exception
740 * handler was vectored to.
741 *
742 * If this parameter is set to 'null', then an infinite while loop is
743 * entered when an exception occurs. This setting minimizes code and
744 * data footprint but provides no automatic exception decoding.
745 */
746 config ExcHandlerFuncPtr excHandlerFunc = excHandlerMax;
747
748 /*
749 * SMP Interrupt affinity mappings
750 *
751 * In SMP mode, this array maps an interrupt number to the
752 * coreId it is to be tied to. By default, all ints are mapped to
753 * core 0.
754 *
755 * For example, to make Timer 1 from the
756 * ti.sysbios.family.arm.ducati.Timer
757 * module interrupt on core 1 rather than core 0, add the following to
758 * your config file:
759 *
760 * @p(code)
761 * var m3Hwi = xdc.useModule('ti.sysbios.family.arm.m3.Hwi');
762 * m3Hwi.intAffinity[22] = 1;
763 * @p
764 *
765 * @a(constraints)
766 * Valid core Ids are 0 and 1 for Ducati/Benelli SMP applications.
767 *
768 * Interrupt numbers below 16 are ignored.
769 * Only interrupt numbers greater than or equal to #16 can be routed to
770 * either Ducati/Benelli core.
771 *
772 * Interrupt #19, the Ducati inter-core interrupt, is reserved for
773 * exclusive use within the SMP kernel.
774 */
775 metaonlyconfig UInt8 intAffinity[];
776
777 /*!
778 * Enable full exception decoding
779 *
780 * When this is enabled, the exception handler will fully
781 * decode an exception and dump the registers to the
782 * system console.
783 */
784 metaonlyconfig Bool enableException = true;
785
786 /*!
787 * User Exception Context Buffer Address
788 *
789 * By default, when an exception occurs, an {@link #ExcContext}
790 * structure is allocated on the ISR stack and filled in within the
791 * exception handler.
792 *
793 * If {@link #excContextBuffer} is initialized by the user, the
794 * {@link #ExcContext} structure will be placed at that address instead.
795 *
796 * The buffer must be large enough to contain an {@link #ExcContext}
797 * structure.
798 */
799 metaonlyconfig Ptr excContextBuffer;
800 metaonlyconfig Ptr excContextBuffers[];
801
802 /*!
803 * User Exception Stack Buffer Address
804 *
805 * By default, when an exception occurs, a pointer to the base address
806 * of the stack being used by the thread causing the exception is placed
807 *
808 * If {@link #excStackBuffer} is initialized by the user, the
809 * stack contents of the thread causing the exception will be
810 * copied to that address instead.
811 *
812 * The buffer must be large enough to contain the largest task stack
813 * or ISR stack defined in the application.
814 */
815 metaonlyconfig Ptr excStackBuffer;
816 metaonlyconfig Ptr excStackBuffers[];
817
818
819 /*!
820 * User Exception hook function.
821 *
822 * Called just after the exception context has been initialized.
823 *
824 * This function will be run on the ISR stack.
825 *
826 * This function must run to completion.
827 *
828 * It is called without any Task or Swi scheduling protection
829 * and therefore can not call any functions that may cause a Swi or Task
830 * scheduling operation (Swi_post(), Semaphore_post(), Event_post(), etc).
831 */
832 config ExceptionHookFuncPtr excHookFunc = null;
833 config ExceptionHookFuncPtr excHookFuncs[];
834
835 /*!
836 * NVIC CCR register settings
837 *
838 * These setting are written to Hwi_nvic.CCR at startup time.
839 *
840 * See the Cortex M3 architecture reference manual for details
841 * on the meanings of these parameters.
842 */
843 metaonlyconfig CCR nvicCCR = {
844 STKALIGN: 1,
845 BFHFNMIGN: 0,
846 DIV_0_TRP: 0,
847 UNALIGN_TRP: 0,
848 USERSETMPEND: 0,
849 NONEBASETHRDENA: 0
850 };
851
852 /*!
853 * The priority that BASEPRI is set to by Hwi_disable().
854 *
855 * All interrupts configured with equal or less priority (equal or
856 * higher number) than disablePriority are disabled by
857 * {@link #disable Hwi_disable}.
858 * Interrupts configured with higher priority (smaller number) than
859 * Hwi.disablePriority are non-maskable (ie zero-latency).
860 *
861 * The default setting is the second highest interrupt priority
862 * defined for the device (typically '0x20' for devices
863 * which support 8 priority values).
864 * This results in priority 0 (and all
865 * other values in the same priority group, ie 0x00 thru 0x1f)
866 * being the zero-latency, non-maskable interrupt priority.
867 * All other priorities are disabled with Hwi_disable().
868 */
869 config UInt disablePriority;
870
871 /*!
872 * The PRIGROUP setting. Default is 0.
873 *
874 * This value will be written to the PRIGROUP field
875 * within the NVIC's Application Interrupt and Reset Control
876 * Register (Hwi_nvic.AIRCR). It defines how the 8 bit priority
877 * values are interpreted by the hardware.
878 *
879 * Valid settings are 0-7.
880 *
881 * The default setting of 0 causes bits 7-1 of an interrupt's
882 * priority value to be used as pre-emption priority, while bit 0
883 * is used to determine which of two simultaneous interrupts with
884 * the same pre-emption priority will be serviced first.
885 *
886 * For most TI MCU devices, this means that each of the 8 supported
887 * priority values are unique pre-emption priorities and are not
888 * subdivided into priority groups.
889 */
890 config UInt priGroup = 0;
891
892 // -------- Module Functions --------
893
894 /*!
895 * ======== disable ========
896 * Disable all non zero-latency interrupts
897 *
898 * Hwi_disable disables all non zero-latency hardware interrupts and
899 * returns an
900 * opaque key indicating whether interrupts were globally enabled or
901 * disabled on entry to Hwi_disable().
902 * The actual value of the key is target/device specific and is meant
903 * to be passed to Hwi_restore().
904 *
905 * Call Hwi_disable before a portion of a function that needs
906 * to run without interruption. When critical processing is complete, call
907 * Hwi_restore or Hwi_enable to reenable hardware interrupts.
908 *
909 * Servicing of interrupts that occur while interrupts are disabled is
910 * postponed until interrupts are reenabled. However, if the same type
911 * of interrupt occurs several times while interrupts are disabled,
912 * the interrupt's function is executed only once when interrupts are
913 * reenabled.
914 *
915 * A context switch can occur when calling Hwi_enable or Hwi_restore if
916 * an enabled interrupt occurred while interrupts are disabled.
917 *
918 * Hwi_disable may be called from main(). However, since Hwi interrupts
919 * are already disabled in main(), such a call has no effect.
920 *
921 * @a(Implementation Note) 922 * In order to support zero latency interrupts, rather
923 * than setting PRIMASK (which would globally disable all NVIC
924 * interrupts), Hwi_disable() instead writes the value of
925 * {@link #disablePriority Hwi.disablePriority}
926 * to the BASEPRI register. In doing so, all interrupts of equal or
927 * lower priority than Hwi.disablePriority are disabled.
928 *
929 * @a(constraints) 930 * If a Task switching API such as
931 * {@link ti.sysbios.knl.Semaphore#pend Semaphore_pend()},
932 * {@link ti.sysbios.knl.Semaphore#post Semaphore_post()},
933 * {@link ti.sysbios.knl.Task#sleep Task_sleep()}, or
934 * {@link ti.sysbios.knl.Task#yield Task_yield()}
935 * is invoked which results in a context switch while
936 * interrupts are disabled, an embedded call to
937 * {@link #enable Hwi_enable} occurs
938 * on the way to the new thread context which unconditionally re-enables
939 * interrupts. Interrupts will remain enabled until a subsequent
940 * {@link #disable Hwi_disable}
941 * invocation.
942 *
943 * Swis always run with interrupts enabled.
944 * See {@link ti.sysbios.knl.Swi#post Swi_post()} for a discussion Swis and
945 * interrupts.
946 *
947 * @b(returns) opaque key for use by Hwi_restore()
948 */
949 @Macro
950 override UInt disable();
951
952 /*!
953 * ======== enable ========
954 */
955 @Macro
956 override UInt enable();
957
958 /*!
959 * ======== restore ========
960 */
961 @Macro
962 override Void restore(UInt key);
963
964 /*!
965 * @_nodoc 966 * ======== disableFxn ========
967 * function call implementation
968 */
969 UInt disableFxn();
970
971 /*!
972 * @_nodoc 973 * ======== enableFxn ========
974 * function call implementation
975 */
976 UInt enableFxn();
977
978 /*!
979 * @_nodoc 980 * ======== restoreFxn ========
981 * function call implementation
982 */
983 Void restoreFxn(UInt key);
984
985 /*!
986 * ======== inUseMeta ========
987 * @_nodoc 988 * Check for Hwi already in use.
989 * For internal SYS/BIOS use only.
990 * Should be called prior to any internal Hwi.create().
991 *
992 * @param(intNum) interrupt number
993 */
994 metaonly Bool inUseMeta(UInt intNum);
995
996 /*!
997 * @_nodoc 998 * ======== plug ========
999 * Plug a non dispatched interrupt vector with an ISR address.
1000 *
1001 * @param(intNum) interrupt number
1002 * @param(fxn) pointer to ISR function
1003 */
1004 Void plug(UInt intNum, Void *fxn);
1005
1006 /*!
1007 * ======== getHandle ========
1008 * Returns Hwi_handle associated with intNum
1009 *
1010 * @param(intNum) interrupt number
1011 */
1012 Handle getHandle(UInt intNum);
1013
1014 /*!
1015 * ======== setPriority ========
1016 * Set an interrupt's relative priority.
1017 *
1018 * Valid priorities are 0 - 255. 0 is highest priority.
1019 *
1020 * @a(WARNING) 1021 * Setting the priority of a dispatched Hwi to a value higher
1022 * than {@link #disablePriority Hwi.disablePriority} will make
1023 * it become non-maskable by {@link #disable Hwi_disable()}.
1024 * The behavior of your application after that will be
1025 * unpredictable and will likely yield catastrophic results!
1026 *
1027 * @param(intNum) ID of interrupt
1028 * @param(priority) priority
1029 */
1030 Void setPriority(UInt intNum, UInt priority);
1031
1032 /*!
1033 * ======== excSetBuffers ========
1034 * Set the exception context and stack buffer pointers
1035 *
1036 * @param(excContextBuffer) Address to place ExcContext
1037 * @param(excStackBuffer) Address to place ExcStack
1038 */
1039 Void excSetBuffers(Ptr excContextBuffer, Ptr excStackBuffer);
1040
1041 /*!
1042 * @_nodoc 1043 * ======== initNVIC ========
1044 * initialize everything but leave ints disabled
1045 */
1046 Void initNVIC();
1047
1048 /*!
1049 * @_nodoc 1050 * ======== initStacks ========
1051 * set up M3 split stacks
1052 */
1053 Void initStacks(Ptr hwiStack);
1054
1055 /*!
1056 * @_nodoc 1057 * ======== flushVnvic ========
1058 * Reconfigure a dispatched interrupt.
1059 *
1060 * Called by the internal function "Hwi_updateNvic()".
1061 *
1062 * This is a public API because it is also called by "Core_hwiFunc()".
1063 */
1064 Void flushVnvic();
1065
1066 instance:
1067
1068 /*!
1069 * Interrupt priority.
1070 * The default is 255 which is the lowest priority.
1071 *
1072 * Priority 0 is the highest priority and by default is
1073 * reserved for zero latency interrupts
1074 * (see {@link #disablePriority}).
1075 *
1076 * Valid priorities values are device dependent and their
1077 * nesting behaviors depend on the {@link #priGroup} setting.
1078 *
1079 * See the Cortex M3 architecture reference manual for details
1080 * on the meanings of these parameters.
1081 */
1082 overrideconfig Int priority = 255;
1083
1084 /*!
1085 * Interrupt Masking Option. Only MaskingOption_LOWER is supported.
1086 *
1087 * The NVIC interrupt controller is designed for priority based
1088 * interrupts. No support is provided for anything but
1089 * Hwi.MaskingOption_LOWER.
1090 */
1091 overrideconfig IHwi.MaskingOption maskSetting = IHwi.MaskingOption_LOWER;
1092
1093 /*!
1094 * Use the interrupt dispatcher with this interrupt. Default is true.
1095 *
1096 * If set to false, the interrupt dispatcher is NOT used. Instead,
1097 * the configured Hwi function address is placed directly in the
1098 * vector table, which results in the dispatcher being bypassed.
1099 *
1100 * @a(Warning) 1101 * Interrupts configured to bupass the dispatcher are not allowed
1102 * to call ANY SYS/BIOS APIs that effect thread scheduling. Examples
1103 * of API that should no be invoked are:
1104 *
1105 * @p(dlist) 1106 * - Swi_post(),
1107 * - Semaphore_post(),
1108 * - Event_post(),
1109 * - Task_yield()
1110 * @p 1111 *
1112 * Additionally, although the signature for a non-dispatched interrupt
1113 * function is the same as that for a dispatched interrupt
1114 * (see {@link #FuncPtr}), no argument is actually passed
1115 * to the non-dispatched ISR handler.
1116 */
1117 config Bool useDispatcher = true;
1118
1119 /*!
1120 * ======== reconfig ========
1121 * Reconfigure a dispatched interrupt.
1122 */
1123 Void reconfig(FuncPtr fxn, const Params *params);
1124
1125 internal: /* not for client use */
1126
1127 /*!
1128 * If Hwi.dispatchTableSize is initialized by the user then
1129 * Hwi.numSparseInterrupts is set to the value of Hwi.dispatchTableSize
1130 *
1131 * If Hwi.dispatchTableSize is NOT set by the user, the normal
1132 * intNum-indexed Hwi dispatchTable mechanism is used by
1133 * the dispatcher to find the corresponding Hwi object.
1134 *
1135 * If Hwi.dispatchTableSize is set by the user, then a
1136 * RAM-based fixed sized interrupt jump table is generated
1137 * that contains a repeating pattern of the following 3 word
1138 * assembly code snippets:
1139 *
1140 * hwiX: ldr r3, hwiObjectX
1141 * ldr pc, ti_sysbios_family_arm_m3_Hwi_dispatch__I
1142 * hwiObjectX: .word 0
1143 * hwiY: ldr r3, hwiObjectY
1144 * ldr pc, ti_sysbios_family_arm_m3_Hwi_dispatch__I
1145 * hwiObjectY: .word 0
1146 * ...
1147 *
1148 * Each dispatched interrupt vector is then initialized to point
1149 * to one of these tuples, and the address of the corresponding Hwi
1150 * object is written into the hwiObjectX field.
1151 *
1152 * The low level assembly code in Hwi_dispatch__I preserves the
1153 * value of r3 when it calls Hwi_dispatchC(), which results in
1154 * the Hwi object being passed as the arg3.
1155 *
1156 * Depending on the boolean value of Hwi_numSparseInterrupts, the
1157 * dispatcher either uses the value passed in arg3 as the
1158 * Hwi object, or uses intNum to index into the standard
1159 * dispatchTable to fetch the Hwi object.
1160 */
1161 config UInt numSparseInterrupts = 0;
1162
1163 /*
1164 * Boolean to indicate whether the current target is being
1165 * built using tiva platform.
1166 */
1167 metaonlyconfig Bool isTiva = false;
1168
1169 /*
1170 * The omap4430 ES1 devices have a nasty bug in the unicache
1171 * that locks the bus up when an interrupt occurs at a specific
1172 * time during an internal cache operation.
1173 * The flag below, when set to true, activates special
1174 * code in the Hwi module to work around this bug.
1175 * "WA1_1" comes from "WorkAround 1.1" from a list of potential
1176 * solutions to the problem developed by the design team.
1177 */
1178 metaonlyconfig Bool enableWA1_1 = false;
1179
1180 /*
1181 * Swi and Task module function pointers.
1182 * Used to decouple Hwi from Swi and Task when
1183 * dispatcherSwiSupport or
1184 * dispatcherTaskSupport is false.
1185 */
1186 config UInt (*swiDisable)();
1187 config Void (*swiRestoreHwi)(UInt);
1188 config UInt (*taskDisable)();
1189 config Void (*taskRestoreHwi)(UInt);
1190
1191 /* initial Hwi_nvic.CCR value */
1192 config UInt32 ccr;
1193
1194 /*!
1195 * const array to hold all HookSet objects.
1196 */
1197 config HookSet hooks[length] = [];
1198
1199 /*
1200 * ======== postInit ========
1201 * finish initializing static and dynamic Hwis
1202 */
1203 Int postInit(Object *hwi, Error.Block *eb);
1204
1205 /*!
1206 * ======== updateNvic ========
1207 * Internal SMP function to cause the virtual NVIC to be flushed to the
1208 * actual NVIC.
1209 *
1210 * This function is called by the various user APIs that manipulate
1211 * individual NVIC register bits
1212 * (ie Hwi_enable/disable/restore/clearInterrupt())
1213 *
1214 * If the current core is the owner of "intNum", flushVnvic() is called
1215 * immediately.
1216 *
1217 * Otherwise an intercore interrupt is generated to force the other core
1218 * to perform the flushVnvic().
1219 *
1220 */
1221 Void updateNvic(UInt intNum);
1222
1223 /*!
1224 * ======== excHandlerAsm ========
1225 * asm code exception handler
1226 */
1227 Void excHandlerAsm();
1228
1229 /*!
1230 * ======== excHandler ========
1231 * exception Handler routes to
1232 * either min, max, or spin exception handler
1233 */
1234 Void excHandler(UInt *excStack, UInt lr);
1235
1236 /*!
1237 * ======== excHandlerMin ========
1238 * Minimal Exception Handler
1239 */
1240 Void excHandlerMin(UInt *excStack, UInt lr);
1241
1242 /*!
1243 * ======== excHandlerMax ========
1244 * Full Featured Exception Handler
1245 */
1246 Void excHandlerMax(UInt *excStack, UInt lr);
1247
1248 /*!
1249 * ======== excFillContext ========
1250 */
1251 Void excFillContext(UInt *excStack);
1252
1253 /*!
1254 * ======== excNmi ========
1255 */
1256 Void excNmi(UInt *excStack);
1257
1258 /*!
1259 * ======== excHardFault ========
1260 */
1261 Void excHardFault(UInt *excStack);
1262
1263 /*!
1264 * ======== excMemFault ========
1265 */
1266 Void excMemFault(UInt *excStack);
1267
1268 /*!
1269 * ======== excBusFault ========
1270 */
1271 Void excBusFault(UInt *excStack);
1272
1273 /*!
1274 * ======== excUsageFault ========
1275 */
1276 Void excUsageFault(UInt *excStack);
1277
1278 /*!
1279 * ======== excSvCall ========
1280 */
1281 Void excSvCall(UInt *excStack);
1282
1283 /*!
1284 * ======== excDebugMon ========
1285 */
1286 Void excDebugMon(UInt *excStack);
1287
1288 /*!
1289 * ======== excReserved ========
1290 */
1291 Void excReserved(UInt *excStack, UInt excNum);
1292
1293 /*!
1294 * ======== excNoIsr ========
1295 */
1296 Void excNoIsr(UInt *excStack, UInt excNum);
1297
1298 /*!
1299 * ======== excDumpRegs ========
1300 */
1301 Void excDumpRegs(UInt lr);
1302
1303 /*!
1304 * ======== pendSV ========
1305 * Used by dispatcher
1306 */
1307 Void pendSV();
1308
1309 /*! Hwi vector function type definition. */
1310 typedef Void (*HandlerFuncPtr)(Handle, UInt);
1311
1312 /* Low Level Interrupt Dispatcher Wrapper */
1313 Void dispatch();
1314
1315 /*
1316 * ======== cc26xxRomInitNVIC ========
1317 * Fix for SDOCM00114681: broken Hwi_initNVIC() function.
1318 * Installed rather than Hwi.initNVIC for CC26xx ROM build
1319 * when Hwi.resetVectorAddress is not 0x00000000.
1320 */
1321 Void cc26xxRomInitNVIC();
1322
1323 /*
1324 * "Top Half" of Interrupt Dispatcher
1325 * Does not include Swi_restore() and Task_restore()
1326 */
1327 UInt dispatchC(Irp irp, UInt32 dummy1, UInt32 dummy2, Object *hwi);
1328
1329 /* "Bottom half", run swi scheduler */
1330 Void doSwiRestore(UInt tskKey);
1331
1332 /* "Bottom half", run task scheduler */
1333 Void doTaskRestore(UInt tskKey);
1334
1335 /*! Meta World Only Hwi Configuration Object. */
1336 metaonlystruct InterruptObj {
1337 String name; /* symbol used for vector table entry */
1338 Bool used; /* Interrupt already defined? */
1339 Bool useDispatcher; /* Should dispatcher handle this Int? */
1340 UInt priority; /* priority */
1341 FuncPtr fxn; /* Dispatched ISR function */
1342 Handle hwi; /* Hwi object address */
1343 };
1344
1345 /*!
1346 * Meta-only array of interrupt objects.
1347 * This meta-only array of Hwi config objects is initialized
1348 * in Hwi.xs:module$meta$init().
1349 */
1350 metaonlyconfig InterruptObj interrupt[];
1351
1352 struct Instance_State {
1353 UArg arg; // Argument to Hwi function.
1354 FuncPtr fxn; // Hwi function.
1355 Irp irp; // current IRP/enabled flag
1356 // for static Hwis
1357 UInt8 priority; // Interrupt priorty
1358 Int16 intNum; // Interrupt number. 16 bits used to
1359 // encode non-dispatched interrupt
1360 // as negative intNum
1361 Ptr hookEnv[];
1362 };
1363
1364 struct Module_State {
1365 Char *taskSP; // Temporary storage of interrupted
1366 // Task's SP during ISR execution
1367 Bool excActive[]; // TRUE if an exception has occurred
1368 ExcContext *excContext[]; // Exception context
1369 Ptr excStack[]; // Exception thread stack
1370 Ptr isrStack; // Points to isrStack address
1371 Ptr isrStackBase; // = __TI_STACK_BASE
1372 SizeT isrStackSize; // = Program.stack
1373 Ptr vectorTableBase; // Points to base of vector table
1374 UInt swiTaskKeys; // dispatcher Swi and Task key storage
1375 Ptr dispatchTable; // Ptr to dispatchTable or sparseInterruptTable
1376 volatile Bool vnvicFlushRequired; // if TRUE, Hwi_vnvicFlush will copy
1377 // changed vnvic regs to nvic
1378 UInt8 intAffinity[]; // smp int-to-coreId mappings
1379 UInt32 intAffinityMasks[][]; // smp per-core NVIC register masks
1380 };
1381 }