Instance: GPIO
Component: GPIO
Base address: 0x40022000
MCU GPIO - I/F for controlling and reading IO status and IO event status
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
RW |
32 |
0x0000 0000 |
0x0000 0000 |
0x4002 2000 |
|
RW |
32 |
0x0000 0000 |
0x0000 0004 |
0x4002 2004 |
|
RW |
32 |
0x0000 0000 |
0x0000 0008 |
0x4002 2008 |
|
RW |
32 |
0x0000 0000 |
0x0000 000C |
0x4002 200C |
|
RW |
32 |
0x0000 0000 |
0x0000 0010 |
0x4002 2010 |
|
RW |
32 |
0x0000 0000 |
0x0000 0014 |
0x4002 2014 |
|
RW |
32 |
0x0000 0000 |
0x0000 0018 |
0x4002 2018 |
|
RW |
32 |
0x0000 0000 |
0x0000 001C |
0x4002 201C |
|
RW |
32 |
0x0000 0000 |
0x0000 0080 |
0x4002 2080 |
|
WO |
32 |
0x0000 0000 |
0x0000 0090 |
0x4002 2090 |
|
WO |
32 |
0x0000 0000 |
0x0000 00A0 |
0x4002 20A0 |
|
RW |
32 |
0x0000 0000 |
0x0000 00B0 |
0x4002 20B0 |
|
RO |
32 |
0x0000 0000 |
0x0000 00C0 |
0x4002 20C0 |
|
RW |
32 |
0x0000 0000 |
0x0000 00D0 |
0x4002 20D0 |
|
RW |
32 |
0x0000 0000 |
0x0000 00E0 |
0x4002 20E0 |
Address Offset | 0x0000 0000 | ||
Physical Address | 0x4002 2000 | Instance | 0x4002 2000 |
Description | Data Out 0 to 3 Alias register for byte access to each bit in DOUT31_0 |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:25 | RESERVED25 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
24 | DIO3 | Sets the state of the pin that is configured as DIO#3, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
23:17 | RESERVED17 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
16 | DIO2 | Sets the state of the pin that is configured as DIO#2, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
15:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
8 | DIO1 | Sets the state of the pin that is configured as DIO#1, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
7:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
0 | DIO0 | Sets the state of the pin that is configured as DIO#0, if the corresponding DOE31_0 bitfield is set. | WO | 0 |
Address Offset | 0x0000 0004 | ||
Physical Address | 0x4002 2004 | Instance | 0x4002 2004 |
Description | Data Out 4 to 7 Alias register for byte access to each bit in DOUT31_0 |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:25 | RESERVED25 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
24 | DIO7 | Sets the state of the pin that is configured as DIO#7, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
23:17 | RESERVED17 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
16 | DIO6 | Sets the state of the pin that is configured as DIO#6, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
15:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
8 | DIO5 | Sets the state of the pin that is configured as DIO#5, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
7:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
0 | DIO4 | Sets the state of the pin that is configured as DIO#4, if the corresponding DOE31_0 bitfield is set. | WO | 0 |
Address Offset | 0x0000 0008 | ||
Physical Address | 0x4002 2008 | Instance | 0x4002 2008 |
Description | Data Out 8 to 11 Alias register for byte access to each bit in DOUT31_0 |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:25 | RESERVED25 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
24 | DIO11 | Sets the state of the pin that is configured as DIO#11, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
23:17 | RESERVED17 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
16 | DIO10 | Sets the state of the pin that is configured as DIO#10, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
15:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
8 | DIO9 | Sets the state of the pin that is configured as DIO#9, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
7:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
0 | DIO8 | Sets the state of the pin that is configured as DIO#8, if the corresponding DOE31_0 bitfield is set. | WO | 0 |
Address Offset | 0x0000 000C | ||
Physical Address | 0x4002 200C | Instance | 0x4002 200C |
Description | Data Out 12 to 15 Alias register for byte access to each bit in DOUT31_0 |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:25 | RESERVED25 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
24 | DIO15 | Sets the state of the pin that is configured as DIO#15, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
23:17 | RESERVED17 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
16 | DIO14 | Sets the state of the pin that is configured as DIO#14, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
15:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
8 | DIO13 | Sets the state of the pin that is configured as DIO#13, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
7:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
0 | DIO12 | Sets the state of the pin that is configured as DIO#12, if the corresponding DOE31_0 bitfield is set. | WO | 0 |
Address Offset | 0x0000 0010 | ||
Physical Address | 0x4002 2010 | Instance | 0x4002 2010 |
Description | Data Out 16 to 19 Alias register for byte access to each bit in DOUT31_0 |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:25 | RESERVED25 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
24 | DIO19 | Sets the state of the pin that is configured as DIO#19, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
23:17 | RESERVED17 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
16 | DIO18 | Sets the state of the pin that is configured as DIO#18, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
15:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
8 | DIO17 | Sets the state of the pin that is configured as DIO#17, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
7:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
0 | DIO16 | Sets the state of the pin that is configured as DIO#16, if the corresponding DOE31_0 bitfield is set. | WO | 0 |
Address Offset | 0x0000 0014 | ||
Physical Address | 0x4002 2014 | Instance | 0x4002 2014 |
Description | Data Out 20 to 23 Alias register for byte access to each bit in DOUT31_0 |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:25 | RESERVED25 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
24 | DIO23 | Sets the state of the pin that is configured as DIO#23, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
23:17 | RESERVED17 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
16 | DIO22 | Sets the state of the pin that is configured as DIO#22, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
15:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
8 | DIO21 | Sets the state of the pin that is configured as DIO#21, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
7:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
0 | DIO20 | Sets the state of the pin that is configured as DIO#20, if the corresponding DOE31_0 bitfield is set. | WO | 0 |
Address Offset | 0x0000 0018 | ||
Physical Address | 0x4002 2018 | Instance | 0x4002 2018 |
Description | Data Out 24 to 27 Alias register for byte access to each bit in DOUT31_0 |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:25 | RESERVED25 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
24 | DIO27 | Sets the state of the pin that is configured as DIO#27, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
23:17 | RESERVED17 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
16 | DIO26 | Sets the state of the pin that is configured as DIO#26, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
15:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
8 | DIO25 | Sets the state of the pin that is configured as DIO#25, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
7:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
0 | DIO24 | Sets the state of the pin that is configured as DIO#24, if the corresponding DOE31_0 bitfield is set. | WO | 0 |
Address Offset | 0x0000 001C | ||
Physical Address | 0x4002 201C | Instance | 0x4002 201C |
Description | Data Out 28 to 31 Alias register for byte access to each bit in DOUT31_0 |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:25 | RESERVED25 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
24 | DIO31 | Sets the state of the pin that is configured as DIO#31, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
23:17 | RESERVED17 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
16 | DIO30 | Sets the state of the pin that is configured as DIO#30, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
15:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
8 | DIO29 | Sets the state of the pin that is configured as DIO#29, if the corresponding DOE31_0 bitfield is set. | WO | 0 | ||
7:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 | ||
0 | DIO28 | Sets the state of the pin that is configured as DIO#28, if the corresponding DOE31_0 bitfield is set. | WO | 0 |
Address Offset | 0x0000 0080 | ||
Physical Address | 0x4002 2080 | Instance | 0x4002 2080 |
Description | Data Output for DIO 0 to 31 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31 | DIO31 | Data output for DIO 31 | RW | 0 | ||
30 | DIO30 | Data output for DIO 30 | RW | 0 | ||
29 | DIO29 | Data output for DIO 29 | RW | 0 | ||
28 | DIO28 | Data output for DIO 28 | RW | 0 | ||
27 | DIO27 | Data output for DIO 27 | RW | 0 | ||
26 | DIO26 | Data output for DIO 26 | RW | 0 | ||
25 | DIO25 | Data output for DIO 25 | RW | 0 | ||
24 | DIO24 | Data output for DIO 24 | RW | 0 | ||
23 | DIO23 | Data output for DIO 23 | RW | 0 | ||
22 | DIO22 | Data output for DIO 22 | RW | 0 | ||
21 | DIO21 | Data output for DIO 21 | RW | 0 | ||
20 | DIO20 | Data output for DIO 20 | RW | 0 | ||
19 | DIO19 | Data output for DIO 19 | RW | 0 | ||
18 | DIO18 | Data output for DIO 18 | RW | 0 | ||
17 | DIO17 | Data output for DIO 17 | RW | 0 | ||
16 | DIO16 | Data output for DIO 16 | RW | 0 | ||
15 | DIO15 | Data output for DIO 15 | RW | 0 | ||
14 | DIO14 | Data output for DIO 14 | RW | 0 | ||
13 | DIO13 | Data output for DIO 13 | RW | 0 | ||
12 | DIO12 | Data output for DIO 12 | RW | 0 | ||
11 | DIO11 | Data output for DIO 11 | RW | 0 | ||
10 | DIO10 | Data output for DIO 10 | RW | 0 | ||
9 | DIO9 | Data output for DIO 9 | RW | 0 | ||
8 | DIO8 | Data output for DIO 8 | RW | 0 | ||
7 | DIO7 | Data output for DIO 7 | RW | 0 | ||
6 | DIO6 | Data output for DIO 6 | RW | 0 | ||
5 | DIO5 | Data output for DIO 5 | RW | 0 | ||
4 | DIO4 | Data output for DIO 4 | RW | 0 | ||
3 | DIO3 | Data output for DIO 3 | RW | 0 | ||
2 | DIO2 | Data output for DIO 2 | RW | 0 | ||
1 | DIO1 | Data output for DIO 1 | RW | 0 | ||
0 | DIO0 | Data output for DIO 0 | RW | 0 |
Address Offset | 0x0000 0090 | ||
Physical Address | 0x4002 2090 | Instance | 0x4002 2090 |
Description | Data Out Set Writing 1 to a bit position sets the corresponding bit in the DOUT31_0 register |
||
Type | WO |
Bits | Field Name | Description | Type | Reset | ||
31 | DIO31 | Set bit 31 | WO | 0 | ||
30 | DIO30 | Set bit 30 | WO | 0 | ||
29 | DIO29 | Set bit 29 | WO | 0 | ||
28 | DIO28 | Set bit 28 | WO | 0 | ||
27 | DIO27 | Set bit 27 | WO | 0 | ||
26 | DIO26 | Set bit 26 | WO | 0 | ||
25 | DIO25 | Set bit 25 | WO | 0 | ||
24 | DIO24 | Set bit 24 | WO | 0 | ||
23 | DIO23 | Set bit 23 | WO | 0 | ||
22 | DIO22 | Set bit 22 | WO | 0 | ||
21 | DIO21 | Set bit 21 | WO | 0 | ||
20 | DIO20 | Set bit 20 | WO | 0 | ||
19 | DIO19 | Set bit 19 | WO | 0 | ||
18 | DIO18 | Set bit 18 | WO | 0 | ||
17 | DIO17 | Set bit 17 | WO | 0 | ||
16 | DIO16 | Set bit 16 | WO | 0 | ||
15 | DIO15 | Set bit 15 | WO | 0 | ||
14 | DIO14 | Set bit 14 | WO | 0 | ||
13 | DIO13 | Set bit 13 | WO | 0 | ||
12 | DIO12 | Set bit 12 | WO | 0 | ||
11 | DIO11 | Set bit 11 | WO | 0 | ||
10 | DIO10 | Set bit 10 | WO | 0 | ||
9 | DIO9 | Set bit 9 | WO | 0 | ||
8 | DIO8 | Set bit 8 | WO | 0 | ||
7 | DIO7 | Set bit 7 | WO | 0 | ||
6 | DIO6 | Set bit 6 | WO | 0 | ||
5 | DIO5 | Set bit 5 | WO | 0 | ||
4 | DIO4 | Set bit 4 | WO | 0 | ||
3 | DIO3 | Set bit 3 | WO | 0 | ||
2 | DIO2 | Set bit 2 | WO | 0 | ||
1 | DIO1 | Set bit 1 | WO | 0 | ||
0 | DIO0 | Set bit 0 | WO | 0 |
Address Offset | 0x0000 00A0 | ||
Physical Address | 0x4002 20A0 | Instance | 0x4002 20A0 |
Description | Data Out Clear Writing 1 to a bit position clears the corresponding bit in the DOUT31_0 register |
||
Type | WO |
Bits | Field Name | Description | Type | Reset | ||
31 | DIO31 | Clears bit 31 | WO | 0 | ||
30 | DIO30 | Clears bit 30 | WO | 0 | ||
29 | DIO29 | Clears bit 29 | WO | 0 | ||
28 | DIO28 | Clears bit 28 | WO | 0 | ||
27 | DIO27 | Clears bit 27 | WO | 0 | ||
26 | DIO26 | Clears bit 26 | WO | 0 | ||
25 | DIO25 | Clears bit 25 | WO | 0 | ||
24 | DIO24 | Clears bit 24 | WO | 0 | ||
23 | DIO23 | Clears bit 23 | WO | 0 | ||
22 | DIO22 | Clears bit 22 | WO | 0 | ||
21 | DIO21 | Clears bit 21 | WO | 0 | ||
20 | DIO20 | Clears bit 20 | WO | 0 | ||
19 | DIO19 | Clears bit 19 | WO | 0 | ||
18 | DIO18 | Clears bit 18 | WO | 0 | ||
17 | DIO17 | Clears bit 17 | WO | 0 | ||
16 | DIO16 | Clears bit 16 | WO | 0 | ||
15 | DIO15 | Clears bit 15 | WO | 0 | ||
14 | DIO14 | Clears bit 14 | WO | 0 | ||
13 | DIO13 | Clears bit 13 | WO | 0 | ||
12 | DIO12 | Clears bit 12 | WO | 0 | ||
11 | DIO11 | Clears bit 11 | WO | 0 | ||
10 | DIO10 | Clears bit 10 | WO | 0 | ||
9 | DIO9 | Clears bit 9 | WO | 0 | ||
8 | DIO8 | Clears bit 8 | WO | 0 | ||
7 | DIO7 | Clears bit 7 | WO | 0 | ||
6 | DIO6 | Clears bit 6 | WO | 0 | ||
5 | DIO5 | Clears bit 5 | WO | 0 | ||
4 | DIO4 | Clears bit 4 | WO | 0 | ||
3 | DIO3 | Clears bit 3 | WO | 0 | ||
2 | DIO2 | Clears bit 2 | WO | 0 | ||
1 | DIO1 | Clears bit 1 | WO | 0 | ||
0 | DIO0 | Clears bit 0 | WO | 0 |
Address Offset | 0x0000 00B0 | ||
Physical Address | 0x4002 20B0 | Instance | 0x4002 20B0 |
Description | Data Out Toggle Writing 1 to a bit position will invert the corresponding DIO output. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31 | DIO31 | Toggles bit 31 | RW | 0 | ||
30 | DIO30 | Toggles bit 30 | RW | 0 | ||
29 | DIO29 | Toggles bit 29 | RW | 0 | ||
28 | DIO28 | Toggles bit 28 | RW | 0 | ||
27 | DIO27 | Toggles bit 27 | RW | 0 | ||
26 | DIO26 | Toggles bit 26 | RW | 0 | ||
25 | DIO25 | Toggles bit 25 | RW | 0 | ||
24 | DIO24 | Toggles bit 24 | RW | 0 | ||
23 | DIO23 | Toggles bit 23 | RW | 0 | ||
22 | DIO22 | Toggles bit 22 | RW | 0 | ||
21 | DIO21 | Toggles bit 21 | RW | 0 | ||
20 | DIO20 | Toggles bit 20 | RW | 0 | ||
19 | DIO19 | Toggles bit 19 | RW | 0 | ||
18 | DIO18 | Toggles bit 18 | RW | 0 | ||
17 | DIO17 | Toggles bit 17 | RW | 0 | ||
16 | DIO16 | Toggles bit 16 | RW | 0 | ||
15 | DIO15 | Toggles bit 15 | RW | 0 | ||
14 | DIO14 | Toggles bit 14 | RW | 0 | ||
13 | DIO13 | Toggles bit 13 | RW | 0 | ||
12 | DIO12 | Toggles bit 12 | RW | 0 | ||
11 | DIO11 | Toggles bit 11 | RW | 0 | ||
10 | DIO10 | Toggles bit 10 | RW | 0 | ||
9 | DIO9 | Toggles bit 9 | RW | 0 | ||
8 | DIO8 | Toggles bit 8 | RW | 0 | ||
7 | DIO7 | Toggles bit 7 | RW | 0 | ||
6 | DIO6 | Toggles bit 6 | RW | 0 | ||
5 | DIO5 | Toggles bit 5 | RW | 0 | ||
4 | DIO4 | Toggles bit 4 | RW | 0 | ||
3 | DIO3 | Toggles bit 3 | RW | 0 | ||
2 | DIO2 | Toggles bit 2 | RW | 0 | ||
1 | DIO1 | Toggles bit 1 | RW | 0 | ||
0 | DIO0 | Toggles bit 0 | RW | 0 |
Address Offset | 0x0000 00C0 | ||
Physical Address | 0x4002 20C0 | Instance | 0x4002 20C0 |
Description | Data Input from DIO 0 to 31 | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31 | DIO31 | Data input from DIO 31 | RO | 0 | ||
30 | DIO30 | Data input from DIO 30 | RO | 0 | ||
29 | DIO29 | Data input from DIO 29 | RO | 0 | ||
28 | DIO28 | Data input from DIO 28 | RO | 0 | ||
27 | DIO27 | Data input from DIO 27 | RO | 0 | ||
26 | DIO26 | Data input from DIO 26 | RO | 0 | ||
25 | DIO25 | Data input from DIO 25 | RO | 0 | ||
24 | DIO24 | Data input from DIO 24 | RO | 0 | ||
23 | DIO23 | Data input from DIO 23 | RO | 0 | ||
22 | DIO22 | Data input from DIO 22 | RO | 0 | ||
21 | DIO21 | Data input from DIO 21 | RO | 0 | ||
20 | DIO20 | Data input from DIO 20 | RO | 0 | ||
19 | DIO19 | Data input from DIO 19 | RO | 0 | ||
18 | DIO18 | Data input from DIO 18 | RO | 0 | ||
17 | DIO17 | Data input from DIO 17 | RO | 0 | ||
16 | DIO16 | Data input from DIO 16 | RO | 0 | ||
15 | DIO15 | Data input from DIO 15 | RO | 0 | ||
14 | DIO14 | Data input from DIO 14 | RO | 0 | ||
13 | DIO13 | Data input from DIO 13 | RO | 0 | ||
12 | DIO12 | Data input from DIO 12 | RO | 0 | ||
11 | DIO11 | Data input from DIO 11 | RO | 0 | ||
10 | DIO10 | Data input from DIO 10 | RO | 0 | ||
9 | DIO9 | Data input from DIO 9 | RO | 0 | ||
8 | DIO8 | Data input from DIO 8 | RO | 0 | ||
7 | DIO7 | Data input from DIO 7 | RO | 0 | ||
6 | DIO6 | Data input from DIO 6 | RO | 0 | ||
5 | DIO5 | Data input from DIO 5 | RO | 0 | ||
4 | DIO4 | Data input from DIO 4 | RO | 0 | ||
3 | DIO3 | Data input from DIO 3 | RO | 0 | ||
2 | DIO2 | Data input from DIO 2 | RO | 0 | ||
1 | DIO1 | Data input from DIO 1 | RO | 0 | ||
0 | DIO0 | Data input from DIO 0 | RO | 0 |
Address Offset | 0x0000 00D0 | ||
Physical Address | 0x4002 20D0 | Instance | 0x4002 20D0 |
Description | Data Output Enable for DIO 0 to 31 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31 | DIO31 | Data output enable for DIO 31 | RW | 0 | ||
30 | DIO30 | Data output enable for DIO 30 | RW | 0 | ||
29 | DIO29 | Data output enable for DIO 29 | RW | 0 | ||
28 | DIO28 | Data output enable for DIO 28 | RW | 0 | ||
27 | DIO27 | Data output enable for DIO 27 | RW | 0 | ||
26 | DIO26 | Data output enable for DIO 26 | RW | 0 | ||
25 | DIO25 | Data output enable for DIO 25 | RW | 0 | ||
24 | DIO24 | Data output enable for DIO 24 | RW | 0 | ||
23 | DIO23 | Data output enable for DIO 23 | RW | 0 | ||
22 | DIO22 | Data output enable for DIO 22 | RW | 0 | ||
21 | DIO21 | Data output enable for DIO 21 | RW | 0 | ||
20 | DIO20 | Data output enable for DIO 20 | RW | 0 | ||
19 | DIO19 | Data output enable for DIO 19 | RW | 0 | ||
18 | DIO18 | Data output enable for DIO 18 | RW | 0 | ||
17 | DIO17 | Data output enable for DIO 17 | RW | 0 | ||
16 | DIO16 | Data output enable for DIO 16 | RW | 0 | ||
15 | DIO15 | Data output enable for DIO 15 | RW | 0 | ||
14 | DIO14 | Data output enable for DIO 14 | RW | 0 | ||
13 | DIO13 | Data output enable for DIO 13 | RW | 0 | ||
12 | DIO12 | Data output enable for DIO 12 | RW | 0 | ||
11 | DIO11 | Data output enable for DIO 11 | RW | 0 | ||
10 | DIO10 | Data output enable for DIO 10 | RW | 0 | ||
9 | DIO9 | Data output enable for DIO 9 | RW | 0 | ||
8 | DIO8 | Data output enable for DIO 8 | RW | 0 | ||
7 | DIO7 | Data output enable for DIO 7 | RW | 0 | ||
6 | DIO6 | Data output enable for DIO 6 | RW | 0 | ||
5 | DIO5 | Data output enable for DIO 5 | RW | 0 | ||
4 | DIO4 | Data output enable for DIO 4 | RW | 0 | ||
3 | DIO3 | Data output enable for DIO 3 | RW | 0 | ||
2 | DIO2 | Data output enable for DIO 2 | RW | 0 | ||
1 | DIO1 | Data output enable for DIO 1 | RW | 0 | ||
0 | DIO0 | Data output enable for DIO 0 | RW | 0 |
Address Offset | 0x0000 00E0 | ||
Physical Address | 0x4002 20E0 | Instance | 0x4002 20E0 |
Description | Event Register for DIO 0 to 31 Reading this registers will return 1 for triggered event and 0 for non-triggered events. Writing a 1 to a bit field will clear the event. The configuration of events is done inside MCU IOC, e.g. events for DIO #0 is configured in IOC:IOCFG0.EDGE_DET and IOC:IOCFG0.EDGE_IRQ_EN. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31 | DIO31 | Event for DIO 31 | RW | 0 | ||
30 | DIO30 | Event for DIO 30 | RW | 0 | ||
29 | DIO29 | Event for DIO 29 | RW | 0 | ||
28 | DIO28 | Event for DIO 28 | RW | 0 | ||
27 | DIO27 | Event for DIO 27 | RW | 0 | ||
26 | DIO26 | Event for DIO 26 | RW | 0 | ||
25 | DIO25 | Event for DIO 25 | RW | 0 | ||
24 | DIO24 | Event for DIO 24 | RW | 0 | ||
23 | DIO23 | Event for DIO 23 | RW | 0 | ||
22 | DIO22 | Event for DIO 22 | RW | 0 | ||
21 | DIO21 | Event for DIO 21 | RW | 0 | ||
20 | DIO20 | Event for DIO 20 | RW | 0 | ||
19 | DIO19 | Event for DIO 19 | RW | 0 | ||
18 | DIO18 | Event for DIO 18 | RW | 0 | ||
17 | DIO17 | Event for DIO 17 | RW | 0 | ||
16 | DIO16 | Event for DIO 16 | RW | 0 | ||
15 | DIO15 | Event for DIO 15 | RW | 0 | ||
14 | DIO14 | Event for DIO 14 | RW | 0 | ||
13 | DIO13 | Event for DIO 13 | RW | 0 | ||
12 | DIO12 | Event for DIO 12 | RW | 0 | ||
11 | DIO11 | Event for DIO 11 | RW | 0 | ||
10 | DIO10 | Event for DIO 10 | RW | 0 | ||
9 | DIO9 | Event for DIO 9 | RW | 0 | ||
8 | DIO8 | Event for DIO 8 | RW | 0 | ||
7 | DIO7 | Event for DIO 7 | RW | 0 | ||
6 | DIO6 | Event for DIO 6 | RW | 0 | ||
5 | DIO5 | Event for DIO 5 | RW | 0 | ||
4 | DIO4 | Event for DIO 4 | RW | 0 | ||
3 | DIO3 | Event for DIO 3 | RW | 0 | ||
2 | DIO2 | Event for DIO 2 | RW | 0 | ||
1 | DIO1 | Event for DIO 1 | RW | 0 | ||
0 | DIO0 | Event for DIO 0 | RW | 0 |
© 2015. Texas Instruments | All Rights Reserved |