1    /*
     2     * Copyright (c) 2013-2015, Texas Instruments Incorporated
     3     * All rights reserved.
     4     *
     5     * Redistribution and use in source and binary forms, with or without
     6     * modification, are permitted provided that the following conditions
     7     * are met:
     8     *
     9     * *  Redistributions of source code must retain the above copyright
    10     *    notice, this list of conditions and the following disclaimer.
    11     *
    12     * *  Redistributions in binary form must reproduce the above copyright
    13     *    notice, this list of conditions and the following disclaimer in the
    14     *    documentation and/or other materials provided with the distribution.
    15     *
    16     * *  Neither the name of Texas Instruments Incorporated nor the names of
    17     *    its contributors may be used to endorse or promote products derived
    18     *    from this software without specific prior written permission.
    19     *
    20     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
    21     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
    22     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
    23     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
    24     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
    25     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
    26     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
    27     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
    28     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
    29     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
    30     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    31     */
    32    /*
    33     *  ======== Clock.xdc ========
    34     *
    35     *
    36     */
    37    
    38    package ti.sysbios.knl;
    39    
    40    import xdc.rov.ViewInfo;
    41    
    42    import xdc.runtime.Assert;
    43    import xdc.runtime.Diags;
    44    import xdc.runtime.Log;
    45    
    46    /*!
    47     *  ======== Clock ========
    48     *  System Clock Manager
    49     *
    50     *  The System Clock Manager is responsible for all timing services in
    51     *  SYS/BIOS.
    52     *  It generates the periodic system tick. The tick period is configurable.
    53     *  The timeout and period for all Clock Instances and timeout values in
    54     *  other SYS/BIOS modules are specified in terms of Clock ticks.
    55     *
    56     *  The Clock Manager supports two tick "modes": a periodic mode with an
    57     *  interrupt on each tick (TickMode_PERIODIC), and a tick suppression
    58     *  mode (TickMode_DYNAMIC), which reduces the number of timer interrupts to
    59     *  the minimum required to support the scheduled timeouts.  For devices that
    60     *  support it (e.g., MSP430 devices), TickMode_DYNAMIC may be the default
    61     *  mode if one is not specified in the application configuration; otherwise,
    62     *  the default mode will be TickMode_PERIODIC.  The following example shows
    63     *  how the tick mode  can be specified in the application configuration:
    64     *
    65     *  @p(code)
    66     *  var Clock = xdc.useModule('ti.sysbios.knl.Clock');
    67     *
    68     *  // Tell the Clock module to use TickMode_PERIODIC
    69     *  Clock.tickMode = Clock.TickMode_PERIODIC;
    70     *  @p
    71     *
    72     *  Clock objects contain functions that can be scheduled to run after a
    73     *  certain number of Clock ticks.
    74     *  Clock objects are either one-shot or periodic. Instances are started
    75     *  when created or they are started later using the Clock_start() function.
    76     *  Instances can be stopped using the Clock_stop() function. All Clock
    77     *  Instances are executed when they expire in the context of a software
    78     *  interrupt.
    79     *
    80     *  Clock objects are placed in the Clock object service list when
    81     *  created/constructed and remain there until deleted/destructed.
    82     *  To minimize processing overhead, unused or expired Clock objects
    83     *  should be deleted or destructed.
    84     *
    85     *  By default, all Clock functions run in the context of a Swi.
    86     *  That is, the Clock module automatically creates a Swi for
    87     *  its use and runs the Clock functions within that Swi.
    88     *  The priority of the Swi used by Clock can be changed
    89     *  by configuring {@link #swiPriority Clock.swiPriority}.
    90     *
    91     *  If Swis are disabled in an application
    92     *  (ie {@link ti.sysbios.BIOS#swiEnabled BIOS.swiEnabled} = false),
    93     *  then all Clock functions are executed within the context of
    94     *  a Timer Hwi.
    95     *
    96     *  @a(Note)
    97     *  @p(blist)
    98     *  As Clock functions execute in either a Swi or Hwi context, they
    99     *  are not permitted to call blocking APIs.
   100     *  @p
   101     *  @a
   102     *
   103     *  The getTicks() function returns number of clock ticks since startup.
   104     *
   105     *  By default, the Timer module defined by {@link #TimerProxy} is used to
   106     *  statically create a timer instance that provides a periodic 1 ms 
   107     *  tick interrupt.
   108     *
   109     *  If you want to use a custom configured timer for the Clock module's
   110     *  tick source, use the following example configuration as a guide:
   111     *
   112     *  @p(code)
   113     *  var Clock = xdc.useModule('ti.sysbios.knl.Clock');
   114     *
   115     *  // Tell the Clock module that YOU are providing the periodic interrupt
   116     *  Clock.tickSource = Clock.TickSource_USER;
   117     *
   118     *  // this example uses the ti.sysbios.timers.dmtimer.Timer module
   119     *  var Timer = xdc.useModule('ti.sysbios.timers.dmtimer.Timer');
   120     *
   121     *  // Change Timer 3 frequency to 24 Mhz from default if necessary
   122     *  Timer.intFreqs[3] = { hi:0, lo:24000000 };
   123     *
   124     *  // create a dmtimer config parameter object
   125     *  var timerParams = new Timer.Params();
   126     *
   127     *  // make sure you set the period to 1000 us (1ms)
   128     *  timerParams.period = 1000;
   129     *
   130     *  // custom dmtimer config parameters here...
   131     *  timerParams.twer.ovf_wup_ena = 1;
   132     *
   133     *  // Create the timer.
   134     *  // This example uses timer id 3.
   135     *  // Provide your own timer interrupt handler function.
   136     *  Timer.create(3, '&myTimerTick', timerParams);
   137     *  @p
   138     *
   139     *  In your 'C' code, add your timer interrupt handler and have it
   140     *  call Clock_tick(), which will perform all of the Clock module
   141     *  tick duties:
   142     *
   143     *  @p(code)
   144     *  #include <ti/sysbios/knl/Clock.h>
   145     *
   146     *  Void myTimerTick(UArg arg)
   147     *  {
   148     *       Clock_tick();
   149     *       ...
   150     *  }
   151     *  @p
   152     *
   153     *  @p(html)
   154     *  <h3> Calling Context </h3>
   155     *  <table border="1" cellpadding="3">
   156     *    <colgroup span="1"></colgroup> <colgroup span="5" align="center">
   157     *    </colgroup>
   158     *
   159     *    <tr><th> Function                </th><th>  Hwi   </th><th>  Swi   </th>
   160     *    <th>  Task  </th><th>  Main  </th><th>  Startup  </th></tr>
   161     *    <!--                                                                -->
   162     *    <tr><td> {@link #construct}      </td><td>   N    </td><td>   N    </td>
   163     *    <td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   164     *    <tr><td> {@link #create}         </td><td>   N    </td><td>   N    </td>
   165     *    <td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   166     *    <tr><td> {@link #delete}         </td><td>   N    </td><td>   N    </td>
   167     *    <td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   168     *    <tr><td> {@link #destruct}       </td><td>   N    </td><td>   N    </td>
   169     *    <td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   170     *    <tr><td> {@link #getTicks}       </td><td>   Y    </td><td>   Y    </td>
   171     *    <td>   Y    </td><td>   N    </td><td>   N    </td></tr>
   172     *    <tr><td> {@link #getTimerHandle} </td><td>   Y    </td><td>   Y    </td>
   173     *    <td>   Y    </td><td>   Y    </td><td>   Y    </td></tr>
   174     *    <tr><td> {@link #Params_init}    </td><td>   Y    </td><td>   Y    </td>
   175     *    <td>   Y    </td><td>   Y    </td><td>   Y    </td></tr>
   176     *    <tr><td> {@link #tick}           </td><td>   Y    </td><td>   Y    </td>
   177     *    <td>   Y    </td><td>   N    </td><td>   N    </td></tr>
   178     *    <tr><td> {@link #tickReconfig}   </td><td>   Y    </td><td>   Y    </td>
   179     *    <td>   Y    </td><td>   N    </td><td>   N    </td></tr>
   180     *    <tr><td> {@link #tickStart}      </td><td>   Y    </td><td>   Y    </td>
   181     *    <td>   Y    </td><td>   N    </td><td>   N    </td></tr>
   182     *    <tr><td> {@link #tickStop}       </td><td>   Y    </td><td>   Y    </td>
   183     *    <td>   Y    </td><td>   N    </td><td>   N    </td></tr>
   184     *
   185     *    <tr><td> {@link #getTimeout}     </td><td>   Y    </td><td>   Y    </td>
   186     *    <td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   187     *    <tr><td> {@link #isActive}       </td><td>   Y    </td><td>   Y    </td>
   188     *    <td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   189     *    <tr><td> {@link #setFunc}        </td><td>   Y    </td><td>   Y    </td>
   190     *    <td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   191     *    <tr><td> {@link #setPeriod}      </td><td>   Y    </td><td>   Y    </td>
   192     *    <td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   193     *    <tr><td> {@link #setTimeout}     </td><td>   Y    </td><td>   Y    </td>
   194     *    <td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   195     *    <tr><td> {@link #start}          </td><td>   Y    </td><td>   Y    </td>
   196     *    <td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   197     *    <tr><td> {@link #stop}           </td><td>   Y    </td><td>   Y    </td>
   198     *    <td>   Y    </td><td>   Y    </td><td>   N    </td></tr>
   199     *    <tr><td colspan="6"> Definitions: <br />
   200     *       <ul>
   201     *         <li> <b>Hwi</b>: API is callable from a Hwi thread. </li>
   202     *         <li> <b>Swi</b>: API is callable from a Swi thread. </li>
   203     *         <li> <b>Task</b>: API is callable from a Task thread. </li>
   204     *         <li> <b>Main</b>: API is callable during any of these phases: </li>
   205     *           <ul>
   206     *             <li> In your module startup after this module is started
   207     *    (e.g. Clock_Module_startupDone() returns TRUE). </li>
   208     *             <li> During
   209     *    {@link xdc.runtime.Startup#lastFxns Startup.lastFxns}. </li>
   210     *             <li> During main().</li>
   211     *             <li> During
   212     *    {@link ti.sysbios.BIOS#startupFxns BIOS.startupFxns}.</li>
   213     *           </ul>
   214     *         <li> <b>Startup</b>: API is callable during any of these phases:</li>
   215     *           <ul>
   216     *             <li> During
   217     *    {@link xdc.runtime.Startup#firstFxns Startup.firstFxns}.</li>
   218     *             <li> In your module startup before this module is started
   219     *    (e.g. Clock_Module_startupDone() returns FALSE).</li>
   220     *           </ul>
   221     *       </ul>
   222     *    </td></tr>
   223     *
   224     *  </table>
   225     *  @p
   226     */
   227    
   228    @DirectCall
   229    @ModuleStartup
   230    @InstanceInitStatic /* Construct/Destruct CAN becalled at runtime */
   231    @InstanceFinalize   /* generate call to Clock_Instance_finalize on delete */
   232    @Template("./Clock.xdt")
   233    
   234    module Clock
   235    {
   236        /*!
   237         *  ======== TickSource ========
   238         *  Clock tick source
   239         *
   240         *  @field(TickSource_TIMER) The Clock module automatically configures a
   241         *  a Timer instance (see {@link #TimerProxy}) to drive the Clock tick.
   242         *  The specific timer and its period can be controlled via
   243         *  {@link #timerId} and {@link #tickPeriod}.
   244         *
   245         *  @field(TickSource_USER) The Application is responsible for calling
   246         *  {@link #tick Clock_tick()} periodically. Make sure {@link #tickPeriod
   247         *  Clock.tickPeriod} is set to the period that Clock_tick() is called.
   248         *
   249         *  Like most other module configuration parameters, the Clock.tickPeriod
   250         *  config parameter value is accessible in runtime C code as
   251         *  "Clock_tickPeriod".
   252         *
   253         *  @field(TickSource_NULL) The Clock module is disabled.
   254         *  In this case, it is an error for the application to ever call
   255         *  Clock_tick().
   256         *
   257         *  @see #tickPeriod
   258         *  @see #timerId
   259         */
   260        enum  TickSource {
   261            TickSource_TIMER,   /*! Internally configure a Timer to periodically call Clock_tick() */
   262            TickSource_USER,    /*! Application code calls Clock_tick() */
   263            TickSource_NULL     /*! The Clock module is disabled */
   264        };
   265    
   266        /*!
   267         *  ======== TickMode ========
   268         *  Clock Tick Mode
   269         */
   270        enum  TickMode {
   271            TickMode_PERIODIC,  /*! Timer will interrupt every period */
   272            TickMode_DYNAMIC    /*! Unnecessary timer ticks will be suppressed */
   273        };
   274    
   275        /*!
   276         *  ======== BasicView ========
   277         *  @_nodoc
   278         */
   279        metaonly struct BasicView {
   280            String          label;
   281            UInt32          timeout;
   282            UInt            period;
   283            String          fxn[];
   284            UArg            arg;
   285            Bool            started;        /* Instance running? */
   286            String          tRemaining;     /* Remaining timeout */
   287            Bool            periodic;       /* Periodic? (vs. one-shot) */
   288        }
   289    
   290        /*!
   291         *  ======== ModuleView ========
   292         *  @_nodoc
   293         */
   294        metaonly struct ModuleView {
   295            String          ticks;
   296            String          tickSource;
   297            String          tickMode;
   298            String          timerHandle;
   299            UInt            timerId;
   300            UInt            swiPriority;
   301            UInt32          tickPeriod;
   302            volatile UInt   nSkip;
   303        }
   304    
   305        /*
   306         *  ======== rovViewInfo ========
   307         *  @_nodoc
   308         */
   309        @Facet
   310        metaonly config ViewInfo.Instance rovViewInfo =
   311            ViewInfo.create({
   312                viewMap: [
   313                  ['Basic',    {type: ViewInfo.INSTANCE, viewInitFxn: 'viewInitBasic',  structName: 'BasicView'}],
   314                  ['Module',   {type: ViewInfo.MODULE,   viewInitFxn: 'viewInitModule', structName: 'ModuleView'}],
   315                ]
   316            });
   317    
   318        /*!
   319         *  ======== FuncPtr ========
   320         * Instance function prototype
   321         */
   322        typedef Void (*FuncPtr)(UArg);
   323    
   324        /*! 
   325         *  ======== TimerProxy ========
   326         *  target/device-specific Timer implementation.
   327         *
   328         *  The Timer module used by the Clock module to
   329         *  create a Timer instance when Clock.tickSource_TIMER is configured.
   330         *
   331         *  By default, a target specific Timer module is internally selected 
   332         *  for this purpose. If the user wishes to use a different Timer module
   333         *  then the following configuration script will serve as an example for
   334         *  achieving that:
   335         *
   336         *  @p(code)
   337         *  var Clock = xdc.useModule('ti.sysbios.knl.Clock');
   338         *
   339         *  // Use a dmtimer Timer instance
   340         *  Clock.TimerProxy = xdc.useModule('ti.sysbios.timers.dmtimer.Timer');
   341         *  @p
   342         *
   343         */
   344        proxy TimerProxy inherits ti.sysbios.interfaces.ITimer;
   345    
   346        /*!
   347         *  ======== LW_delayed ========
   348         *  Logged if Clock Swi delayed by >= 1 tick
   349         */
   350        config Log.Event LW_delayed = {
   351            mask: Diags.USER3,
   352            msg: "LW_delayed: delay: %d"
   353        };
   354    
   355        /*!
   356         *  ======== LM_tick ========
   357         *  Logged in every Clock tick interrupt
   358         */
   359        config Log.Event LM_tick = {
   360            mask: Diags.USER1 | Diags.USER2,
   361            msg: "LM_tick: tick: %d"
   362        };
   363    
   364        /*!
   365         *  ======== LM_begin ========
   366         *  Logged just prior to calling each Clock function
   367         */
   368        config Log.Event LM_begin = {
   369            mask: Diags.USER1 | Diags.USER2,
   370            msg: "LM_begin: clk: 0x%x, func: 0x%x"
   371        };
   372    
   373        /*!
   374         *  ======== A_clockDisabled ========
   375         *  Asserted in Clock_create()
   376         */
   377        config Assert.Id A_clockDisabled = {
   378            msg: "A_clockDisabled: Cannot create a clock instance when BIOS.clockEnabled is false."
   379        };
   380    
   381        /*!
   382         *  ======== A_badThreadType ========
   383         *  Asserted in Clock_create and Clock_delete
   384         */
   385        config Assert.Id A_badThreadType = {
   386            msg: "A_badThreadType: Cannot create/delete a Clock from Hwi or Swi thread."
   387        };
   388    
   389        /*!
   390         *  @_nodoc
   391         *  !!! Do not delete. Required for ROM compatibility !!!
   392         */
   393        config UInt32 serviceMargin = 0;
   394    
   395        /*!
   396         *  ======== tickSource ========
   397         *  Source of clock ticks
   398         *
   399         *  If this parameter is not set to TickSource_TIMER,
   400         *  {@link #tickStart Clock_tickStart()},
   401         *  {@link #tickStop Clock_tickStop()}, and
   402         *  {@link #tickReconfig Clock_tickReconfig()}, have no effect.
   403         *
   404         *  The default is TickSource_TIMER.
   405         */
   406        config TickSource tickSource = TickSource_TIMER;
   407    
   408        /*!
   409         *  ======== tickMode ========
   410         *  Timer tick mode
   411         *
   412         *  This parameter specifies the tick mode to be used by the underlying
   413         *  Timer.
   414         *
   415         *  With TickMode_PERIODIC the timer will interrupt the CPU at
   416         *  a fixed rate, defined by the tickPeriod.
   417         *
   418         *  With TickMode_DYNAMIC the timer can be dynamically reprogrammed by
   419         *  Clock, to interrupt the CPU when the next tick is actually needed for
   420         *  a scheduled timeout. TickMode_DYNAMIC is not supported on all devices,
   421         *  and may have some application constraints (for example, for MSP430,
   422         *  see a description on this wiki page:
   423         *  https://processors.wiki.ti.com/index.php/SYS/BIOS_for_the_MSP430#Clock_Tick_Suppression).
   424         */
   425        config TickMode tickMode;
   426    
   427        /*!
   428         *  ======== timerId ========
   429         *  Timer Id used to create a Timer instance
   430         *
   431         *  If {@link #tickSource Clock.tickSource} is set to TickSource_TIMER,
   432         *  the Clock module internally creates a
   433         *  static Timer instance (see {@link #TimerProxy}) that automatically calls
   434         *  Clock_doTick() on a periodic basis (as specified by
   435         *  {@link #tickPeriod tickPeriod} and {@link #periodType periodType}.)
   436         *
   437         *  This configuration parameter allows you to control which timer is
   438         *  used to drive the Clock module.
   439         *
   440         *  The default value is {@link ti.sysbios.hal.Timer#ANY Timer.ANY} (~0)
   441         *  and the maximum timerId possible is family and device specific.
   442         */
   443        config UInt timerId = ~0;
   444    
   445        /*!
   446         *  ======== swiPriority ========
   447         *  The priority of Swi used by Clock to process its instances
   448         *
   449         *  All Clock instances are executed in the context of a single
   450         *  {@link Swi}.  This parameter allows you to control the priority of
   451         *  that Swi.
   452         *
   453         *  The default value of this parameter is Swi.numPriorities - 1; i.e.,
   454         *  the maximum Swi priority.
   455         *
   456         *  @see ti.sysbios.knl.Swi#numPriorities
   457         */
   458        metaonly config UInt swiPriority;
   459    
   460        /*!
   461         *  ======== tickPeriod ========
   462         *  Tick period specified in microseconds
   463         *
   464         *  Default value is family dependent. For example, Linux systems often
   465         *  only support a minimum period of 10000 us and multiples of 10000 us.
   466         *  TI platforms have a default of 1000 us.
   467         *
   468         *  Like most other module configuration parameters, the Clock.tickPeriod
   469         *  config parameter value is accessible in runtime C code as
   470         *  "Clock_tickPeriod".
   471         */
   472        config UInt32 tickPeriod;
   473    
   474        /*!
   475         *  @_nodoc
   476         *  ======== stopCheckNext ========
   477         *  Boolean to control whether a check is made upon each Clock_stop() call
   478         *  to determine if the Clock object being stopped is due to timeout on the
   479         *  next scheduled tick.  If this feature is enabled, and the timeout
   480         *  coincides with the next scheduled tick, then a special 'trigger' Clock
   481         *  will be started to force a reschedule of the next tick, as soon as
   482         *  possible. This feature is only applicable for Clock.TickMode_DYNAMIC.
   483         *
   484         *  For most use cases it is most efficient to simply stop
   485         *  a Clock object, and then let the next scheduled tick occur naturally.
   486         *  But some low power application use cases (that routinely stop the next
   487         *  expiring Clock object) can benefit by scheduling an immediate tick, to
   488         *  suppress the next scheduled tick.  The default value for most
   489         *  targets is 'false', for cc26xx/cc13xx it is 'true'.  The default is
   490         *  established in Clock.xs, if the application has not explicitly
   491         *  specified a value.
   492         */
   493        metaonly config Bool stopCheckNext;
   494    
   495        /*!
   496         *  ======== getTicks ========
   497         *  Time in Clock ticks
   498         *
   499         *  The value returned will wrap back to zero after it reaches the max
   500         *  value that can be stored in 32 bits.
   501         *
   502         *  @b(returns)     time in clock ticks
   503         */
   504        UInt32 getTicks();
   505    
   506        /*!
   507         *  @_nodoc
   508         *  ======== getTimerHandle ========
   509         *  Get timer Handle
   510         *
   511         *  Used when it is necessary to change family
   512         *  specific options for the timer and its Hwi Object.
   513         *
   514         *  @b(returns)     Timer Handle
   515         */
   516        TimerProxy.Handle getTimerHandle();
   517    
   518        /*!
   519         *  @_nodoc
   520         *  ======== setTicks ========
   521         *  Set the internal Clock tick counter
   522         *
   523         *  Used internally by Power modules.
   524         */
   525        Void setTicks(UInt32 ticks);
   526    
   527        /*!
   528         *  ======== tickStop ========
   529         *  Stop clock for reconfiguration
   530         *
   531         *  This function is used to stop the timer used for generation of
   532         *  clock ticks. It is used along with Clock_tickStart() and
   533         *  Clock_tickReconfig() to allow reconfiguration of timer at runtime.
   534         *
   535         *  Stopping the timer may not be supported for some types of timers, and
   536         *  is not supported for Clock.TickMode_DYNAMIC; in these cases, this
   537         *  this function call will have no effect.
   538         *
   539         *  @a(constraints)
   540         *  This function is non-reentrant and appropriate locks must be used to
   541         *  protect against  re-entrancy.
   542         */
   543        Void tickStop();
   544    
   545        /*!
   546         *  ======== tickReconfig ========
   547         *  Reconfigure clock for new cpu frequency
   548         *
   549         *  This function uses the new cpu frequency to reconfigure the timer used
   550         *  for generation of clock ticks such that tick period is
   551         *  accurate.  This function is used along with Clock_tickStop() and
   552         *  Clock_tickStart() to allow reconfiguration of timer at runtime.
   553         *
   554         *  Reconfiguration may not be supported for some types of timers, and is
   555         *  not supported for Clock.TickMode_DYNAMIC; in these cases, this
   556         *  this function call will have no effect, and will return false.
   557         *
   558         *  When calling Clock_tickReconfig outside of main(), you must also call
   559         *  Clock_tickStop and Clock_tickStart to stop and restart the timer.
   560         *  Use the following call sequence:
   561         *
   562         *  @p(code)
   563         *  // disable interrupts if an interrupt could lead to
   564         *  // another call to Clock_tickReconfig or if interrupt
   565         *  // processing relies on having a running timer
   566         *  Hwi_disable() or Swi_disable();
   567         *  BIOS_setCpuFreq(&freq);
   568         *  Clock_tickStop();
   569         *  Clock_tickReconfig();
   570         *  Clock_tickStart();
   571         *  Hwi_restore() or Swi_enable()
   572         *  @p
   573         *
   574         *  When calling Clock_tickReconfig from main(), the timer has not yet
   575         *  been started because the timer is started as part of BIOS_start().
   576         *  As a result, you can use the following simplified call sequence
   577         *  in main():
   578         *
   579         *  @p(code)
   580         *  BIOS_setCpuFrequency(Types.FreqHz *freq);
   581         *  Clock_tickReconfig(Void);
   582         *  @p
   583         *
   584         *  The return value is false if the timer cannot support the new
   585         *  frequency
   586         *
   587         *  @b(returns)     true if successful
   588         *
   589         *  @a(constraints)
   590         *  This function is non-reentrant and appropriate locks must be used to
   591         *  protect against  re-entrancy.
   592         */
   593        Bool tickReconfig();
   594    
   595        /*!
   596         *  ======== tickStart ========
   597         *  Start clock after reconfiguration
   598         *
   599         *  This function starts the timer used for generation of clock ticks
   600         *  It is used along with Clock_tickStop() and Clock_tickReconfig() to
   601         *  allow reconfiguration of timer at runtime. The new timer configuration
   602         *  reflects changes caused by a call to reconfig().
   603         *
   604         *  Reconfiguration and restart of a timer may not be supported for some
   605         *  types of timers, and is not supported for Clock.TickMode_DYNAMIC; in
   606         *  these cases, this function call will have no effect.
   607         *
   608         *  @a(constraints)
   609         *  This function is non-reentrant and appropriate locks must be used to
   610         *  protect against  re-entrancy.
   611         */
   612        Void tickStart();
   613    
   614        /*!
   615         *  ======== tick ========
   616         *  Advance Clock time by one tick
   617         *
   618         *  After incrementing a global tick counter, this function posts a Swi
   619         *  that processes the clock instances.
   620         *
   621         *  This function is automatically called by a timer ISR when
   622         *  {@link #tickSource} is set to {@link #TickSource_TIMER}.
   623         *
   624         *  When {@link #tickSource} is set to
   625         *  {@link #TickSource_USER}, Clock_tick() must be called by the
   626         *  application.  Usually, this is done within a user defined {@link ti.sysbios.hal.Hwi Hwi},
   627         *  {@link Swi}, or {@link Task}.
   628         *
   629         *  Note that this function is not re-entrant.  The application is
   630         *  responsible for ensuring that invocations of this function are
   631         *  serialized: either only one thread in the system ever calls this
   632         *  function or all calls are "wrapped" by an appropriate mutex.
   633         *
   634         *  @see #tickSource
   635         */
   636        Void tick();
   637    
   638        /*!
   639         *  @_nodoc
   640         *  ======== workFunc ========
   641         *  Clock Q service routine
   642         *
   643         *  @param(arg0)    Unused. required to match Swi.FuncPtr
   644         *  @param(arg1)    Unused. required to match Swi.FuncPtr
   645         */
   646        Void workFunc(UArg arg0, UArg arg1);
   647    
   648        /*!
   649         *  @_nodoc
   650         *  ======== workFuncDynamic ========
   651         *  Clock Q service routine for TickMode_DYNAMIC
   652         *
   653         *  @param(arg0)    Unused. required to match Swi.FuncPtr
   654         *  @param(arg1)    Unused. required to match Swi.FuncPtr
   655         */
   656        Void workFuncDynamic(UArg arg0, UArg arg1);
   657    
   658        /*!
   659         *  @_nodoc
   660         *  ======= logTick ========
   661         *  Log the LD_tick from within Clock module scope
   662         */
   663        Void logTick();
   664    
   665        /*!
   666         *  @_nodoc
   667         *  ======== getCompletedTicks ========
   668         *  Get the number of Clock ticks that have completed
   669         *
   670         *  Returns the number of ticks completed, to the point where
   671         *  the underlying Timer interrupt has been serviced.
   672         *
   673         *  Used by some TimestampProviders
   674         *
   675         *  @b(returns)     time in clock ticks
   676         */
   677        UInt32 getCompletedTicks();
   678    
   679        /*!
   680         *  @_nodoc
   681         *  ======== getTickPeriod ========
   682         *  Get the Clock tick period in timer counts
   683         *
   684         *  The period is in units returned by the underlying Timer.
   685         *
   686         *  Used by some TimestampProviders
   687         *
   688         *  @b(returns)     period in timer counts
   689         */
   690        UInt32 getTickPeriod();
   691    
   692        /*!
   693         *  @_nodoc
   694         *  ======== getTicksUntilInterrupt ========
   695         *  Get the number of Clock tick periods expected to expire between now
   696         *  and the next interrupt from the timer peripheral
   697         *
   698         *  Used internally by Power modules.
   699         *
   700         *  @b(returns)     count in ticks
   701         */
   702        UInt32 getTicksUntilInterrupt();
   703    
   704        /*!
   705         *  @_nodoc
   706         *  ======== getTicksUntilTimeout ========
   707         *  Get the number of Clock tick periods between now and the next
   708         *  active Clock object timeout.
   709         *
   710         *  Used internally by Power modules.
   711         *
   712         *  @a(constraints)
   713         *  Must be called with interrupts disabled.  Only applicable for
   714         *  Clock.TickSource_TIMER.
   715         *
   716         *  @b(returns)     count in ticks
   717         */
   718        UInt32 getTicksUntilTimeout();
   719    
   720        /*!
   721         *  @_nodoc
   722         *  ======= walkQueueDynamic ========
   723         *  Walk Clock's work queue for TickMode_DYNAMIC
   724         */
   725        UInt32 walkQueueDynamic(Bool service, UInt32 tick);
   726    
   727        /*!
   728         *  @_nodoc
   729         *  ======= walkQueuePeriodic ========
   730         *  Walk Clock's work queue for TickMode_PERIODIC
   731         */
   732        UInt32 walkQueuePeriodic();
   733    
   734        /*!
   735         *  @_nodoc
   736         *  ======= scheduleNextTick ========
   737         *  Reprogram Clock's Timer for earliest required tick
   738         */
   739        Void scheduleNextTick(UInt32 deltaTicks, UInt32 absTick);
   740    
   741    instance:
   742    
   743        /*!
   744         *  ======== create ========
   745         *  Creates a Clock Instance
   746         *
   747         *  The first argument is the function that gets called when the timeout
   748         *  expires.
   749         *
   750         *  The 'timeout' argument is used to specify the initial timeout
   751         *  for both one-shot and periodic Clock instances (in Clock ticks).
   752         *
   753         *  The {@link #period} parameter is used to set the subsequent timeout
   754         *  interval (in Clock ticks) for periodic instances.
   755         *
   756         *  For one-shot instances, the period parameter must be set to zero.
   757         *
   758         *  When instances are created they are placed upon a linked list managed
   759         *  by the Clock module.  For this reason, instances cannot be created
   760         *  from either Hwi or Swi context.
   761         *
   762         *  By default, all Clock functions run in the context of a Swi.
   763         *  That is, the Clock module automatically creates a Swi for
   764         *  its use and runs the Clock functions within that Swi. 
   765         *  The priority of the Swi used by Clock can be changed
   766         *  by configuring {@link #swiPriority Clock.swiPriority}.
   767         *  
   768         *  If Swis are disabled in an application
   769         *  (ie {@link ti.sysbios.BIOS#swiEnabled BIOS.swiEnabled} = false),
   770         *  then all Clock functions are executed within the context of
   771         *  a Timer Hwi. 
   772         *  
   773         *  @a(constraint)
   774         *  @p(blist)
   775         *  As Clock functions execute in either a Swi or Hwi context, they
   776         *  are not permitted to call blocking APIs.
   777         *  @p
   778         *  @a
   779         *
   780         *  @param(clockFxn)  Function that runs upon timeout
   781         *  @param(timeout)   One-shot timeout or initial start delay (in clock
   782         *                    ticks)
   783         */
   784        create(FuncPtr clockFxn, UInt timeout);
   785    
   786        /*!
   787         *  ======== startFlag ========
   788         *  Start immediately after instance is created
   789         *
   790         *  When this flag is set to false, the user will have to call
   791         *  Clock_start() to start the instance.
   792         *
   793         *  When set to true, both statically created Clock objects and Clock
   794         *  objects created in main() are started at the end of main() when the
   795         *  user calls BIOS_start(). Dynamically created Clock objects created
   796         *  after main() (ie within a task) will be started immediately.
   797         *
   798         *  The default setting for this parameter is false.
   799         *
   800         *  The configured Clock function will be called initially after an
   801         *  interval equal to the 'timeout' argument for both one-shot and
   802         *  periodic Clock objects.
   803         *
   804         *  Periodic Clock objects will subsequently be called at the rate
   805         *  specified by the {@link #period} parameter.
   806         *
   807         */
   808        config Bool startFlag = false;
   809    
   810        /*!
   811         *  ======== period ========
   812         *  Period of this instance (in clock ticks)
   813         *
   814         *  The default value of this parameter is 0, which indicates this is
   815         *  a one-shot Clock object.
   816         *
   817         *  A non zero value for this parameter specifies that the Clock
   818         *  object is to be called periodically, and also specifies the
   819         *  rate (in Clock ticks) that the Clock function will be called
   820         *  AFTER the initial 'timeout' argument period.
   821         *
   822         *  For one-shot Clock instances, this parameter must be set to zero.
   823         */
   824        config UInt32 period = 0;
   825    
   826        /*!
   827         *  ======== arg ========
   828         *  Uninterpreted argument passed to instance function
   829         *
   830         *  The default is null.
   831         */
   832        config UArg arg = null;
   833    
   834        /*!
   835         *  @_nodoc
   836         *  ======== addI ========
   837         *  Lightweight One-Shot Clock create for internal SYS/BIOS timeout APIs
   838         *  Does NOT start the timeout (ie requires Clock_startI() to be called)
   839         *  Does NOT assume Hwis are disabled
   840         */
   841        Void addI(FuncPtr clockFxn, UInt32 timeout, UArg arg);
   842    
   843        /*!
   844         *  @_nodoc
   845         *  ======== removeI ========
   846         *  Lightweight Clock delete for internal SYS/BIOS timeout APIs
   847         *  Assumes Hwis are disabled
   848         */
   849        Void removeI();
   850    
   851        /*!
   852         *  ======== start ========
   853         *  Start instance
   854         *
   855         *  The {@link #timeout} and {@link #period} values set during create()
   856         *  or by calling Clock_setTimeout() and Clock_setPeriod() are used and
   857         *  the expiry is recomputed.
   858         *  Note that for periodic instances, the first expiry is
   859         *  computed using the timeout specified. All subsequent expiries use the
   860         *  period value.
   861         *
   862         *  @a(constraints)
   863         *  Timeout of instance cannot be zero
   864         */
   865        Void start();
   866    
   867        /*!
   868         *  @_nodoc
   869         *  ======== startI ========
   870         *  Internal start function which assumes Hwis disabled
   871         */
   872        Void startI();
   873    
   874        /*!
   875         *  ======== stop ========
   876         *  Stop instance
   877         */
   878        Void stop();
   879    
   880        /*!
   881         *  ======== setPeriod ========
   882         *  Set periodic interval
   883         *
   884         *  @param(period)          periodic interval in Clock ticks
   885         *
   886         *  @a(constraints)
   887         *  Cannot change period of instance that has been started.
   888         */
   889        Void setPeriod(UInt32 period);
   890    
   891        /*!
   892         *  ======== setTimeout ========
   893         *  Set the initial timeout
   894         *
   895         *  @param(timeout)         initial timeout in Clock ticks
   896         *
   897         *  @a(constraints)
   898         *  Cannot change the initial timeout of instance that has been started.
   899         */
   900        Void setTimeout(UInt32 timeout);
   901    
   902        /*!
   903         *  ======== setFunc ========
   904         *  Overwrite Clock function and arg
   905         *
   906         *  Replaces a Clock object's clockFxn function originally
   907         *  provided in {@link #create}.
   908         *
   909         *  @param(clockFxn)        function of type FuncPtr
   910         *  @param(arg)             argument to clockFxn
   911         *
   912         *  @a(constraints)
   913         *  Cannot change function and arg of Clock object that has been started.
   914         */
   915        Void setFunc(FuncPtr fxn, UArg arg);
   916    
   917        /*!
   918         *  ======== getPeriod ========
   919         *  Get period of instance
   920         *
   921         *  Returns the period of an instance.
   922         *
   923         *  @b(returns)             returns periodic interval in Clock ticks
   924         */
   925        UInt32 getPeriod();
   926    
   927        /*!
   928         *  ======== getTimeout ========
   929         *  Get timeout of instance
   930         *
   931         *  Returns the remaining time if instance has been started.
   932         *
   933         *  @b(returns)             returns timeout in clock ticks
   934         */
   935        UInt32 getTimeout();
   936    
   937        /*!
   938         *  ======== isActive ========
   939         *  Determine if Clock object is currently active (ie running)
   940         *
   941         *  Returns TRUE if Clock object is currently active
   942         *
   943         *  @b(returns)             returns active state
   944         */
   945        Bool isActive();
   946    
   947    internal:
   948    
   949        /*
   950         * ======== timerSupportsDynamic ========
   951         * used in Clock.xml to enable/disable tickMode setting
   952         */
   953        metaonly config Bool timerSupportsDynamic = false;
   954    
   955        /*
   956         *  ======== doTickFunc =======
   957         *  access doTick through a func ptr so that
   958         *  ROM'd BIOS code doesn't reference a generated function.
   959         */
   960        config Void (*doTickFunc)(UArg);
   961    
   962        /*!
   963         *  ======== doTick ========
   964         *  Function called by the timer interrupt handler
   965         *
   966         *  @param(arg)     Unused. Required to match signature of Hwi.FuncPtr
   967         */
   968        Void doTick(UArg arg);
   969    
   970        /*
   971         *  ======== triggerClock ========
   972         *  Special Clock object created when Clock.stopCheckNext is 'true'.
   973         */
   974        config Clock.Handle triggerClock;
   975    
   976        /*
   977         *  ======== triggerFunc ========
   978         *  Empty function used by Clock.triggerClock
   979         */
   980        Void triggerFunc(UArg arg);
   981    
   982        /*
   983         *  ======== Instance_State ========
   984         */
   985        struct Instance_State {
   986            Queue.Elem      elem;           // required for clock queue
   987            UInt32          timeout;        // in clock ticks
   988            UInt32          currTimeout;    // working timeout
   989            UInt32          period;         // periodic instance if > 0
   990            volatile Bool   active;         // active/idle flag
   991            FuncPtr         fxn;            // instance function
   992            UArg            arg;            // function arg
   993        };
   994    
   995        /*
   996         *  ======== Module_State ========
   997         */
   998        struct Module_State {
   999            volatile UInt32     ticks;          // last tick serviced
  1000            UInt                swiCount;       // num of Swi posts before Swi runs
  1001            TimerProxy.Handle   timer;          // timer used
  1002                                                // points to generated Clock_doTick()
  1003            Queue.Object        clockQ;         // clock que
  1004            Swi.Handle          swi;            // clock swi
  1005            volatile UInt       numTickSkip;    // number of ticks being suppressed
  1006            UInt32              nextScheduledTick;
  1007            UInt32              maxSkippable;   // timer dependent (in tickPeriods)
  1008            Bool                inWorkFunc;     // true if in Clock Swi servicing Q
  1009            Bool                startDuringWorkFunc; // Clock_start during workFunc?
  1010            Bool                ticking;        // set true during first Clock tick
  1011        };
  1012    }