package ti.sysbios.family

Contains family-specific modules for SYS/BIOS

The ti.sysbios.family package contains family-specific implementations of modules in the Hardware Abstraction Layer (HAL) package. [ more ... ]
XDCspec declarations sourced in ti/sysbios/family/package.xdc
 
package ti.sysbios.family [2, 0, 0, 0] {
 
    module Settings;
    // Select the device-specific family modules
}
DETAILS
The ti.sysbios.family package contains family-specific implementations of modules in the Hardware Abstraction Layer (HAL) package.
The SYS/BIOS ti.sysbios.hal package requires target/device-specific API implementations to achieve their functionality. To provide a common set of APIs for these modules across all supported families/devices, SYS/BIOS uses the RTSC proxy-delegate module mechanism. That is, the HAL modules serve as a proxies for a corresponding family-specific module implementation.
The generic HAL APIs are designed to cover the great majority of use cases. If you are concerned with easy portability between different TI devices, you should use the generic HAL APIs as much as possible. However, if the generic APIs cannot enable use of a device-specific hardware feature that is advantageous to the software application, you may choose to use the target/device-specific APIs.
During the configuration step of the application build, the modules in the ti.sysbios.hal package locate and bind themselves to appropriate delegate module implementations based on the current target and platform specified in your config.bld file. The delegate binding process is done internally.
For example, if your config.bld file specifies that one of your build targets is the C64P family, the ti.sysbios.hal.Hwi knows to bind itself to the ti.sysbios.family.c64p.Hwi implementation.
The SYS/BIOS Delegates Usage page lists the delegates available for every target and platform.
generated on Thu, 21 Apr 2016 21:00:26 GMT