TI-RTOS Drivers  tidrivers_tivac_2_16_01_13
EMACSnow.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2014-2015, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
52 #ifndef ti_drivers_emac_EMACSnow__include
53 #define ti_drivers_emac_EMACSnow__include
54 
55 #ifdef __cplusplus
56 extern "C" {
57 #endif
58 
59 #include <stdint.h>
60 #include <ti/sysbios/knl/Swi.h>
61 #define ti_sysbios_family_arm_m3_Hwi__nolocalnames
62 #include <ti/sysbios/family/arm/m3/Hwi.h>
63 
64 #include <ti/drivers/EMAC.h>
65 
66 #ifndef _INCLUDE_NIMU_CODE
67 #define _INCLUDE_NIMU_CODE
68 #endif
69 #include <ti/ndk/inc/stkmain.h>
70 
72 extern const EMAC_FxnTable EMACSnow_fxnTable;
73 
87 typedef struct EMACSnow_HWAttrs {
88  unsigned int baseAddr;
89  unsigned int intNum;
90  unsigned int intPriority;
91  uint8_t *macAddress;
93 
101 typedef struct EMACSnow_Object {
102  Swi_Handle swi;
103  Hwi_Handle hwi;
105 
114 extern void EMACSnow_init(uint32_t index);
115 
123 extern bool EMACSnow_isLinkUp(uint32_t index);
124 
129 extern int EMACSnow_NIMUInit(STKEVENT_Handle hEvent);
130 
131 /* Do not interfere with the app if they include the family Hwi module */
132 #undef ti_sysbios_family_arm_m3_Hwi__nolocalnames
133 
134 #ifdef __cplusplus
135 }
136 #endif
137 
138 #endif /* ti_drivers_emac_EMACSnow__include */
EMACSnow Hardware attributes.
Definition: EMACSnow.h:87
uint8_t * macAddress
Definition: EMACSnow.h:91
EMAC Function table structure.
Definition: EMAC.h:161
unsigned int intPriority
Definition: EMACSnow.h:90
unsigned int baseAddr
Definition: EMACSnow.h:88
struct EMACSnow_Object EMACSnow_Object
EMACSnow Object.
bool EMACSnow_isLinkUp(uint32_t index)
This function sets the EMACSnow driver.
unsigned int intNum
Definition: EMACSnow.h:89
int EMACSnow_NIMUInit(STKEVENT_Handle hEvent)
This function is needed in the NIMUDeviceTable that is required by the NDK.
Hwi_Handle hwi
Definition: EMACSnow.h:103
EMACSnow Object.
Definition: EMACSnow.h:101
Swi_Handle swi
Definition: EMACSnow.h:102
struct EMACSnow_HWAttrs EMACSnow_HWAttrs
EMACSnow Hardware attributes.
void EMACSnow_init(uint32_t index)
This function initializes the EMACSnow driver.
EMAC driver interface.
const EMAC_FxnTable EMACSnow_fxnTable
EMACSnow function table.
Copyright 2016, Texas Instruments Incorporated