TI-RTOS Drivers  tidrivers_tivac_2_16_01_13
Camera.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
101 #ifndef ti_drivers_Camera__include
102 #define ti_drivers_Camera__include
103 
104 #ifdef __cplusplus
105 extern "C" {
106 #endif
107 
108 #include <stdint.h>
109 #include <stddef.h>
110 
128 #define CAMERA_CMD_RESERVED 32
129 
142 #define CAMERA_STATUS_RESERVED -32
143 
157 #define CAMERA_STATUS_SUCCESS 0
158 
165 #define CAMERA_STATUS_ERROR -1
166 
174 #define CAMERA_STATUS_UNDEFINEDCMD -2
175 
185 /* Add Camera_CMD_<commands> here */
186 
194 #define Camera_WAIT_FOREVER ~(0)
195 
199 typedef struct Camera_Config *Camera_Handle;
200 
212 typedef void (*Camera_Callback) (Camera_Handle, void *buf,
213  size_t bufferLength);
214 
221 typedef enum Camera_CaptureMode {
227 
235 
241 typedef enum Camera_HSyncPolarity {
245 
251 typedef enum Camera_VSyncPolarity {
255 
261 typedef enum Camera_PixelClkConfig {
265 
277 typedef enum Camera_ByteOrder {
281 
292 
302 
312 
328 typedef struct Camera_Params {
331 
333  uint32_t outputClock;
334 
337 
340 
343 
346 
349 
352 
355 
357  uint32_t captureTimeout;
358 
361 
363  uintptr_t custom;
364 } Camera_Params;
365 
370 typedef void (*Camera_CloseFxn) (Camera_Handle handle);
371 
376 typedef int (*Camera_ControlFxn) (Camera_Handle handle,
377  unsigned int cmd,
378  void *arg);
379 
384 typedef void (*Camera_InitFxn) (Camera_Handle handle);
385 
390 typedef Camera_Handle (*Camera_OpenFxn) (Camera_Handle handle,
391  Camera_Params *params);
392 
397 typedef int (*Camera_CaptureFxn) (Camera_Handle handle,
398  void *buffer, size_t bufferlen);
399 
405 typedef struct Camera_FxnTable {
408 
411 
414 
417 
421 
433 typedef struct Camera_Config {
436 
438  void *object;
439 
441  void const *hwAttrs;
442 } Camera_Config;
443 
453 extern void Camera_close(Camera_Handle handle);
454 
492 extern int Camera_control(Camera_Handle handle, uint32_t cmd, void *arg);
493 
502 extern void Camera_init(void);
503 
524 extern Camera_Handle Camera_open(uint32_t index, Camera_Params *params);
525 
545 extern void Camera_Params_init(Camera_Params *params);
546 
569 extern int Camera_capture(Camera_Handle handle, void *buffer, size_t bufferlen);
570 
571 #ifdef __cplusplus
572 }
573 #endif
574 
575 #endif /* ti_drivers_Camera__include */
Camera_CaptureMode captureMode
Definition: Camera.h:330
Definition: Camera.h:226
Camera_IfSynchoronisation interfaceSync
Definition: Camera.h:348
int(* Camera_ControlFxn)(Camera_Handle handle, unsigned int cmd, void *arg)
A function pointer to a driver specific implementation of Camera_control().
Definition: Camera.h:376
Camera_Callback captureCallback
Definition: Camera.h:360
Camera_VSyncPolarity
Camera VSync polarity.
Definition: Camera.h:251
The definition of a Camera function table that contains the required set of functions to control a sp...
Definition: Camera.h:405
Definition: Camera.h:299
void(* Camera_Callback)(Camera_Handle, void *buf, size_t bufferLength)
The definition of a callback function used by the Camera driver when used in Camera_MODE_CALLBACK.
Definition: Camera.h:212
Definition: Camera.h:252
int(* Camera_CaptureFxn)(Camera_Handle handle, void *buffer, size_t bufferlen)
A function pointer to a driver specific implementation of Camera_capture().
Definition: Camera.h:397
Camera_IfSynchoronisation
Camera interface synchoronisation.
Definition: Camera.h:288
Camera_ControlFxn controlFxn
Definition: Camera.h:410
int Camera_control(Camera_Handle handle, uint32_t cmd, void *arg)
Function performs implementation specific features on a given Camera_Handle.
Camera_FxnTable const * fxnTablePtr
Definition: Camera.h:435
Camera_OpenFxn openFxn
Definition: Camera.h:416
Definition: Camera.h:310
Definition: Camera.h:300
Camera_InitFxn initFxn
Definition: Camera.h:413
Definition: Camera.h:289
void Camera_init(void)
Function to initializes the Camera module.
Camera_ByteOrder byteOrder
Definition: Camera.h:345
struct Camera_Config * Camera_Handle
A handle that is returned from a Camera_open() call.
Definition: Camera.h:199
void(* Camera_InitFxn)(Camera_Handle handle)
A function pointer to a driver specific implementation of Camera_init().
Definition: Camera.h:384
Camera_CloseFxn closeFxn
Definition: Camera.h:407
uint32_t outputClock
Definition: Camera.h:333
Camera_ByteOrder
Camera byte order.
Definition: Camera.h:277
Camera_PixelClkConfig
Camera pixel clock configuration.
Definition: Camera.h:261
uint32_t captureTimeout
Definition: Camera.h:357
void Camera_Params_init(Camera_Params *params)
Function to initialize the Camera_Params structure to its defaults.
Camera_StopCaptureConfig
Camera stop capture configuration.
Definition: Camera.h:298
int Camera_capture(Camera_Handle handle, void *buffer, size_t bufferlen)
Function that handles the Camera capture of a frame.
Definition: Camera.h:278
Camera_HSyncPolarity hsyncPolarity
Definition: Camera.h:336
void * object
Definition: Camera.h:438
void(* Camera_CloseFxn)(Camera_Handle handle)
A function pointer to a driver specific implementation of Camera_close().
Definition: Camera.h:370
struct Camera_FxnTable Camera_FxnTable
The definition of a Camera function table that contains the required set of functions to control a sp...
Camera_PixelClkConfig pixelClkConfig
Definition: Camera.h:342
Camera_Handle(* Camera_OpenFxn)(Camera_Handle handle, Camera_Params *params)
A function pointer to a driver specific implementation of Camera_open().
Definition: Camera.h:390
Definition: Camera.h:253
Definition: Camera.h:262
void Camera_close(Camera_Handle handle)
Function to close a Camera peripheral specified by the Camera handle.
Definition: Camera.h:290
Definition: Camera.h:243
struct Camera_Config Camera_Config
Camera Global configuration.
uintptr_t custom
Definition: Camera.h:363
Definition: Camera.h:242
Definition: Camera.h:263
Camera_CaptureFxn captureFxn
Definition: Camera.h:419
Camera_VSyncPolarity vsyncPolarity
Definition: Camera.h:339
void const * hwAttrs
Definition: Camera.h:441
Camera_CaptureMode
Camera capture mode settings.
Definition: Camera.h:221
Camera Global configuration.
Definition: Camera.h:433
Definition: Camera.h:233
struct Camera_Params Camera_Params
Camera Parameters.
Camera Parameters.
Definition: Camera.h:328
Camera_StartCaptureConfig
Camera start capture configuration.
Definition: Camera.h:308
Camera_StopCaptureConfig stopConfig
Definition: Camera.h:351
Definition: Camera.h:309
Camera_StartCaptureConfig startConfig
Definition: Camera.h:354
Definition: Camera.h:279
Camera_Handle Camera_open(uint32_t index, Camera_Params *params)
Function to initialize a given Camera peripheral specified by the particular index value...
Camera_HSyncPolarity
Camera HSync polarity.
Definition: Camera.h:241
Copyright 2016, Texas Instruments Incorporated