50 #ifndef ti_drivers_i2c_I2CMSP432__include
51 #define ti_drivers_i2c_I2CMSP432__include
I2C_Transaction * currentTransaction
Definition: I2CMSP432.h:156
Definition: I2CMSP432.h:104
I2CMSP432 Object.
Definition: I2CMSP432.h:150
uint32_t baseAddr
Definition: I2CMSP432.h:139
volatile I2CMSP432_Mode mode
Definition: I2CMSP432.h:172
void(* I2C_CallbackFxn)(I2C_Handle, I2C_Transaction *, bool)
I2C callback function.
Definition: I2C.h:268
I2CMSP432 Hardware attributes These fields, with the exception of intPriority, are used by driverlib ...
Definition: I2CMSP432.h:138
I2CMSP432_Mode
I2CMSP432 mode.
Definition: I2CMSP432.h:102
SemaphoreP_Handle transferComplete
Definition: I2CMSP432.h:152
I2C_BitRate
I2C bitRate.
Definition: I2C.h:276
Definition: I2CMSP432.h:106
const I2C_FxnTable I2CMSP432_fxnTable
I2C_CallbackFxn transferCallbackFxn
Definition: I2CMSP432.h:157
uint8_t * readBufIdx
Definition: I2CMSP432.h:166
struct I2CMSP432_Object I2CMSP432_Object
I2CMSP432 Object.
I2C_TransferMode
I2C transfer mode.
Definition: I2C.h:250
uint32_t intPriority
Definition: I2CMSP432.h:141
void * SemaphoreP_Handle
Opaque client reference to an instance of a SemaphoreP.
Definition: SemaphoreP.h:96
Semaphore module for the RTOS Porting Interface.
The definition of a I2C function table that contains the required set of functions to control a speci...
Definition: I2C.h:348
I2C_Transaction * tailPtr
Definition: I2CMSP432.h:161
Definition: I2CMSP432.h:105
SemaphoreP_Handle mutex
Definition: I2CMSP432.h:151
struct I2CMSP432_HWAttrs I2CMSP432_HWAttrs
I2CMSP432 Hardware attributes These fields, with the exception of intPriority, are used by driverlib ...
size_t readCountIdx
Definition: I2CMSP432.h:167
I2C_BitRate bitRate
Definition: I2CMSP432.h:174
Power notify object structure.
Definition: Power.h:112
uint32_t intNum
Definition: I2CMSP432.h:140
I2C_Transaction * headPtr
Definition: I2CMSP432.h:160
Power_NotifyObj perfChangeNotify
Definition: I2CMSP432.h:169
uint8_t * writeBufIdx
Definition: I2CMSP432.h:163
size_t writeCountIdx
Definition: I2CMSP432.h:164
uint32_t perfConstraintMask
Definition: I2CMSP432.h:170
I2C_TransferMode transferMode
Definition: I2CMSP432.h:173
bool isOpen
Definition: I2CMSP432.h:175
void * HwiP_Handle
Opaque client reference to an instance of a HwiP.
Definition: HwiP.h:66
uint8_t clockSource
Definition: I2CMSP432.h:142
I2C transaction.
Definition: I2C.h:230
Hardware Interrupt module for the RTOS Porting Interface.
Definition: I2CMSP432.h:103
HwiP_Handle hwiHandle
Definition: I2CMSP432.h:154