|
|
|
TI-Drivers is a software component that includes device drivers for the assorted peripherals on a given device (i.e., UART, SPI, I2C, etc.).
These device drivers are also included in the TI-RTOS product. They are provided here as a separate component so that they can be used as a stand-alone library in non-TI-RTOS environments. To avoid duplication, TI-RTOS includes this versioned component in the tirtos/products directory.
The following documentation is provided with this release.
License and manifest.
Release notes from previous releases are also available in the release notes archive directory.
| Key | Summary |
|---|---|
| TIDRIVERS-181 | crypto API is stuck at forever loop |
| TIDRIVERS-184 | Incorrect RAT timer count after waking up from RF_yield() |
| TIDRIVERS-191 | RCOSC_HF calibration check should have hysteresis to avoid likelihood of 2 TDC measurements |
| TIDRIVERS-193 | Posting Commands Rapidly When Using nInactivityTimeout of Zero Causes Hang |
| TIDRIVERS-264 | Add WCSP board file |
| TIDRIVERS-308 | Sometimes RF_postCmd() gets stuck |
| TIDRIVERS-314 | Radio failed to wake up after 40 to 80 minutes |
| TIDRIVERS-317 | Improperly power down in RF_yield() while current command is not completed |
| TIDRIVERS-324 | Call to RF_getCurrentTime Can Cause a System Fault and Hang |
| TIDRIVERS-335 | DisplayDogm1286 returns handle on open when SPI fails to open |
| TIDRIVERS-337 | Radio driver failed to wakeup in TIMAC beacon mode |
| TIDRIVERS-338 | TIMAC assert on “RAT negative channel” on beacon mode coordinator or end device |
| TIDRIVERS-340 | BLE Advertising Appears to Stop Working When PM Is Used |
| TIDRIVERS-349 | g_hwiInt in crypto API should be declared as volatile |
| TIDRIVERS-354 | RTRIM from FCFG or override list |
| TIDRIVERS-359 | RAT timer callback is missing sometimes |
| TIDRIVERS-362 | LMAC TX stuck during the ASYNC message |
| TIDRIVERS-364 | BLE PM Timing Problem When Using CCS |
| TIDRIVERS-365 | PDM streaming test with full heap only works w/o optimisations in CCS |
| TIDRIVERS-373 | Incorrect RAT timer count after waking up from RF_yield |
| TIDRIVERS-382 | Change request to support switching between hardware and software based SSI chip select handling on the fly |
| TIDRIVERS-383 | Bug in SPICC26XXDMA SSI Driver breaks hardware chip handling in given scenarios |
| TIDRIVERS-401 | CC1350LP board file needs update |
| TIDRIVERS-404 | PDM driver decimationFilterInRAM too big |
| TIDRIVERS-412 | Warnings in SensorI2C.c |
Supported Operating Systems:
This release requires the following software components and tools versions to successfully function:
This release was validated using the following components:
All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, alpha/EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 6.30.00.00-eng or 6.30.00.10-beta).
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and bb is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory.
Subsequent releases of patch upgrades will be identified by the patch number. Typically, these patches only include critical bug fixes.
Last updated: April 21, 2016 Build Ver: 2.16.01.13