1 /*
2 * Copyright (c) 2015-2016, Texas Instruments Incorporated
3 * All rights reserved.
4 *
5 * Redistribution and use in source and binary forms, with or without
6 * modification, are permitted provided that the following conditions
7 * are met:
8 *
9 * * Redistributions of source code must retain the above copyright
10 * notice, this list of conditions and the following disclaimer.
11 *
12 * * Redistributions in binary form must reproduce the above copyright
13 * notice, this list of conditions and the following disclaimer in the
14 * documentation and/or other materials provided with the distribution.
15 *
16 * * Neither the name of Texas Instruments Incorporated nor the names of
17 * its contributors may be used to endorse or promote products derived
18 * from this software without specific prior written permission.
19 *
20 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31 */
32 /*
33 * ======== BIOS.xdc ========
34 *
35 */
36
37 package ti.sysbios;
38
39 import xdc.rov.ViewInfo;
40
41 import xdc.runtime.Error;
42 import xdc.runtime.Types;
43
44 /*! ======== BIOS ========
45 * SYS/BIOS Top-Level Manager
46 *
47 * This module is responsible for setting up global parameters
48 * pertaining to SYS/BIOS and for performing the SYS/BIOS startup
49 * sequence.
50 *
51 * SYS/BIOS configures the
52 * {@link xdc.runtime.Memory#defaultHeapInstance Memory.defaultHeapInstance}
53 * using a {@link ti.sysbios.heaps.HeapMem HeapMem} instance of size
54 * {@link #heapSize}.
55 *
56 * The SYS/BIOS startup sequence is logically divided into two phases: those
57 * operations that occur prior to the application's "main()" function being
58 * called, and those operations that are performed after the application's
59 * "main()" function is invoked.
60 *
61 * The "before main()" startup sequence is governed completely by the RTSC
62 * runtime package's {@link xdc.runtime.Startup Startup} module.
63 *
64 * The "after main()" startup sequence is governed by SYS/BIOS and is
65 * initiated by an explicit call to the {@link #start BIOS_start()} function
66 * at the end of the application's main() function.
67 *
68 * Control points are provided at various places in each of the two startup
69 * sequences for user startup operations to be inserted.
70 *
71 * The RTSC runtime startup sequence is as follows:
72 *
73 * @p(nlist) 74 * - Immediately after CPU reset, perform target-specific CPU
75 * initialization (beginning at c_int00).
76 * - Prior to cinit(), run the user-supplied "reset functions"
77 * (see {@link xdc.runtime.Reset#fxns Reset.fxns}).
78 * - Run cinit() to initialize C runtime environment.
79 * - Run the user-supplied "first functions"
80 * (see {@link xdc.runtime.Startup#firstFxns Startup.firstFxns}).
81 * - Run all the module initialization functions.
82 * - Run pinit().
83 * - Run the user-supplied "last functions"
84 * (see {@link xdc.runtime.Startup#lastFxns Startup.lastFxns}).
85 * - Run main().
86 * @p 87 *
88 * The SYS/BIOS startup sequence begins at the end of main() when
89 * BIOS_start() is called:
90 *
91 * @p(nlist) 92 * - Run the user-supplied "startup functions"
93 * (see {@link #startupFxns BIOS.startupFxns}).
94 * - Enable Hardware Interrupts.
95 * - Enable Software Interrupts. If the system supports Software Interrupts
96 * (Swis) (see {@link #swiEnabled BIOS.swiEnabled}), then the SYS/BIOS
97 * startup sequence enables Swis at this point.
98 * - Timer Startup. If the system supports Timers, then at this point all
99 * statically configured timers are initialized per their
100 * user-configuration.
101 * If a timer was configured to start "automatically", it is started here.
102 * - Task Startup. If the system supports Tasks
103 * (see {@link #taskEnabled BIOS.taskEnabled}),
104 * then task scheduling begins here. If there are no statically or
105 * dynamically created Tasks in the system, then execution proceeds
106 * directly to the Idle loop.
107 * @p 108 *
109 * @a(Note) 110 * Local variables defined in main() no longer exist once BIOS_start() is
111 * called. The RAM where main's local variables reside is reassigned for
112 * use as the interrupt stack during the execution of BIOS_start().
113 *
114 * Below is a configuration script excerpt that installs a user-supplied
115 * startup function at every possible control point in the RTSC and
116 * SYS/BIOS startup
117 * sequence:
118 *
119 * @p(code) 120 * // get handle to xdc Startup module
121 * var Startup = xdc.useModule('xdc.runtime.Startup');
122 *
123 * // install "reset function"
124 * Startup.resetFxn = '&myReset';
125 *
126 * // install a "first function"
127 * var len = Startup.firstFxns.length
128 * Startup.firstFxns.length++;
129 * Startup.firstFxns[len] = '&myFirst';
130 *
131 * // install a "last function"
132 * var len = Startup.lastFxns.length
133 * Startup.lastFxns.length++;
134 * Startup.lastFxns[len] = '&myLast';
135 *
136 * // get handle to SYS/BIOS module
137 * var BIOS = xdc.useModule('ti.sysbios.BIOS');
138 *
139 * // install a SYS/BIOS startup function
140 * BIOS.addUserStartupFunction('&myBiosStartup');
141 * @p 142 *
143 * @p(html) 144 * <h3> Calling Context </h3>
145 * <table border="1" cellpadding="3">
146 * <colgroup span="1"></colgroup> <colgroup span="5" align="center">
147 * </colgroup>
148 *
149 * <tr><th> Function </th><th> Hwi </th><th> Swi </th>
150 * <th> Task </th><th> Main </th><th> Startup </th></tr>
151 * <!-- -->
152 * <tr><td> {@link #getCpuFreq} </td><td> Y </td><td> Y </td>
153 * <td> Y </td><td> Y </td><td> Y </td></tr>
154 * <tr><td> {@link #getThreadType} </td><td> Y </td><td> Y </td>
155 * <td> Y </td><td> Y </td><td> N </td></tr>
156 * <tr><td> {@link #setCpuFreq} </td><td> Y </td><td> Y </td>
157 * <td> Y </td><td> Y </td><td> Y </td></tr>
158 * <tr><td> {@link #start} </td><td> N </td><td> N </td>
159 * <td> N </td><td> Y </td><td> N </td></tr>
160 * <tr><td colspan="6"> Definitions: <br />
161 * <ul>
162 * <li> <b>Hwi</b>: API is callable from a Hwi thread. </li>
163 * <li> <b>Swi</b>: API is callable from a Swi thread. </li>
164 * <li> <b>Task</b>: API is callable from a Task thread. </li>
165 * <li> <b>Main</b>: API is callable during any of these phases: </li>
166 * <ul>
167 * <li> In your module startup after this module is started
168 * (e.g. BIOS_Module_startupDone() returns TRUE). </li>
169 * <li> During xdc.runtime.Startup.lastFxns. </li>
170 * <li> During main().</li>
171 * <li> During BIOS.startupFxns.</li>
172 * </ul>
173 * <li> <b>Startup</b>: API is callable during any of these phases:</li>
174 * <ul>
175 * <li> During xdc.runtime.Startup.firstFxns.</li>
176 * <li> In your module startup before this module is started
177 * (e.g. BIOS_Module_startupDone() returns FALSE).</li>
178 * </ul>
179 * </ul>
180 * </td></tr>
181 *
182 * </table>
183 * @p 184 */
185
186 @CustomHeader /* to check for codegen compatibility */
187 @Template("./BIOS.xdt")
188
189 @DirectCall
190 module BIOS
191 {
192 /*!
193 * ======== ThreadType ========
194 * Current thread type definitions
195 *
196 * These values are returned by {@link #getThreadType BIOS_getThreadType}.
197 *
198 * @see #getThreadType
199 */
200 enum ThreadType {
201 ThreadType_Hwi, /*! Current thread is a Hwi */
202 ThreadType_Swi, /*! Current thread is a Swi */
203 ThreadType_Task, /*! Current thread is a Task */
204 ThreadType_Main /*! Current thread is Boot/Main */
205 };
206
207 /*!
208 * ======== RtsLockType ========
209 * Type of Gate to use in the TI RTS library
210 *
211 * @field(NoLocking) no gate is added to the RTS library. In this case,
212 * the application needs to be careful to always serialize access to the
213 * inherently non-reentrant ANSI C functions (such as `malloc()`,
214 * `printf()`, etc.).
215 *
216 * @field(GateHwi) Interrupts are disabled and restored to maintain
217 * re-entrancy. This is a very efficient lock but will also result in
218 * unbounded interrupt latency times. If real-time response to interrupts
219 * is important, you should not use this gate to lock the RTS library.
220 *
221 * @field(GateSwi) Swis are disabled and restored to maintain
222 * re-entrancy.
223 *
224 * @field(GateMutex) A single mutex is used to maintain re-entrancy.
225 *
226 * @field(GateMutexPri) A single priority inheriting mutex is used to
227 * maintain re-entrancy.
228 *
229 * @see #rtsGateType
230 */
231 enum RtsLockType {
232 NoLocking,
233 GateHwi,
234 GateSwi,
235 GateMutex,
236 GateMutexPri
237 };
238
239 /*!
240 * ======== LibType ========
241 * SYS/BIOS library selection options
242 *
243 * This enumeration defines all the SYS/BIOS library types
244 * provided by the product. You can select the library type by setting
245 * the {@link #libType BIOS.libType} configuration parameter.
246 *
247 * @field(LibType_Instrumented) The library supplied is prebuilt with
248 * logging and assertions enabled.
249 *
250 * @field(LibType_NonInstrumented) The library supplied is prebuilt
251 * with logging and assertions disabled.
252 *
253 * @field(LibType_Custom) This option builds the
254 * SYS/BIOS library from sources using the options specified by
255 * {@link #customCCOpts}. Only the modules and APIs that your application
256 * needs to access are contained in the resulting executable. Program
257 * optimization is performed to reduce the size of the executable and improve
258 * its performance. Enough debug information is retained to allow you to
259 * step through the application code in CCS and locate global variables.
260 *
261 * @field(LibType_Debug) This option is similar to the LibType_Custom option
262 * in that it builds the SYS/BIOS library from sources and omits modules and
263 * APIs that your code does not use. However, no program
264 * optimization is performed. The resulting executable is fully debuggable,
265 * and you can step into SYS/BIOS code. The tradeoff is that the executable
266 * is larger and runs slower than builds that use the LibType_Custom option.
267 *
268 * @see #libType
269 */
270 enum LibType {
271 LibType_Instrumented, /*! Instrumented (Asserts and Logs enabled) */
272 LibType_NonInstrumented, /*! Non-instrumented (Asserts and Logs disabled) */
273 LibType_Custom, /*! Custom (Fully configurable) */
274 LibType_Debug /*! Debug (Fully configurable) */
275 };
276
277 /*! Used in APIs that take a timeout to specify wait forever */
278 const UInt WAIT_FOREVER = ~(0);
279
280 /*! Used in APIs that take a timeout to specify no waiting */
281 const UInt NO_WAIT = 0;
282
283 /*! User startup function type definition. */
284 typedef Void (*StartupFuncPtr)(Void);
285
286 /*!
287 * ======== ModuleView ========
288 * @_nodoc 289 */
290 metaonlystruct ModuleView {
291 String currentThreadType[];
292 String rtsGateType;
293 Int cpuFreqLow;
294 Int cpuFreqHigh;
295 Bool clockEnabled;
296 Bool swiEnabled;
297 Bool taskEnabled;
298 String startFunc;
299 }
300
301 /*!
302 * ======== ErrorView ========
303 * @_nodoc 304 */
305 metaonlystruct ErrorView {
306 String mod;
307 String tab;
308 String inst;
309 String field;
310 String message;
311 }
312
313 /*!
314 * ======== rovViewInfo ========
315 * @_nodoc 316 */
317 @Facet
318 metaonlyconfig ViewInfo.Instance rovViewInfo =
319 ViewInfo.create({
320 viewMap: [
321 [
322 'Module',
323 {
324 type: ViewInfo.MODULE,
325 viewInitFxn: 'viewInitModule',
326 structName: 'ModuleView'
327 }
328 ],
329 [
330 'Scan for errors...',
331 {
332 type: ViewInfo.MODULE_DATA,
333 viewInitFxn: 'viewInitErrorScan',
334 structName: 'ErrorView'
335 }
336 ],
337 ]
338 });
339
340 /*!
341 * ======== libType ========
342 * SYS/BIOS Library type
343 *
344 * The SYS/BIOS runtime is provided in the form of a library that is
345 * linked with your application. Several forms of this library are
346 * provided with the SYS/BIOS product. In addition, there is an
347 * option to build the library from source. This configuration parameter
348 * allows you to select the form of the SYS/BIOS library to use.
349 *
350 * The default value of libType is
351 * {@link #LibType_Instrumented BIOS_LibType_Instrumented}. For a
352 * complete list of options and what they offer see {@link #LibType}.
353 */
354 metaonlyconfig LibType libType = LibType_Instrumented;
355
356 /*!
357 * ======== customCCOpts ========
358 * Compiler options used when building a custom SYS/BIOS library
359 *
360 * When {@link #libType BIOS.libType} is set to
361 * {@link #LibType_Custom BIOS_LibType_Custom} or
362 * {@link #LibType_Debug BIOS_LibType_Debug},
363 * this string contains the options passed to the compiler during any
364 * re-build of the SYS/BIOS sources.
365 *
366 * In addition to the options
367 * specified by `BIOS.customCCOpts`, several `-D` and `-I` options are also
368 * passed to the compiler. The options specified by `BIOS.customCCOpts` are,
369 * however, the first options passed to the compiler on the command line.
370 *
371 * To view the custom compiler options, add the following line to your
372 * config script:
373 *
374 * @p(code) 375 * print(BIOS.customCCOpts);
376 * @p 377 *
378 * When {@link #libType BIOS.libType} is set to
379 * {@link #LibType_Custom BIOS_LibType_Custom},
380 * `BIOS.customCCOpts` is initialized to settings that create a highly
381 * optimized SYS/BIOS library.
382 *
383 * When {@link #libType BIOS.libType} is set to
384 * {@link #LibType_Debug BIOS_LibType_Debug},
385 * `BIOS.customCCOpts` is initialized to settings that create a non-optimized
386 * SYS/BIOS library that can be used to single-step through the APIs with
387 * the CCS debugger.
388 *
389 * More information about using `BIOS.customCCOpts` is provided in the
390 * {@link https://processors.wiki.ti.com/index.php/SYS/BIOS_FAQs SYS/BIOS FAQs}.
391 *
392 * @a(Warning) 393 * The default value of `BIOS.customCCOpts`, which is derived from the target
394 * specified by your configuration, includes runtime model options
395 * (such as endianess) that must be the same for all sources built and
396 * linked into your application. You must not change or add any options
397 * that can alter the runtime model specified by the default value of
398 * `BIOS.customCCOpts`.
399 */
400 metaonlyconfig String customCCOpts;
401
402 /*!
403 * ======== includeXdcRuntime ========
404 * Include xdc.runtime sources in custom built library
405 *
406 * By default, the xdc.runtime library sources are not included in the
407 * custom SYS/BIOS library created for the application. Instead,
408 * the pre-built xdc.runtime library is provided by the respective target
409 * used to build the application.
410 *
411 * Setting this parameter to true will cause the xdc.runtime library
412 * sources to be included in the custom SYS/BIOS library. This setting
413 * yields the most efficient library in both code size and runtime
414 * performance.
415 */
416 metaonlyconfig Bool includeXdcRuntime = false;
417
418 /*!
419 * ======== smpEnabled ========
420 * Enables multi core SMP task scheduling
421 *
422 * This functionality is available on only select multi-core devices.
423 *
424 * More information about SMP/BIOS is provided here:
425 * {@link https://processors.wiki.ti.com/index.php/SMP/BIOS SMP/BIOS}.
426 */
427 config Bool smpEnabled = false;
428
429 /*!
430 * ======== cpuFreq ========
431 * CPU frequency in Hz
432 *
433 * This configuration parameter allow SYS/BIOS to convert various
434 * periods between timer ticks (or instruction cycles) and real-time
435 * units. For example, timer periods expressed in micro-seconds need
436 * to be converted into timer ticks in order to properly program the
437 * timers.
438 *
439 * The default value of this parameter is obtained from the platform
440 * (the clockRate property of {@link xdc.cfg.Program#cpu Program.cpu})
441 * which is the CPU clock rate when the processor is reset.
442 *
443 * @a(Example) 444 * If CPU frequency is 720MHz, the following configuration script
445 * configures SYS/BIOS with the proper clock frequency:
446 * @p(code) 447 * var BIOS = xdc.useModule('ti.sysbios.BIOS');
448 * BIOS.cpuFreq.hi = 0;
449 * BIOS.cpuFreq.lo = 720000000;
450 * @p 451 */
452 config Types.FreqHz cpuFreq;
453
454 /*!
455 * ======== runtimeCreatesEnabled ========
456 * Runtime instance creation enable flag.
457 *
458 * true = Mod_create() & Mod_delete() callable at runtime
459 * false = Mod_create() & Mod_delete() not callable at runtime
460 */
461 config Bool runtimeCreatesEnabled = true;
462
463 /*!
464 * ======== taskEnabled ========
465 * SYS/BIOS Task services enable flag
466 *
467 * The following behaviors occur when {@link #taskEnabled} is
468 * set to false:
469 *
470 * @p(blist) 471 * - Static {@link ti.sysbios.knl.Task Task} creation will
472 * result in a fatal build error.
473 * - The Idle task object is not created.
474 * (The Idle functions are invoked within the {@link #start()}
475 * thread.)
476 * - Runtime calls to Task_create will trigger an assertion violation
477 * via {@link xdc.runtime.Assert#isTrue}.
478 * @p 479 */
480 config Bool taskEnabled = true;
481
482 /*!
483 * ======== swiEnabled ========
484 * SYS/BIOS Swi services enable flag
485 *
486 * The following behaviors occur when {@link #swiEnabled} is
487 * set to false:
488 *
489 * @p(blist) 490 * - Static {@link ti.sysbios.knl.Swi Swi} creation will
491 * result in a fatal build error.
492 * - See other effects as noted for {@link #clockEnabled} = false;
493 * - Runtime calls to Swi_create will trigger an assertion violation
494 * via {@link xdc.runtime.Assert#isTrue}.
495 * @p 496 */
497 config Bool swiEnabled = true;
498
499 /*!
500 * ======== clockEnabled ========
501 * SYS/BIOS Clock services enable flag
502 *
503 * The following behaviors occur when {@link #clockEnabled} is
504 * set to false:
505 *
506 * @p(blist) 507 * - Static Clock creation will result in a fatal build error.
508 * - No Clock Swi is created.
509 * - The {@link ti.sysbios.knl.Clock#tickSource Clock_tickSource}
510 * is set to
511 * {@link ti.sysbios.knl.Clock#TickSource_NULL Clock_TickSource_NULL}
512 * to prevent a Timer object from being created.
513 * - For APIs that take a timeout, values other than {@link #NO_WAIT}
514 * will be equivalent to {@link #WAIT_FOREVER}.
515 * @p 516 */
517 config Bool clockEnabled = true;
518
519 /*!
520 * ======== assertsEnabled ========
521 * SYS/BIOS Assert checking in Custom SYS/BIOS library enable flag
522 *
523 * When set to true, Assert checking code is compiled into
524 * the custom library created when {@link #libType BIOS.libType}
525 * is set to {@link #LibType_Custom BIOS_LibType_Custom} or
526 * {@link #LibType_Debug BIOS_LibType_Debug}.
527 *
528 * When set to false, Assert checking code is removed from
529 * the custom library created when BIOS.libType is set to BIOS.LibType_Custom
530 * or BIOS.LibType_Debug.
531 * This option can considerably improve runtime performance as well
532 * significantly reduce the application's code size.
533 *
534 * see {@link #libType BIOS.libType}.
535 */
536 metaonlyconfig Bool assertsEnabled = true;
537
538 /*!
539 * ======== logsEnabled ========
540 * SYS/BIOS Log support in Custom SYS/BIOS library enable flag
541 *
542 * When set to true, SYS/BIOS execution Log code is compiled into
543 * the custom library created when {@link #libType BIOS.libType}
544 * is set to {@link #LibType_Custom BIOS_LibType_Custom} or
545 * {@link #LibType_Debug BIOS_LibType_Debug}.
546 *
547 * When set to false, all Log code is removed from
548 * the custom library created when BIOS.libType = BIOS.LibType_Custom
549 * or BIOS.LibType_Debug.
550 * This option can considerably improve runtime performance as well
551 * significantly reduce the application's code size.
552 *
553 * see {@link #libType BIOS.libType}.
554 *
555 * @a(Warning) Since interrupts
556 * are enabled when logs are generated, this setting will have the
557 * side effect of requiring task stacks to be sized large enough
558 * to absorb two interrupt contexts rather than one.
559 * See the discussion on task stacks in {@link ti.sysbios.knl.Task
560 * Task} for more information.
561 */
562 metaonlyconfig Bool logsEnabled = true;
563
564 /*!
565 * ======== heapSize ========
566 * Size of system heap, units are in MAUs
567 *
568 * The system heap is, by default, used to allocate instance object
569 * state structures, such as {@link ti.sysbios.knl.Task Task} objects
570 * and their stacks, {@link ti.sysbios.knl.Semaphore Semaphore} objects,
571 * etc.
572 *
573 * If the application configuration does not set
574 * Memory.defaultHeapInstance, then SYS/BIOS will create a
575 * {@link ti.sysbios.heaps.HeapMem HeapMem} heap of this size. This
576 * heap will be assigned to
577 * {@link xdc.runtime.Memory#defaultHeapInstance Memory.defaultHeapInstance}
578 * and will therefore be used as the default system heap. This heap
579 * will also be used by the SYS/BIOS version of the standard C library
580 * functions malloc(), calloc() and free().
581 */
582 config SizeT heapSize = 0x1000;
583
584 /*!
585 * ======== heapSection ========
586 * Section to place the system heap
587 *
588 * This configuration parameter allows you to specify a named output
589 * section that will contain the SYS/BIOS system heap. The system heap
590 * is, by default, used to allocate {@link ti.sysbios.knl.Task Task}
591 * stacks and instance object state structures. So, giving this section
592 * a name and explicitly placing it via a linker command file can
593 * significantly improve system performance.
594 *
595 * If heapSection is `null` (or `undefined`) the system heap is placed
596 * in the target's default data section.
597 */
598 config String heapSection = null;
599
600 /*!
601 * ======== heapTrackEnabled ========
602 * Use HeapTrack with system default heap
603 *
604 * This configuration parameter will add a HeapTrack instance on top of
605 * the system heap. HeapTrack adds a tracker packet to every allocated
606 * buffer and displays the information in RTOS Object Viewer (ROV).
607 * An assert will be raised on a free if there was a buffer overflow.
608 */
609 config Bool heapTrackEnabled = false;
610
611 /*!
612 * ======== setupSecureContext ========
613 * @_nodoc 614 * Sets up a secure context when using secure version of BIOS
615 *
616 * This is available for some C66 secure devices only.
617 * This parameter take effect only when 'useSK' is set to true.
618 * If set to true, a call to Hwi_setupSC() is done in a last function.
619 */
620 config Bool setupSecureContext = false;
621
622 /*!
623 * ======== useSK ========
624 * @_nodoc 625 * use the secure version of BIOS
626 *
627 * This is available for some C66 secure devices only.
628 * This parameter can only be used with the custom build.
629 */
630 config Bool useSK = false;
631
632 /*!
633 * ======== rtsGateType ========
634 * Gate to make sure TI RTS library APIs are re-entrant
635 *
636 * The application gets to determine the type of gate (lock) that is used
637 * in the TI RTS library. The gate will be used to guarantee re-entrancy
638 * of the RTS APIs.
639 *
640 * The type of gate depends on the type of threads that are going to
641 * be calling into the RTS library. For example, if both Swi and Task
642 * threads are going to be calling the RTS library's printf, GateSwi
643 * should be used. In this case, Hwi threads are not impacted (i.e.
644 * disabled) during the printf calls from the Swi or Task threads.
645 *
646 * If NoLocking is used, the RTS lock is not plugged and re-entrancy for
647 * the TI RTS library calls are not guaranteed. The application can plug
648 * the RTS locks directly if it wants.
649 *
650 * Numerous gate types are provided by SYS/BIOS. Each has its advantages
651 * and disadvantages. The following list summarizes when each type is
652 * appropriate for protecting an underlying non-reentrant RTS library.
653 * @p(dlist) 654 * - {@link #GateHwi}:
655 * Interrupts are disabled and restored to maintain re-entrancy.
656 * Use if only making RTS calls from a Hwi, Swi and/or Task.
657 *
658 * - {@link #GateSwi}:
659 * Swis are disabled and restored to maintain re-entrancy. Use if
660 * only making RTS calls from a Swi and/or Task.
661 *
662 * - {@link #GateMutex}:
663 * A single mutex is used to maintain re-entrancy. Use if only
664 * making RTS calls from a Task. Blocks only Tasks that are
665 * also trying to execute critical regions of RTS library.
666 *
667 * - {@link #GateMutexPri}:
668 * A priority inheriting mutex is used to maintain re-entrancy.
669 * Blocks only Tasks that are also trying to execute critical
670 * regions of RTS library. Raises the priority of the Task that
671 * is executing the critical region in the RTS library to the
672 * level of the highest priority Task that is block by the mutex.
673 * @p 674 *
675 * The default value of rtsGateType depends on the type of threading
676 * model enabled by other configuration parameters.
677 * If {@link #taskEnabled} is true, {@link #GateMutex} is used.
678 * If {@link #swiEnabled} is true and {@link #taskEnabled} is false:
679 * {@link #GateSwi} is used.
680 * If both {@link #swiEnabled} and {@link #taskEnabled} are false:
681 * {@link xdc.runtime#GateNull} is used.
682 *
683 * If {@link #taskEnabled} is false, the user should not select
684 * {@link #GateMutex} (or other Task level gates). Similarly, if
685 * {@link #taskEnabled} and {@link #swiEnabled}are false, the user
686 * should not select {@link #GateSwi} or the Task level gates.
687 */
688 metaonlyconfig RtsLockType rtsGateType;
689
690 /*!
691 * ======== startupFxns ========
692 * Functions to be executed at the beginning of BIOS_start()
693 *
694 * These user (or middleware) functions are executed before Hwis,
695 * Swis, and Tasks are started.
696 */
697 metaonlyconfig StartupFuncPtr startupFxns[] = [];
698
699 /*!
700 * ======== version ========
701 * SYS/BIOS version number macro
702 *
703 * This macro has a hex value that represents the SYS/BIOS version
704 * number. The hex value has the version format 0xMmmpp, where
705 * M is a single digit Major number, mm is a 2 digit minor number
706 * and pp is a 2 digit patch number.
707 *
708 * Example: A macro hex value of 0x64501 implies that the SYS/BIOS
709 * product version number is 6.45.01
710 */
711 const UInt32 version = 0x64502;
712
713 /*!
714 * ======== addUserStartupFunction ========
715 * @_nodoc 716 * Statically add a function to the startupFxns table.
717 */
718 metaonly Void addUserStartupFunction(StartupFuncPtr func);
719
720
721 /*!
722 * ======== start ========
723 * Start SYS/BIOS
724 *
725 * The user's main() function is required to call this function
726 * after all other user initializations have been performed.
727 *
728 * This function does not return.
729 *
730 * This function performs any remaining SYS/BIOS initializations
731 * and then transfers control to the highest priority ready
732 * task if {@link #taskEnabled} is true. If {@link #taskEnabled}
733 * is false, control is transferred directly to the Idle Loop.
734 *
735 * The SYS/BIOS start sequence is as follows:
736 * @p(blist) 737 * - Invoke all the functions in the {@link #startupFxns} array.
738 * - call {@link ti.sysbios.hal.Hwi#enable Hwi_startup()}
739 * to enable interrupts.
740 * - if {@link #swiEnabled} is true, call
741 * {@link ti.sysbios.knl.Swi#enable Swi_startup()} to enable
742 * the Swi scheduler.
743 * - Start any statically created or constructed Timers
744 * in the {@link ti.sysbios.hal.Timer#StartMode Timer_StartMode_AUTO}
745 * mode.
746 * - if {@link #taskEnabled} is true, enable the Task scheduler
747 * and transfer the execution thread to the highest priority
748 * task in the {@link ti.sysbios.knl.Task#Mode Task_Mode_READY}
749 * mode.
750 * - Otherwise, fall directly into the Idle Loop.
751 * @p 752 *
753 */
754 Void start();
755
756 /*!
757 * ======== exit ========
758 * Exit currently running SYS/BIOS executable
759 *
760 * This function is called when a SYS/BIOS executable needs to terminate
761 * normally. This function sets the internal SYS/BIOS threadType to
762 * {@link #ThreadType_Main} and then calls
763 * {@link xdc.runtime.System#exit System_exit}(stat), passing along
764 * the 'stat' argument.
765 *
766 * All functions bound via
767 * `{@link xdc.runtime.System#atexit System_atexit}` or the ANSI C
768 * Standard Library `atexit` function are then executed.
769 *
770 * @param(stat) exit status to return to calling environment.
771 */
772 Void exit(Int stat);
773
774 /*!
775 * ======== getThreadType ========
776 * Get the current thread type
777 *
778 * @b(returns) Current thread type
779 */
780 ThreadType getThreadType();
781
782 /*!
783 * @_nodoc 784 * ======== setThreadType ========
785 * Set the current thread type
786 *
787 * Called by the various threadType owners.
788 *
789 * @param(ttype) New thread type value
790 * @b(returns) Previous thread type
791 */
792 ThreadType setThreadType(ThreadType ttype);
793
794 /*!
795 * ======== setCpuFreq ========
796 * Set CPU Frequency in Hz
797 *
798 * This API is not thread safe. Please use appropriate locks.
799 */
800 Void setCpuFreq(Types.FreqHz *freq);
801
802 /*!
803 * ======== getCpuFreq ========
804 * Get CPU frequency in Hz
805 *
806 * This API is not thread safe. Please use appropriate locks.
807 */
808 Void getCpuFreq(Types.FreqHz *freq);
809
810 /*!
811 * @_nodoc 812 * ======== getCpuFrequency ========
813 * Get CPU frequency in Hz.
814 *
815 * This function is currently used by UIA and is called in the
816 * UIAMetaData validate() function.
817 * NOTE: Javascript does not support UInt64, so this only works
818 * if the frequency is less than 4GHz. Keep this function for
819 * backwards compatibility (for awhile).
820 */
821 metaonly UInt64 getCpuFrequency();
822
823 /*!
824 * @_nodoc 825 * ======== getCpuFreqMeta ========
826 * Get CPU frequency in Hz.
827 *
828 * This function is currently used by UIA and is called in the
829 * UIAMetaData validate() function.
830 */
831 metaonly Types.FreqHz getCpuFreqMeta();
832
833 /*!
834 * @_nodoc 835 * ======== getTimestampFrequency ========
836 * Get timestamp frequency in Hz. If we don't know the timestamp
837 * frequency of the device, return 0.
838 *
839 * This function is currently used by UIA and is called in the
840 * UIAMetaData validate() function.
841 * NOTE: Javascript does not support UInt64, so this only works
842 * if the frequency is less than 4GHz. Keep this function for
843 * backwards compatability (for awhile).
844 */
845 metaonly UInt64 getTimestampFrequency();
846
847 /*!
848 * @_nodoc 849 * ======== getTimestampFreqMeta ========
850 * Get timestamp frequency in Hz. If we don't know the timestamp
851 * frequency of the device, return 0.
852 *
853 * This function is currently used by UIA and is called in the
854 * UIAMetaData validate() function.
855 */
856 metaonly Types.FreqHz getTimestampFreqMeta();
857
858 /*!
859 * @_nodoc 860 * ======== getDefaultTimestampProvider ========
861 * Returns the name of the TimestampProvider module BIOS will set
862 * xdc.runtime.Timestamp.SupportProxy to if it hasn't been configured
863 * in the user's config script.
864 *
865 * This function is meant to be used by modules that have their own
866 * TimestampProvider proxies if they want to initialize them to the
867 * default xdc.runtime.Timestamp.SupportProxy binding selected by BIOS:
868 *
869 * if (!this.$written("TimestampProxy")) {
870 * if (xdc.runtime.$written("Timestamp.SupportProxy") {
871 * this.TimestampProxy = xdc.runtime.Timestamp.SupportProxy;
872 * }
873 * else {
874 * this.TimestampProxy = xdc.module(BIOS.getDefaultTimestampProvider());
875 * }
876 * }
877 */
878 metaonly String getDefaultTimestampProvider();
879
880 internal:
881
882 /*
883 * ======== buildingAppLib ========
884 * Enable custom build of SYS/BIOS from source
885 *
886 * true = building application-specific custom lib
887 * false = building internal instrumented/nonInstrumented lib
888 */
889 metaonlyconfig Bool buildingAppLib = true;
890
891 /*
892 * ======== libDir ========
893 * Specify output library directory
894 */
895 metaonlyconfig String libDir = null;
896
897 /*
898 * ======== getCCOpts ========
899 * Get the compiler options necessary to build
900 */
901 metaonly String getCCOpts(String target);
902
903 /*
904 * ======== intSize ========
905 * Used to determine number of bits in an Int
906 */
907 struct intSize {
908 Int intSize;
909 }
910
911 /*
912 * ======== bitsPerInt ========
913 * Number of bits in an integer
914 *
915 * Used for error checking
916 */
917 metaonlyconfig Char bitsPerInt;
918
919 /*
920 * ======== installedErrorHook ========
921 * User/default Error.raiseHook
922 *
923 * BIOS_errorRaiseHook() calls this after setting threadType
924 * to Main so that GateMutex's threadType check will
925 * pass.
926 */
927 config Void (*installedErrorHook)(Error.Block *);
928
929 /*
930 * ======== errorRaiseHook ========
931 * Error.raiseHook that sets threadType to Main so
932 * threadType checking Asserts will pass.
933 */
934 Void errorRaiseHook(Error.Block *eb);
935
936 /*
937 * ======== startFunc ========
938 * Generated BIOS_start function
939 */
940 Void startFunc();
941
942 /*
943 * ======== atExitFunc ========
944 * Generated BIOS_atExitFunc function
945 */
946 Void atExitFunc(Int stat);
947
948 /*
949 * ======== exitFunc ========
950 * Generated BIOS_exitFunc function
951 */
952 Void exitFunc(Int stat);
953
954 /*
955 * ======== registerRTSLock ========
956 * Register the RTS lock
957 *
958 * Added as a startup function in BIOS.xs.
959 */
960 Void registerRTSLock();
961
962 /*
963 * ======== removeRTSLock ========
964 * Remove the RTS locks
965 *
966 * This function is called by BIOS_exit().
967 */
968 Void removeRTSLock();
969
970 /*
971 * ======== rtsLock ========
972 * Called by rts _lock() function
973 */
974 Void rtsLock();
975
976 /*
977 * ======== rtsUnLock ========
978 * Called by rts _unlock() function
979 */
980 Void rtsUnlock();
981
982 /*
983 * ======== nullFunc ========
984 */
985 Void nullFunc();
986
987 /*
988 * ======== fireFrequencyUpdate ========
989 */
990 function fireFrequencyUpdate(newFreq);
991
992 /*
993 * ======== RtsGateProxy ========
994 * Gate proxy to be used for the rts gate
995 */
996 proxy RtsGateProxy inherits xdc.runtime.IGateProvider;
997
998 /*
999 * ======== StartFuncPtr ========
1000 * Function prototype for the generated BIOS_start
1001 */
1002 typedef Void (*StartFuncPtr)(void);
1003
1004 /*
1005 * ======== ExitFuncPtr ========
1006 * Function prototype for the generated BIOS_exit
1007 */
1008 typedef Void (*ExitFuncPtr)(Int);
1009
1010 /*
1011 * ======== Module_State ========
1012 */
1013 struct Module_State {
1014 Types.FreqHz cpuFreq; /* in KHz */
1015 UInt rtsGateCount; /* count for nesting */
1016 IArg rtsGateKey; /* key for unlocking */
1017 RtsGateProxy.Handle rtsGate; /* gate for RTS calls */
1018 ThreadType threadType; /* Curr Thread Type */
1019 /* (Hwi, Swi, Task) */
1020 ThreadType smpThreadType[]; /* SMP Core specific */
1021 /* Thread Type */
1022 volatile StartFuncPtr startFunc;
1023 volatile ExitFuncPtr exitFunc;
1024 };
1025 }