TI-RTOS Drivers  tidrivers_c2000_2_16_00_08
diskio.h
Go to the documentation of this file.
1 /*-----------------------------------------------------------------------/
2 / Low level disk interface modlue include file (C)ChaN, 2014 /
3 /-----------------------------------------------------------------------*/
4 
5 #ifndef _DISKIO_DEFINED
6 #define _DISKIO_DEFINED
7 
8 #ifdef __cplusplus
9 extern "C" {
10 #endif
11 
12 #define _USE_WRITE 1 /* 1: Enable disk_write function */
13 #define _USE_IOCTL 1 /* 1: Enable disk_ioctl fucntion */
14 
15 #include "integer.h"
16 
17 
18 /* Status of Disk Functions */
19 typedef BYTE DSTATUS;
20 
21 /* Results of Disk Functions */
22 typedef enum {
23  RES_OK = 0, /* 0: Successful */
24  RES_ERROR, /* 1: R/W Error */
25  RES_WRPRT, /* 2: Write Protected */
26  RES_NOTRDY, /* 3: Not Ready */
27  RES_PARERR /* 4: Invalid Parameter */
28 } DRESULT;
29 
30 
31 /*---------------------------------------*/
32 /* Prototypes for disk control functions */
33 
34 
35 DSTATUS disk_initialize (BYTE pdrv);
36 DSTATUS disk_status (BYTE pdrv);
37 DRESULT disk_read (BYTE pdrv, BYTE* buff, DWORD sector, UINT count);
38 DRESULT disk_write (BYTE pdrv, const BYTE* buff, DWORD sector, UINT count);
39 DRESULT disk_ioctl (BYTE pdrv, BYTE cmd, void* buff);
40 
41 
42 /* Disk Status Bits (DSTATUS) */
43 
44 #define STA_NOINIT 0x01 /* Drive not initialized */
45 #define STA_NODISK 0x02 /* No medium in the drive */
46 #define STA_PROTECT 0x04 /* Write protected */
47 
48 
49 /* Command code for disk_ioctrl fucntion */
50 
51 /* Generic command (Used by FatFs) */
52 #define CTRL_SYNC 0 /* Complete pending write process (needed at _FS_READONLY == 0) */
53 #define GET_SECTOR_COUNT 1 /* Get media size (needed at _USE_MKFS == 1) */
54 #define GET_SECTOR_SIZE 2 /* Get sector size (needed at _MAX_SS != _MIN_SS) */
55 #define GET_BLOCK_SIZE 3 /* Get erase block size (needed at _USE_MKFS == 1) */
56 #define CTRL_TRIM 4 /* Inform device that the data on the block of sectors is no longer used (needed at _USE_TRIM == 1) */
57 
58 /* Generic command (Not used by FatFs) */
59 #define CTRL_POWER 5 /* Get/Set power status */
60 #define CTRL_LOCK 6 /* Lock/Unlock media removal */
61 #define CTRL_EJECT 7 /* Eject media */
62 #define CTRL_FORMAT 8 /* Create physical format on the media */
63 
64 /* MMC/SDC specific ioctl command */
65 #define MMC_GET_TYPE 10 /* Get card type */
66 #define MMC_GET_CSD 11 /* Get CSD */
67 #define MMC_GET_CID 12 /* Get CID */
68 #define MMC_GET_OCR 13 /* Get OCR */
69 #define MMC_GET_SDSTAT 14 /* Get SD status */
70 
71 /* ATA/CF specific ioctl command */
72 #define ATA_GET_REV 20 /* Get F/W revision */
73 #define ATA_GET_MODEL 21 /* Get model name */
74 #define ATA_GET_SN 22 /* Get serial number */
75 
76 
77 /*
78  * Updates made by Texas Instruments
79  *
80  * The following additions are needed in order to control the total number of
81  * volumes supported and to allow the disk_* APIs to call media specific disk
82  * functions which are registered in a table of type 'diskio_fxns'
83  */
84 
85 /* Disk I/O function table object, used to map media specific implementations */
86 typedef struct {
87  DSTATUS (*d_init) (BYTE drive);
88  DSTATUS (*d_status) (BYTE drive);
89  DRESULT (*d_read) (BYTE drive, BYTE *buf, DWORD sector, UINT num);
90  DRESULT (*d_write) (BYTE drive, const BYTE *buf, DWORD sector, UINT num);
91  DRESULT (*d_ioctl) (BYTE drive, BYTE cmd, void * buf);
92 } diskio_fxns;
93 
95  BYTE drive,
96  DSTATUS (*d_init) (BYTE drive),
97  DSTATUS (*d_status) (BYTE drive),
98  DRESULT (*d_read) (BYTE drive, BYTE *buf, DWORD sector, UINT num),
99  DRESULT (*d_write) (BYTE drive, const BYTE *buf, DWORD sector, UINT num),
100  DRESULT (*d_ioctl) (BYTE drive, BYTE cmd, void * buf)
101 );
102 
104 
105 #ifdef __cplusplus
106 }
107 #endif
108 
109 #endif
Definition: diskio.h:26
DRESULT disk_write(BYTE pdrv, const BYTE *buff, DWORD sector, UINT count)
Definition: diskio.h:24
DRESULT disk_unregister(BYTE drive)
Definition: diskio.h:86
Definition: diskio.h:27
unsigned long DWORD
Definition: integer.h:29
DSTATUS disk_status(BYTE pdrv)
BYTE DSTATUS
Definition: diskio.h:19
DRESULT
Definition: diskio.h:22
unsigned char BYTE
Definition: integer.h:16
DRESULT disk_read(BYTE pdrv, BYTE *buff, DWORD sector, UINT count)
Definition: diskio.h:23
DSTATUS disk_initialize(BYTE pdrv)
DRESULT disk_ioctl(BYTE pdrv, BYTE cmd, void *buff)
unsigned int UINT
Definition: integer.h:25
DRESULT disk_register(BYTE drive, DSTATUS(*d_init)(BYTE drive), DSTATUS(*d_status)(BYTE drive), DRESULT(*d_read)(BYTE drive, BYTE *buf, DWORD sector, UINT num), DRESULT(*d_write)(BYTE drive, const BYTE *buf, DWORD sector, UINT num), DRESULT(*d_ioctl)(BYTE drive, BYTE cmd, void *buf))
Definition: diskio.h:25
Copyright 2016, Texas Instruments Incorporated