UDMA0

Instance: UDMA0
Component: UDMA
Base address: 0x40020000


ARM Micro Direct Memory Access Controller

TOP:UDMA0 Register Summary

Register Name

Type

Register Width (Bits)

Register Reset

Address Offset

Physical Address

STATUS

RO

32

0x001F 0000

0x0000 0000

0x4002 0000

CFG

WO

32

0x0000 0000

0x0000 0004

0x4002 0004

CTRL

RW

32

0x0000 0000

0x0000 0008

0x4002 0008

ALTCTRL

RO

32

0x0000 0200

0x0000 000C

0x4002 000C

WAITONREQ

RO

32

0xFFFF 1EFF

0x0000 0010

0x4002 0010

SOFTREQ

WO

32

0x0000 0000

0x0000 0014

0x4002 0014

SETBURST

RW

32

0x0000 0000

0x0000 0018

0x4002 0018

CLEARBURST

WO

32

0x0000 0000

0x0000 001C

0x4002 001C

SETREQMASK

RW

32

0x0000 0000

0x0000 0020

0x4002 0020

CLEARREQMASK

WO

32

0x0000 0000

0x0000 0024

0x4002 0024

SETCHANNELEN

RW

32

0x0000 0000

0x0000 0028

0x4002 0028

CLEARCHANNELEN

WO

32

0x0000 0000

0x0000 002C

0x4002 002C

SETCHNLPRIALT

RW

32

0x0000 0000

0x0000 0030

0x4002 0030

CLEARCHNLPRIALT

WO

32

0x0000 0000

0x0000 0034

0x4002 0034

SETCHNLPRIORITY

RW

32

0x0000 0000

0x0000 0038

0x4002 0038

CLEARCHNLPRIORITY

WO

32

0x0000 0000

0x0000 003C

0x4002 003C

ERROR

RW

32

0x0000 0000

0x0000 004C

0x4002 004C

REQDONE

RW

32

0x0000 0000

0x0000 0504

0x4002 0504

DONEMASK

RW

32

0x0000 0000

0x0000 0520

0x4002 0520

TOP:UDMA0 Register Descriptions

TOP:UDMA0:STATUS

Address Offset 0x0000 0000
Physical Address 0x4002 0000 Instance 0x4002 0000
Description Status
Type RO
Bits Field Name Description Type Reset
31:28 TEST
0x0: Controller does not include the integration test logic
0x1: Controller includes the integration test logic
0x2: Undefined
...
0xF: Undefined
RO 0x0
27:21 RESERVED21 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
20:16 TOTALCHANNELS Register value returns number of available uDMA channels minus one. For example a read out value of:

0x00: Show that the controller is configured to use 1 uDMA channel
0x01: Shows that the controller is configured to use 2 uDMA channels
...
0x1F: Shows that the controller is configured to use 32 uDMA channels (32-1=31=0x1F)
RO 0b1 1111
15:8 RESERVED8 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x00
7:4 STATE Current state of the control state machine. State can be one of the following:

0x0: Idle
0x1: Reading channel controller data
0x2: Reading source data end pointer
0x3: Reading destination data end pointer
0x4: Reading source data
0x5: Writing destination data
0x6: Waiting for uDMA request to clear
0x7: Writing channel controller data
0x8: Stalled
0x9: Done
0xA: Peripheral scatter-gather transition
0xB: Undefined
...
0xF: Undefined.
RO 0x0
3:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000
0 MASTERENABLE Shows the enable status of the controller as configured by CFG.MASTERENABLE:

0: Controller is disabled
1: Controller is enabled
RO 0

TOP:UDMA0:CFG

Address Offset 0x0000 0004
Physical Address 0x4002 0004 Instance 0x4002 0004
Description Configuration
Type WO
Bits Field Name Description Type Reset
31:8 RESERVED8 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. WO 0x00 0000
7:5 PRTOCTRL Sets the AHB-Lite bus protocol protection state by controlling the AHB signal HProt[3:1] as follows:

Bit [7] Controls HProt[3] to indicate if a cacheable access is occurring.
Bit [6] Controls HProt[2] to indicate if a bufferable access is occurring.
Bit [5] Controls HProt[1] to indicate if a privileged access is occurring.

When bit [n] = 1 then the corresponding HProt bit is high.
When bit [n] = 0 then the corresponding HProt bit is low.

This field controls HProt[3:1] signal for all transactions initiated by uDMA except two transactions below:
- the read from the address indicated by source address pointer
- the write to the address indicated by destination address pointer
HProt[3:1] for these two exceptions can be controlled by dedicated fields in the channel configutation descriptor.
WO 0b000
4:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. WO 0x0
0 MASTERENABLE Enables the controller:

0: Disables the controller
1: Enables the controller
WO 0

TOP:UDMA0:CTRL

Address Offset 0x0000 0008
Physical Address 0x4002 0008 Instance 0x4002 0008
Description Channel Control Data Base Pointer
Type RW
Bits Field Name Description Type Reset
31:10 BASEPTR This register point to the base address for the primary data structures of each DMA channel. This is not stored in module, but in system memory, thus space must be allocated for this usage when DMA is in usage RW 0b00 0000 0000 0000 0000 0000
9:0 RESERVED0 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b00 0000 0000

TOP:UDMA0:ALTCTRL

Address Offset 0x0000 000C
Physical Address 0x4002 000C Instance 0x4002 000C
Description Channel Alternate Control Data Base Pointer
Type RO
Bits Field Name Description Type Reset
31:0 BASEPTR This register shows the base address for the alternate data structures and is calculated by module, thus read only RO 0x0000 0200

TOP:UDMA0:WAITONREQ

Address Offset 0x0000 0010
Physical Address 0x4002 0010 Instance 0x4002 0010
Description Channel Wait On Request Status
Type RO
Bits Field Name Description Type Reset
31:0 CHNLSTATUS Channel wait on request status:

Bit [Ch] = 0: Once uDMA receives a single or burst request on channel Ch, this channel may come out of active state even if request is still present.
Bit [Ch] = 1: Once uDMA receives a single or burst request on channel Ch, it keeps channel Ch in active state until the requests are deasserted. This handshake is necessary for channels where the requester is in an asynchronous domain or can run at slower clock speed than uDMA
RO 0xFFFF 1EFF

TOP:UDMA0:SOFTREQ

Address Offset 0x0000 0014
Physical Address 0x4002 0014 Instance 0x4002 0014
Description Channel Software Request
Type WO
Bits Field Name Description Type Reset
31:0 CHNLS Set the appropriate bit to generate a software uDMA request on the corresponding uDMA channel

Bit [Ch] = 0: Does not create a uDMA request for channel Ch
Bit [Ch] = 1: Creates a uDMA request for channel Ch

Writing to a bit where a uDMA channel is not implemented does not create a uDMA request for that channel
WO 0x0000 0000

TOP:UDMA0:SETBURST

Address Offset 0x0000 0018
Physical Address 0x4002 0018 Instance 0x4002 0018
Description Channel Set UseBurst
Type RW
Bits Field Name Description Type Reset
31:0 CHNLS Returns the useburst status, or disables individual channels from generating single uDMA requests. The value R is the arbitration rate and stored in the controller data structure.

Read as:

Bit [Ch] = 0: uDMA channel Ch responds to both burst and single requests on channel C. The controller performs 2^R, or single, bus transfers.

Bit [Ch] = 1: uDMA channel Ch does not respond to single transfer requests. The controller only responds to burst transfer requests and performs 2^R transfers.

Write as:
Bit [Ch] = 0: No effect. Use the CLEARBURST.CHNLS to set bit [Ch] to 0.
Bit [Ch] = 1: Disables single transfer requests on channel Ch. The controller performs 2^R transfers for burst requests.

Writing to a bit where a uDMA channel is not implemented has no effect
RW 0x0000 0000

TOP:UDMA0:CLEARBURST

Address Offset 0x0000 001C
Physical Address 0x4002 001C Instance 0x4002 001C
Description Channel Clear UseBurst
Type WO
Bits Field Name Description Type Reset
31:0 CHNLS Set the appropriate bit to enable single transfer requests.

Write as:

Bit [Ch] = 0: No effect. Use the SETBURST.CHNLS to disable single transfer requests.

Bit [Ch] = 1: Enables single transfer requests on channel Ch.

Writing to a bit where a DMA channel is not implemented has no effect.
WO 0x0000 0000

TOP:UDMA0:SETREQMASK

Address Offset 0x0000 0020
Physical Address 0x4002 0020 Instance 0x4002 0020
Description Channel Set Request Mask
Type RW
Bits Field Name Description Type Reset
31:0 CHNLS Returns the burst and single request mask status, or disables the corresponding channel from generating uDMA requests.

Read as:
Bit [Ch] = 0: External requests are enabled for channel Ch.
Bit [Ch] = 1: External requests are disabled for channel Ch.

Write as:
Bit [Ch] = 0: No effect. Use the CLEARREQMASK.CHNLS to enable uDMA requests.
Bit [Ch] = 1: Disables uDMA burst request channel [C] and uDMA single request channel [C] input from generating uDMA requests.

Writing to a bit where a uDMA channel is not implemented has no effect
RW 0x0000 0000

TOP:UDMA0:CLEARREQMASK

Address Offset 0x0000 0024
Physical Address 0x4002 0024 Instance 0x4002 0024
Description Clear Channel Request Mask
Type WO
Bits Field Name Description Type Reset
31:0 CHNLS Set the appropriate bit to enable DMA request for the channel.

Write as:
Bit [Ch] = 0: No effect. Use the SETREQMASK.CHNLS to disable channel C from generating requests.
Bit [Ch] = 1: Enables channel [C] to generate DMA requests.

Writing to a bit where a DMA channel is not implemented has no effect.
WO 0x0000 0000

TOP:UDMA0:SETCHANNELEN

Address Offset 0x0000 0028
Physical Address 0x4002 0028 Instance 0x4002 0028
Description Set Channel Enable
Type RW
Bits Field Name Description Type Reset
31:0 CHNLS Returns the enable status of the channels, or enables the corresponding channels.

Read as:
Bit [Ch] = 0: Channel Ch is disabled.
Bit [Ch] = 1: Channel Ch is enabled.

Write as:
Bit [Ch] = 0: No effect. Use the CLEARCHANNELEN.CHNLS to disable a channel
Bit [Ch] = 1: Enables channel Ch

Writing to a bit where a DMA channel is not implemented has no effect
RW 0x0000 0000

TOP:UDMA0:CLEARCHANNELEN

Address Offset 0x0000 002C
Physical Address 0x4002 002C Instance 0x4002 002C
Description Clear Channel Enable
Type WO
Bits Field Name Description Type Reset
31:0 CHNLS Set the appropriate bit to disable the corresponding uDMA channel.

Write as:
Bit [Ch] = 0: No effect. Use the SETCHANNELEN.CHNLS to enable uDMA channels.
Bit [Ch] = 1: Disables channel Ch

Writing to a bit where a uDMA channel is not implemented has no effect
WO 0x0000 0000

TOP:UDMA0:SETCHNLPRIALT

Address Offset 0x0000 0030
Physical Address 0x4002 0030 Instance 0x4002 0030
Description Channel Set Primary-Alternate
Type RW
Bits Field Name Description Type Reset
31:0 CHNLS Returns the channel control data structure status, or selects the alternate data structure for the corresponding uDMA channel.

Read as:
Bit [Ch] = 0: uDMA channel Ch is using the primary data structure.
Bit [Ch] = 1: uDMA channel Ch is using the alternate data structure.

Write as:
Bit [Ch] = 0: No effect. Use the CLEARCHNLPRIALT.CHNLS to disable a channel
Bit [Ch] = 1: Selects the alternate data structure for channel Ch

Writing to a bit where a uDMA channel is not implemented has no effect
RW 0x0000 0000

TOP:UDMA0:CLEARCHNLPRIALT

Address Offset 0x0000 0034
Physical Address 0x4002 0034 Instance 0x4002 0034
Description Channel Clear Primary-Alternate
Type WO
Bits Field Name Description Type Reset
31:0 CHNLS Clears the appropriate bit to select the primary data structure for the corresponding uDMA channel.

Write as:
Bit [Ch] = 0: No effect. Use the SETCHNLPRIALT.CHNLS to select the alternate data structure.
Bit [Ch] = 1: Selects the primary data structure for channel Ch.

Writing to a bit where a uDMA channel is not implemented has no effect
WO 0x0000 0000

TOP:UDMA0:SETCHNLPRIORITY

Address Offset 0x0000 0038
Physical Address 0x4002 0038 Instance 0x4002 0038
Description Set Channel Priority
Type RW
Bits Field Name Description Type Reset
31:0 CHNLS Returns the channel priority mask status, or sets the channel priority to high.

Read as:
Bit [Ch] = 0: uDMA channel Ch is using the default priority level.
Bit [Ch] = 1: uDMA channel Ch is using a high priority level.

Write as:
Bit [Ch] = 0: No effect. Use the CLEARCHNLPRIORITY.CHNLS to set channel Ch to the default priority level.
Bit [Ch] = 1: Channel Ch uses the high priority level.

Writing to a bit where a uDMA channel is not implemented has no effect
RW 0x0000 0000

TOP:UDMA0:CLEARCHNLPRIORITY

Address Offset 0x0000 003C
Physical Address 0x4002 003C Instance 0x4002 003C
Description Clear Channel Priority
Type WO
Bits Field Name Description Type Reset
31:0 CHNLS Clear the appropriate bit to select the default priority level for the specified uDMA channel.

Write as:
Bit [Ch] = 0: No effect. Use the SETCHNLPRIORITY.CHNLS to set channel Ch to the high priority level.
Bit [Ch] = 1: Channel Ch uses the default priority level.

Writing to a bit where a uDMA channel is not implemented has no effect
WO 0x0000 0000

TOP:UDMA0:ERROR

Address Offset 0x0000 004C
Physical Address 0x4002 004C Instance 0x4002 004C
Description Error Status and Clear
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. WO 0b000 0000 0000 0000 0000 0000 0000 0000
0 STATUS Returns the status of bus error flag in uDMA, or clears this bit

Read as:

0: No bus error detected
1: Bus error detected

Write as:

0: No effect, status of bus error flag is unchanged.
1: Clears the bus error flag.
RW 0

TOP:UDMA0:REQDONE

Address Offset 0x0000 0504
Physical Address 0x4002 0504 Instance 0x4002 0504
Description Channel Request Done
Type RW
Bits Field Name Description Type Reset
31:0 CHNLS Reflects the uDMA done status for the given channel, channel [Ch]. It's a sticky done bit. Unless cleared by writing a 1, it holds the value of 1.

Read as:
Bit [Ch] = 0: Request has not completed for channel Ch
Bit [Ch] = 1: Request has completed for the channel Ch

Writing a 1 to individual bits would clear the corresponding bit.

Write as:
Bit [Ch] = 0: No effect.
Bit [Ch] = 1: The corresponding [Ch] bit is cleared and is set to 0
RW 0x0000 0000

TOP:UDMA0:DONEMASK

Address Offset 0x0000 0520
Physical Address 0x4002 0520 Instance 0x4002 0520
Description Channel Request Done Mask
Type RW
Bits Field Name Description Type Reset
31:0 CHNLS Controls the propagation of the uDMA done and active state to the assigned peripheral. Specifically used for software channels.

Read as:
Bit [Ch] = 0: uDMA done and active state for channel Ch is not blocked from reaching to the peripherals.
Note that the uDMA done state for channel [Ch] is blocked from contributing to generation of combined uDMA done signal

Bit [Ch] = 1: uDMA done and active state for channel Ch is blocked from reaching to the peripherals.
Note that the uDMA done state for channel [Ch] is not blocked from contributing to generation of combined uDMA done signal

Write as:
Bit [Ch] = 0: Allows uDMA done and active stat to propagate to the peripherals.
Note that this disables uDMA done state for channel [Ch] from contributing to generation of combined uDMA done signal

Bit [Ch] = 1: Blocks uDMA done and active state to propagate to the peripherals.
Note that this enables uDMA done for channel [Ch] to contribute to generation of combined uDMA done signal.
RW 0x0000 0000