I2S0

Instance: I2S0
Component: I2S
Base address: 0x40021000


I2S Audio DMA module supporting formats I2S, LJF, RJF and DSP

TOP:I2S0 Register Summary

Register Name

Type

Register Width (Bits)

Register Reset

Address Offset

Physical Address

AIFWCLKSRC

RW

32

0x0000 0000

0x0000 0000

0x4002 1000

AIFDMACFG

RW

32

0x0000 0000

0x0000 0004

0x4002 1004

AIFDIRCFG

RW

32

0x0000 0000

0x0000 0008

0x4002 1008

AIFFMTCFG

RW

32

0x0000 0170

0x0000 000C

0x4002 100C

AIFWMASK0

RW

32

0x0000 0003

0x0000 0010

0x4002 1010

AIFWMASK1

RW

32

0x0000 0003

0x0000 0014

0x4002 1014

AIFWMASK2

RW

32

0x0000 0003

0x0000 0018

0x4002 1018

AIFPWMVALUE

RW

32

0x0000 0000

0x0000 001C

0x4002 101C

AIFINPTRNEXT

RW

32

0x0000 0000

0x0000 0020

0x4002 1020

AIFINPTR

RW

32

0x0000 0000

0x0000 0024

0x4002 1024

AIFOUTPTRNEXT

RW

32

0x0000 0000

0x0000 0028

0x4002 1028

AIFOUTPTR

RW

32

0x0000 0000

0x0000 002C

0x4002 102C

STMPCTL

RW

32

0x0000 0000

0x0000 0034

0x4002 1034

STMPXCNTCAPT0

RO

32

0x0000 0000

0x0000 0038

0x4002 1038

STMPXPER

RO

32

0x0000 0000

0x0000 003C

0x4002 103C

STMPWCNTCAPT0

RO

32

0x0000 0000

0x0000 0040

0x4002 1040

STMPWPER

RW

32

0x0000 0000

0x0000 0044

0x4002 1044

STMPINTRIG

RW

32

0x0000 0000

0x0000 0048

0x4002 1048

STMPOUTTRIG

RW

32

0x0000 0000

0x0000 004C

0x4002 104C

STMPWSET

RW

32

0x0000 0000

0x0000 0050

0x4002 1050

STMPWADD

RW

32

0x0000 0000

0x0000 0054

0x4002 1054

STMPXPERMIN

RW

32

0x0000 FFFF

0x0000 0058

0x4002 1058

STMPWCNT

RO

32

0x0000 0000

0x0000 005C

0x4002 105C

STMPXCNT

RO

32

0x0000 0000

0x0000 0060

0x4002 1060

STMPXCNTCAPT1

RO

32

0x0000 0000

0x0000 0064

0x4002 1064

STMPWCNTCAPT1

RO

32

0x0000 0000

0x0000 0068

0x4002 1068

IRQMASK

RW

32

0x0000 0000

0x0000 0070

0x4002 1070

IRQFLAGS

RO

32

0x0000 0000

0x0000 0074

0x4002 1074

IRQSET

WO

32

0x0000 0000

0x0000 0078

0x4002 1078

IRQCLR

WO

32

0x0000 0000

0x0000 007C

0x4002 107C

TOP:I2S0 Register Descriptions

TOP:I2S0:AIFWCLKSRC

Address Offset 0x0000 0000
Physical Address 0x4002 1000 Instance 0x4002 1000
Description WCLK Source Selection
Type RW
Bits Field Name Description Type Reset
31:3 RESERVED3 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000 0000 0000 0000 0000 0000 0000
2 WCLK_INV Inverts WCLK source (pad or internal) when set.

0: Not inverted
1: Inverted
RW 0
1:0 WCLK_SRC Selects WCLK source for AIF (should be the same as the BCLK source). The BCLK source is defined in the PRCM:I2SBCLKSEL.SRC
Value ENUM Name Description
0x0 NONE None ('0')
0x1 EXT External WCLK generator, from pad
0x2 INT Internal WCLK generator, from module PRCM/ClkCtrl
0x3 RESERVED Not supported. Will give same WCLK as 'NONE' ('00')
RW 0b00

TOP:I2S0:AIFDMACFG

Address Offset 0x0000 0004
Physical Address 0x4002 1004 Instance 0x4002 1004
Description DMA Buffer Size Configuration
Type RW
Bits Field Name Description Type Reset
31:8 RESERVED8 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x00 0000
7:0 END_FRAME_IDX Defines the length of the Writing a non-zero value to this registerfield enables and initializes AIF. Note that before doing so, all other configuration must have been done, and AIFINPTR/AIFOUTPTR must have been loaded. RW 0x00

TOP:I2S0:AIFDIRCFG

Address Offset 0x0000 0008
Physical Address 0x4002 1008 Instance 0x4002 1008
Description Pin Direction
Type RW
Bits Field Name Description Type Reset
31:10 RESERVED10 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000 0000 0000
9:8 AD2 Configures the AD2 audio data pin usage

0x3: Reserved
Value ENUM Name Description
0x0 DIS Not in use (disabled)
0x1 IN Input mode
0x2 OUT Output mode
RW 0b00
7:6 RESERVED6 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00
5:4 AD1 Configures the AD1 audio data pin usage:

0x3: Reserved
Value ENUM Name Description
0x0 DIS Not in use (disabled)
0x1 IN Input mode
0x2 OUT Output mode
RW 0b00
3:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00
1:0 AD0 Configures the AD0 audio data pin usage:

0x3: Reserved
Value ENUM Name Description
0x0 DIS Not in use (disabled)
0x1 IN Input mode
0x2 OUT Output mode
RW 0b00

TOP:I2S0:AIFFMTCFG

Address Offset 0x0000 000C
Physical Address 0x4002 100C Instance 0x4002 100C
Description Serial Interface Format Configuration
Type RW
Bits Field Name Description Type Reset
31:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
15:8 DATA_DELAY The number of BCLK periods between a WCLK edge and MSB of the first word in a phase:

0x00: LJF format
0x01: I2S and DSP format
0x02: RJF format
...
0xFF: RJF format

Note: When 0, MSB of the next word will be output in the idle period between LSB of the previous word and the start of the next word. Otherwise logical 0 will be output until the data delay has expired.
RW 0x01
7 MEM_LEN_24 The size of each word stored to or loaded from memory:
Value ENUM Name Description
0x0 16BIT 16-bit (one 16 bit access per sample)
0x1 24BIT 24-bit (one 8 bit and one 16 bit locked access per sample)
RW 0
6 SMPL_EDGE On the serial audio interface, data (and wclk) is sampled and clocked out on opposite edges of BCLK.
Value ENUM Name Description
0x0 NEG Data is sampled on the negative edge and clocked out on the positive edge.
0x1 POS Data is sampled on the positive edge and clocked out on the negative edge.
RW 1
5 DUAL_PHASE Selects dual- or single-phase format.

0: Single-phase
1: Dual-phase
RW 1
4:0 WORD_LEN Number of bits per word (8-24):
In single-phase format, this is the exact number of bits per word.
In dual-phase format, this is the maximum number of bits per word.

Values below 8 and above 24 give undefined behavior. Data written to memory is always aligned to 16 or 24 bits as defined by MEM_LEN_24. Bit widths that differ from this alignment will either be truncated or zero padded.
RW 0b1 0000

TOP:I2S0:AIFWMASK0

Address Offset 0x0000 0010
Physical Address 0x4002 1010 Instance 0x4002 1010
Description Word Selection Bit Mask for Pin 0
Type RW
Bits Field Name Description Type Reset
31:8 RESERVED8 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0x00 0000
7:0 MASK Bit-mask indicating valid channels in a frame on AD0.

In single-phase mode, each bit represents one channel, starting with LSB for the first word in the frame. A frame can contain up to 8 channels. Channels that are not included in the mask will not be sampled and stored in memory, and clocked out as '0'.

In dual-phase mode, only the two LSBs are considered. For a stereo configuration, set both bits. For a mono configuration, set bit 0 only. In mono mode, only channel 0 will be sampled and stored to memory, and channel 0 will be repeated when clocked out.

In mono mode, only channel 0 will be sampled and stored to memory, and channel 0 will be repeated in the second phase when clocked out.

If all bits are zero, no input words will be stored to memory, and the output data lines will be constant '0'. This can be utilized when PWM debug output is desired without any actively used output pins.
RW 0x03

TOP:I2S0:AIFWMASK1

Address Offset 0x0000 0014
Physical Address 0x4002 1014 Instance 0x4002 1014
Description Word Selection Bit Mask for Pin 1
Type RW
Bits Field Name Description Type Reset
31:8 RESERVED8 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x00 0000
7:0 MASK Bit-mask indicating valid channels in a frame on AD1.

In single-phase mode, each bit represents one channel, starting with LSB for the first word in the frame. A frame can contain up to 8 channels. Channels that are not included in the mask will not be sampled and stored in memory, and clocked out as '0'.

In dual-phase mode, only the two LSBs are considered. For a stereo configuration, set both bits. For a mono configuration, set bit 0 only. In mono mode, only channel 0 will be sampled and stored to memory, and channel 0 will be repeated when clocked out.

In mono mode, only channel 0 will be sampled and stored to memory, and channel 0 will be repeated in the second phase when clocked out.

If all bits are zero, no input words will be stored to memory, and the output data lines will be constant '0'. This can be utilized when PWM debug output is desired without any actively used output pins.
RW 0x03

TOP:I2S0:AIFWMASK2

Address Offset 0x0000 0018
Physical Address 0x4002 1018 Instance 0x4002 1018
Description Word Selection Bit Mask for Pin 2
Type RW
Bits Field Name Description Type Reset
31:8 RESERVED8 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x00 0000
7:0 MASK Bit-mask indicating valid channels in a frame on AD2

In single-phase mode, each bit represents one channel, starting with LSB for the first word in the frame. A frame can contain up to 8 channels. Channels that are not included in the mask will not be sampled and stored in memory, and clocked out as '0'.

In dual-phase mode, only the two LSBs are considered. For a stereo configuration, set both bits. For a mono configuration, set bit 0 only. In mono mode, only channel 0 will be sampled and stored to memory, and channel 0 will be repeated when clocked out.

In mono mode, only channel 0 will be sampled and stored to memory, and channel 0 will be repeated in the second phase when clocked out.

If all bits are zero, no input words will be stored to memory, and the output data lines will be constant '0'. This can be utilized when PWM debug output is desired without any actively used output pins.
RW 0x03

TOP:I2S0:AIFPWMVALUE

Address Offset 0x0000 001C
Physical Address 0x4002 101C Instance 0x4002 101C
Description Audio Interface PWM Debug Value
Type RW
Bits Field Name Description Type Reset
31:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
15:0 PULSE_WIDTH The value written to this register determines the width of the active high PWM pulse (pwm_debug), which starts together with MSB of the first output word in a DMA buffer:

0x0000: Constant low
0x0001: Width of the pulse (number of BCLK cycles, here 1).
...
0xFFFE: Width of the pulse (number of BCLK cycles, here 65534).
0xFFFF: Constant high
RW 0x0000

TOP:I2S0:AIFINPTRNEXT

Address Offset 0x0000 0020
Physical Address 0x4002 1020 Instance 0x4002 1020
Description DMA Input Buffer Next Pointer
Type RW
Bits Field Name Description Type Reset
31:0 PTR Pointer to the first byte in the next DMA input buffer.

The read value equals the last written value until the currently used DMA input buffer is completed, and then becomes null when the last written value is transferred to the DMA controller to start on the next buffer. This event is signalized by aif_dma_in_irq.

At startup, the value must be written once before and once after configuring the DMA buffer size in AIFDMACFG.

The next pointer must be written to this register while the DMA function uses the previously written pointer. If not written in time, IRQFLAGS.PTR_ERR will be raised and all input pins will be disabled.

Note the following limitations:
- Address space wrapping is not supported. That means address(last sample) must be higher than address(first sample.
- A DMA block cannot be aligned with the end of the address space, that means a block cannot contain the address 0xFFFF.
RW 0x0000 0000

TOP:I2S0:AIFINPTR

Address Offset 0x0000 0024
Physical Address 0x4002 1024 Instance 0x4002 1024
Description DMA Input Buffer Current Pointer
Type RW
Bits Field Name Description Type Reset
31:0 PTR Value of the DMA input buffer pointer currently used by the DMA controller. Incremented by 1 (byte) or 2 (word) for each AHB access. RW 0x0000 0000

TOP:I2S0:AIFOUTPTRNEXT

Address Offset 0x0000 0028
Physical Address 0x4002 1028 Instance 0x4002 1028
Description DMA Output Buffer Next Pointer
Type RW
Bits Field Name Description Type Reset
31:0 PTR Pointer to the first byte in the next DMA output buffer.

The read value equals the last written value until the currently used DMA output buffer is completed, and then becomes null when the last written value is transferred to the DMA controller to start on the next buffer. This event is signalized by aif_dma_out_irq.

At startup, the value must be written once before and once after configuring the DMA buffer size in AIFDMACFG. At this time, the first two samples will be fetched from memory.

The next pointer must be written to this register while the DMA function uses the previously written pointer. If not written in time, IRQFLAGS.PTR_ERR will be raised and all output pins will be disabled.

Note the following limitations:
- Address space wrapping is not supported. That means address(last sample) must be higher than address(first sample.
- A DMA block cannot be aligned with the end of the address space, that means a block cannot contain the address 0xFFFF.
RW 0x0000 0000

TOP:I2S0:AIFOUTPTR

Address Offset 0x0000 002C
Physical Address 0x4002 102C Instance 0x4002 102C
Description DMA Output Buffer Current Pointer
Type RW
Bits Field Name Description Type Reset
31:0 PTR Value of the DMA output buffer pointer currently used by the DMA controller Incremented by 1 (byte) or 2 (word) for each AHB access. RW 0x0000 0000

TOP:I2S0:STMPCTL

Address Offset 0x0000 0034
Physical Address 0x4002 1034 Instance 0x4002 1034
Description SampleStaMP Generator Control Register
Type RW
Bits Field Name Description Type Reset
31:3 RESERVED3 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000 0000 0000 0000 0000 0000 0000
2 OUT_RDY Low until the output pins are ready to be started by the samplestamp generator. When started (that is STMPOUTTRIG equals the WCLK counter) the bit goes back low. RO 0
1 IN_RDY Low until the input pins are ready to be started by the samplestamp generator. When started (that is STMPINTRIG equals the WCLK counter) the bit goes back low. RO 0
0 STMP_EN Enables the samplestamp generator. The samplestamp generator must only be enabled after it has been properly configured.
When cleared, all samplestamp generator counters and capture values are cleared.
RW 0

TOP:I2S0:STMPXCNTCAPT0

Address Offset 0x0000 0038
Physical Address 0x4002 1038 Instance 0x4002 1038
Description Captured XOSC Counter Value, Capture Channel 0
Type RO
Bits Field Name Description Type Reset
31:16 RESERVED Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
15:0 CAPT_VALUE The value of the samplestamp XOSC counter (STMPXCNT.CURR_VALUE) last time an event was pulsed (event source selected in [EVENT.I2SSTMPSEL0.EV] for channel 0). This number corresponds to the number of 24 MHz clock cycles since the last positive edge of the selected WCLK.
The value is cleared when STMPCTL.STMP_EN = 0.
Note: Due to buffering and synchronization, WCLK is delayed by a small number of BCLK periods and clk periods.
Note: When calculating the fractional part of the sample stamp, STMPXPER may be less than this bit field.
RO 0x0000

TOP:I2S0:STMPXPER

Address Offset 0x0000 003C
Physical Address 0x4002 103C Instance 0x4002 103C
Description XOSC Period Value
Type RO
Bits Field Name Description Type Reset
31:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
15:0 VALUE The number of 24 MHz clock cycles in the previous WCLK period (that is - the next value of the XOSC counter at the positive WCLK edge, had it not been reset to 0).
The value is cleared when STMPCTL.STMP_EN = 0.
RO 0x0000

TOP:I2S0:STMPWCNTCAPT0

Address Offset 0x0000 0040
Physical Address 0x4002 1040 Instance 0x4002 1040
Description Captured WCLK Counter Value, Capture Channel 0
Type RO
Bits Field Name Description Type Reset
31:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
15:0 CAPT_VALUE The value of the samplestamp WCLK counter (STMPWCNT.CURR_VALUE) last time an event was pulsed (event source selected in EVENT:I2SSTMPSEL0.EV for channel 0). This number corresponds to the number of positive WCLK edges since the samplestamp generator was enabled (not taking modification through STMPWADD/STMPWSET into account).
The value is cleared when STMPCTL.STMP_EN = 0.
RO 0x0000

TOP:I2S0:STMPWPER

Address Offset 0x0000 0044
Physical Address 0x4002 1044 Instance 0x4002 1044
Description WCLK Counter Period Value
Type RW
Bits Field Name Description Type Reset
31:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
15:0 VALUE Used to define when STMPWCNT is to be reset so number of WCLK edges are found for the size of the sample buffer. This is thus a modulo value for the WCLK counter. This number must correspond to the size of the sample buffer used by the system (that is the index of the last sample plus 1). RW 0x0000

TOP:I2S0:STMPINTRIG

Address Offset 0x0000 0048
Physical Address 0x4002 1048 Instance 0x4002 1048
Description WCLK Counter Trigger Value for Input Pins
Type RW
Bits Field Name Description Type Reset
31:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
15:0 IN_START_WCNT Compare value used to start the incoming audio streams.
This bit field shall equal the WCLK counter value during the WCLK period in which the first input word(s) are sampled and stored to memory (that is the sample at the start of the very first DMA input buffer).

The value of this register takes effect when the following conditions are met:
- One or more pins are configured as inputs in AIFDIRCFG.
- AIFDMACFG has been configured for the correct buffer size, and at least 32 BCLK cycle ticks have happened.

Note: To avoid false triggers, this bit field should be set higher than STMPWPER.VALUE.
RW 0x0000

TOP:I2S0:STMPOUTTRIG

Address Offset 0x0000 004C
Physical Address 0x4002 104C Instance 0x4002 104C
Description WCLK Counter Trigger Value for Output Pins
Type RW
Bits Field Name Description Type Reset
31:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
15:0 OUT_START_WCNT Compare value used to start the outgoing audio streams.

This bit field must equal the WCLK counter value during the WCLK period in which the first output word(s) read from memory are clocked out (that is the sample at the start of the very first DMA output buffer).

The value of this register takes effect when the following conditions are met:
- One or more pins are configured as outputs in AIFDIRCFG.
- AIFDMACFG has been configured for the correct buffer size, and 32 BCLK cycle ticks have happened.
- 2 samples have been preloaded from memory (examine the AIFOUTPTR register if necessary).
Note: The memory read access is only performed when required, that is channels 0/1 must be selected in AIFWMASK0/AIFWMASK1.

Note: To avoid false triggers, this bit field should be set higher than STMPWPER.VALUE.
RW 0x0000

TOP:I2S0:STMPWSET

Address Offset 0x0000 0050
Physical Address 0x4002 1050 Instance 0x4002 1050
Description WCLK Counter Set Operation
Type RW
Bits Field Name Description Type Reset
31:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
15:0 VALUE WCLK counter modification: Sets the running WCLK counter equal to the written value. RW 0x0000

TOP:I2S0:STMPWADD

Address Offset 0x0000 0054
Physical Address 0x4002 1054 Instance 0x4002 1054
Description WCLK Counter Add Operation
Type RW
Bits Field Name Description Type Reset
31:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
15:0 VALUE_INC WCLK counter modification: Adds the written value to the running WCLK counter. If a positive edge of WCLK occurs at the same time as the operation, this will be taken into account.
To add a negative value, write "STMPWPER.VALUE - value".
RW 0x0000

TOP:I2S0:STMPXPERMIN

Address Offset 0x0000 0058
Physical Address 0x4002 1058 Instance 0x4002 1058
Description XOSC Minimum Period Value
Minimum Value of STMPXPER
Type RW
Bits Field Name Description Type Reset
31:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
15:0 VALUE Each time STMPXPER is updated, the value is also loaded into this register, provided that the value is smaller than the current value in this register.
When written, the register is reset to 0xFFFF (65535), regardless of the value written.
The minimum value can be used to detect extra WCLK pulses (this registers value will be significantly smaller than STMPXPER.VALUE).
RW 0xFFFF

TOP:I2S0:STMPWCNT

Address Offset 0x0000 005C
Physical Address 0x4002 105C Instance 0x4002 105C
Description Current Value of WCNT
Type RO
Bits Field Name Description Type Reset
31:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
15:0 CURR_VALUE Current value of the WCLK counter RO 0x0000

TOP:I2S0:STMPXCNT

Address Offset 0x0000 0060
Physical Address 0x4002 1060 Instance 0x4002 1060
Description Current Value of XCNT
Type RO
Bits Field Name Description Type Reset
31:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
15:0 CURR_VALUE Current value of the XOSC counter, latched when reading STMPWCNT. RO 0x0000

TOP:I2S0:STMPXCNTCAPT1

Address Offset 0x0000 0064
Physical Address 0x4002 1064 Instance 0x4002 1064
Description Captured XOSC Counter Value, Capture Channel 1
Type RO
Bits Field Name Description Type Reset
31:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
15:0 CAPT_VALUE Channel 1 is idle and can not be sampled from an external pulse as with Channel 0 STMPXCNTCAPT0 RO 0x0000

TOP:I2S0:STMPWCNTCAPT1

Address Offset 0x0000 0068
Physical Address 0x4002 1068 Instance 0x4002 1068
Description Captured WCLK Counter Value, Capture Channel 1
Type RO
Bits Field Name Description Type Reset
31:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0000
15:0 CAPT_VALUE Channel 1 is idle and can not be sampled from an external event as with Channel 0 STMPWCNTCAPT0 RO 0x0000

TOP:I2S0:IRQMASK

Address Offset 0x0000 0070
Physical Address 0x4002 1070 Instance 0x4002 1070
Description Masked Interrupt Status Register
Type RW
Bits Field Name Description Type Reset
31:6 RESERVED6 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b00 0000 0000 0000 0000 0000 0000
5 AIF_DMA_IN Defines the masks state for the interrupt of IRQFLAGS.AIF_DMA_IN

0: Disable
1: Enable
RW 0
4 AIF_DMA_OUT Defines the masks state for the interrupt of IRQFLAGS.AIF_DMA_OUT

0: Disable
1: Enable
RW 0
3 WCLK_TIMEOUT Defines the masks state for the interrupt of IRQFLAGS.WCLK_TIMEOUT

0: Disable
1: Enable
RW 0
2 BUS_ERR Defines the masks state for the interrupt of IRQFLAGS.BUS_ERR

0: Disable
1: Enable
RW 0
1 WCLK_ERR Defines the masks state for the interrupt of IRQFLAGS.WCLK_ERR

0: Disable
1: Enable
RW 0
0 PTR_ERR Defines the masks state for the interrupt of IRQFLAGS.PTR_ERR

0: Disable
1: Enable
RW 0

TOP:I2S0:IRQFLAGS

Address Offset 0x0000 0074
Physical Address 0x4002 1074 Instance 0x4002 1074
Description Raw Interrupt Status Register
Type RO
Bits Field Name Description Type Reset
31:6 RESERVED6 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000 0000 0000 0000
5 AIF_DMA_IN Set when condition for this bit field event occurs (auto cleared when input pointer is updated - AIFINPTR), see description of AIFINPTR register RO 0
4 AIF_DMA_OUT Set when condition for this bit field event occurs (auto cleared when output pointer is updated - AIFOUTPTR), see description of AIFOUTPTR register for details RO 0
3 WCLK_TIMEOUT Set when the sample stamp generator does not detect a positive WCLK edge for 65535 clk periods. This signalizes that the internal or external BCLK and WCLK generator source has been disabled.

The bit is sticky and may only be cleared by software (by writing '1' to IRQCLR.WCLK_TIMEOUT).
RO 0
2 BUS_ERR Set when a DMA operation is not completed in time (that is audio output buffer underflow, or audio input buffer overflow).
This error requires a complete restart since word synchronization has been lost. The bit is sticky and may only be cleared by software (by writing '1' to IRQCLR.BUS_ERR).

Note that DMA initiated transactions to illegal addresses will not trigger an interrupt. The response to such transactions is undefined.
RO 0
1 WCLK_ERR Set when:
- An unexpected WCLK edge occurs during the data delay period of a phase. Note unexpected WCLK edges during the word and idle periods of the phase are not detected.
- In dual-phase mode, when two WCLK edges are less than 4 BCLK cycles apart.
- In single-phase mode, when a WCLK pulse occurs before the last channel.
This error requires a complete restart since word synchronization has been lost. The bit is sticky and may only be cleared by software (by writing '1' to IRQCLR.WCLK_ERR).
RO 0
0 PTR_ERR Set when AIFINPTRNEXT or AIFOUTPTRNEXT has not been loaded with the next block address in time.
This error requires a complete restart since word synchronization has been lost. The bit is sticky and may only be cleared by software (by writing '1' to IRQCLR.PTR_ERR).
RO 0

TOP:I2S0:IRQSET

Address Offset 0x0000 0078
Physical Address 0x4002 1078 Instance 0x4002 1078
Description Interrupt Set Register
Type WO
Bits Field Name Description Type Reset
31:6 RESERVED6 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. WO 0b00 0000 0000 0000 0000 0000 0000
5 AIF_DMA_IN 1: Sets the interrupt of IRQFLAGS.AIF_DMA_IN (unless a auto clear criteria was given at the same time, in which the set will be ignored) WO 0
4 AIF_DMA_OUT 1: Sets the interrupt of IRQFLAGS.AIF_DMA_OUT (unless a auto clear criteria was given at the same time, in which the set will be ignored) WO 0
3 WCLK_TIMEOUT 1: Sets the interrupt of IRQFLAGS.WCLK_TIMEOUT WO 0
2 BUS_ERR 1: Sets the interrupt of IRQFLAGS.BUS_ERR WO 0
1 WCLK_ERR 1: Sets the interrupt of IRQFLAGS.WCLK_ERR WO 0
0 PTR_ERR 1: Sets the interrupt of IRQFLAGS.PTR_ERR WO 0

TOP:I2S0:IRQCLR

Address Offset 0x0000 007C
Physical Address 0x4002 107C Instance 0x4002 107C
Description Interrupt Clear Register
Type WO
Bits Field Name Description Type Reset
31:6 RESERVED6 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. WO 0b00 0000 0000 0000 0000 0000 0000
5 AIF_DMA_IN 1: Clears the interrupt of IRQFLAGS.AIF_DMA_IN (unless a set criteria was given at the same time in which the clear will be ignored) WO 0
4 AIF_DMA_OUT 1: Clears the interrupt of IRQFLAGS.AIF_DMA_OUT (unless a set criteria was given at the same time in which the clear will be ignored) WO 0
3 WCLK_TIMEOUT 1: Clears the interrupt of IRQFLAGS.WCLK_TIMEOUT (unless a set criteria was given at the same time in which the clear will be ignored) WO 0
2 BUS_ERR 1: Clears the interrupt of IRQFLAGS.BUS_ERR (unless a set criteria was given at the same time in which the clear will be ignored) WO 0
1 WCLK_ERR 1: Clears the interrupt of IRQFLAGS.WCLK_ERR (unless a set criteria was given at the same time in which the clear will be ignored) WO 0
0 PTR_ERR 1: Clears the interrupt of IRQFLAGS.PTR_ERR (unless a set criteria was given at the same time in which the clear will be ignored) WO 0