AON_SYSCTL

Instance: AON_SYSCTL
Component: AON_SYSCTL
Base address: 0x40090000


This component controls AON_SYSCTL, which is the device's system controller.

Note: This module is only supporting 32 bit ReadWrite access from MCU

TOP:AON_SYSCTL Register Summary

Register Name

Type

Register Width (Bits)

Register Reset

Address Offset

Physical Address

PWRCTL

RW

32

0b0000 0000 0000 0000 0000 0XXX 0000 0000

0x0000 0000

0x4009 0000

RESETCTL

RW

32

0x0000 00E0

0x0000 0004

0x4009 0004

SLEEPCTL

RW

32

0x0000 0000

0x0000 0008

0x4009 0008

TOP:AON_SYSCTL Register Descriptions

TOP:AON_SYSCTL:PWRCTL

Address Offset 0x0000 0000
Physical Address 0x4009 0000 Instance 0x4009 0000
Description Power Management

This register controls bitfields for setting low level power management features such as selection of regulator for VDDR supply and control of IO ring where certain segments can be enabled / disabled.
Type RW
Bits Field Name Description Type Reset
31:3 RESERVED3 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b0 0000 0000 0000 0000 0000 XXX0 0000
2 DCDC_ACTIVE Select to use DCDC regulator for VDDR in active mode

0: Use GLDO for regulation of VDDRin active mode.
1: Use DCDC for regulation of VDDRin active mode.
RW 0
1 EXT_REG_MODE Status of source for VDDRsupply:

0: DCDC/GLDO are generating VDDR
1: DCDC/GLDO are bypassed, external regulator supplies VDDR
RO 0
0 DCDC_EN Select to use DCDC regulator during recharge of VDDR

0: Use GLDO for recharge of VDDR
1: Use DCDC for recharge of VDDR

Note: This bitfield should be set to the same as DCDC_ACTIVE
RW 0

TOP:AON_SYSCTL:RESETCTL

Address Offset 0x0000 0004
Physical Address 0x4009 0004 Instance 0x4009 0004
Description Reset Management

This register contains bitfields releated to system reset such as reset source and reset request and control of brown out resets.
Type RW
Bits Field Name Description Type Reset
31 SYSRESET Cold reset register. Writing 1 to this bitfield will reset the entire chip and cause boot code to run again.

0: No effect
1: Generate system reset. Appears as SYSRESET in RESET_SRC.
WO 0
30:26 RESERVED26 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000
25 BOOT_DET_1_CLR Internal. Only to be used through TI provided API. RW 0
24 BOOT_DET_0_CLR Internal. Only to be used through TI provided API. RW 0
23:18 RESERVED18 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000
17 BOOT_DET_1_SET Internal. Only to be used through TI provided API. RW 0
16 BOOT_DET_0_SET Internal. Only to be used through TI provided API. RW 0
15 WU_FROM_SD A Wakeup from SHUTDOWN on an IO event has occurred, or a wakeup from SHUTDOWN has occurred as a result of the debugger being attached.. (TCK pin being forced low)

Please refer to [IOC:IOCFGn,.WU_CFG] for configuring the IO's as wakeup sources.

0: Wakeup occurred from cold reset or brown out as seen in RESET_SRC
1: A wakeup has occurred from SHUTDOWN

Note: This flag can not be cleared and will therefor remain valid untill poweroff/reset
RO 0
14 GPIO_WU_FROM_SD A wakeup from SHUTDOWN on an IO event has occurred

Please refer to [IOC:IOCFGn,.WU_CFG] for configuring the IO's as wakeup sources.

0: The wakeup did not occur from SHUTDOWN on an IO event
1: A wakeup from SHUTDOWN occurred from an IO event

The case where WU_FROM_SD is asserted but this bitfield is not asserted will only occur in a debug session. The boot code will not proceed with wakeup from SHUTDOWN procedure until this bitfield is asserted as well.

Note: This flag can not be cleared and will therefor remain valid untill poweroff/reset
RO 0
13 BOOT_DET_1 Internal. Only to be used through TI provided API. RO 0
12 BOOT_DET_0 Internal. Only to be used through TI provided API. RO 0
11 VDDS_LOSS_EN_OVR Override of VDDS_LOSS_EN

0: Brown out detect of VDDS is ignored, unless VDDS_LOSS_EN=1
1: Brown out detect of VDDS generates system reset (regardless of VDDS_LOSS_EN)

This bit can be locked
RW 0
10 VDDR_LOSS_EN_OVR Override of VDDR_LOSS_EN

0: Brown out detect of VDDR is ignored, unless VDDR_LOSS_EN=1
1: Brown out detect of VDDR generates system reset (regardless of VDDR_LOSS_EN)

This bit can be locked
RW 0
9 VDD_LOSS_EN_OVR Override of VDD_LOSS_EN

0: Brown out detect of VDD is ignored, unless VDD_LOSS_EN=1
1: Brown out detect of VDD generates system reset (regardless of VDD_LOSS_EN)

This bit can be locked
RW 0
8 RESERVED8 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0
7 VDDS_LOSS_EN Controls reset generation in case VDDS is lost

0: Brown out detect of VDDS is ignored, unless VDDS_LOSS_EN_OVR=1
1: Brown out detect of VDDS generates system reset
RW 1
6 VDDR_LOSS_EN Controls reset generation in case VDDR is lost

0: Brown out detect of VDDR is ignored, unless VDDR_LOSS_EN_OVR=1
1: Brown out detect of VDDR generates system reset
RW 1
5 VDD_LOSS_EN Controls reset generation in case VDD is lost

0: Brown out detect of VDD is ignored, unless VDD_LOSS_EN_OVR=1
1: Brown out detect of VDD generates system reset
RW 1
4 CLK_LOSS_EN Controls reset generation in case SCLK_LF is lost. (provided that clock loss detection is enabled by DDI_0_OSC:CTL0.CLK_LOSS_EN)

Note: Clock loss reset generation must be disabled before SCLK_LF clock source is changed in DDI_0_OSC:CTL0.SCLK_LF_SRC_SEL and remain disabled untill the change is confirmed in DDI_0_OSC:STAT0.SCLK_LF_SRC. Failure to do so may result in a spurious system reset. Clock loss reset generation can be disabled through this bitfield or by clearing DDI_0_OSC:CTL0.CLK_LOSS_EN

0: Clock loss is ignored
1: Clock loss generates system reset
RW 0
3:1 RESET_SRC Shows the source of the last system reset:
Occurrence of one of the reset sources may trigger several other reset sources as essential parts of the system are undergoing reset. This field will report the root cause of the reset (not the other resets that are consequence of the system reset).
To support this feature the actual register is not captured before the reset source being released. If a new reset source is triggered, in a window of four 32 kHz periods after the previous has been released, this register may indicate Power on reset as source.
Value ENUM Name Description
0x0 PWR_ON Power on reset
0x1 PIN_RESET Reset pin
0x2 VDDS_LOSS Brown out detect on VDDS
0x3 VDD_LOSS Brown out detect on VDD
0x4 VDDR_LOSS Brown out detect on VDDR
0x5 CLK_LOSS Clock loss detect
0x6 SYSRESET Software reset via SYSRESET register
0x7 WARMRESET Software reset via PRCM warm reset request
RO 0b000
0 RESERVED0 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0

TOP:AON_SYSCTL:SLEEPCTL

Address Offset 0x0000 0008
Physical Address 0x4009 0008 Instance 0x4009 0008
Description Sleep Mode

This register is used to unfreeze the IO pad ring after waking up from SHUTDOWN
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 IO_PAD_SLEEP_DIS Controls the I/O pad sleep mode. The boot code will set this bitfield automatically unless waking up from a SHUTDOWN ( RESETCTL.WU_FROM_SD is set ).

0: I/O pad sleep mode is enabled, ie all pads are latched and can not toggle.
1: I/O pad sleep mode is disabled

Application software may want to reconfigure the state for all IO's before setting this bitfield upon waking up from a SHUTDOWN.
RW 0