CC13xx Driver Library
Analog Domain

Modules

 [adi] Analog to Digital Interface
 
 [ddi] Digital to Digital Interface
 

Detailed Description

Access to registers in the analog domain of the device goes through master modules controlling slave modules which contain the actual registers. The master module is located in the digital domain of the device. The interfaces between master and slave modules are called ADI (Analog-to-Digital Interface) and DDI (Digital-to-Digital Interface) depending on the type of module to access and thus the slave modules are referred to as ADI slave and DDI slave.

The ADI and DDI APIs provide access to these registers:

The register descriptions of CPU memory map document the ADI/DDI masters. The register descriptions of analog memory map document the ADI/DDI slaves. The ADI/DDI APIs allow the programmer to focus on the slave registers of interest without being concerned with the ADI/DDI master part of the interface.

Although the ADI/DDI APIs make the master "transparent" it can be useful to know a few details about the ADI/DDI protocol and how the master handles transactions as it can affect how the system CPU performs.

Making posted/buffered writes from the system CPU (default) to the ADI/DDI allows the system CPU to continue while the ADI/DDI master handles the transactions on the ADI/DDI protocol. If using non-posted/non-buffered writes the system CPU will wait for ADI/DDI master to complete the transactions to the slave before continuing execution.

Reading from ADI/DDI requires that all transactions on the ADI/DDI protocol have completed before the system CPU receives the response thus the programmer must understand that the response time depends on the number of bytes read. However, due to the 'set', 'clear' and 'masked write' features of the ADI/DDI most writes can be done without the typical read-modify-write sequence thus reducing the need for reads to a minimum.

Consequently, if making posted/buffered writes then the written value will not take effect in the analog domain until some point later in time. An alternative to non-posted/non-buffered writes - in order to make sure a written value has taken effect - is to read from the same ADI/DDI as the write as this will keep the system CPU waiting until both the write and the read have completed.

Note
Do NOT use masked write when writing bit fields spanning the "masked write boundary" i.e. the widest possible masked write that the protocol supports (ADI = 4 bits, DDI = 16 bits). This will put the device into a temporary state - which is potentially harmful to the device - as the bit field will be written over two transactions. Thus to use masked writes:
  • For ADI the bit field(s) must be within bit 0 to 3 (REG[3:0]) or bit 4 to 7 (REG[7:4]).
  • For DDI the bit field(s) must be within bit 0 to 15 (REG[15:0]) or bit 16 to 31 (REG[31:16]).
If masked write is not allowed, a regular read-modify-write is necessary.