Release date: August 4, 2015
IMPORTANT NOTICE
This is a pre-release version of software for the CC1310, and it should not be used in production of CC1310 devices.
The CC1310 production release software is in its final stages of development and verification, and it should be expected that radio-specific timings and parameters will change in that release.
New features
- [RF_SRC] GenFSK: Added new GenFSK command - CMD_TX_POWER_BOOST.
- [DRV_SRC] Event: Added functions to set and clear software events (EventSwEventSet, EventSwEventClear and EventSwEventGet).
- [DRV_SRC] AON_RTC: Added function AONRTCCurrent64BitValueGet(), returning the SEC and SUB_SEC registers as one 64 bits result.
- [DRV_SRC] CCFGRead: Added new module with a set of functions returning most of the CCFG bit fields.
- [DRV_SRC] CCFG: Add CCFG configuration option to use CACHE RAM as general purpose RAM (GPRAM) - (Choosing between having cache or having 8 K-bytes of extra RAM).
- [DRV_SRC] CCFG: Added ability to change the CCFG struct location. This is a special functionality needed only if executing entirely from RAM. Note that the prebuilt library is built with default CCFG location and will not work properly if CCFG location is changed.
Improvements
- [RF_SRC] General: TX performance enhancements.
- [DRV_SRC] AON_RTC: Changed function AONRTCCurrentCompareValueGet() to avoid disabling interrupts.
- [DRV_SRC] General: Code size optimization of several modules.
- [RF_DOC] General: Integrated "RF" documentation into the existing documentation structure.
Bug fixes
- [DRV_SRC] OSC: XOSC startup time calculation done by function OSCHF_GetStartupTime() returned maximum startup time too early.
- [DRV_SRC] CPU: Corrected compiler error when compiled with GCC.
Known Issues
- None
- For an updated list of known issues (including issues found after the release), see CC13xxWare on the Texas Instruments wiki.