1 /*
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * */
13 /*
14 * ======== Log.xdc ========
15 */
16
17 /*!
18 * ======== Log ========
19 * Event logging manager
20 *
21 * RTSC modules and the application code generate `{@link #Event Log_Event}`
22 * events by calling the `Log` module's functions. The `Log` module then
23 * passes those events to an `{@link ILogger}` instance assigned to the event
24 * originating module, specified by that module's configuration parameter
25 * `common$.logger`. `ILogger` instances handle events, usually converting
26 * events to `{@link #EventRec Log_EventRec}` records prior to recording,
27 * transmitting, or displaying them.
28 *
29 * All events generated by a target module are stored and displayed by an
30 * `ILogger`, examples of which are instances of
31 * `{@link LoggerBuf xdc.runtime.LoggerBuf}` or
32 * `{@link LoggerSys xdc.runtime.LoggerSys}`. At runtime, modules
33 * generate events through this module, rather than invoking directly their
34 * `ILogger`s. By doing so, modules can be configured to use different
35 * `ILogger` implementations without any changes to their source code.
36 *
37 * A logger instance can accept `Log` events from any module, but a module
38 * can put `Log` events to only one logger instance. There can be one or
39 * more logger instances in a system. All `Log` calls that are not in a
40 * module are controlled by the module `{@link Main xdc.runtime.Main}`.
41 * For example, top-level application code or any existing sources that
42 * simply call the `Log` or `Assert` methods implicitly use the logger
43 * associated with the `Main` module.
44 *
45 * The generation of a `Log` event is controlled by a module's diagnostics
46 * mask, which is described in details in `{@link Diags}`. Each `Log` event
47 * is associated with a mask. `Log` events are generated only when a
48 * particular bit is set in both the `Log` event mask and the module's
49 * diagnostics mask. For example, a `Log` event mask with the
50 * `{@link Diags#USER1 USER1}` bit set is generated only when the `USER1`
51 * bit is also set in the module's diagnostics mask.
52 *
53 * There are two ways to generate `Log` events:
54 *
55 * @p(blist) 56 * - `{@link #write8 Log_write()}`, which is tailored for module writers
57 * and takes full advantage of the XDC configuration model. For example,
58 * the message string associated with the `Log` event need not be a part of
59 * the final application, significantly reducing the "footprint overhead"
60 * of embedding diagnostics in deployed systems. The `Log_write[0-8]()`
61 * functions allow up to 8 values to be passed to the logger. They expect
62 * the logger to handle any formatting. A `Log` event type allows you to
63 * specify the type of event.
64 * - `{@link #print6 Log_print()}`, which is designed for arbitrary C code.
65 * The `Log_print[0-6]()` functions allow up to 6 values to be passed along
66 * with a printf-like format string to the logger. They handle printf-style
67 * formatting.
68 * @p 69 *
70 * Both functions are controlled by the module's diagnostics mask. Their
71 * storage or output is defined by the logger that is assigned to the
72 * module that calls the `Log` methods or to the
73 * `{@link Main xdc.runtime.Main}` module if the caller is not part of a
74 * module.
75 *
76 * The `Log` function call sites are implemented in such a way that an
77 * optimizer can completely eliminate `Log` code from the program if the
78 * `Log` functions have been permanently disabled at configuration time. If
79 * the `Log` functions are permanently turned on at configuration time,
80 * then the optimizer can eliminate all runtime conditional checking and
81 * simply invoke the `Log` functions directly. Runtime checking is performed
82 * only when the `Log` functions are configured to be runtime modifiable.
83 *
84 * The Log calls can also be completely removed by defining the symbol
85 * `xdc_runtime_Log_DISABLE_ALL`. This can be done on the compile line, e.g.
86 * `-Dxdc_runtime_Log_DISABLE_ALL`. This will completely remove the `Log`
87 * statements from any code compiled with this flag, regardless of the
88 * application's logging configuration or your compiler's optimization
89 * settings.
90 *
91 * It is also possible to remove all logging except for
92 * `{@link #error Log_error}`, `{@link #warning Log_warning}`, or
93 * `{@link #info Log_info}` statements. This is done by first defining
94 * `xdc_runtime_Log_DISABLE_ALL`, followed by defining one or more of the
95 * symbols below to leave that type of logging enabled:
96 * @p(blist) 97 * - `xdc_runtime_Log_ENABLE_ERROR`
98 * - `xdc_runtime_Log_ENABLE_WARNING`
99 * - `xdc_runtime_Log_ENABLE_INFO`
100 * @p 101 * For example, to disable all `Log` statements except for `Log_error`, add
102 * the following to the compile line:
103 * @p(code) 104 * -Dxdc_runtime_Log_DISABLE_ALL -Dxdc_runtime_Log_ENABLE_ERROR
105 * @p 106 *
107 * @a(Examples) 108 * Example 1: The following example defines a `Log` event, uses that `Log`
109 * event in a module, and configures the program to generate the `Log`
110 * event. In this example, both `USER1` and `USER2` bits are set in the
111 * event mask. This means that if either bit is set in the module's
112 * diagnostics mask, then the `Log` event will be generated.
113 *
114 * This is a part of the XDC specification file for the `Mod` module
115 * (Mod.xdc):
116 *
117 * @p(code) 118 * import xdc.runtime.Diags;
119 * import xdc.runtime.Log;
120 *
121 * config Log.Event L_someEvent = {
122 * mask: Diags.USER1 | Diags.USER2,
123 * level: Diags.LEVEL1,
124 * msg: "my log event message, arg1: 0x%x, arg2: 0x%x"
125 * };
126 * @p 127 *
128 * This is a part of the C code implementation of the Mod module:
129 *
130 * @p(code) 131 * #include <xdc/runtime/Log.h>
132 * UInt x, y;
133 *
134 * Log_write2(Mod_L_someEvent, (IArg)x, (IArg)y);
135 * @p 136 *
137 * The following configuration script demonstrates how the application might
138 * control the `Log` statements embedded in the `Mod` module at configuration
139 * time. In this case, the configuration script arranges for the `Log`
140 * statements within the `Mod` module (shown above) to always generate events.
141 * Without these configuration statements, no `Log` events would be generated
142 * by this module.
143 *
144 * This is part of the XDC configuration file for the application:
145 *
146 * @p(code) 147 * var Diags = xdc.useModule('xdc.runtime.Diags');
148 * var LoggerSys = xdc.useModule('xdc.runtime.LoggerSys');
149 * var Mod = xdc.useModule('my.pkg.Mod');
150 * Mod.common$.diags_USER1 = Diags.ALWAYS_ON;
151 * Mod.common$.logger = LoggerSys.create();
152 * @p 153 *
154 * @p(html) 155 * <hr />
156 * @p 157 *
158 * Example 2: The following XDC configuration statements turn on enter
159 * and exit logging at configuration time for a module. Without any other
160 * changes in the runtime code, every time a module `Mod`'s function is
161 * being called or exits, an event will be logged.
162 *
163 * @p(code) 164 * var Diags = xdc.useModule('xdc.runtime.Diags');
165 * var Mod = xdc.useModule('my.pkg.Mod');
166 *
167 * Mod.common$.diags_ENTER = Diags.ALWAYS_ON;
168 * Mod.common$.diags_EXIT = Diags.ALWAYS_ON;
169 * @p 170 *
171 * @p(html) 172 * <hr />
173 * @p 174 *
175 * Example 3: The following example configures a module to support enter and
176 * exit logging, but defers the actual activation and deactivation of the
177 * logging until runtime. See the `{@link Diags#setMask Diags_setMask()}`
178 * function for details on specifying the control string.
179 *
180 * This is a part of the XDC configuration file for the application:
181 *
182 * @p(code) 183 * var Diags = xdc.useModule('xdc.runtime.Diags');
184 * var Mod = xdc.useModule('my.pkg.Mod');
185 *
186 * Mod.common$.diags_ENTER = Diags.RUNTIME_OFF;
187 * Mod.common$.diags_EXIT = Diags.RUNTIME_OFF;
188 * @p 189 *
190 * This is a part of the C code for the application:
191 *
192 * @p(code) 193 * // turn on enter and exit logging in the module
194 * Diags_setMask("my.pkg.Mod+EX");
195 *
196 * // turn off enter and exit logging in the module
197 * Diags_setMask("my.pkg.Mod-EX");
198 * @p 199 */
200
201 @CustomHeader
202 @DirectCall
203
204 module Log {
205
206 /*!
207 * ======== NUMARGS ========
208 * Maximum number of arguments supported in `Log` events.
209 */
210 const Int NUMARGS = 8;
211
212 /*!
213 * ======== PRINTFID ========
214 * The `EventId` for `Log_print()` events
215 */
216 const EventId PRINTFID = 0;
217
218 /*!
219 * ======== EventDesc ========
220 * `Log` event descriptor
221 *
222 * Each `Log` event is defined by a `Log` event descriptor.
223 *
224 * The `mask` defines which bits in the module's diagnostics mask
225 * enable this `Log` event. Events "posted" via `Log_write` are only
226 * written to the underlying logger if one of the mask's bits matches
227 * the caller's module diagnostics settings (see
228 * `{@link xdc.runtime.Types#common$}`).
229 *
230 * The 'level' defines the event level of the event. While the diags
231 * bits selected in the 'mask' signify the "category" of the event (e.g.
232 * Entry/Exit, Analysis, Info), the 'level' field allows you to assign
233 * a "priority" or "detail level" to the event relative to other events in
234 * that category. There are four event levels defined by
235 * '{@link xdc.runtime.Diags#EventLevel}'.
236 *
237 * Filtering of events by level is handled by the ILogger implementation.
238 * ILogger implementations which also implement the {@link IFilterLogger}
239 * interface support filtering of events based on priority level.
240 *
241 * Specifying an event level is optional. Events that don't specify a
242 * level will receive Diags.LEVEL1 by default, making them the highest
243 * priority and ensuring that they will not inadvertently be filtered out
244 * by level-based filtering.
245 *
246 * The `msg` defines a printf style format string that defines how to
247 * render the arguments passed along the event in a `Log_write` call.
248 * For a description of the allowable format strings see
249 * `{@link #print6}`.
250 *
251 * @see #write8
252 * @see #print6
253 */
254 metaonlystruct EventDesc {
255 Diags.Mask mask; /*! event enable mask */
256 Diags.EventLevel level; /*! event level relative to other events */
257 String msg; /*! event "printf" message format string */
258 };
259
260 /*!
261 * ======== EventRec ========
262 * The target representation of a recorded event
263 *
264 * This structure defines how events are recorded on the target.
265 */
266 struct EventRec {
267 Types.Timestamp64 tstamp; /*! time event was written */
268 Bits32 serial; /*! serial number of event */
269 Types.Event evt; /*! target encoding of an Event */
270 IArg arg[NUMARGS]; /*! arguments passed via Log_write/print */
271 }
272
273 /*!
274 * ======== Event ========
275 * `Log` event type
276 *
277 * An `Event` is represented on the target as a 32-bit value that can
278 * be decoded offline to recover the `Event` information defined in
279 * a corresponding metaonly `EventDesc`. In addition, `Event`s may be
280 * decoded at runtime via methods provided in this module; see
281 * `{@link #getMask}` and `{@link #getEventId}`.
282 *
283 * When an event is "raised" a `{@link Types#Event Types_Event}` is
284 * created which has the same event ID as the `Log_Event` but also
285 * encodes the module ID of the caller. This new event is passed to
286 * the underlying `{@link ILogger}` module along with any arguments
287 * associated with the event.
288 *
289 * @see #getMask
290 * @see #getEventId
291 */
292 @Encoded typedef EventDesc Event;
293
294 /*!
295 * ======== EventId ========
296 * Unique ID embedded in each `{@link #Event}`
297 *
298 * This ID must be used to compare two `Event`s for equality. Event
299 * ids are not guaranteed to remain constant between different
300 * configurations of an application. For example, adding a module
301 * may cause the event ids of another module to change.
302 *
303 * However, event ids declared by a module are guaranteed to be
304 * consecutive values starting from the first declared
305 * `{@link #Event Log_Event}` and increasing to the last declared
306 * event. As a result, clients of a module can efficiently test ranges
307 * of events and modules can add new events, such as internal trace
308 * events, without breaking clients; simply be careful to add new events
309 * after any existing events in you module's `.xdc` specification.
310 *
311 * @see #getEventId
312 * @see #Event
313 */
314 typedef Types.RopeId EventId;
315
316 /*!
317 * ======== L_construct ========
318 * Lifecycle event posted when an instance is constructed
319 */
320 config Log.Event L_construct = {
321 mask: Diags.LIFECYCLE,
322 msg: "<-- construct: %p('%s')"
323 };
324
325 /*!
326 * ======== L_create ========
327 * Lifecycle event posted when an instance is created
328 */
329 config Log.Event L_create = {
330 mask: Diags.LIFECYCLE,
331 msg: "<-- create: %p('%s')"
332 };
333
334 /*!
335 * ======== L_destruct ========
336 * Lifecycle event posted when an instance is destructed
337 */
338 config Log.Event L_destruct = {
339 mask: Diags.LIFECYCLE,
340 msg: "--> destruct: (%p)"
341 };
342
343 /*!
344 * ======== L_delete ========
345 * Lifecycle event posted when an instance is deleted
346 */
347 config Log.Event L_delete = {
348 mask: Diags.LIFECYCLE,
349 msg: "--> delete: (%p)"
350 };
351
352 /*!
353 * ======== L_error ========
354 * Error event posted by Log_errorX API
355 *
356 * This event is marked as a STATUS event and given the priority level
357 * of ERROR.
358 *
359 * This event prints the Log call site (%$F) and a format string (%$S)
360 * which is recursively formatted with any additional arguments.
361 */
362 config Log.Event L_error = {
363 mask: Diags.STATUS,
364 level: Diags.ERROR,
365 msg: "ERROR: %$F%$S"
366 };
367
368 /*!
369 * ======== L_warning ========
370 * Warning event posted by Log_warningX API
371 *
372 * This event is marked as a STATUS event and given the priority level of
373 * WARNING.
374 *
375 * This event prints the Log call site (%$F) and a format string (%$S)
376 * which is recursively formatted with any addition arguments.
377 */
378 config xdc.runtime.Log.Event L_warning = {
379 mask: Diags.STATUS,
380 level: Diags.WARNING,
381 msg: "WARNING: %$F%$S"
382 };
383
384 /*!
385 * ======== L_info ========
386 * Info event posted by Log_infoX API
387 *
388 * This event is marked as an INFO event. The event priority is not
389 * specified in the event definition. Rather, it is specified as an
390 * argument to the Log_infoX APIs.
391 *
392 * This event prints the Log call site (%$F) and a format string (%$S)
393 * which is recursively formatted with any addition arguments.
394 */
395 config xdc.runtime.Log.Event L_info = {
396 mask: Diags.INFO,
397 msg: "%$F%$S"
398 };
399
400 /*!
401 * ======== L_start ========
402 * Benchmark event used to log the start of an operation
403 * @_nodoc 404 *
405 * @a(Example) 406 * The following C code shows how to log a simple
407 * benchmark 'start' event along with a user-specified
408 * format string describing the event.
409 *
410 * @p(code) 411 * #include <xdc/runtime/Log.h>
412 * ...
413 * Log_write2(Log_L_start, (IArg)"My benchmark event", (IArg)myUniqueId);
414 * Log_write2(Log_L_stop, (IArg)"My benchmark event", (IArg)myUniqueId);
415 * @p 416 *
417 * @param(fmt) a constant string that provides format specifiers for
418 * up to 6 additional parameters
419 * @param(id) a unique ID used to match benchmark start and stop
420 * events
421 */
422 config xdc.runtime.Log.Event L_start = {
423 mask: Diags.ANALYSIS,
424 msg: "Start: %$S"};
425
426 /*!
427 * ======== L_stop ========
428 * Benchmark event used to log the end of an operation
429 * @_nodoc 430 *
431 * @a(Example) 432 * The following C code shows how to log a simple
433 * benchmark 'stop' event along with a user-specified
434 * format string describing the event.
435 *
436 * @p(code) 437 * #include <xdc/runtime/Log.h>
438 * ...
439 * Log_write2(Log_L_start, (IArg)"My benchmark event", (IArg)myUniqueId);
440 * Log_write2(Log_L_stop, (IArg)"My benchmark event", (IArg)myUniqueId);
441 * @p 442 *
443 * @param(fmt) a constant string that provides format specifiers for
444 * up to 6 additional parameters
445 * @param(id) a unique ID used to match benchmark start and stop
446 * events
447 */
448 config xdc.runtime.Log.Event L_stop = {
449 mask: Diags.ANALYSIS,
450 msg: "Stop: %$S"};
451
452 /*!
453 * ======== L_startInstance ========
454 * Benchmark event used to log the start of an operation instance
455 * @_nodoc 456 *
457 * Event parameter provides instance data to differentiate
458 * between multiple instances that can run in parallel.
459 *
460 * @a(Example) 461 * The following C code shows how to log a benchmark
462 * 'startInstance' event along with a user-specified
463 * instance identifier and a format string describing the event.
464 *
465 * @p(code) 466 * #include <xdc/runtime/Log.h>
467 * ...
468 * Log_write3(Log_L_startInstance, (IArg)"My benchmark event", (IArg)uniqueId, (IArg)instId);
469 * ...
470 * Log_write3(Log_L_stopInstance, (IArg)"My benchmark event", (IArg)uniqueId, (IArg)instId);
471 * @p 472 *
473 * @param(fmt) a constant string that provides format specifiers for
474 * up to 6 additional parameters
475 * @param(id) a unique ID used to match benchmark start and stop
476 * events
477 * @param(instId) a unique instance ID that can be used to match
478 * instance events
479 */
480 config xdc.runtime.Log.Event L_startInstance = {
481 mask: Diags.ANALYSIS,
482 msg: "StartInstance: %$S"
483 };
484
485 /*!
486 * ======== L_stopInstance ========
487 * Benchmark event used to log the end of an operation instance
488 * @_nodoc 489 *
490 * Event parameter provides instance data to differentiate
491 * between multiple instances that can run in parallel.
492 *
493 * @a(Example) 494 * The following C code shows how to log a benchmark
495 * 'stopInstance' event along with a user-specified
496 * instance identifier and a format string describing the event.
497 *
498 * @p(code) 499 * #include <xdc/runtime/Log.h>
500 * ...
501 * Log_write3(Log_L_startInstance, (IArg)"My benchmark event", (IArg)uniqueId, (IArg)instId);
502 * ...
503 * Log_write3(Log_L_stopInstance, (IArg)"My benchmark event", (IArg)uniqueId, (IArg)instId);
504 * @p 505 *
506 * @param(fmt) a constant string that provides format specifiers for
507 * up to 6 additional parameters
508 * @param(id) a unique ID used to match benchmark start and stop
509 * events
510 * @param(instId) a unique instance ID that can be used to match
511 * instance events
512 */
513 config xdc.runtime.Log.Event L_stopInstance = {
514 mask: Diags.ANALYSIS,
515 msg: "StopInstance: %$S"
516 };
517
518 /*!
519 * ======== getMask ========
520 * Get the `Diags` mask for the specified (encoded) event
521 *
522 * @param(evt) the `Log` event encoding a mask and event ID
523 *
524 * @a(returns) `Diags` mask for the specified event
525 */
526 @Macro Diags.Mask getMask(Event evt);
527
528 /*!
529 * ======== getRope ========
530 * Get RopeId of the Event.msg for the specified (encoded) event
531 * @_nodoc 532 */
533 @Macro Text.RopeId getRope(Event evt);
534
535 /*!
536 * ======== getEventId ========
537 * Get event ID of the specified (encoded) event
538 *
539 * This method is used to compare "known" `Log` events with
540 * "raised" `{@link Types#Event Types_Event}`.
541 *
542 * @param(evt) the `Log` event encoding a mask and event ID
543 *
544 * @a(returns) event ID of the specified event
545 *
546 * @see Types#getEventId
547 */
548 @Macro EventId getEventId(Event evt);
549
550 /*!
551 * ======== print0 ========
552 * Generate a `Log` "print event" with 0 arguments
553 *
554 * @see #print6
555 */
556 @Macro Void print0(Diags.Mask mask, CString fmt);
557
558 /*!
559 * ======== print1 ========
560 * Generate a `Log` "print event" with 1 argument
561 *
562 * @see #print6
563 */
564 @Macro Void print1(Diags.Mask mask, CString fmt, IArg a1);
565
566 /*!
567 * ======== print2 ========
568 * Generate a `Log` "print event" with 2 arguments
569 *
570 * @see #print6
571 */
572 @Macro Void print2(Diags.Mask mask, CString fmt, IArg a1, IArg a2);
573
574 /*!
575 * ======== print3 ========
576 * Generate a `Log` "print event" with 3 arguments
577 *
578 * @see #print6
579 */
580 @Macro Void print3(Diags.Mask mask, CString fmt, IArg a1, IArg a2,
581 IArg a3);
582
583 /*!
584 * ======== print4 ========
585 * Generate a `Log` "print event" with 4 arguments
586 *
587 * @see #print6
588 */
589 @Macro Void print4(Diags.Mask mask, CString fmt, IArg a1, IArg a2,
590 IArg a3, IArg a4);
591
592 /*!
593 * ======== print5 ========
594 * Generate a `Log` "print event" with 5 arguments
595 *
596 * @see #print6
597 */
598 @Macro Void print5(Diags.Mask mask, CString fmt, IArg a1, IArg a2,
599 IArg a3, IArg a4, IArg a5);
600
601 /*!
602 * ======== print6 ========
603 * Generate a `Log` "print event" with 6 arguments
604 *
605 * As a convenience to C (as well as assembly language) programmers,
606 * the `Log` module provides a variation of the ever-popular `printf`
607 * function.
608 * The `print[0-6]` functions generate a `Log` "print event" and route
609 * it to the current module's logger.
610 *
611 * The arguments passed to `print[0-6]` may be characters, integers,
612 * strings, or pointers. However, because the declared type of the
613 * arguments is `{@link xdc IArg}`, all pointer arguments must be cast
614 * to an `IArg` type. `IArg` is an integral type large enough to hold
615 * any pointer or an `int`. So, casting a pointer to an `IArg` does
616 * not cause any loss of information and C's normal integer conversions
617 * make the cast unnecessary for integral arguments.
618 *
619 * The format string can use the following conversion characters.
620 * However, it is important to recall that all arguments referenced by
621 * these conversion characters have been converted to an `IArg`
622 * prior to conversion; so, the use of "length modifiers" should be
623 * avoided.
624 *
625 * @p(code) 626 * Conversion Character Description
627 * ------------------------------------------------
628 * %c Character
629 * %d Signed integer
630 * %u Unsigned integer
631 * %x Unsigned hexadecimal integer
632 * %o Unsigned octal integer
633 * %s Character string
634 * %p Pointer
635 * %f Single precision floating point (float)
636 * @p 637 *
638 * Format strings, while very convenient, are a well known source of
639 * portability problems: each format specification must precisely match
640 * the types of the arguments passed. Underlying "printf" functions use
641 * the format string to determine how far to advance through their
642 * argument list. For targets where pointer types and integers are the
643 * same size there are no problems. However, suppose a target's pointer
644 * type is larger than its integer type. In this case, because integer
645 * arguments are widened to be of type `IArg`, a format specification of
646 * "%d" causes an underlying `printf()` implementation to read the
647 * extended part of the integer argument as part of the next argument(!).
648 *
649 * To get around this problem and still allow the use of "natural"
650 * format specifications (e.g., `%d` and `%x` with optional width
651 * specifications), `{@link System#aprintf()}` is used which assumes
652 * that all arguments have been widened to be of type `IArg`.
653 *
654 * See `{@link System#printf}` for complete details.
655 *
656 * The `%f` format specifier is used to print a single precision float
657 * value. Note that `%f` assumes that sizeof(Float) <= sizeof(IArg).
658 * Most clients that interpret float values expect that they are
659 * represented in IEEE 754 floating point format. Therefore, it is
660 * recommended that the float values be converted into that format prior
661 * to supplying the values to `Log` functions in cases where targets do
662 * not generate the float values in IEEE 754 floating point format by
663 * default.
664 *
665 * The first argument to a `Log_print` call is the diags category to be
666 * associated with the event.
667 *
668 * It is also possible to associate an event level with the event to
669 * enable filtering of events based on event level. Conceptually, it is
670 * best to regard the event level as completely separate from the event's
671 * diags category; however, the priority value actually occupies a part
672 * of the diags mask. For this reason, it is possible to specify an event
673 * level by OR'ing the level with the diags mask. For example, to print
674 * an `Diags_INFO` event of `Diags_LEVEL2`, you'd simply write:
675 * (Diags_INFO | Diags_LEVEL2)
676 *
677 * Specifying an event level is optional. `Log_print` calls which do not
678 * specify a level will receive the highest priority by default.
679 *
680 * @param(mask) enable bits and optional detail level for this event
681 * @param(fmt) a `printf` style format string
682 * @param(a1) value for first format conversion character
683 * @param(a2) value for second format conversion character
684 * @param(a3) value for third format conversion character
685 * @param(a4) value for fourth format conversion character
686 * @param(a5) value for fifth format conversion character
687 * @param(a6) value for sixth format conversion character
688 *
689 * @a(Examples) 690 * The following example demonstrates a typical usage.
691 * @p(code) 692 * String list[];
693 * UInt i;
694 *
695 * Log_print2(Diags_USER2, "list[%u] = %s\n", i, (IArg)list[i]);
696 * @p 697 * Note that the `IArg` cast above is only necessary for pointer
698 * arguments; C's normal parameter conversions implicitly convert
699 * integral arguments.
700 *
701 * To simplify the conversion from `float` arguments to `IArg`,
702 * the standard header `xdc/std.h` provides a macro, named floatToArg(),
703 * to do this conversion in a type safe manner. So, the following
704 * statement will print "`float = 2.3456`":
705 * @p(code) 706 * Log_print1(Diags_USER1, "float = %f", floatToArg(2.34567));
707 * @p 708 *
709 * Note that, if you are formatting events on the target, you must
710 * also add support for floating point to ASCII conversion to
711 * `{@link System#printf}`; for more information, see the
712 * `{@link System#extendedFormats}` reference documenation. For example:
713 * @p(code) 714 * var System = xdc.useModule('xdc.runtime.System');
715 * System.extendedFormats = "%f";
716 * @p 717 */
718 @Macro Void print6(Diags.Mask mask, CString fmt, IArg a1, IArg a2,
719 IArg a3, IArg a4, IArg a5, IArg a6);
720
721 /*!
722 * ======== error0 ========
723 * Generate a `Log` "error event" with 0 arguments
724 *
725 * @see #error5
726 */
727 @Macro Void error0(CString fmt);
728
729 /*!
730 * ======== error1 ========
731 * Generate a `Log` "error event" with 1 argument
732 *
733 * @see #error5
734 */
735 @Macro Void error1(CString fmt, IArg a1);
736
737 /*!
738 * ======== error2 ========
739 * Generate a `Log` "error event" with 2 arguments
740 *
741 * @see #error5
742 */
743 @Macro Void error2(CString fmt, IArg a1, IArg a2);
744
745 /*!
746 * ======== error3 ========
747 * Generate a `Log` "error event" with 3 arguments
748 *
749 * @see #error5
750 */
751 @Macro Void error3(CString fmt, IArg a1, IArg a2, IArg a3);
752
753 /*!
754 * ======== error4 ========
755 * Generate a `Log` "error event" with 4 arguments
756 *
757 * @see #error5
758 */
759 @Macro Void error4(CString fmt, IArg a1, IArg a2, IArg a3,
760 IArg a4);
761
762 /*!
763 * ======== error5 ========
764 * Generate a `Log` "error event" with 5 arguments
765 *
766 * The Log_error APIs are intended to allow users to easily log error
767 * events in their code. Similar to the Log_print APIs, Log_error does not
768 * require that you define an event. You simply pass an informative error
769 * string which can optionally be formatted with additional arguments. The
770 * error is logged with the predefined event {@link #L_error}.
771 *
772 * Log_error prepends a string to the message which identifies it as an
773 * ERROR and specifies the filename and line number of the Log_error call
774 * site. A simple example:
775 *
776 * @p(code) 777 * Log_error0("Invalid argument");
778 * @p 779 * This event will be formatted as (assuming that the above call was line
780 * 35 of "MyCode.c")
781 * @p(code) 782 * ERROR at "MyCode.c", line 35: Invalid argument
783 * @p 784 *
785 * Users may provide additional information in the error event, such as
786 * a predefined error code or details of the error. These additional
787 * values will be used to format the string passed to Log_error.
788 * @see #print6 for information about format strings.
789 *
790 * Log_error does not use a variable length argument list--you must call
791 * the appropriate Log_errorX API based on the number of arguments.
792 *
793 * @param(fmt) a reference to a constant error string / fmt string
794 * @param(a1) value for an additional parameter (e.g. an error code)
795 * @param(a2) value for an additional parameter
796 * @param(a3) value for an additional parameter
797 * @param(a4) value for an additional parameter
798 * @param(a5) value for an additional parameter
799 *
800 * @a(Examples) 801 * The following example demonstrates a typical usage.
802 * @p(code) 803 * Int myArg;
804 *
805 * Log_error1("Invalid argument: %d", myArg);
806 * @p 807 * The above event is formatted as, for example:
808 * @p(code) 809 * ERROR: "MyCode.c", line 35: Invalid argument: -1
810 * @p 811 */
812 @Macro Void error5(CString fmt, IArg a1, IArg a2, IArg a3,
813 IArg a4, IArg a5);
814
815 /*!
816 * ======== warning0 ========
817 * Generate a `Log` "warning event" with 0 arguments
818 *
819 * @see #warning5
820 */
821 @Macro Void warning0(CString fmt);
822
823 /*!
824 * ======== warning1 ========
825 * Generate a `Log` "warning event" with 1 argument
826 *
827 * @see #warning5
828 */
829 @Macro Void warning1(CString fmt, IArg a1);
830
831 /*!
832 * ======== warning2 ========
833 * Generate a `Log` "warning event" with 2 arguments
834 *
835 * @see #warning5
836 */
837 @Macro Void warning2(CString fmt, IArg a1, IArg a2);
838
839 /*!
840 * ======== warning3 ========
841 * Generate a `Log` "warning event" with 3 arguments
842 *
843 * @see #warning5
844 */
845 @Macro Void warning3(CString fmt, IArg a1, IArg a2, IArg a3);
846
847 /*!
848 * ======== warning4 ========
849 * Generate a `Log` "warning event" with 4 arguments
850 *
851 * @see #warning5
852 */
853 @Macro Void warning4(CString fmt, IArg a1, IArg a2, IArg a3,
854 IArg a4);
855
856 /*!
857 * ======== warning5 ========
858 * Generate a `Log` "warning event" with 5 arguments
859 *
860 * The Log_warning APIs provide the same features as the Log_error APIs,
861 * but are used to specifically log "warning" events.
862 * @see #error5
863 *
864 * The Log_warning APIs are equivalent to the Log_error APIs except that
865 * they use the predefined {@link #L_warning} event. Log_warning prepends
866 * a string to the message which identifies it as a WARNING and specifies
867 * the filename and line number of the Log_warning call site.
868 *
869 * @param(fmt) reference to a constant warning string / fmt string
870 * @param(a1) value for an additional parameter (e.g. a warning code)
871 * @param(a2) value for an additional parameter
872 * @param(a3) value for an additional parameter
873 * @param(a4) value for an additional parameter
874 * @param(a5) value for an additional parameter
875 *
876 * @a(Examples) 877 * The following example demonstrates a typical usage.
878 * @p(code) 879 * Int myArg;
880 *
881 * Log_warning1("Value may be too high: %d", myArg);
882 * @p 883 * The above event is formatted as:
884 * @p(code) 885 * WARNING: "MyCode.c", line 50: Value may be too high: 4096
886 * @p 887 */
888 @Macro Void warning5(CString fmt, IArg a1, IArg a2, IArg a3,
889 IArg a4, IArg a5);
890
891 /*!
892 * ======== info0 ========
893 * Generate a `Log` "info event" with 0 arguments
894 *
895 * @see #info5
896 */
897 @Macro Void info0(CString fmt);
898
899 /*!
900 * ======== info1 ========
901 * Generate a `Log` "info event" with 1 argument
902 *
903 * @see #info5
904 */
905 @Macro Void info1(CString fmt, IArg a1);
906
907 /*!
908 * ======== info2 ========
909 * Generate a `Log` "info event" with 2 arguments
910 *
911 * @see #info5
912 */
913 @Macro Void info2(CString fmt, IArg a1, IArg a2);
914
915 /*!
916 * ======== info3 ========
917 * Generate a `Log` "info event" with 3 arguments
918 *
919 * @see #info5
920 */
921 @Macro Void info3(CString fmt, IArg a1, IArg a2, IArg a3);
922
923 /*!
924 * ======== info4 ========
925 * Generate a `Log` "info event" with 4 arguments
926 *
927 * @see #info5
928 */
929 @Macro Void info4(CString fmt, IArg a1, IArg a2, IArg a3, IArg a4);
930
931 /*!
932 * ======== info5 ========
933 * Generate a `Log` "info event" with 5 arguments
934 *
935 * The Log_info APIs are provided for easily logging generic
936 * "informational" events with call site information. They are similar to
937 * the Log_print APIs in that they do not require you to define an event--
938 * you simply pass an informative printf-style string which can optionally
939 * be formatted with additional arguments. The info record is logged with
940 * the predefined event '{@link #L_info}'.
941 *
942 * The Log_info APIs log the {@link #L_info} event which uses the 'INFO'
943 * diags category. They do not allow you to specify an event priority.
944 *
945 * Log_info prepends the filename and line number of the call site to the
946 * message.
947 *
948 * @param(fmt) reference to a constant event string / fmt string
949 * @param(a1) value for an additional parameter (e.g. an event code)
950 * @param(a2) value for an additional parameter
951 * @param(a3) value for an additional parameter
952 * @param(a4) value for an additional parameter
953 * @param(a5) value for an additional parameter
954 *
955 * @a(Examples) 956 * The following example demonstrates a typical usage.
957 * @p(code) 958 * Int load;
959 *
960 * Log_info1("Current load: %d", load);
961 * @p 962 * The above event is formatted as, for example:
963 * @p(code) 964 * "MyCode.c", line 15: Current load: 25
965 * @p 966 */
967 @Macro Void info5(CString fmt, IArg a1, IArg a2, IArg a3, IArg a4,
968 IArg a5);
969
970 /*!
971 * ======== put0 ========
972 * Unconditionally put the specified Log event with 0 arguments
973 *
974 * @see #put8
975 */
976 @Macro Void put0(Log.Event evt, Types.ModuleId mid);
977
978 /*!
979 * ======== put1 ========
980 * Unconditionally put the specified Log event and 1 argument
981 *
982 * @see #put8
983 */
984 @Macro Void put1(Log.Event evt, Types.ModuleId mid, IArg a1);
985
986 /*!
987 * ======== put2 ========
988 * Unconditionally put the specified Log event and 2 arguments
989 *
990 * @see #put8
991 */
992 @Macro Void put2(Log.Event evt, Types.ModuleId mid, IArg a1, IArg a2);
993
994 /*!
995 * ======== put4 ========
996 * Unconditionally put the specified Log event and 4 arguments
997 *
998 * @see #put8
999 */
1000 @Macro Void put4(Log.Event evt, Types.ModuleId mid, IArg a1, IArg a2,
1001 IArg a3, IArg a4);
1002
1003 /*!
1004 * ======== put8 ========
1005 * Unconditionally put the specified Log event and 8 arguments
1006 *
1007 * This method unconditionally puts the specified `{@link Event}`
1008 * `evt` into the log. The `{@link Types#ModuleId}` `mid` should be the
1009 * module ID of the module which is putting the event.
1010 *
1011 * @param(evt) the Log event to put into the log
1012 * @param(mid) module ID of the module putting the event
1013 * @param(a1) value for first format conversion character
1014 * @param(a2) value for second format conversion character
1015 * @param(a3) value for third format conversion character
1016 * @param(a4) value for fourth format conversion character
1017 * @param(a5) value for fifth format conversion character
1018 * @param(a6) value for sixth format conversion character
1019 * @param(a7) value for seventh format conversion character
1020 * @param(a8) value for eighth format conversion character
1021 */
1022 @Macro Void put8(Log.Event evt, Types.ModuleId mid, IArg a1, IArg a2,
1023 IArg a3, IArg a4, IArg a5, IArg a6, IArg a7, IArg a8);
1024
1025 /*!
1026 * ======== write0 ========
1027 * Generate a `Log` event with 0 arguments
1028 *
1029 * @see #write8
1030 */
1031 @Macro Void write0(Event evt);
1032
1033 /*!
1034 * ======== write1 ========
1035 * Generate a `Log` event with 1 argument
1036 *
1037 * @see #write8
1038 */
1039 @Macro Void write1(Event evt, IArg a1);
1040
1041 /*!
1042 * ======== write2 ========
1043 * Generate a `Log` event with 2 arguments
1044 *
1045 * @see #write8
1046 */
1047 @Macro Void write2(Event evt, IArg a1, IArg a2);
1048
1049 /*!
1050 * ======== write3 ========
1051 * Generate a `Log` event with 3 arguments
1052 *
1053 * @see #write8
1054 */
1055 @Macro Void write3(Event evt, IArg a1, IArg a2, IArg a3);
1056
1057 /*!
1058 * ======== write4 ========
1059 * Generate a `Log` event with 4 arguments
1060 *
1061 * @see #write8
1062 */
1063 @Macro Void write4(Event evt, IArg a1, IArg a2, IArg a3, IArg a4);
1064
1065 /*!
1066 * ======== write5 ========
1067 * Generate a `Log` event with 5 arguments
1068 *
1069 * @see #write8
1070 */
1071 @Macro Void write5(Event evt, IArg a1, IArg a2, IArg a3, IArg a4, IArg a5);
1072
1073 /*!
1074 * ======== write6 ========
1075 * Generate a `Log` event with 6 arguments
1076 *
1077 * @see #write8
1078 */
1079 @Macro Void write6(Event evt, IArg a1, IArg a2, IArg a3, IArg a4,
1080 IArg a5, IArg a6);
1081
1082 /*!
1083 * ======== write7 ========
1084 * Generate a `Log` event with 7 arguments
1085 *
1086 * @see #write8
1087 */
1088 @Macro Void write7(Event evt, IArg a1, IArg a2, IArg a3, IArg a4,
1089 IArg a5, IArg a6, IArg a7);
1090
1091 /*!
1092 * ======== write8 ========
1093 * Generate a `Log` event with 8 arguments
1094 *
1095 * If the mask in the specified `Log` event has any bit set which is
1096 * also set in the current module's diagnostics mask, then this call to
1097 * write will "raise" the given `Log` event.
1098 *
1099 * @param(evt) the `Log` event to write
1100 * @param(a1) value for first format conversion character
1101 * @param(a2) value for second format conversion character
1102 * @param(a3) value for third format conversion character
1103 * @param(a4) value for fourth format conversion character
1104 * @param(a5) value for fifth format conversion character
1105 * @param(a6) value for sixth format conversion character
1106 * @param(a7) value for seventh format conversion character
1107 * @param(a8) value for eighth format conversion character
1108 */
1109 @Macro Void write8(Event evt, IArg a1, IArg a2, IArg a3, IArg a4,
1110 IArg a5, IArg a6, IArg a7, IArg a8);
1111
1112 /*!
1113 * ======== doPrint ========
1114 * Render an event as text via `{@link System#printf System_printf}`
1115 *
1116 * This method is not gated and may make more than one call to
1117 * `System_printf`. This utility method is typically used within the
1118 * implementation of a logger which initializes
1119 * `{@link #EventRec Log_EventRec}` structures based on `Log` events
1120 * produced by the application.
1121 *
1122 * @param(evRec) a non`NULL` pointer to an initialized `Log_EventRec`
1123 * structure to be formated via
1124 * `{@link System#printf System_printf}`.
1125 */
1126 Void doPrint(EventRec *evRec);
1127
1128 /*!
1129 * @_nodoc 1130 * ======== lookupEventMessage ========
1131 * Returns the format string for the event with the given id.
1132 */
1133 function lookupEventMessage(eventId);
1134
1135 /*!
1136 * @_nodoc 1137 * ======== getTargetArgSize ========
1138 * Returns the target size of a record argument in bytes (not MAUs).
1139 */
1140 function getTargetArgSize();
1141
1142 /*!
1143 * @_nodoc 1144 * ======== lookupEventName ========
1145 */
1146 function lookupEventName(eventId);
1147
1148 /*!
1149 * @_nodoc 1150 * ======== lookupModuleName ========
1151 */
1152 function lookupModuleName(modId);
1153
1154 /*!
1155 * @_nodoc 1156 * ======== getTargetEventRecSize ========
1157 * Returns the record size in bytes (not MAUs).
1158 */
1159 function getTargetEventRecSize();
1160
1161 internal:
1162
1163 /*
1164 * ======== idToInfo ========
1165 * Map event ID strings into a string of the form <eventName>::<eventMsg>
1166 */
1167 metaonlyconfig String idToInfo[string] = [];
1168 }
1169 /*
1170 * @(#) xdc.runtime; 2, 1, 0,0; 4-24-2015 12:34:12; /db/ztree/library/trees/xdc/xdc-A71/src/packages/
1171 */
1172