void MYTIME_exit(void)
Stops and deletes the Clock instance created in the init function.
void MYTIME_settime(uint32_t newtime)
Sets the time to the value passed in via the newtime parameter (units in seconds).
uint32_t MYTIME_gettime(void)
Returns the number of seconds since the Epoch (January 1, 1970).
void MYTIME_init(void)
Create a new Clock instance that ticks every second.