WDT

Instance: WDT
Component: WDT
Base address: 0x40080000


Watchdog Timer

TOP:WDT Register Summary

Register Name

Type

Register Width (Bits)

Register Reset

Address Offset

Physical Address

LOAD

RW

32

0xFFFF FFFF

0x0000 0000

0x4008 0000

VALUE

RO

32

0xFFFF FFFF

0x0000 0004

0x4008 0004

CTL

RW

32

0x0000 0000

0x0000 0008

0x4008 0008

ICR

WO

32

0x0000 0000

0x0000 000C

0x4008 000C

RIS

RO

32

0x0000 0000

0x0000 0010

0x4008 0010

MIS

RO

32

0x0000 0000

0x0000 0014

0x4008 0014

TEST

RW

32

0x0000 0000

0x0000 0418

0x4008 0418

INT_CAUS

RO

32

0x0000 0000

0x0000 041C

0x4008 041C

LOCK

RW

32

0x0000 0000

0x0000 0C00

0x4008 0C00

TOP:WDT Register Descriptions

TOP:WDT:LOAD

Address Offset 0x0000 0000
Physical Address 0x4008 0000 Instance 0x4008 0000
Description Configuration
Type RW
Bits Field Name Description Type Reset
31:0 WDTLOAD This register is the 32-bit interval value used by the 32-bit counter. When this register is written, the value is immediately loaded and the counter is restarted to count down from the new value. If this register is loaded with 0x0000.0000, an interrupt is immediately generated. RW 0xFFFF FFFF

TOP:WDT:VALUE

Address Offset 0x0000 0004
Physical Address 0x4008 0004 Instance 0x4008 0004
Description Current Count Value
Type RO
Bits Field Name Description Type Reset
31:0 WDTVALUE This register contains the current count value of the timer. RO 0xFFFF FFFF

TOP:WDT:CTL

Address Offset 0x0000 0008
Physical Address 0x4008 0008 Instance 0x4008 0008
Description Control
Type RW
Bits Field Name Description Type Reset
31:3 RESERVED3 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000 0000 0000 0000 0000 0000 0000
2 INTTYPE WDT Interrupt Type

0: WDT interrupt is a standard interrupt.
1: WDT interrupt is a non-maskable interrupt.
Value ENUM Name Description
0x0 MASKABLE Maskable interrupt
0x1 NONMASKABLE Non-maskable interrupt
RW 0
1 RESEN WDT Reset Enable. Defines the function of the WDT reset source (see PRCM:WARMRESET.WDT_STAT if enabled)

0: Disabled.
1: Enable the Watchdog reset output.
Value ENUM Name Description
0x0 DIS Reset output Disabled
0x1 EN Reset output Enabled
RW 0
0 INTEN WDT Interrupt Enable

0: Interrupt event disabled.
1: Interrupt event enabled. Once set, this bit can only be cleared by a hardware reset.
Value ENUM Name Description
0x0 DIS Interrupt Disabled
0x1 EN Interrupt Enabled
RW 0

TOP:WDT:ICR

Address Offset 0x0000 000C
Physical Address 0x4008 000C Instance 0x4008 000C
Description Interrupt Clear
Type WO
Bits Field Name Description Type Reset
31:0 WDTICR This register is the interrupt clear register. A write of any value to this register clears the WDT interrupt and reloads the 32-bit counter from the LOAD register. WO 0x0000 0000

TOP:WDT:RIS

Address Offset 0x0000 0010
Physical Address 0x4008 0010 Instance 0x4008 0010
Description Raw Interrupt Status
Type RO
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 WDTRIS This register is the raw interrupt status register. WDT interrupt events can be monitored via this register if the controller interrupt is masked.

Value Description

0: The WDT has not timed out
1: A WDT time-out event has occurred
RO 0

TOP:WDT:MIS

Address Offset 0x0000 0014
Physical Address 0x4008 0014 Instance 0x4008 0014
Description Masked Interrupt Status
Type RO
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 WDTMIS This register is the masked interrupt status register. The value of this register is the logical AND of the raw interrupt bit and the WDT interrupt enable bit CTL.INTEN.

Value Description

0: The WDT has not timed out or is masked.
1: An unmasked WDT time-out event has occurred.
RO 0

TOP:WDT:TEST

Address Offset 0x0000 0418
Physical Address 0x4008 0418 Instance 0x4008 0418
Description Test Mode
Type RW
Bits Field Name Description Type Reset
31:9 RESERVED9 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000
8 STALL WDT Stall Enable

0: The WDT timer continues counting if the CPU is stopped with a debugger.
1: If the CPU is stopped with a debugger, the WDT stops counting. Once the CPU is restarted, the WDT resumes counting.
Value ENUM Name Description
0x0 DIS Disable STALL
0x1 EN Enable STALL
RW 0
7:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
0 TEST_EN The test enable bit

0: Enable external reset
1: Disables the generation of an external reset. Instead bit 1 of the INT_CAUS register is set and an interrupt is generated
Value ENUM Name Description
0x0 DIS Test mode Disabled
0x1 EN Test mode Enabled
RW 0

TOP:WDT:INT_CAUS

Address Offset 0x0000 041C
Physical Address 0x4008 041C Instance 0x4008 041C
Description Interrupt Cause Test Mode

ITERNAL_NOTE: This register shows the status of Reset and Interrupt when test mode is enabled, TEST.TEST_EN
Type RO
Bits Field Name Description Type Reset
31:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000 0000 0000 0000 0000
1 CAUSE_RESET Indicates that the cause of an interrupt was a reset generated but blocked due to TEST.TEST_EN (only possible when TEST.TEST_EN is set). RO 0
0 CAUSE_INTR Replica of RIS.WDTRIS RO 0

TOP:WDT:LOCK

Address Offset 0x0000 0C00
Physical Address 0x4008 0C00 Instance 0x4008 0C00
Description Lock
Type RW
Bits Field Name Description Type Reset
31:0 WDTLOCK WDT Lock: A write of the value 0x1ACC.E551 unlocks the watchdog registers for write access. A write of any other value reapplies the lock, preventing any register updates (NOTE: TEST.TEST_EN bit is not lockable).

A read of this register returns the following values:

0x0000.0000: Unlocked
0x0000.0001: Locked
RW 0x0000 0000