I2C0

Instance: I2C0
Component: I2C
Base address: 0x40002000


I2CMaster/Slave Serial Controler

TOP:I2C0 Register Summary

Register Name

Type

Register Width (Bits)

Register Reset

Address Offset

Physical Address

SOAR

RW

32

0x0000 0000

0x0000 0000

0x4000 2000

SSTAT

RO

32

0x0000 0000

0x0000 0004

0x4000 2004

SCTL

WO

32

0x0000 0000

0x0000 0004

0x4000 2004

SDR

RW

32

0x0000 0000

0x0000 0008

0x4000 2008

SIMR

RW

32

0x0000 0000

0x0000 000C

0x4000 200C

SRIS

RO

32

0x0000 0000

0x0000 0010

0x4000 2010

SMIS

RO

32

0x0000 0000

0x0000 0014

0x4000 2014

SICR

WO

32

0x0000 0000

0x0000 0018

0x4000 2018

MSA

RW

32

0x0000 0000

0x0000 0800

0x4000 2800

MSTAT

RO

32

0x0000 0020

0x0000 0804

0x4000 2804

MCTRL

WO

32

0x0000 0000

0x0000 0804

0x4000 2804

MDR

RW

32

0x0000 0000

0x0000 0808

0x4000 2808

MTPR

RW

32

0x0000 0001

0x0000 080C

0x4000 280C

MIMR

RW

32

0x0000 0000

0x0000 0810

0x4000 2810

MRIS

RO

32

0x0000 0000

0x0000 0814

0x4000 2814

MMIS

RO

32

0x0000 0000

0x0000 0818

0x4000 2818

MICR

WO

32

0x0000 0000

0x0000 081C

0x4000 281C

MCR

RW

32

0b0000 0000 0000 0000 00XX XXXX 0000 0000

0x0000 0820

0x4000 2820

TOP:I2C0 Register Descriptions

TOP:I2C0:SOAR

Address Offset 0x0000 0000
Physical Address 0x4000 2000 Instance 0x4000 2000
Description Slave Own Address
This register consists of seven address bits that identify this I2C device on the I2C bus.
Type RW
Bits Field Name Description Type Reset
31:7 RESERVED7 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000 0000 0000 0000 0000 0000
6:0 OAR I2C slave own address
This field specifies bits a6 through a0 of the slave address.
RW 0b000 0000

TOP:I2C0:SSTAT

Address Offset 0x0000 0004
Physical Address 0x4000 2004 Instance 0x4000 2004
Description Slave Status
Internal Note: This register shares address with SCTL, meaning that this register functions as a control register when written, and a status register when read.
Type RO
Bits Field Name Description Type Reset
31:3 RESERVED3 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000 0000 0000 0000 0000 0000 0000
2 FBR First byte received

0: The first byte has not been received.
1: The first byte following the slave's own address has been received.

This bit is only valid when the RREQ bit is set and is automatically cleared when data has been read from the SDR register.
Note: This bit is not used for slave transmit operations.
RO 0
1 TREQ Transmit request

0: No outstanding transmit request.
1: The I2C controller has been addressed as a slave transmitter and is using clock stretching to delay the master until data has been written to the SDR register.
RO 0
0 RREQ Receive request

0: No outstanding receive data
1: The I2C controller has outstanding receive data from the I2C master and is using clock stretching to delay the master until data has been read from the SDR register.
RO 0

TOP:I2C0:SCTL

Address Offset 0x0000 0004
Physical Address 0x4000 2004 Instance 0x4000 2004
Description Slave Control
Note: This register shares address with SSTAT, meaning that this register functions as a control register when written, and a status register when read.
Type WO
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved field. Writing any other value may result in undefined behavior. WO 0b000 0000 0000 0000 0000 0000 0000 0000
0 DA Device active

0: Disables the I2C slave operation
1: Enables the I2C slave operation
WO 0

TOP:I2C0:SDR

Address Offset 0x0000 0008
Physical Address 0x4000 2008 Instance 0x4000 2008
Description Slave Data
This register contains the data to be transmitted when in the Slave Transmit state, and the data received when in the Slave Receive state.
Type RW
Bits Field Name Description Type Reset
31:8 RESERVED8 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x00 0000
7:0 DATA Data for transfer
This field contains the data for transfer during a slave receive or transmit operation. When written the register data is used as transmit data. When read, this register returns the last data received.
Data is stored until next update, either by a system write for transmit or by an external master for receive.
RW 0x00

TOP:I2C0:SIMR

Address Offset 0x0000 000C
Physical Address 0x4000 200C Instance 0x4000 200C
Description Slave Interrupt Mask
This register controls whether a raw interrupt is promoted to a controller interrupt.
Type RW
Bits Field Name Description Type Reset
31:3 RESERVED3 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000 0000 0000 0000 0000 0000 0000
2 STOPIM Stop condition interrupt mask

0: The SRIS.STOPRIS interrupt is suppressed and not sent to the interrupt controller.
1: The SRIS.STOPRIS interrupt is enabled and sent to the interrupt controller.
Value ENUM Name Description
0x0 DIS Disable Interrupt
0x1 EN Enable Interrupt
RW 0
1 STARTIM Start condition interrupt mask

0: The SRIS.STARTRIS interrupt is suppressed and not sent to the interrupt controller.
1: The SRIS.STARTRIS interrupt is enabled and sent to the interrupt controller.
Value ENUM Name Description
0x0 DIS Disable Interrupt
0x1 EN Enable Interrupt
RW 0
0 DATAIM Data interrupt mask

0: The SRIS.DATARIS interrupt is suppressed and not sent to the interrupt controller.
1: The SRIS.DATARIS interrupt is enabled and sent to the interrupt controller.
RW 0

TOP:I2C0:SRIS

Address Offset 0x0000 0010
Physical Address 0x4000 2010 Instance 0x4000 2010
Description Slave Raw Interrupt Status
This register shows the unmasked interrupt status.
Type RO
Bits Field Name Description Type Reset
31:3 RESERVED3 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000 0000 0000 0000 0000 0000 0000
2 STOPRIS Stop condition raw interrupt status

0: No interrupt
1: A Stop condition interrupt is pending.

This bit is cleared by writing a 1 to SICR.STOPIC.
RO 0
1 STARTRIS Start condition raw interrupt status

0: No interrupt
1: A Start condition interrupt is pending.

This bit is cleared by writing a 1 to SICR.STARTIC.
RO 0
0 DATARIS Data raw interrupt status

0: No interrupt
1: A data received or data requested interrupt is pending.

This bit is cleared by writing a 1 to the SICR.DATAIC.
RO 0

TOP:I2C0:SMIS

Address Offset 0x0000 0014
Physical Address 0x4000 2014 Instance 0x4000 2014
Description Slave Masked Interrupt Status
This register show which interrupt is active (based on result from SRIS and SIMR).
Type RO
Bits Field Name Description Type Reset
31:3 RESERVED3 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000 0000 0000 0000 0000 0000 0000
2 STOPMIS Stop condition masked interrupt status

0: An interrupt has not occurred or is masked/disabled.
1: An unmasked Stop condition interrupt is pending.

This bit is cleared by writing a 1 to the SICR.STOPIC.
RO 0
1 STARTMIS Start condition masked interrupt status

0: An interrupt has not occurred or is masked/disabled.
1: An unmasked Start condition interrupt is pending.

This bit is cleared by writing a 1 to the SICR.STARTIC.
RO 0
0 DATAMIS Data masked interrupt status

0: An interrupt has not occurred or is masked/disabled.
1: An unmasked data received or data requested interrupt is pending.

This bit is cleared by writing a 1 to the SICR.DATAIC.
RO 0

TOP:I2C0:SICR

Address Offset 0x0000 0018
Physical Address 0x4000 2018 Instance 0x4000 2018
Description Slave Interrupt Clear
This register clears the raw interrupt SRIS.
Type WO
Bits Field Name Description Type Reset
31:3 RESERVED3 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. WO 0b0 0000 0000 0000 0000 0000 0000 0000
2 STOPIC Stop condition interrupt clear

Writing 1 to this bit clears SRIS.STOPRIS and SMIS.STOPMIS.
WO 0
1 STARTIC Start condition interrupt clear

Writing 1 to this bit clears SRIS.STARTRIS SMIS.STARTMIS.
WO 0
0 DATAIC Data interrupt clear

Writing 1 to this bit clears SRIS.DATARIS SMIS.DATAMIS.
WO 0

TOP:I2C0:MSA

Address Offset 0x0000 0800
Physical Address 0x4000 2800 Instance 0x4000 2800
Description Master Salve Address
This register contains seven address bits of the slave to be accessed by the master (a6-a0), and an RS bit determining if the next operation is a receive or transmit.
Type RW
Bits Field Name Description Type Reset
31:8 RESERVED8 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x00 0000
7:1 SA I2C master slave address
Defines which slave is addressed for the transaction in master mode
RW 0b000 0000
0 RS Receive or Send
This bit-field specifies if the next operation is a receive (high) or a transmit/send (low) from the addressed slave SA.
Value ENUM Name Description
0x0 TX Transmit/send data to slave
0x1 RX Receive data from slave
RW 0

TOP:I2C0:MSTAT

Address Offset 0x0000 0804
Physical Address 0x4000 2804 Instance 0x4000 2804
Description Master Status
Type RO
Bits Field Name Description Type Reset
31:7 RESERVED7 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000 0000 0000 0000 0000 0000
6 BUSBSY Bus busy

0: The I2C bus is idle.
1: The I2C bus is busy.

The bit changes based on the MCTRL.START and MCTRL.STOP conditions.
RO 0
5 IDLE I2C idle

0: The I2C controller is not idle.
1: The I2C controller is idle.
RO 1
4 ARBLST Arbitration lost

0: The I2C controller won arbitration.
1: The I2C controller lost arbitration.
RO 0
3 DATACK_N Data Was Not Acknowledge

0: The transmitted data was acknowledged.
1: The transmitted data was not acknowledged.
RO 0
2 ADRACK_N Address Was Not Acknowledge

0: The transmitted address was acknowledged.
1: The transmitted address was not acknowledged.
RO 0
1 ERR Error

0: No error was detected on the last operation.
1: An error occurred on the last operation.
RO 0
0 BUSY I2C busy

0: The controller is idle.
1: The controller is busy.

When this bit-field is set, the other status bits are not valid.

Note: The I2C controller requires four SYSBUS clock cycles to assert the BUSY status after I2C master operation has been initiated through MCTRL register.
Hence after programming MCTRL register, application is requested to wait for four SYSBUS clock cycles before issuing a controller status inquiry through MSTAT register.
Any prior inquiry would result in wrong status being reported.
RO 0

TOP:I2C0:MCTRL

Address Offset 0x0000 0804
Physical Address 0x4000 2804 Instance 0x4000 2804
Description Master Control

This register accesses status bits when read and control bits when written. When read, the status register indicates the state of the I2C bus controller as stated in MSTAT. When written, the control register configures the I2C controller operation.

To generate a single transmit cycle, the I2C Master Slave Address (MSA) register is written with the desired address, the MSA.RS bit is cleared, and this register is written with
* ACK=X (0 or 1),
* STOP=1,
* START=1,
* RUN=1
to perform the operation and stop.
When the operation is completed (or aborted due an error), an interrupt becomes active and the data may be read from the MDR register.
Type WO
Bits Field Name Description Type Reset
31:4 RESERVED4 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. WO 0x000 0000
3 ACK Data acknowledge enable

0: The received data byte is not acknowledged automatically by the master.
1: The received data byte is acknowledged automatically by the master.

This bit-field must be cleared when the I2C bus controller requires no further data to be transmitted from the slave transmitter.
Value ENUM Name Description
0x0 DIS Disable acknowledge
0x1 EN Enable acknowledge
WO 0
2 STOP This bit-field determines if the cycle stops at the end of the data cycle or continues on to a repeated START condition.

0: The controller does not generate the Stop condition.
1: The controller generates the Stop condition.
Value ENUM Name Description
0x0 DIS Disable STOP
0x1 EN Enable STOP
WO 0
1 START This bit-field generates the Start or Repeated Start condition.

0: The controller does not generate the Start condition.
1: The controller generates the Start condition.
Value ENUM Name Description
0x0 DIS Disable START
0x1 EN Enable START
WO 0
0 RUN I2C master enable

0: The master is disabled.
1: The master is enabled to transmit or receive data.
Value ENUM Name Description
0x0 DIS Disable Master
0x1 EN Enable Master
WO 0

TOP:I2C0:MDR

Address Offset 0x0000 0808
Physical Address 0x4000 2808 Instance 0x4000 2808
Description Master Data
This register contains the data to be transmitted when in the Master Transmit state and the data received when in the Master Receive state.
Type RW
Bits Field Name Description Type Reset
31:8 RESERVED8 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x00 0000
7:0 DATA When Read: Last RX Data is returned
When Written: Data is transferred during TX transaction
RW 0x00

TOP:I2C0:MTPR

Address Offset 0x0000 080C
Physical Address 0x4000 280C Instance 0x4000 280C
Description I2C Master Timer Period
This register specifies the period of the SCL clock.
Type RW
Bits Field Name Description Type Reset
31:8 RESERVED8 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x00 0000
7 TPR_7 Must be set to 0 to set TPR. If set to 1, a write to TPR will be ignored. RW 0
6:0 TPR SCL clock period
This field specifies the period of the SCL clock.
SCL_PRD = 2*(1+TPR)*(SCL_LP + SCL_HP)*CLK_PRD
where:
SCL_PRD is the SCL line period (I2C clock).
TPR is the timer period register value (range of 1 to 127)
SCL_LP is the SCL low period (fixed at 6).
SCL_HP is the SCL high period (fixed at 4).
CLK_PRD is the system clock period in ns.
RW 0b000 0001

TOP:I2C0:MIMR

Address Offset 0x0000 0810
Physical Address 0x4000 2810 Instance 0x4000 2810
Description Master Interrupt Mask
This register controls whether a raw interrupt is promoted to a controller interrupt.
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 IM Interrupt mask

0: The MRIS.RIS interrupt is suppressed and not sent to the interrupt controller.
1: The master interrupt is sent to the interrupt controller when the MRIS.RIS is set.
Value ENUM Name Description
0x0 DIS Disable Interrupt
0x1 EN Enable Interrupt
RW 0

TOP:I2C0:MRIS

Address Offset 0x0000 0814
Physical Address 0x4000 2814 Instance 0x4000 2814
Description Master Raw Interrupt Status
This register show the unmasked interrupt status.
Type RO
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 RIS Raw interrupt status

0: No interrupt
1: A master interrupt is pending.

This bit is cleared by writing 1 to the MICR.IC bit .
RO 0

TOP:I2C0:MMIS

Address Offset 0x0000 0818
Physical Address 0x4000 2818 Instance 0x4000 2818
Description Master Masked Interrupt Status
This register show which interrupt is active (based on result from MRIS and MIMR).
Type RO
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 MIS Masked interrupt status

0: An interrupt has not occurred or is masked.
1: A master interrupt is pending.

This bit is cleared by writing 1 to the MICR.IC bit .
RO 0

TOP:I2C0:MICR

Address Offset 0x0000 081C
Physical Address 0x4000 281C Instance 0x4000 281C
Description Master Interrupt Clear
This register clears the raw and masked interrupt.
Type WO
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. WO 0b000 0000 0000 0000 0000 0000 0000 0000
0 IC Interrupt clear
Writing 1 to this bit clears MRIS.RIS and MMIS.MIS .

Reading this register returns no meaningful data.
WO 0

TOP:I2C0:MCR

Address Offset 0x0000 0820
Physical Address 0x4000 2820 Instance 0x4000 2820
Description Master Configuration
This register configures the mode (Master or Slave) and sets the interface for test mode loopback.
Type RW
Bits Field Name Description Type Reset
31:6 RESERVED6 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RW 0b00 0000 0000 0000 0000 XXXX XX00
5 SFE I2C slave function enable
Value ENUM Name Description
0x0 DIS Slave mode is disabled.
0x1 EN Slave mode is enabled.
RW 0
4 MFE I2C master function enable
Value ENUM Name Description
0x0 DIS Master mode is disabled.
0x1 EN Master mode is enabled.
RW 0
3:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000
0 LPBK I2C loopback

0: Normal operation
1: Loopback operation (test mode)
Value ENUM Name Description
0x0 DIS Disable Test Mode
0x1 EN Enable Test Mode
RW 0