Instance: AON_SYSCTL
Component: AON_SYSCTL
Base address: 0x40090000
This component controls AON_SYSCTL, which is the device's system controller.
Note: This module is only supporting 32 bit ReadWrite access from MCU
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
RW |
32 |
0b0000 0000 0000 0000 0000 0XXX 0000 0000 |
0x0000 0000 |
0x4009 0000 |
|
RW |
32 |
0x0000 00E0 |
0x0000 0004 |
0x4009 0004 |
|
RW |
32 |
0x0000 0000 |
0x0000 0008 |
0x4009 0008 |
Address Offset | 0x0000 0000 | ||
Physical Address | 0x4009 0000 | Instance | 0x4009 0000 |
Description | Power Management This register controls bitfields for setting low level power management features such as selection of regulator for VDDR supply and control of IO ring where certain segments can be enabled / disabled. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:3 | RESERVED3 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b0 0000 0000 0000 0000 0000 XXX0 0000 | ||
2 | DCDC_ACTIVE | Select to use DCDC regulator for VDDR in active mode 0: Use GLDO for regulation of VDDRin active mode. 1: Use DCDC for regulation of VDDRin active mode. |
RW | 0 | ||
1 | EXT_REG_MODE | Status of source for VDDRsupply: 0: DCDC/GLDO are generating VDDR 1: DCDC/GLDO are bypassed, external regulator supplies VDDR |
RO | 0 | ||
0 | DCDC_EN | Select to use DCDC regulator during recharge of VDDR 0: Use GLDO for recharge of VDDR 1: Use DCDC for recharge of VDDR Note: This bitfield should be set to the same as DCDC_ACTIVE |
RW | 0 |
Address Offset | 0x0000 0004 | ||
Physical Address | 0x4009 0004 | Instance | 0x4009 0004 |
Description | Reset Management This register contains bitfields releated to system reset such as reset source and reset request and control of brown out resets. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||||||||||||||||||||
31 | SYSRESET | Cold reset register. Writing 1 to this bitfield will reset the entire chip and cause boot code to run again. 0: No effect 1: Generate system reset. Appears as SYSRESET in RESET_SRC. |
WO | 0 | |||||||||||||||||||||||||||||
30:26 | RESERVED26 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b0 0000 | |||||||||||||||||||||||||||||
25 | BOOT_DET_1_CLR | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||||||||||||||
24 | BOOT_DET_0_CLR | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||||||||||||||
23:18 | RESERVED18 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 | |||||||||||||||||||||||||||||
17 | BOOT_DET_1_SET | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||||||||||||||
16 | BOOT_DET_0_SET | Internal. Only to be used through TI provided API. | RW | 0 | |||||||||||||||||||||||||||||
15 | WU_FROM_SD | A Wakeup from SHUTDOWN on an IO event has occurred, or a wakeup from SHUTDOWN has occurred as a result of the debugger being attached.. (TCK pin being forced low) Please refer to [IOC:IOCFGn,.WU_CFG] for configuring the IO's as wakeup sources. 0: Wakeup occurred from cold reset or brown out as seen in RESET_SRC 1: A wakeup has occurred from SHUTDOWN Note: This flag can not be cleared and will therefor remain valid untill poweroff/reset |
RO | 0 | |||||||||||||||||||||||||||||
14 | GPIO_WU_FROM_SD | A wakeup from SHUTDOWN on an IO event has occurred Please refer to [IOC:IOCFGn,.WU_CFG] for configuring the IO's as wakeup sources. 0: The wakeup did not occur from SHUTDOWN on an IO event 1: A wakeup from SHUTDOWN occurred from an IO event The case where WU_FROM_SD is asserted but this bitfield is not asserted will only occur in a debug session. The boot code will not proceed with wakeup from SHUTDOWN procedure until this bitfield is asserted as well. Note: This flag can not be cleared and will therefor remain valid untill poweroff/reset |
RO | 0 | |||||||||||||||||||||||||||||
13 | BOOT_DET_1 | Internal. Only to be used through TI provided API. | RO | 0 | |||||||||||||||||||||||||||||
12 | BOOT_DET_0 | Internal. Only to be used through TI provided API. | RO | 0 | |||||||||||||||||||||||||||||
11 | VDDS_LOSS_EN_OVR | Override of VDDS_LOSS_EN 0: Brown out detect of VDDS is ignored, unless VDDS_LOSS_EN=1 1: Brown out detect of VDDS generates system reset (regardless of VDDS_LOSS_EN) This bit can be locked |
RW | 0 | |||||||||||||||||||||||||||||
10 | VDDR_LOSS_EN_OVR | Override of VDDR_LOSS_EN 0: Brown out detect of VDDR is ignored, unless VDDR_LOSS_EN=1 1: Brown out detect of VDDR generates system reset (regardless of VDDR_LOSS_EN) This bit can be locked |
RW | 0 | |||||||||||||||||||||||||||||
9 | VDD_LOSS_EN_OVR | Override of VDD_LOSS_EN 0: Brown out detect of VDD is ignored, unless VDD_LOSS_EN=1 1: Brown out detect of VDD generates system reset (regardless of VDD_LOSS_EN) This bit can be locked |
RW | 0 | |||||||||||||||||||||||||||||
8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 | |||||||||||||||||||||||||||||
7 | VDDS_LOSS_EN | Controls reset generation in case VDDS is lost 0: Brown out detect of VDDS is ignored, unless VDDS_LOSS_EN_OVR=1 1: Brown out detect of VDDS generates system reset |
RW | 1 | |||||||||||||||||||||||||||||
6 | VDDR_LOSS_EN | Controls reset generation in case VDDR is lost 0: Brown out detect of VDDR is ignored, unless VDDR_LOSS_EN_OVR=1 1: Brown out detect of VDDR generates system reset |
RW | 1 | |||||||||||||||||||||||||||||
5 | VDD_LOSS_EN | Controls reset generation in case VDD is lost 0: Brown out detect of VDD is ignored, unless VDD_LOSS_EN_OVR=1 1: Brown out detect of VDD generates system reset |
RW | 1 | |||||||||||||||||||||||||||||
4 | CLK_LOSS_EN | Controls reset generation in case SCLK_LF is lost. (provided that clock loss detection is enabled by DDI_0_OSC:CTL0.CLK_LOSS_EN) Note: Clock loss reset generation must be disabled before SCLK_LF clock source is changed in DDI_0_OSC:CTL0.SCLK_LF_SRC_SEL and remain disabled untill the change is confirmed in DDI_0_OSC:STAT0.SCLK_LF_SRC. Failure to do so may result in a spurious system reset. Clock loss reset generation can be disabled through this bitfield or by clearing DDI_0_OSC:CTL0.CLK_LOSS_EN 0: Clock loss is ignored 1: Clock loss generates system reset |
RW | 0 | |||||||||||||||||||||||||||||
3:1 | RESET_SRC | Shows the source of the last system reset: Occurrence of one of the reset sources may trigger several other reset sources as essential parts of the system are undergoing reset. This field will report the root cause of the reset (not the other resets that are consequence of the system reset). To support this feature the actual register is not captured before the reset source being released. If a new reset source is triggered, in a window of four 32 kHz periods after the previous has been released, this register may indicate Power on reset as source.
|
RO | 0b000 | |||||||||||||||||||||||||||||
0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 |
Address Offset | 0x0000 0008 | ||
Physical Address | 0x4009 0008 | Instance | 0x4009 0008 |
Description | Sleep Mode This register is used to unfreeze the IO pad ring after waking up from SHUTDOWN |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | IO_PAD_SLEEP_DIS | Controls the I/O pad sleep mode. The boot code will set this bitfield automatically unless waking up from a SHUTDOWN ( RESETCTL.WU_FROM_SD is set ). 0: I/O pad sleep mode is enabled, ie all pads are latched and can not toggle. 1: I/O pad sleep mode is disabled Application software may want to reconfigure the state for all IO's before setting this bitfield upon waking up from a SHUTDOWN. |
RW | 0 |
© 2015. Texas Instruments | All Rights Reserved |