Instance: AUX_TIMER
Component: AUX_TIMER
Base address: 0x400C7000
AUX Timer
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
RW |
32 |
0x0000 0000 |
0x0000 0000 |
0x400C 7000 |
|
RW |
32 |
0x0000 0000 |
0x0000 0004 |
0x400C 7004 |
|
RW |
32 |
0x0000 0000 |
0x0000 0008 |
0x400C 7008 |
|
RW |
32 |
0x0000 0000 |
0x0000 000C |
0x400C 700C |
|
RW |
32 |
0x0000 0000 |
0x0000 0010 |
0x400C 7010 |
|
RW |
32 |
0x0000 0000 |
0x0000 0014 |
0x400C 7014 |
Address Offset | 0x0000 0000 | ||
Physical Address | 0x400C 7000 | Instance | 0x400C 7000 |
Description | Timer 0 Configuration | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
31:14 | RESERVED14 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
13 | TICK_SRC_POL | Source count polarity for timer 0
|
RW | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
12:8 | TICK_SRC | Selected tick source for timer 0
|
RW | 0b0 0000 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
7:4 | PRE | Prescaler division ratio is 2^PRE | RW | 0x0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
3:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
1 | MODE | Timer 0 mode
|
RW | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
0 | RELOAD | Timer 0 reload setting
|
RW | 0 |
Address Offset | 0x0000 0004 | ||
Physical Address | 0x400C 7004 | Instance | 0x400C 7004 |
Description | Timer 1 Configuration | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
31:14 | RESERVED14 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 0000 0000 0000 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
13 | TICK_SRC_POL | Source count polarity for timer 1
|
RW | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
12:8 | TICK_SRC | Selected tick source for timer 1
|
RW | 0b0 0000 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
7:4 | PRE | Prescaler division ratio is 2^PRE | RW | 0x0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
3:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
1 | MODE | Timer 1 mode
|
RW | 0 | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
0 | RELOAD | Timer 1 reload setting
|
RW | 0 |
Address Offset | 0x0000 0008 | ||
Physical Address | 0x400C 7008 | Instance | 0x400C 7008 |
Description | Timer 0 Control Run control/status for timer 0 |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | EN | Timer 0 run enable control. The counter restarts when enabling the timer. If T0CFG.RELOAD = 0, the timer is automatically disabled when reaching T0TARGET.VALUE 0: Disable timer 0 1: Enable timer 0 |
RW | 0 |
Address Offset | 0x0000 000C | ||
Physical Address | 0x400C 700C | Instance | 0x400C 700C |
Description | Timer 0 Target Target counter value for timer 0 |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | ||
15:0 | VALUE | Timer 0 counts from 0 to VALUE. Then gives an event and restarts if configured to do to so in the T0CFG.RELOAD setting. If VALUE is changed while timer 0 is running so that the count becomes higher than VALUE timer 0 will also restart if configured to do so. If T0CFG.MODE=0,no prescaler is used, and VALUE equals 1, the TIMER0_EV event line will be always set |
RW | 0x0000 |
Address Offset | 0x0000 0010 | ||
Physical Address | 0x400C 7010 | Instance | 0x400C 7010 |
Description | Timer 1 Target Target Counter Value Timer 1 |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED8 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7:0 | VALUE | Timer 1 counts from 0 to VALUE. Then gives an event and restarts if configured to do to so in the T1CFG.RELOAD setting. If VALUE is changed while timer 1 is running so that the count becomes higher than VALUE timer 1 will also restart if configured to do so. If T1CFG.MODE=0,no prescaler is used, and VALUE equals 1, the TIMER1_EV event line will be always set |
RW | 0x00 |
Address Offset | 0x0000 0014 | ||
Physical Address | 0x400C 7014 | Instance | 0x400C 7014 |
Description | Timer 1 Control Run Control/Status For Timer 1 |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:1 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | ||
0 | EN | Timer 1 run enable control. The counter restarts when enabling the timer. If T1CFG.RELOAD = 0, the timer is automatically disabled when reaching T1TARGET.VALUE 0: Disable timer 1 1: Enable timer 1 |
RW | 0 |
© 2015. Texas Instruments | All Rights Reserved |