![]() |
![]() |
This is an General Availability release of TI-RTOS . This version of TI-RTOS requires CCS 5.5.
MSP430 support in this release is at a "beta" level. All of the other components in this release of TI-RTOS are at a GA level.The following documentation is available:
Release notes from previous releases are also available in the release notes archive directory.ID | Headline |
SDOCM00105001 | TI-RTOS EMAC drivers should use Hwi instead of NDK's interrupt module |
SDOCM00105047 | ROV for I2C for MSP430 does not work |
SDOCM00105385 | USB Mouse Device readme has incorrect Example Summary |
SDOCM00105605 | TI-RTOS drivers use too much stack space |
SDOCM00105607 | Add support for MSP-EXP430F5529 Experimenter board into TI-RTOS |
SDOCM00105696 | GPIO is missing graphical configuration |
SDOCM00105717 | Graphical Config should not allow modules not available on that device (e.g. NDK on MSP430) |
SDOCM00105718 | Add examples and ROV support into IAR workbench |
SDOCM00105719 | TI-RTOS needs to support GCC for ARM boards |
SDOCM00105721 | Use new TivaWare version (2.0.1.11577) |
This release requires the following other software components and tools versions to successfully function:
ID | Headline |
SDOCM00088081 | SD Card driver lacks CRC support |
SDOCM00093268 | Add parity and error checking for UART driver |
SDOCM00093967 | TI-RTOS Windows install will fail if installed in multiple or single directory that contains more than 38 characters in path |
SDOCM00094053 | TI-RTOS sub-products (e.g. UIA, IPC) are not linked into CCS Help |
SDOCM00097626 | Giving Priorities to Hwis from TI-RTOS Drivers |
SDOCM00098063 | UART driver needs to support DMA |
SDOCM00099017 | TI-RTOS needs to make sub-products examples accessible |
SDOCM00099460 | ping flood causes Concerto board to stop receiving interrupts |
SDOCM00099858 | Stellaris launchpad doesn't detect a USB disconnect event |
SDOCM00100494 | SPI driver was not tested in Slave Open Drain mode |
SDOCM00100864 | Multithreaded CC3000 Host Driver does not work properly |
SDOCM00100865 | TI-RTOS drivers should have top-level enable and disable APIs |
SDOCM00100945 | Make TCP/UDP Echo for CC3000 examples more like NDK TCP/UDP Echo examples |
SDOCM00101155 | Intermittent spin lock in USB library's USBHCDPipeRead() for LM4F232 |
SDOCM00101176 | SPIMessageQTransport does not support static creates |
SDOCM00101229 | HTTP demo doesn't show the current SD Card logging state |
SDOCM00101240 | Coverity for WiFi driver reports several defects in the CC3000 Host Driver |
SDOCM00102477 | I2CTiva driver get's stuck at a Semaphore_pend() when I2C bus arbitration was lost |
SDOCM00102563 | WiFi driver should not create Hwi instance |
SDOCM00103028 | Add USB Host examples to EK_TM4C123GXL |
SDOCM00103637 | MSP430 UART[USCIA] LibType_Instrumented is not recommended at baudrates > 9600 |
SDOCM00104253 | MSP430 Launchpad ez-FET UART emulation issue at
buadrate > 28.8kbps |
SDOCM00104686 | UART in Stellaris launchpad not working above 9600 baud when used with windows apps that use rxtxSerial.dll driver |
SDOCM00104691 | USBMSCHFatFsTiva_open requires a heap since no task stack is provided to the Task_construct |
SDOCM00104772 | Support for USB in a MSP430 Empty project wizard |
SDOCM00105002 | TI-RTOS examples with no heap get an error if they call BIOS_exit |
SDOCM00105005 | The EMACSnow driver needs a new name |
SDOCM00105006 | Build warnings for IAR when doing a top-level build |
SDOCM00105311 | EK_LM4F120XL.h: EK_LM4F120XL_I2C0 should be EK_LM4F120XL_I2C1 |
SDOCM00105737 | GCC examples cannot print (e.g. fatsdraw) to console in CCS 5.5 |
SDOCM00105761 | CC3000 Wi-Fi examples not working with GCC |
SDOCM00105762 | TI Resource Explorer can't distinguish between boards of the same device or same boards with different toolchains |
SDOCM00105778 | MSP430 UART logging to System Analyzer does not work |
SDOCM00105836 | TI-RTOS GNU example for TM4C129x devices do not work with CCS 5.5 (see Dependencies) |
All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 1.01.00.15_eng or 1.01.00.21-beta).
This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. tirtos_1_00_01_11.
Subsequent releases of patch upgrades will be identified by the patch number, ex. TI-RTOS 1.00.00.68 with directory tirtos_1_00_01_70. Typically, these patches only include critical bug fixes.
Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.
For technical support, please refer to the Texas Instruments E2E BIOS Support Forum http://e2e.ti.com/support/embedded/bios/default.aspx or other forums in http://e2e.ti.com/ as needed.
Last updated: January 06, 2014