Package
Name |
The name of the application or
files |
Version |
Version of the application or files |
License |
Name of the license or licenses that apply to the
Package. |
Location |
The directory name and path on the media (or in an
archive) where the Package is located. |
Delivered
As |
This field will either be “Source”, “Binary” or “Source
and Binary” and is the form the content of the Package is delivered in.
If the Package is delivered in an archive format, this field applies to
the contents of the archive. |
Modified |
This field will either be “Yes” or “No”. A “Yes” means
TI had made changes to the Package. A “No” means TI has not made any
changes. |
Obtained
from[1] |
This field specifies where TI obtained the Package
from. It may be a URL to an Open Source site, a 3rd party company name
or TI. If this field contains a link to an Open Source package, the
date it was downloaded is also recorded. |