1 /*
2 * Copyright (c) 2008-2017 Texas Instruments Incorporated
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * */
13 /*
14 * ======== Error.xdc ========
15 */
16
17 /*!
18 * ======== Error ========
19 * Runtime error manager
20 *
21 * The `Error` module provides mechanisms for raising, checking, and
22 * handling errors in a program. At the configuration time, you can use the
23 * parameters `{@link Error#policy Error.policy}`,
24 * `{@link Error#policyFxn Error.policyFxn}` and
25 * `{@link Error#raiseHook Error.raiseHook}` to specify what happens when an
26 * error takes place. You can control how much debugging information is
27 * available in that case, while also controlling the memory footprint that the
28 * `Error' module adds to the program.
29 *
30 * Module producers use this module to define specific error types and
31 * reference these when raising an error. Each error type has a custom error
32 * message and can be parameterized with up to `{@link #NUMARGS}` arguments. A
33 * generic error type is provided for raising errors when not in a module.
34 *
35 * Use the `{@link #check Error_check()}` function in your application or
36 * module to determine if an error has been raised in a function that takes an
37 * `{@link #Block Error_Block}` as an argument. It is important to understand
38 * that it is the caller's responsibility to check the error block after
39 * calling such a function. Otherwise, a raised error may go undetected, which
40 * could compromise the integrity of the system. For example:
41 *
42 * @p(code) 43 * Task_create(..., &eb);
44 *
45 * if (Error_check(&eb)) {
46 * ...an error has been raised...
47 * }
48 * @p 49 *
50 * The function assigned to the parameter
51 * `{@link Error#policyFxn Error.policyFxn}` is the central part of the
52 * error handling mechanism in this module. Most of the users will either leave
53 * this parameter at its default value, or select one of the alternative
54 * implementations that are included with the `Error` module. However, this
55 * configuration parameter also allows users to completely take over the error
56 * handling by setting this parameter to their own implementation. In that
57 * case, we recommend that users first review the included implementations,
58 * and base their implementation on one of these function. The included
59 * implementations are `{@link #policyDefault}`, `{@link #policyMin}`, and
60 * `{@link #policySpin}`.
61 *
62 * The `{@link #raiseHook Error.raiseHook}` configuration parameter allows
63 * a configured function to be invoked when an error is raised.
64 * This function is invoked from the default implementation of
65 * `{@link Error#policyFxn Error.policyFxn}`. Therefore, if a different
66 * implementation of `Error.policyFxn` is used, the function specified by
67 * `Error.raiseHook` may or may not be called.
68 * This function is passed a pointer to the error's error block and makes it
69 * easy to manage all errors from a common point. For example, you can
70 * trap any error (fatal or not) by simply setting a breakpoint in this
71 * function. You can use the following functions to extract information
72 * from an error block.
73 *
74 * @p(blist) 75 * - `{@link #getData Error_getData()}`
76 * - `{@link #getCode Error_getCode()}`
77 * - `{@link #getId Error_getId()}`
78 * - `{@link #getMsg Error_getMsg()}`
79 * - `{@link #getSite Error_getSite()}`
80 * @p 81 *
82 * The Error module provides facilities for handling errors, but the Log
83 * module also provides features for logging error events. These are separate
84 * concepts; however, to ensure that users do not have to both raise and log
85 * an error, the Error module will automatically log an error event when one
86 * is raised. The Error module logs the standard {@link Log#L_error} event,
87 * passing it the error message and arguments.
88 *
89 * The error event is logged to the Error module's logger using the Error
90 * module's diags mask. Logging of errors is enabled by default in the diags
91 * mask, but the event will not be logged unless a logger is configured for
92 * the Error module as well.
93 *
94 * To make the error event appear as though it is coming from the module which
95 * called Error_raise, the event is logged with the caller's module id and
96 * with the caller's call site information.
97 *
98 * @a(Examples) 99 * Example 1: The following example shows how a module, named ModA,
100 * defines a custom error type and shows how this error is raised by
101 * the module. The module defines an `Id` of `E_notEven` in its module
102 * specification file (in this case, `ModA.xdc`). The error's message
103 * string takes only one argument. The module also defines a `mayFail()`
104 * function that takes an error block. In the module's C source file,
105 * the function checks for the error condition and raises the error if
106 * needed.
107 *
108 * This is part of ModA's XDC specification file for the module:
109 *
110 * @p(code) 111 * config xdc.runtime.Error.Id E_notEven = {
112 * msg: "expected an even number (%d)"
113 * };
114 *
115 * Void mayFail(Int x, xdc.runtime.Error.Block *eb);
116 * @p 117 *
118 * This is part of the C code for the module:
119 *
120 * @p(code) 121 * Void ModA_mayFail(Int x, Error_Block *eb)
122 * {
123 * if ((x % 2) != 0) {
124 * Error_raise(eb, ModA_E_notEven, x, 0);
125 * ...add error handling code here...
126 * return;
127 * }
128 * ...
129 * }
130 * @p 131 *
132 * @p(html) 133 * <hr />
134 * @p 135 *
136 * Example 2: The following C code supplies an error block to a function
137 * that requires one and tests the error block to see if the function
138 * raised an error. Note that an error block must be initialized before
139 * it can be used and same error block may be passed to several functions.
140 *
141 * @p(code) 142 * #include <xdc/runtime/Error.h>
143 * #include <ti/sysbios/knl/Task.h>
144 * Error_Block eb;
145 * Task_Handle tsk;
146 *
147 * Error_init(&eb);
148 * tsk = Task_create(..., &eb);
149 *
150 * if (Error_check(&eb)) {
151 * ...an error has been raised...
152 * }
153 * @p 154 *
155 * @p(html) 156 * <hr />
157 * @p 158 *
159 * Example 3: The following C code shows that you may pass a special constant
160 * `Error_ABORT` in place of an error block to a function requiring an error
161 * block. In this case, if the function raises an error, the program is aborted
162 * (via `{@link System#abort xdc_runtime_System_abort()}`), thus execution
163 * control will never return to the caller.
164 *
165 * @p(code) 166 * #include <xdc/runtime/Error.h>
167 * #include <ti/sysbios/knl/Task.h>
168 *
169 * tsk = Task_create(..., Error_ABORT);
170 * ...will never get here if an error was raised in Task_create...
171 * @p 172 *
173 * @p(html) 174 * <hr />
175 * @p 176 *
177 * Example 4: The following C code shows that you may pass a special constant
178 * `Error_IGNORE` in place of an error block to a function requiring an error
179 * block. The purpose of this constant is to avoid allocating an error block on
180 * stack in the use case where the caller is not checking the error block after
181 * the call returns.
182 * In this example, the caller only checks the returned value but not the error
183 * block. If the function raises an error, the program will return to the
184 * caller, assuming `Error_policy` is set to `{@link #Policy UNWIND}`.
185 *
186 * @p(code) 187 * #include <xdc/runtime/Error.h>
188 * #include <ti/sysbios/knl/Task.h>
189 *
190 * tsk = Task_create(..., Error_IGNORE);
191 * if (tsk != NULL) {
192 * ...
193 * }
194 * @p 195 *
196 * @p(html) 197 * <hr />
198 * @p 199 *
200 * Example 5: The following C code shows how to write a function that
201 * is not part of a module and that takes an error block and raises
202 * the generic error type provided by the Error module. Note, if the
203 * caller passes `Error_ABORT` for the error block or if the error policy is
204 * `{@link #Policy TERMINATE}`, then the call to
205 * `{@link #raise Error_raise()}` will call
206 * `{@link System#abort xdc_runtime_System_abort()}` and never return.
207 *
208 * @p(code) 209 * #include <xdc/runtime/Error.h>
210 *
211 * Void myFunc(..., Error_Block *eb)
212 * {
213 * ...
214 *
215 * if (...error condition detected...) {
216 * String myErrorMsg = "my custom error message";
217 * Error_raise(eb, Error_E_generic, myErrorMsg, 0);
218 * ...add error handling code here...
219 * return;
220 * }
221 * }
222 * @p 223 */
224 @DirectCall
225 @Template("./Error.xdt")
226
227 module Error {
228
229 /*!
230 * ======== Policy ========
231 * Error handling policies
232 *
233 * These constants are assigned to `{@link Error#policy Error.policy}` to
234 * control the flow of the program when an error is raised.
235 *
236 * @field(TERMINATE) All raised errors are fatal. A call to
237 * `{@link #raise Error_raise}` will never return to the caller. The
238 * program calls `System_abort` instead.
239 *
240 * @field(UNWIND) Errors are returned to the caller. A call to
241 * `{@link #raise Error_raise}` will return back to the caller.
242 */
243 enum Policy {
244 TERMINATE,
245 UNWIND
246 };
247
248 /*!
249 * ======== Desc ========
250 * Error descriptor
251 *
252 * Each type of error is defined with an error descriptor. This
253 * structure groups common information about the errors of this type.
254 *
255 * @field(msg) The error message using a `printf` style format string,
256 * but limited to `{@link #NUMARGS}` arguments.
257 * This format string together with the two arguments passed
258 * to `Error_raise`` are used to create a human readable
259 * error message.
260 *
261 * @field(code) A user assignable code, 0 by default. The user may
262 * optionally set this field during config to give the
263 * error a well-known numeric code.
264 */
265 metaonlystruct Desc {
266 String msg;
267 UInt16 code;
268 };
269
270 /*!
271 * ======== Id ========
272 * Error identifier
273 *
274 * Each type of error raised is defined with a metaonly
275 * `{@link Error#Desc}`. An `Error_Id` is a 32-bit target value that
276 * encodes the information in the `Desc`. Target programs use
277 * `Error_Id` values to "raise" and check for specific errors.
278 *
279 * @a(Warning) `{@link #Id}` values may vary among different
280 * configurations of an application. For example, the addition of a
281 * new module to a program may result in a different absolute value for
282 * `{@link #E_generic}`. If you need error numbers that remain
283 * invariant, use the user definable `{@link #Desc Desc.code}` field.
284 */
285 @Encoded typedef Desc Id;
286
287 /*!
288 * ======== HookFxn ========
289 * Function called whenever an error is raised
290 *
291 * The first parameter and only parameter passed to this function is a
292 * pointer to an `Error_Block`. Even if the client passes a `NULL` error
293 * block pointer to `{@link #raise Error_raise}`, this parameter passed
294 * to this "hook" function is always `non-NULL`.
295 */
296 typedef Void (*HookFxn)(Block *);
297
298 /*!
299 * ======== NUMARGS ========
300 * Maximum number of arguments supported by an error
301 */
302 const Int NUMARGS = 2;
303
304 /*!
305 * ======== Data ========
306 * Error args
307 *
308 * The two arguments (arg1, arg2) passed to `{@link #raise}` are
309 * stored in one of these arrays within the associated Error_Block.
310 * To access these arguments use `{@link #getData}` to obtain a
311 * pointer to the Error_Block's Data array.
312 *
313 * @see #getData
314 */
315 struct Data {
316 IArg arg[NUMARGS];
317 }
318
319 /*!
320 * ======== Block ========
321 * Error block
322 *
323 * An opaque structure used to store information about errors once raised.
324 * This structure must be initialized via `{@link #init Error_init()}`
325 * before being used for the first time.
326 */
327 @Opaque struct Block {
328 UInt16 unused; /* for backward compatibility (was code) */
329 Data data; /* arguments passed to raise() */
330 Id id; /* id passed to raise() */
331 CString msg; /* msg associated with id */
332 Types.Site site; /* info about Error_raise call site */
333 };
334
335 /*!
336 * ======== IGNORE ========
337 * Special Error_Block used when the caller does not want to check
338 * Error_Block
339 *
340 * This constant should be used when the caller does not plan to check
341 * `Error_Block` after the call returns, but wants the call to return even
342 * in the case when an error is raised. `{@link #policy Error_policy}` is
343 * still in effect and the application will still terminate when an error
344 * is raised if `Error_policy` is not set to
345 * `{@link #Policy Error_UNWIND}`.
346 */
347 const Block IGNORE;
348
349 /*!
350 * ======== ABORT ========
351 * Special Error_Block that terminates the application in case of an error
352 *
353 * This constant has the same effect as passing `NULL` in place of an
354 * `Error_Block`. If an error is raised when `Error_ABORT` is passed, the
355 * application terminates regardless of `{@link #policy Error_policy}`.
356 */
357 const Block ABORT;
358
359 /*!
360 * ======== PolicyFxn ========
361 * Error policy function signature
362 *
363 * @a(Parameters) 364 * A policy function is passed the following parameters:
365 * @p(dlist) 366 * - `eb`
367 * A pointer to an `{@link #Block Error_Block}` structure to be
368 * initialized using the subsequent arguments. This pointer may
369 * be `NULL`.
370 * - `modId`
371 * The module ID of the module calling
372 * `{@link #raise Error_raise()}`
373 * - `fileName`
374 * A string naming the source file which made the call to
375 * `{@link #raise Error_raise()}`
376 * - `lineNumber`
377 * An integer line number within the file named above where
378 * the call `{@link #raise Error_raise()}` occured
379 * - `errId`
380 * The `{@link #Id Error_Id}` of the error being raised
381 * - `arg1` and `arg2`
382 * Two `IArg` arguments associated with the error being raised
383 * @p 384 */
385 typedef Void (*PolicyFxn)(Block *, Types.ModuleId, CString, Int, Id,
386 IArg, IArg);
387
388 /*!
389 * ======== policyFxn ========
390 * Error handler function
391 *
392 * This function is called to handle all raised errors but, unlike
393 * `{@link raiseHook}`, this function is responsible for completely
394 * handling the error (including calling `{@link #raiseHook raiseHook}`
395 * with an appropriately initialized `{@link #Block Error_Block}`, if
396 * `raiseHook` functionality is required).
397 *
398 * The default value is a function which, in addition to calling
399 * `raiseHook` with an initialized `Error_Block` structure, logs the
400 * error using this module's logger.
401 *
402 * Alternately, `{@link #policySpin}`, which simply loops
403 * indefinitely, can be used to minimize target footprint. Note, this
404 * function does NOT call `raiseHook`, and also ignores
405 * `{@link Error#policy Error.policy}`.
406 *
407 * The third implementation, `{@link #policyMin}` finds a middle ground
408 * between the two implementations above in terms of memory footprint and
409 * the available error information. Only the `{@link #Id Error_Id}` of the
410 * error being raised is available in the resulting `Error_Block`,
411 * `raiseHook` is not invoked, but `{@link Error#policy Error.policy}` is
412 * observed.
413 */
414 config PolicyFxn policyFxn = Error.policyDefault;
415
416 /*!
417 * ======== E_generic ========
418 * Generic error
419 *
420 * This error takes advantage of the $S specifier to allow for recursive
421 * formatting of the error message passed to error raise.
422 *
423 * For example, the following is possible:
424 * @p(code) 425 * Error_raise(eb, Error_E_generic, "Error occurred, code: %d", code);
426 * @p 427 *
428 * @see System#extendedFormats
429 * @see System#printf
430 */
431 config Id E_generic = {msg: "%$S"};
432
433 /*!
434 * ======== E_memory ========
435 * Out of memory error
436 *
437 * The first parameter must be the heap instance handle. The second
438 * parameter is the size of the object for which the allocation failed.
439 */
440 config Id E_memory = {msg: "out of memory: heap=0x%x, size=%u"};
441
442 /*!
443 * ======== E_msgCode ========
444 * Generic error that displays a string and a numeric value
445 */
446 config Id E_msgCode = {msg: "%s 0x%x"};
447
448 /*!
449 * ======== policy ========
450 * System-wide error handling policy
451 *
452 * You can use this parameter to decide at the configuration time what
453 * happens when an error is raised. The program can either call
454 * `System_abort()` or return back to the caller. The implementations of
455 * `{@link Error#policyFxn Error.policyFxn}` should consider this
456 * parameter, but some implementations may not do so to save the memory
457 * footprint (`Error_policySpin`, for example).
458 *
459 */
460 config Policy policy = UNWIND;
461
462 /*!
463 * ======== raiseHook ========
464 * The function to call whenever an error is raised
465 *
466 * If set to a non-`null` value, the referenced function is always
467 * called when an error is raised, even if the `Error` policy is
468 * `{@link #Policy TERMINATE}`. In rare cases, it is possible that a
469 * raised error does not trigger a call to `raiseHook`; see
470 * `{@link #maxDepth}`.
471 *
472 * Regardless of the current policy in use, raising an error by
473 * calling `{@link #raise Error_raise}` will always invoke the
474 * error raise hook function assigned to the
475 * `{@link #raiseHook Error.raiseHook}` configuration parameter, if the
476 * default `{@link Error#policyFxn Error.policyFxn}` implementation is
477 * used.
478 *
479 *
480 * By default, this function is set to `{@link #print Error_print}`
481 * which causes the error to be formatted and output via
482 * `{@link xdc.runtime.System#aprintf System_printf}`. Setting this
483 * configuration parameter to `null` indicates that no function hook
484 * should be called.
485 *
486 * @see #maxDepth
487 * @see #HookFxn
488 * @see #print
489 */
490 config HookFxn raiseHook = Error.print;
491
492 /*!
493 * ======== maxDepth ========
494 * Maximum number of concurrent calls to `{@link #raiseHook}`
495 *
496 * To prevent errors that occur in the raiseHook function from
497 * causing an infinite recursion, the maximum number of concurrent
498 * calls to `{@link #raiseHook}` is limited by `Error_maxDepth`. If
499 * the number of concurrent calls exceeds `Error_maxDepth`, the
500 * `raiseHook` function is not called.
501 *
502 * In multi-threaded systems, errors raised by separate threads may
503 * be detected as recursive calls to `raiseHook`. So, setting
504 * `Error.maxDepth` to a small value may - in rare instances - result in
505 * `errorHook` not being called for some raised errors.
506 *
507 * If it is important that all raised errors trigger a call to the
508 * `raiseHook` function, set `Error.maxDepth` to an impossibly large
509 * number (0xffff) and either ensure that the raise hook never calls a
510 * function that can raise an error or add checks in `raiseHook` to
511 * protect against "double faults".
512 */
513 config UInt16 maxDepth = 16;
514
515 /*!
516 * ======== check ========
517 * Return TRUE if an error was raised
518 *
519 * @param(eb) pointer to an `Error_Block`, `Error_ABORT` or `Error_IGNORE`
520 *
521 * @a(returns) 522 * If `eb` is non-`NULL` and `{@link #policy Error.policy} == UNWIND` and
523 * an error was raised on `eb`, this function returns `TRUE`. Otherwise,
524 * it returns `FALSE`.
525 */
526 Bool check(Block *eb);
527
528 /*!
529 * ======== getData ========
530 * Get an error's argument list
531 *
532 * @param(eb) non-`NULL` pointer to an `Error_Block`
533 *
534 * @a(returns) 535 * `getData` returns an array of type `{@link #Data}` with
536 * `{@link #NUMARGS}` elements containing the arguments provided
537 * at the time the error was raised.
538 *
539 * @see #raise
540 */
541 Data *getData(Block *eb);
542
543 /*!
544 * ======== getCode ========
545 * Get an error's code
546 *
547 * @param(eb) non-`NULL` pointer to an `Error_Block`
548 *
549 * @a(returns) 550 * `getCode` returns the error code associated with this error block.
551 *
552 * @see #raise
553 * @see #Desc
554 */
555 UInt16 getCode(Block *eb);
556
557 /*!
558 * ======== getId ========
559 * Get an error's id
560 *
561 * @param(eb) non-`NULL` pointer to an `Error_Block`
562 *
563 * @a(Warning) 564 * `Error_Id` values may vary among different configurations
565 * of an application. For example, the addition of a new module to a
566 * program may result in a different absolute value for
567 * `{@link #E_generic}`. If you need error numbers that remain
568 * invariant, use the user definable `{@link #Desc Desc.code}` field.
569 *
570 * @see #raise
571 * @see #Desc
572 */
573 Id getId(Block *eb);
574
575 /*!
576 * ======== getMsg ========
577 * Get an error's "printf" format string
578 *
579 * @param(eb) non-`NULL` pointer to an `Error_Block`
580 *
581 * @see #raise
582 * @see #Desc
583 */
584 CString getMsg(Block *eb);
585
586 /*!
587 * ======== getSite ========
588 * Get an error's call site info
589 *
590 * @param(eb) non-`NULL` pointer to an `Error_Block`
591 *
592 * @a(returns) 593 * `getSite` returns a pointer to an initialized
594 * `{@link Types#Site Types.Site}` structure. However, in the
595 * event that the call site was compiled with `xdc_FILE` defined to
596 * be `NULL` (to minimize string space overhead) the `file`
597 * field may be set to `NULL`.
598 *
599 * @see #raise
600 * @see #Desc
601 */
602 Types.Site *getSite(Block *eb);
603
604 /*!
605 * ======== idToCode ========
606 * Extract the user's error code associated with an `Error_Id`
607 *
608 * @param(id) `Error_Id` from which to extract the user defined
609 * code
610 * @_nodoc 611 */
612 @Macro UInt16 idToCode(Id id);
613
614 /*!
615 * ======== idToUid ========
616 * Extract the unique error id associated with an `Error_Id`
617 *
618 * @param(id) `Error_Id` from which to extract the system unique
619 * id associated with the specified `Error_Id`
620 * @_nodoc 621 */
622 @Macro UInt16 idToUid(Id id);
623
624 /*!
625 * ======== init ========
626 * Put an error block into its initial state
627 *
628 * To ensure reliable error detection, clients must call `init` for
629 * an `Error_Block` prior to any use.
630 *
631 * If the same Error Block is used multiple times, only the last error
632 * raised is retained.
633 *
634 * @param(eb) pointer to an `Error_Block`, `Error_ABORT` or `Error_IGNORE`
635 *
636 * If `eb` is `NULL` this function simply returns.
637 */
638 Void init(Block *eb);
639
640 /*!
641 * ======== print ========
642 * Print error using System.printf()
643 *
644 * This function prints the error using `System_printf()`. The output
645 * is on a single line terminated with a new line character and has the
646 * following form:
647 * @p(code) 648 * <site>: <file>, line <line_num>: <err_msg>
649 * @p 650 * where `<site>` is the module that raised the error, `<file>` and
651 * `<line_num>` are the file and line number of the containing the call
652 * site of the `Error_raise()`, and `<err_msg>` is the error message
653 * rendered with the arguments associated with the error.
654 *
655 * @param(eb) pointer to an `Error_Block`, `Error_ABORT` or `Error_IGNORE`
656 *
657 * If `eb` is `Error_ABORT` or `Error_IGNORE`, this function simply
658 * returns with no output.
659 *
660 * @a(Warning) 661 * This function is not protected by a gate and, as a result,
662 * if two threads call this method concurrently, the output of the two
663 * calls will be intermingled. To prevent intermingled error output,
664 * you can either wrap all calls to this method with an appropriate
665 * `Gate_enter`/`Gate_leave` pair or simply ensure that only one
666 * thread in the system ever calls this method.
667 */
668 Void print(Block *eb);
669
670 /*!
671 * ======== policyDefault ========
672 * Default implementation of the policyFxn
673 *
674 * This function is the implementation which is plugged in by default to
675 * the `{@link #policyFxn}`. It processes the error and logs it before
676 * returning to the caller or aborting - depending on the error policy
677 * `{@link #policy}`.
678 */
679 Void policyDefault(Block *eb, Types.ModuleId mod, CString file, Int line,
680 Id id, IArg arg1, IArg arg2);
681
682 /*!
683 * ======== policyMin ========
684 * Implementation of the policyFxn with a smaller footprint
685 *
686 * This function is a compromise between a debug-friendly
687 * `{@link #policyDefault}`, which offers more details about any raised
688 * errors, but requires a larger footprint, and `{@link #policySpin}`,
689 * which is small but does not display any debug information.
690 *
691 * This function returns to the caller, unless `{@link #policy}` is set to
692 * `TERMINATE`, or the `Error_Block` passed to it is `NULL`. If it returns,
693 * the only information available in the returned `Error_Block` is the
694 * error ID.
695 */
696 Void policyMin(Block *eb, Types.ModuleId mod, CString file, Int line,
697 Id id, IArg arg1, IArg arg2);
698
699 /*!
700 * ======== policySpin ========
701 * Lightweight implementation of the policyFxn
702 *
703 * This function is a lightweight alternative which can be plugged in to
704 * the `{@link #policyFxn}`. It just loops infinitely.
705 *
706 * @a(Warning) 707 * This function does not call `{@link #raiseHook}` and never returns to
708 * the caller. As a result, ANY error raised by the application will cause
709 * it to indefinitly hang.
710 */
711 Void policySpin(Block *eb, Types.ModuleId mod, CString file, Int line,
712 Id id, IArg arg1, IArg arg2);
713
714 /*!
715 * ======== raise ========
716 * Raise an error
717 *
718 * This function is used to raise an `Error` by writing call site,
719 * error ID, and error argument information into the `Error_Block`
720 * pointed to by `eb`.
721 *
722 * If `Error_raise` is called more than once on an `Error_Block` object,
723 * the previous error information is overwritten; only the last error
724 * is retained in the `Error_Block` object.
725 *
726 * In all cases, any configured `{@link #raiseHook Error.raiseHook}`
727 * function is called with a non-`NULL` pointer to a fully
728 * initialized `Error_Block` object.
729 *
730 * @param(eb) pointer to an `Error_Block`, `Error_ABORT` or `Error_IGNORE`
731 *
732 * If `eb` is `Error_ABORT` or
733 * `{@link #policy Error.policy} == TERMINATE`,
734 * this function does not return to the caller; after calling any
735 * configured `{@link #raiseHook}`, `System_abort` is called with the
736 * string `"xdc.runtime.Error.raise: terminating execution\n"`.
737 *
738 * @param(id) the error to raise
739 *
740 * This pointer identifies the class of error being raised; the error
741 * class indicates how to interpret any subsequent arguments passed to
742 * `{@link #raise}`.
743 *
744 * @param(arg1) error's first argument
745 *
746 * The argument interpreted by the first control character
747 * in the error message format string. It is ignored if not needed.
748 *
749 * @param(arg2) error's second argument
750 *
751 * The argument interpreted by the second control character
752 * in the error message format string. It is ignored if not needed.
753 */
754 @Macro Void raise(Block *eb, Id id, IArg arg1, IArg arg2);
755
756 /*! @_nodoc */
757 Void raiseX(Block *eb, Types.ModuleId mod, CString file, Int line,
758 Id id, IArg arg1, IArg arg2);
759
760 /*! @_nodoc EXPERIMENTAL */
761 Void setX(Block *eb, Types.ModuleId mod, CString file, Int line,
762 Id id, IArg arg1, IArg arg2);
763
764 internal:
765
766 struct Module_State {
767 UInt16 count;
768 };
769
770 }
771 /*
772 * @(#) xdc.runtime; 2, 1, 0,0; 8-8-2017 17:30:58; /db/ztree/library/trees/xdc/xdc-D20/src/packages/
773 */
774