1 /*
2 * Copyright (c) 2015-2017, Texas Instruments Incorporated
3 * All rights reserved.
4 *
5 * Redistribution and use in source and binary forms, with or without
6 * modification, are permitted provided that the following conditions
7 * are met:
8 *
9 * * Redistributions of source code must retain the above copyright
10 * notice, this list of conditions and the following disclaimer.
11 *
12 * * Redistributions in binary form must reproduce the above copyright
13 * notice, this list of conditions and the following disclaimer in the
14 * documentation and/or other materials provided with the distribution.
15 *
16 * * Neither the name of Texas Instruments Incorporated nor the names of
17 * its contributors may be used to endorse or promote products derived
18 * from this software without specific prior written permission.
19 *
20 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31 */
32 /*
33 * ======== Hwi.xdc ========
34 */
35 package ti.sysbios.family.arm.gic;
36
37 import xdc.rov.ViewInfo;
38
39 import xdc.runtime.Diags;
40 import xdc.runtime.Log;
41 import xdc.runtime.Error;
42
43 import ti.sysbios.BIOS;
44 import ti.sysbios.interfaces.IHwi;
45
46 /*!
47 * ======== Hwi ========
48 * Hardware Interrupt Support Module.
49 *
50 * This Hwi module provides ARM cortex-A Generic Interrupt Controller(GIC) v2.0
51 * specific implementations and extensions of the APIs defined in
52 * {@link ti.sysbios.interfaces.IHwi IHwi}.
53 *
54 * The GIC is logically partitioned into 2 blocks, the Distributor block
55 * and CPU interface block. The Distributor block interfaces with the interrupt
56 * sources, prioritizes interrupts and distributes them to the CPU interface
57 * block. The CPU interface block connects to the processors in the system
58 * and is responsible for priority masking and preemption handling for
59 * the processor it is connected to.
60 *
61 * The GIC can implement up to 8 CPU interfaces with each CPU interface
62 * being able to see up to 1020 interrupts. The GIC assigns interrupt ID
63 * numbers 0-1019 as follows:
64 * - Interrupt numbers 0-31 are used for interrupts private to a
65 * CPU interface. These private interrupts are banked in the Distributor.
66 * - Banked interrupt number 0-15 are used for Software Generated Interrupts
67 * or SGIs.
68 * - Banked interrupt number 16-31 are used for Private Peripheral Interrupts
69 * or PPIs.
70 * - Interrupt numbers 32-1019 are used for Shared Peripheral Interrupts
71 * or SPIs.
72 * - Interrupt numbers 1020-1023 are reserved.
73 *
74 * @a(NOTE) 75 * In the SoC Technical Reference Manual, the MPU IRQs 0 to N map to
76 * GIC interrupt numbers 32 to (N+32) where (N+1) is the total number of
77 * Shared Peripheral Interrupts implemented.
78 * For instance on OMAP5430, MPU IRQ 0 to 159 maps to GIC interrupt number
79 * 32 to 191.
80 *
81 * @a(INTERRUPT GROUPING) 82 * GIC allows configuring an interrupt as a Group 0 or a Group 1 interrupt.
83 * Group 0 interrupts are Secure interrupts and Group 1 interrupts are
84 * Non-secure interrupts.
85 *
86 * If {@link #enableSecureMode} is set to true, this module supports both
87 * Group0 and Group 1 interrupts. Group 0 interrupts are delivered to the CPU
88 * using FIQ signal whereas Group 1 interrupts are delivered using IRQ signal.
89 *
90 * If {@link #enableSecureMode} is set to false, this module only supports
91 * Group 1 interrupts which are delivered to the target CPU using IRQ signal.
92 *
93 * @a(INTERRUPT PRIORITIES) 94 * In general GIC supports priority values 0 thru 255.
95 *
96 * In practice valid priority values depend on the particular device used,
97 * security mode and the Binary Point Register (see {@link #BPR} and
98 * {@link #ABPR}) value.
99 *
100 * The device implementation and security mode decide the number of priority
101 * bits that are implemented (see {@link #NUM_PRIORITY_BITS}). Group 0
102 * interrupts always implement one more priority bit than Group 1 interrupts.
103 *
104 * In GIC, interrupts with lower priority numbers have higher priority.
105 *
106 * @a(NOTE) 107 * In this Hwi module implementation, the instance config parameter value
108 * {@link #MaskingOption_LOWER} is equivalent to {@link #MaskingOption_SELF}.
109 * Statically configuring a Hwi object's {@link #Params.maskSetting} to
110 * {@link #MaskingOption_LOWER} will result in the generation of a benign
111 * build warning. Dynamic usages of {@link #MaskingOption_LOWER} will be
112 * silently converted to {@link #MaskingOption_SELF}.
113 *
114 * @a(ZERO LATENCY INTERRUPTS) 115 * On Keystone2 devices, this module supports zero-latency interrupts. A
116 * zero-latency interrupt does not go through the SYS/BIOS dispatcher and
117 * thus has a faster response time. Since zero-latency interrupts bypass the
118 * dispatcher, their handler function cannot call any SYS/BIOS APIs.
119 *
120 * This module implements zero-latency interrupts by forwarding the interrupt
121 * to the target CPU using FIQ signal. Therefore, in order to configure an
122 * interrupt as a zero-latency interrupt, the Hwi type needs to be changed
123 * to FIQ when creating or constructing a Hwi.
124 *
125 * Example showing how to create a zero-latency Hwi:
126 * @p(code) 127 * Void main(Void)
128 * {
129 * Hwi_Params hwiParams;
130 * Hwi_Params_init(&hwiParams);
131 * // Default Hwi type is IRQ
132 * hwiParams.type = Hwi_Type_FIQ;
133 * Hwi_create(INT_NUM_FIQ, myIsrFIQ, &hwiParams, NULL);
134 * ...
135 * }
136 * @p 137 *
138 * FIQs run on their own stack. See {@link #fiqStack} and {@link #fiqStackSize}
139 * for more info on how to control the FIQ stack.
140 *
141 * @a(NOTE) 142 * This module is written for GIC v2.0, however it is backwards compatible
143 * with GIC v1.0
144 */
145
146 @Template("./Hwi.xdt") /* generates the vector table and the dispatcher */
147 @ModuleStartup /* generates call to Hwi_Module_startup at startup */
148 @InstanceInitStatic /* allow constructs in static only systems */
149 @CustomHeader
150
151 module Hwi inherits ti.sysbios.interfaces.IHwi
152 {
153 // -------- Module Constants --------
154
155 /*!
156 * ======== enableSecureMode ========
157 * Security Mode
158 *
159 * This field specifies the MPU's security mode. The MPU's security mode
160 * determines the type of accesses to the GIC i.e. if the MPU is in secure
161 * mode, all accesses to the GIC are secure and if the MPU is in non-secure
162 * mode, all accesses to the GIC are non-secure.
163 *
164 * An exception to the above rule can be seen on certain devices like
165 * Keystone 2, where all GIC acceses are secure irrespective of the MPU's
166 * security state. {@link #enableSecureMode} should be set to true for such
167 * devices.
168 */
169 config Bool enableSecureMode = false;
170
171 /*!
172 * Number of interrupts implemented in GIC
173 *
174 * On OMAP543x GIC implements 192 interrupts.
175 *
176 * See the OMAP543x_ES1 Technical Reference Manual pg 5280 for more
177 * details.
178 */
179 config UInt NUM_INTERRUPTS;
180
181 /*!
182 * Number of Priority bits implemented.
183 *
184 * On OMAP543x running in non-secure mode, only most significant 4
185 * priority bits are available for use. The least significant 4 bits
186 * are always 0.
187 */
188 config UInt NUM_PRIORITY_BITS;
189
190 /*!
191 * Minimum Interrupt Priority.
192 */
193 config UInt MIN_INT_PRIORITY;
194
195 /*!
196 * Default Interrupt Priority.
197 *
198 * Set to one level higher than minimum supported priority.
199 */
200 config UInt DEFAULT_INT_PRIORITY;
201
202 /*!
203 * ======== BPR ========
204 * GIC Binary Point Register value
205 *
206 * Defines the point at which the priority value fields split into
207 * two parts, the group priority field and the sub-priority field.
208 * When running in SECURE mode, BPR applies to Group 0 interrupts
209 * and when running in NON-SECURE mode, BPR applies to Group 1
210 * interrupts.
211 *
212 * The group priority field determines interrupt preemption in case
213 * of nested interrupts whereas sub-priority field is used to determine
214 * priority within a group when multiple interrrupts belonging to the
215 * same group are pending.
216 *
217 * Valid BPR values are from 0-7 with the minimum value supported being
218 * implementation defined and in the range 0-3.
219 *
220 * @p(code) 221 * -------------------------------------------------------
222 * | BPR value | Group priority field | Sub-priority field |
223 * -------------------------------------------------------
224 * | 0 | [7:1] | [0] |
225 * | 1 | [7:2] | [1:0] |
226 * | 2 | [7:3] | [2:0] |
227 * | 3 | [7:4] | [3:0] |
228 * | 4 | [7:5] | [4:0] |
229 * | 5 | [7:6] | [5:0] |
230 * | 6 | [7] | [6:0] |
231 * | 7 | No preemption | [7:0] |
232 * -------------------------------------------------------
233 * @p 234 *
235 */
236 config UInt BPR;
237
238 /*!
239 * ======== ABPR ========
240 * GIC Aliased Binary Point Register value for Grourp 1 interrupts
241 *
242 * Defines the point at which the priority value fields split into
243 * two parts, the group priority field and the sub-priority field.
244 * ABPR is used only when {@link #enableSecureMode} set to true and
245 * is ignored when security mode is set to false. ABPR applies to
246 * Group 1 interrupts.
247 *
248 * The group priority field determines interrupt preemption in case
249 * of nested interrupts whereas sub-priority field is used to determine
250 * priority within a group when multiple interrrupts belonging to the
251 * same group are pending.
252 *
253 * Valid ABPR values are from 1-7 with the minimum value supported being
254 * implementation defined and in the range 1-4. Minimum ABPR value is
255 * 1 more than the minimum BPR value.
256 *
257 * @p(code) 258 * --------------------------------------------------------
259 * | ABPR value | Group priority field | Sub-priority field |
260 * --------------------------------------------------------
261 * | 0 | -- | -- |
262 * | 1 | [7:1] | [0] |
263 * | 2 | [7:2] | [1:0] |
264 * | 3 | [7:3] | [2:0] |
265 * | 4 | [7:4] | [3:0] |
266 * | 5 | [7:5] | [4:0] |
267 * | 6 | [7:6] | [5:0] |
268 * | 7 | [7] | [6:0] |
269 * --------------------------------------------------------
270 * @p 271 *
272 */
273 config UInt ABPR;
274
275 /*!
276 * ======== Type ========
277 * Interrupt type. IRQ or FIQ
278 */
279 enum Type {
280 Type_IRQ, /*! IRQ interrupt. */
281 Type_FIQ /*! FIQ interrupt. */
282 };
283
284 // -------- Module Types --------
285
286 /*! Hwi vector function type definition. */
287 typedef Void (*VectorFuncPtr)(void);
288
289 /*!
290 * ======== BasicView ========
291 * @_nodoc 292 */
293 metaonlystruct BasicView {
294 Ptr halHwiHandle;
295 String label;
296 Int intNum;
297 String absolutePriority;
298 UInt relativeGrpPriority;
299 UInt relativeSubPriority;
300 String fxn;
301 UArg arg;
302 };
303
304 /*!
305 * ======== DetailedView ========
306 * @_nodoc 307 */
308 metaonlystruct DetailedView {
309 Ptr halHwiHandle;
310 String label;
311 Int intNum;
312 String absolutePriority;
313 UInt relativeGrpPriority;
314 UInt relativeSubPriority;
315 String fxn;
316 UArg arg;
317 Ptr irp;
318 Bool enabled;
319 Bool pending;
320 String triggerSensitivity;
321 String targetProcList;
322 };
323
324 /*!
325 * ======== ModuleView ========
326 * @_nodoc 327 */
328 metaonlystruct ModuleView {
329 String options[4];
330 UInt spuriousInterrupts;
331 UInt lastSpuriousInterrupt;
332 String hwiStackPeak;
333 SizeT hwiStackSize;
334 Ptr hwiStackBase;
335 };
336
337 /*!
338 * ======== rovViewInfo ========
339 * @_nodoc 340 */
341 @Facet
342 metaonlyconfig ViewInfo.Instance rovViewInfo =
343 ViewInfo.create({
344 viewMap: [
345 [
346 'Basic',
347 {
348 type: ViewInfo.INSTANCE,
349 viewInitFxn: 'viewInitBasic',
350 structName: 'BasicView'
351 }
352 ],
353 [
354 'Detailed',
355 {
356 type: ViewInfo.INSTANCE,
357 viewInitFxn: 'viewInitDetailed',
358 structName: 'DetailedView'
359 }
360 ],
361 [
362 'Module',
363 {
364 type: ViewInfo.MODULE,
365 viewInitFxn: 'viewInitModule',
366 structName: 'ModuleView'
367 }
368 ]
369 ]
370 });
371
372 /*!
373 * Generic Interrupt Controller Distributor. Symbol "Hwi_gicd" is
374 * a physical device
375 */
376 struct Gicd {
377 UInt32 CTLR; /*! 0x000 Distributor Control Register */
378 UInt32 TYPER; /*! 0x004 Interrupt Controller Type Register */
379 UInt32 IIDR; /*! 0x008 Distributor Implementor Id Register */
380 UInt32 hole0[29]; /*! 0x00C-0x07C */
381 UInt32 IGROUPR[32]; /*! 0x080 Interrupt Group Registers */
382 UInt32 ISENABLER[32]; /*! 0x100 Interrupt Set-Enable Registers */
383 UInt32 ICENABLER[32]; /*! 0x180 Interrupt Clear-Enable Registers */
384 UInt32 ISPENDR[32]; /*! 0x200 Interrupt Set-Pending Registers */
385 UInt32 ICPENDR[32]; /*! 0x280 Interrupt Clear-Pending Registers */
386 UInt32 ISACTIVER[32]; /*! 0x300 Interrupt Set-Active Registers */
387 UInt32 ICACTIVER[32]; /*! 0x380 Interrupt Clear-Active Registers */
388 UInt32 IPRIORITYR[255]; /*! 0x400 Interrupt Priority Registers */
389 UInt32 hole1[1]; /*! 0x7FC */
390 UInt32 ITARGETSR[255]; /*! 0x800 Interrupt Processor Targets Register */
391 UInt32 hole2[1]; /*! 0xBFC */
392 UInt32 ICFGR[64]; /*! 0xC00 Interrupt Configuration Registers */
393 UInt32 PPISR; /*! 0xD00 PPI Status Register */
394 UInt32 SPISR[7]; /*! 0xD04 SPI Status Registers */
395 UInt32 hole3[120]; /*! 0xD20-0xEFC */
396 UInt32 SGIR; /*! 0xF00 Software Generated Interrupt
397 Registers */
398 UInt32 hole4[3]; /*! 0xF04-0xF0C */
399 UInt32 CPENDSGIR[4]; /*! 0xF10 SGI Clear-Pending Registers */
400 UInt32 SPENDSGIR[4]; /*! 0xF20 SGI Set-Pending Registers */
401 UInt32 hole5[40]; /*! 0xF30-0xFCC */
402 UInt32 PIDR4; /*! 0xFD0 Peripheral ID4 Register */
403 UInt32 PIDR5; /*! 0xFD4 Peripheral ID5 Register */
404 UInt32 PIDR6; /*! 0xFD8 Peripheral ID6 Register */
405 UInt32 PIDR7; /*! 0xFDC Peripheral ID7 Register */
406 UInt32 PIDR0; /*! 0xFE0 Peripheral ID0 Register */
407 UInt32 PIDR1; /*! 0xFE4 Peripheral ID1 Register */
408 UInt32 PIDR2; /*! 0xFE8 Peripheral ID2 Register */
409 UInt32 PIDR3; /*! 0xFEC Peripheral ID3 Register */
410 UInt32 CIDR0; /*! 0xFF0 Component ID0 Register */
411 UInt32 CIDR1; /*! 0xFF4 Component ID1 Register */
412 UInt32 CIDR2; /*! 0xFF8 Component ID2 Register */
413 UInt32 CIDR3; /*! 0xFFC Component ID3 Register */
414 };
415
416 extern volatile Gicd gicd;
417
418 /*!
419 * Generic Interrupt Controller CPU Interface. Symbol "Hwi_gicc" is
420 * a physical device.
421 */
422 struct Gicc {
423 UInt32 CTLR; /*! 0x0000 CPU Interface Control Register */
424 UInt32 PMR; /*! 0x0004 Interrupt Priority Mask Register */
425 UInt32 BPR; /*! 0x0008 Binary Point Register */
426 UInt32 IAR; /*! 0x000C Interrupt Acknowledge Register */
427 UInt32 EOIR; /*! 0x0010 End Of Interrupt Register */
428 UInt32 RPR; /*! 0x0014 Running Priority Register */
429 UInt32 HPPIR; /*! 0x0018 Highest Priority Pending Interrupt
430 Register */
431 UInt32 ABPR; /*! 0x001C Aliased Binary Point Register */
432 UInt32 AIAR; /*! 0x0020 Aliased IAR Register */
433 UInt32 AEOIR; /*! 0x0024 Aliased EOI Register */
434 UInt32 AHPPIR; /*! 0x0028 Aliased HPPI Register */
435 UInt32 hole0[41]; /*! 0x002C-0x00CC */
436 UInt32 APR0; /*! 0x00D0 Active Priority Register */
437 UInt32 hole1[3]; /*! 0x00D4-0x00DC */
438 UInt32 NSAPR0; /*! 0x00E0 Non-secure Active Priority Register */
439 UInt32 hole2[6]; /*! 0x00E4-0x00F8 */
440 UInt32 IIDR; /*! 0x00FC CPU Interface Id Register */
441 UInt32 hole3[960]; /*! 0x0100-0x0FFC */
442 UInt32 DIR; /*! 0x1000 Deactivate Interrupt Register */
443 };
444
445 extern volatile Gicc gicc;
446
447 // -------- Module Parameters --------
448
449 /*! Reset Handler. Default is _c_int00 */
450 metaonlyconfig VectorFuncPtr resetFunc;
451
452 /*!
453 * Undefined instruction exception handler.
454 * Default is an internal exception handler.
455 */
456 metaonlyconfig VectorFuncPtr undefinedInstFunc;
457
458 /*!
459 * SVC Handler. Supervisor Call exception handler.
460 * (previously called Software Interrupt or SWI)
461 * Default is an internal exception handler.
462 */
463 metaonlyconfig VectorFuncPtr svcFunc;
464
465 /*!
466 * Prefetch abort exception handler.
467 * Default is an internal exception handler.
468 */
469 metaonlyconfig VectorFuncPtr prefetchAbortFunc;
470
471 /*!
472 * Data abort exception handler.
473 * Default is an internal exception handler.
474 */
475 metaonlyconfig VectorFuncPtr dataAbortFunc;
476
477 /*!
478 * Reserved exception handler.
479 * Default is an internal exception handler.
480 */
481 metaonlyconfig VectorFuncPtr reservedFunc;
482
483 /*! IRQ interrupt handler.
484 * Default is internal IRQ dispatcher
485 */
486 metaonlyconfig VectorFuncPtr irqFunc;
487
488 /*! FIQ interrupt handler.
489 * Default is internal exception handler.
490 */
491 metaonlyconfig VectorFuncPtr fiqFunc;
492
493 /*!
494 * @_nodoc 495 * ======== enableAsidTagging ========
496 * Flag to enable/disable ASID tagging
497 *
498 * If ASID tagging is enabled, the Hwi dispatcher will switch
499 * to ASID 0 (and change the MMU table base address to match
500 * kernel MMU table address) in the Hwi dispatcher prolog
501 * and restore the ASID (and MMU table base address) in the
502 * Hwi dispatcher epilog.
503 */
504 config Bool enableAsidTagging = false;
505
506 /*!
507 * ======== initGicd ========
508 * Initialize all GIC Distributor registers. True by default.
509 *
510 * Flag determines whether to initialize certain global GIC distributor
511 * registers. It is set to false when running under a hypervisor and
512 * should be true if not running under a hypervisor.
513 */
514 config Bool initGicd = true;
515
516 /*!
517 * @_nodoc 518 * ======== irqStackSection ========
519 * Memory section used for IRQ stack on each core
520 * Default is null.
521 */
522 metaonlyconfig String irqStackSection = null;
523
524 /*!
525 * @_nodoc 526 * ======== fiqStack ========
527 * FIQ stack pointer. Default = null.
528 * (Indicates that stack is to be created internally)
529 *
530 * @a(Note) 531 * If running in SMP mode and both fiqStack and fiqStacks[0]
532 * are set, then fiqStack is used on Core0.
533 */
534 metaonlyconfig Ptr fiqStack = null;
535 metaonlyconfig Ptr fiqStacks[];
536
537 /*!
538 * ======== fiqStackSize ========
539 * FIQ stack size in MAUs.
540 * Default is 1024 bytes.
541 *
542 * If running in SMP mode, the FIQ stacks on all cores are
543 * set to this size.
544 */
545 metaonlyconfig SizeT fiqStackSize = 1024;
546
547 /*!
548 * ======== fiqStackSection ========
549 * Memory section used for FIQ stack
550 * Default is null.
551 */
552 metaonlyconfig String fiqStackSection = null;
553
554 /*!
555 * ======== A_badSGIIntNum ========
556 * Assert raised when an interrupt number >= 16 is
557 * passed to Hwi_raiseSGI() function.
558 */
559 config xdc.runtime.Assert.Id A_badSGIIntNum = {
560 msg: "A_badSGIIntNum: SGI intNum should be <= 15."
561 };
562
563 /*!
564 * Error raised when an attempt is made to create a Hwi
565 * that has already been created.
566 */
567 config Error.Id E_alreadyDefined = {
568 msg: "E_alreadyDefined: Hwi already defined, intnum: %d"
569 };
570
571 /*!
572 * Error raised when Hwi handle referenced in Hwi_delete()
573 * is not found in the Hwi dispatch table
574 */
575 config Error.Id E_handleNotFound = {
576 msg: "E_handleNotFound: Hwi handle not found: 0x%x"
577 };
578
579 /*!
580 * Error raised when an undefined interrupt has fired.
581 */
582 config Error.Id E_undefined = {
583 msg: "E_undefined: Hwi undefined, intnum: %d"
584 };
585
586 /*!
587 * Error raised if an attempt is made to create a Hwi
588 * with an interrupt number greater than Hwi_NUM_INTERRUPTS - 1.
589 */
590 config Error.Id E_badIntNum = {
591 msg: "E_badIntNum, intnum: %d is out of range"
592 };
593
594 /*!
595 * Issued just prior to Hwi function invocation (with interrupts disabled)
596 */
597 config Log.Event LM_begin = {
598 mask: Diags.USER1 | Diags.USER2,
599 msg: "LM_begin: hwi: 0x%x, func: 0x%x, preThread: %d, intNum: %d, irp: 0x%x"
600 };
601
602 /*!
603 * Issued just after return from Hwi function (with interrupts disabled)
604 */
605 config Log.Event LD_end = {
606 mask: Diags.USER2,
607 msg: "LD_end: hwi: 0x%x"
608 };
609
610
611 // -------- Module Functions --------
612
613 /*!
614 * ======== disable ========
615 * Globally disable interrupts.
616 *
617 * Hwi_disable globally disables hardware interrupts and returns an
618 * opaque key indicating whether interrupts were globally enabled or
619 * disabled on entry to Hwi_disable().
620 * The actual value of the key is target/device specific and is meant
621 * to be passed to Hwi_restore().
622 *
623 * Call Hwi_disable before a portion of a function that needs
624 * to run without interruption. When critical processing is complete, call
625 * Hwi_restore or Hwi_enable to reenable hardware interrupts.
626 *
627 * Servicing of interrupts that occur while interrupts are disabled is
628 * postponed until interrupts are reenabled. However, if the same type
629 * of interrupt occurs several times while interrupts are disabled,
630 * the interrupt's function is executed only once when interrupts are
631 * reenabled.
632 *
633 * A context switch can occur when calling Hwi_enable or Hwi_restore if
634 * an enabled interrupt occurred while interrupts are disabled.
635 *
636 * Hwi_disable may be called from main(). However, since Hwi interrupts
637 * are already disabled in main(), such a call has no effect.
638 *
639 * @a(NOTE) 640 * Disables only IRQ interrupts
641 *
642 * @a(constraints) 643 * If a Task switching API such as
644 * {@link ti.sysbios.knl.Semaphore#pend Semaphore_pend()},
645 * {@link ti.sysbios.knl.Semaphore#post Semaphore_post()},
646 * {@link ti.sysbios.knl.Task#sleep Task_sleep()}, or
647 * {@link ti.sysbios.knl.Task#yield Task_yield()}
648 * is invoked which results in a context switch while
649 * interrupts are disabled, an embedded call to
650 * {@link #enable Hwi_enable} occurs
651 * on the way to the new thread context which unconditionally re-enables
652 * interrupts. Interrupts will remain enabled until a subsequent
653 * {@link #disable Hwi_disable}
654 * invocation.
655 *
656 * Swis always run with interrupts enabled.
657 * See {@link ti.sysbios.knl.Swi#post Swi_post()} for a discussion Swis and
658 * interrupts.
659 *
660 * @b(returns) opaque key for use by Hwi_restore()
661 */
662 @Macro
663 override UInt disable();
664
665 /*!
666 * ======== enable ========
667 *
668 * @a(NOTE) 669 * Enables only IRQ interrupts
670 */
671 @Macro
672 override UInt enable();
673
674 /*!
675 * ======== restore ========
676 *
677 * @a(NOTE) 678 * Restores only IRQ interrupts
679 */
680 @Macro
681 override Void restore(UInt key);
682
683 /*!
684 * ======== enableIRQ ========
685 * Enable IRQ interrupts.
686 *
687 * @a(NOTE) 688 * Same as Hwi_enable()
689 *
690 * @b(returns) previous IRQ interrupt enable/disable state
691 */
692 @Macro
693 UInt enableIRQ();
694
695 /*!
696 * ======== disableIRQ ========
697 * Disable IRQ interrupts.
698 *
699 * @a(NOTE) 700 * Same as Hwi_disable()
701 *
702 * @b(returns) previous IRQ interrupt enable/disable state
703 */
704 @Macro
705 UInt disableIRQ();
706
707 /*!
708 * ======== restoreIRQ ========
709 * Restore IRQ interrupts.
710 *
711 * @a(NOTE) 712 * Same as Hwi_restore()
713 *
714 * @param(key) enable/disable state to restore
715 */
716 @Macro
717 Void restoreIRQ(UInt key);
718
719 /*!
720 * ======== enableFIQ ========
721 * Enable FIQ interrupts.
722 *
723 * @b(returns) previous FIQ interrupt enable/disable state
724 */
725 @Macro
726 UInt enableFIQ();
727
728 /*!
729 * ======== disableFIQ ========
730 * Disable FIQ interrupts.
731 *
732 * @b(returns) previous FIQ interrupt enable/disable state
733 */
734 @Macro
735 UInt disableFIQ();
736
737 /*!
738 * ======== restoreFIQ ========
739 * Restore FIQ interrupts.
740 *
741 * @param(key) enable/disable state to restore
742 */
743 @Macro
744 Void restoreFIQ(UInt key);
745
746 /*!
747 * @_nodoc 748 * ======== disableFxn ========
749 * function call implementation
750 */
751 UInt disableFxn();
752
753 /*!
754 * @_nodoc 755 * ======== enableFxn ========
756 * function call implementation
757 */
758 UInt enableFxn();
759
760 /*!
761 * @_nodoc 762 * ======== restoreFxn ========
763 * function call implementation
764 */
765 Void restoreFxn(UInt key);
766
767 /*!
768 * ======== getHandle ========
769 * Returns Hwi_Handle associated with intNum
770 *
771 * @param(intNum) interrupt number
772 */
773 Handle getHandle(UInt intNum);
774
775 /*!
776 * @_nodoc 777 * ======== init ========
778 * assembly code mode registers setup
779 */
780 Void init();
781
782 /*!
783 * @_nodoc 784 * ======== initIntControllerCoreX ========
785 */
786 Void initIntControllerCoreX();
787
788 /*!
789 * ======== intAffinity ========
790 * SMP Interrupt affinity mappings
791 *
792 * In SMP mode, this array maps an interrupt number to the
793 * coreId it is to be tied to. By default, all ints are mapped to
794 * core 0.
795 *
796 * For example, to make Timer 1 from the ti.sysbios.timers.dmtimer.Timer
797 * module interrupt on core 1 rather than core 0, add the following to
798 * your config file:
799 *
800 * @p(code) 801 * var Hwi = xdc.useModule('ti.sysbios.family.arm.gic.Hwi');
802 * Hwi.intAffinity[<intNum>] = 1;
803 * @p 804 *
805 * @a(constraints) 806 * Interrupt numbers below 32 are ignored. This config param only
807 * allows routing interrupt numbers greater than or equal to #32.
808 */
809 metaonlyconfig UInt8 intAffinity[];
810
811 /*!
812 * @_nodoc 813 * ======== raiseSGI ========
814 */
815 Void raiseSGI(UInt mask, UInt intNum);
816
817 /*!
818 * ======== setPriority ========
819 * Set an interrupt's priority.
820 *
821 * Not an instance function so that it can be used
822 * with non-dispatched interrupts.
823 *
824 * @param(intNum) ID of interrupt
825 * @param(priority) priority
826 */
827 Void setPriority(UInt intNum, UInt priority);
828
829 instance:
830
831 /*!
832 * ======== type ========
833 * Interrupt type (IRQ/FIQ). Default is IRQ.
834 *
835 * @a(NOTE) 836 * FIQs are only supported when {@link #enableSecureMode} is set to
837 * true.
838 */
839 config Type type = Type_IRQ;
840
841 /*!
842 * ======== triggerSensitivity ========
843 * Set an interrupt's trigger sensitivity
844 *
845 * 2-bit field that configures the trigger sensitivity of an
846 * interrupt.
847 *
848 * On the Cortex-A15, all software generated interrupts (SGI)
849 * are edge-triggered (b10) and all private peripheral interrupts (PPI)
850 * are level-sensitive (b01). The trigger sensitivity of these
851 * interrupt types cannot be changed.
852 *
853 * For shared peripheral interrupts (SPI), the LSB of the bit-pair
854 * is read only and is always 1. The MSB of the bit-pair can be
855 * altered to change trigger sensitivity.
856 *
857 * Possible bit-pair encodings for Cortex-A15 SPIs:
858 * b01 Interrupt is active-High level-sensitive (default)
859 * b11 Interrupt is rising edge-sensitive
860 *
861 * For more information please refer section 4.3.13 on
862 * Interrupt Configuration Registers (GICD_ICFGRn) in
863 * ARM Generic Interrupt Controller Architecure Spec v2.0
864 */
865 config UInt triggerSensitivity = ~(0);
866
867 /*!
868 * ======== targetProcList ========
869 * Set an interrupt's target processor list.
870 *
871 * This is an 8-bit CPU targets field that stores the list of target
872 * processors for the interrupt. That is, it holds the list of CPU
873 * interfaces to which the GIC Distributor will forward the interrupt
874 * if it is asserted and has sufficient priority.
875 *
876 * Each bit in targetProcList refers to the corresponding processor.
877 * For instance, a value of 0x3 means the pending interrupt is
878 * forwarded to processor 0 and 1.
879 *
880 * For more information please refer section 4.3.12 on
881 * Interrupt Processor Targets Registers (GICD_ITARGETSRn) in
882 * ARM Generic Interrupt Controller Architecure Spec v2.0
883 *
884 * If running in {@link ti.sysbios.BIOS#smpEnabled SMP mode}
885 * and both the targetProcList Hwi param as well as the
886 * {@link #intAffinity}[] array entry for the intNum are set,
887 * targetProcList is given precedence and is used to configure
888 * the interrupt's target processors.
889 *
890 * @a(NOTE) 891 * Target processor list is read-only for the first 32 interrupts.
892 * Therefore, this field will have no effect for interrupt numbers
893 * less than 32 (intNum 0-31).
894 */
895 config UInt targetProcList = 0x0;
896
897 /*!
898 * ======== Interrupt priority ========
899 * Hwi instance interrupt priority.
900 *
901 * Valid priorities are device dependent and their
902 * nesting behaviors depend on the {@link #BPR} setting.
903 *
904 * See the ARM GIC Architecture Specification v2.0 document for more
905 * details.
906 */
907 overrideconfig Int priority = -1;
908
909 /*! The interrupt controller is designed for priority based interrupts */
910 overrideconfig IHwi.MaskingOption maskSetting = IHwi.MaskingOption_LOWER;
911
912 /*!
913 * ======== reconfig ========
914 * Reconfigure a dispatched interrupt.
915 */
916 Void reconfig(FuncPtr fxn, const Params *params);
917
918 internal: /* not for client use */
919
920 /*!
921 * ======== inUseMeta ========
922 * @_nodoc 923 * Check for Hwi already in use.
924 * For internal SYS/BIOS use only.
925 * Should be called prior to any internal Hwi.create().
926 *
927 * @param(intNum) interrupt number
928 */
929 metaonly Bool inUseMeta(UInt intNum);
930
931 /*
932 * Swi and Task module function pointers.
933 * Used to decouple Hwi from Swi and Task when
934 * dispatcherSwiSupport or
935 * dispatcherTaskSupport is false.
936 */
937 config UInt (*swiDisable)();
938 config Void (*swiRestoreHwi)(UInt);
939 config UInt (*taskDisable)();
940 config Void (*taskRestoreHwi)(UInt);
941
942 /*
943 * ======== postInit ========
944 * finish initializing static and dynamic Hwis
945 */
946 Int postInit(Object *hwi, Error.Block *eb);
947
948 /*
949 * ======== initIntControllerCore0 ========
950 */
951 Void initIntControllerCore0();
952
953 /* setup FIQ stack pointer */
954 Void initFIQStack(Ptr fiqStack);
955
956 /* default FIQ Interrupt Dispatcher */
957 Void dispatchFIQC();
958
959 /* Interrupt Dispatcher assembly code wrapper */
960 Void dispatchIRQ();
961
962 /* Interrupt Dispatcher C code */
963 Void dispatchIRQC(Irp irp);
964
965 /* non plugged interrupt handler */
966 Void nonPluggedHwiHandler(UArg arg);
967
968 /*!
969 * const array to hold all HookSet objects.
970 */
971 config HookSet hooks[length] = [];
972
973 /*! Meta World Only Hwi Configuration Object. */
974 metaonlystruct InterruptObj {
975 Bool used; /* Interrupt already defined? */
976 FuncPtr fxn; /* Dispatched ISR function */
977 };
978
979 /*!
980 * Meta-only array of interrupt objects.
981 * This meta-only array of Hwi config objects is initialized
982 * in Hwi.xs:module$meta$init().
983 */
984 metaonlyconfig InterruptObj interrupt[];
985
986 /*!
987 * GIC Distributor base address
988 */
989 metaonlyconfig Ptr gicdBaseAddress;
990
991 /*!
992 * GIC cpu interface base address
993 */
994 metaonlyconfig Ptr giccBaseAddress;
995
996 struct Instance_State {
997 Type type; // Interrupt Type
998 UInt priority; // Interrupt Priority
999 UArg arg; // Argument to Hwi function.
1000 FuncPtr fxn; // Hwi function.
1001 Irp irp; // current IRP
1002 Ptr hookEnv[];
1003 UInt triggerSensitivity;
1004 UInt targetProcList;
1005 };
1006
1007 struct Module_State {
1008 Char *taskSP[]; // temporary storage of interrupted
1009 // Task's SP during ISR execution
1010 Char *isrStack[]; // Points to isrStack address
1011 Char hwiStack[][]; // IRQ stack for each core
1012 Ptr isrStackSize; // = Program.stack
1013 // !!! The above three fields MUST be kept
1014 // !!! at the base of the module state
1015 // !!! GNU switchAndRunFunc and
1016 // !!! SMP Core module assumes it
1017 UInt32 iser[32]; // Initial Interrupt Set Enable Reg values
1018 UInt32 icfgr[]; // Initial Trigger sensitivity values
1019 UInt32 itargetsr[]; // Initial interrupt target processors
1020 UInt spuriousInts; // Count of spurious interrupts
1021 UInt lastSpuriousInt;// Most recent spurious interrupt
1022 UInt irp; // temporary irp storage for IRQ handler
1023 Ptr isrStackBase; // = __TI_STACK_BASE
1024 Hwi.Object nonPluggedHwi; // default Hwi object
1025 Handle dispatchTable[];// dispatch table
1026 volatile UInt curIntId; // current Interrupt Id
1027 UInt32 igroupr[]; // Initial Interrupt Group (0/1)
1028 Char fiqStack[][]; // buffers used for FIQ stacks
1029 SizeT fiqStackSize; // FIQ stack size
1030 UInt8 intAffinity[]; // smp int-to-coreId mappings
1031 };
1032 }