1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved.
     3     *  This program and the accompanying materials are made available under the
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*
    14     *  ======== ISystemSupport.xdc ========
    15     */
    16    package xdc.runtime;
    17    
    18    /*!
    19     *  ======== ISystemSupport ========
    20     *  Interface to core system functions.
    21     *
    22     *  Each embedded system requires implementations of these functions but
    23     *  the behavior of these functions varies depending on the context of the
    24     *  embedded system.  For example, some systems will implement `exit()` as
    25     *  an infinite loop because the executable is designed to *never* exit.
    26     */
    27    @DirectCall
    28    interface ISystemSupport {
    29    
    30        /*!
    31         *  ======== abort ========
    32         *  Backend for `{@link System#abort()}`
    33         *
    34         *  This function is called by `{@link System#abort()}` prior to calling
    35         *  the ANSI C Standard library function `abort()`.  So, to ensure the
    36         *  abort processing of the system's ANSI C Standard library completes,
    37         *  this function should return to its caller.
    38         *
    39         *  @param(str)  message to output just prior to aborting
    40         *
    41         *      If non-`NULL`, this string should be output just prior to
    42         *      terminating.
    43         */
    44        Void abort(CString str);
    45    
    46        /*!
    47         *  ======== exit ========
    48         *  Backend for `{@link System#exit()}`
    49         *
    50         *  This function is called as part the normal "atexit" processing
    51         *  performed by the ANSI C Standard Library's `exit()` function;
    52         *  `{@link System#exit()}` directly calls ANSI `exit()`.
    53         *
    54         *  This function is called after all "atexit" handlers bound via
    55         *  `{@link System#atexit()}` are run and it
    56         *  is always called while "inside" the the `System` gate.
    57         *
    58         *  To ensure that all exit processing of the system's ANSI C
    59         *  Standard Library completes, this function should return to its caller.
    60         *  Exit handlers bound using the ANSI C Standard Library `atexit()`
    61         *  function may run before or after this function.
    62         *
    63         *  @param(stat)    status value passed to all "atexit" handlers
    64         *
    65         *      This value is passed to all "atexit" handles bound via
    66         *      `{@link System#atexit()}`. 
    67         *
    68         *  @see System#atexit
    69         */
    70        Void exit(Int stat);
    71    
    72        /*!
    73         *  ======== flush ========
    74         *  Backend for `{@link System#flush()}`
    75         *
    76         *  This function is simply called by `{@link System#flush System_flush}`
    77         *  to output any characters buffered by the underlying `SystemSupport`
    78         *  module to an output device.
    79         */
    80        Void flush();
    81        
    82        /*!
    83         *  ======== putch ========
    84         *  Backend for `{@link System#printf()}` and `{@link System#putch()}`
    85         *
    86         *  Output a single character.  This function is called by
    87         *  `{@link System#printf System_printf()}` to write each character
    88         *  of formated output specified by its arguments.
    89    
    90         *
    91         *  @param(ch)  character to output
    92         */
    93        Void putch(Char ch);
    94    
    95        /*!
    96         *  ======== ready ========
    97         *  Test if character output can proceed
    98         *
    99         *  This function is called by `{@link System}` prior to performing
   100         *  any character output.  If this function returns `FALSE`, the `System`
   101         *  functions that would normally call `putch()` simply return
   102         *  (with an appropriate error status) without ever calling
   103         *  `{@link #putch}`.
   104         */
   105        Bool ready();
   106    }
   107    /*
   108     *  @(#) xdc.runtime; 2, 1, 0,0; 8-8-2017 17:30:59; /db/ztree/library/trees/xdc/xdc-D20/src/packages/
   109     */
   110