1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved. 
     3     *  This program and the accompanying materials are made available under the 
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at 
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*
    14     *  ======== HeapMin.xdc ========
    15     */
    16    
    17    import xdc.rov.ViewInfo;
    18    
    19    /*!
    20     *  ======== HeapMin ========
    21     *  Growth-only based heap implementation.
    22     *
    23     *  `HeapMin` is a minimal footprint heap implementation. This module is 
    24     *  is designed for applications that only create module instances and
    25     *  generally only allocate memory at runtime, but never delete created
    26     *  instances or free memory explicitly.
    27     *  
    28     *  For configuration-time `HeapMin.create`, the heap is aligned to 
    29     *  `{@link Memory#getMaxDefaultTypeAlignMeta()}` for those targets that support
    30     *  static alignment. For targets that do not support static alignment, the
    31     *  buffer alignment is undefined.
    32     *
    33     *  When calling `{@link #create()}` at runtime, the client 
    34     *  is responsible for aligning the buffer.
    35     */
    36    
    37    module HeapMin inherits xdc.runtime.IHeap {
    38    
    39        /*! @_nodoc */
    40        @XmlDtd
    41        metaonly struct BasicView {
    42            String          label;
    43            Ptr             buffer;
    44            Memory.Size     remainSize;
    45            Memory.Size     startSize;
    46        }
    47    
    48        /*! @_nodoc */
    49        @Facet
    50        metaonly config ViewInfo.Instance rovViewInfo =
    51            ViewInfo.create({
    52                viewMap: [
    53                [
    54                    'Basic',
    55                    {
    56                        type: ViewInfo.INSTANCE,
    57                        viewInitFxn: 'viewInitBasic',
    58                        structName: 'BasicView'
    59                    }
    60                ],
    61                ]
    62            });
    63        
    64        /*!
    65         *  ======== A_zeroSize ========
    66         *  Assert that the `{@link #size}` is non-zero on the create
    67         */     
    68        config Assert.Id A_zeroSize  =
    69            {msg: "HeapMin_create cannot have a zero size value"};
    70            
    71        /*! 
    72         *  ======== E_freeError ========
    73         *  Error raised if `{@link #free()}` is called.
    74         *
    75         *  This error is only raised if a `{@link #free()}`
    76         *  is called and `{@link #freeError}` is true.
    77         */
    78        config Error.Id E_freeError = {
    79            msg: "free() invalid in growth-only HeapMin"
    80        };
    81    
    82        /*!
    83         *  ======== freeError ========
    84         *  Flag to control whether `{@link #E_freeError}` is enabled.
    85         * 
    86         *  If true, a `{@link #E_freeError}` error occurs when trying 
    87         *  to free a buffer. 
    88         *
    89         *  If false, no error occurs and the `{@link #free()}` does nothing.
    90         */
    91        config Bool freeError = true;
    92    
    93    instance:
    94    
    95        /*!
    96         *  ======== align ========
    97         *  Alignment of the buffer being managed by this heap instance.
    98         *
    99         *  In the static HeapMin.create() call, the buffer allocated for the
   100         *  HeapMin instance will have the alignment specified by this parameter
   101         *  on targets that support static alignment.
   102         *
   103         *  In the dynamic case, the client must supply the buffer, so it is the
   104         *  client's responsibility to manage the buffer's alignment, and there is
   105         *  no 'align' parameter.
   106         *
   107         *  The specified `align` parameter must be a power of 2.
   108         *
   109         *  The default alignment of zero causes the buffer to get aligned using
   110         *  {@link Memory#getMaxDefaultTypeAlignMeta()}.
   111         */
   112        metaonly config SizeT align;
   113    
   114        /*!
   115         *  ======== create ========
   116         *  Create a `HeapMin` heap
   117         *
   118         *  This heap is a growth-only heap that is intended to be used by
   119         *  systems that never delete objects or free memory.  Objects can be
   120         *  created at runtime based on values determined at runtime, but
   121         *  objects can not be deleted.
   122         *
   123         *  @see HeapMin#Params
   124         */
   125        create();
   126        
   127        /*!
   128         *  ======== sectionName ========
   129         *  Section name of the heap
   130         *
   131         *  When creating heaps during configuration, this parameter specifies
   132         *  where the heap's buffer will be placed. This parameter is passed as
   133         *  the section name in the `{@link Memory#staticPlace}` function.
   134         *
   135         *  @see Memory#staticPlace
   136         */
   137        metaonly config String sectionName = null;
   138    
   139        /*!
   140         *  ======== buf ========
   141         *  Buffer that will be managed by the heap instance.
   142         *
   143         *  When creating a heap at runtime, the user must supply the memory
   144         *  that the heap will manage.  It is up to the caller to align
   145         *  the buffer as needed.
   146         *
   147         *  This parameter is ignored when creating heaps during configuration.
   148         */
   149        config Ptr buf = 0;
   150    
   151        /*!
   152         *  ======== size ========
   153         *  Size (in MADUs) of the heap.
   154         *
   155         *  This parameter specifies the size of the heap managed by a
   156         *  `HeapMin` instance.  In the static case, a buffer of length `size` 
   157         *  will be created.  In the dynamic case, `size` specifies the size of 
   158         *  the buffer (i.e. parameter `buf`) that the caller provides.
   159         *
   160         *  This is a required parameter. It must be set by the caller. Failure
   161         *  to do so, will result in a build error for the static create or an
   162         *  `{@link #A_zeroSize}` assert for the runtime create.
   163         */
   164        config Memory.Size size = 0;
   165        
   166        /*!
   167         *  ======== alloc ========
   168         *  Allocate a block of memory from the heap.
   169         *
   170         *  @a(Constraints)
   171         *  The alignment must be a power of 2.
   172         *
   173         *  @see IHeap#alloc
   174         */
   175        override Ptr alloc(SizeT size, SizeT align, Error.Block *eb);    
   176    
   177        /*!
   178         *  ======== free ========
   179         *  Free a block of memory back to the heap.
   180         *
   181         *  This is a growth only heap. Calling the `HeapMin_free` function
   182         *  will result in a `{@link #E_freeError}` error unless
   183         *  `{@link #freeError}` is set to `false`.
   184         *
   185         *  @see IHeap#free
   186         */
   187        override Void free(Ptr block, SizeT size);
   188        
   189        /*!
   190         *  ======== isBlocking ========
   191         *  Can this heap block the caller
   192         *
   193         *  @a(returns)
   194         *  `HeapMin` always returns `FALSE` since it never blocks on a
   195         *  resource.
   196         */
   197        override Bool isBlocking();    
   198    
   199    internal:
   200    
   201        struct Instance_State {
   202            Char        buf[];             /* Address of buffer being managed  */
   203            Memory.Size remainSize;        /* Size of remaining heap           */
   204            Memory.Size startSize;         /* Size of heap at the start        */
   205        };
   206    }
   207    /*
   208     *  @(#) xdc.runtime; 2, 1, 0,0; 8-8-2017 17:30:58; /db/ztree/library/trees/xdc/xdc-D20/src/packages/
   209     */
   210