1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved.
     3     *  This program and the accompanying materials are made available under the
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*
    14     *  ======== ITimestampClient.xdc ========
    15     */
    16    package xdc.runtime;
    17    
    18    /*!
    19     *  ======== ITimestampClient ========
    20     *  Timestamp Client Interface
    21     *
    22     *  This interface defines the methods used by client applications to
    23     *  get timestamp values.  It is implemented by the
    24     *  `{@link xdc.runtime.Timestamp Timestamp}` module.
    25     */
    26    @DirectCall
    27    interface ITimestampClient {
    28    
    29        /*!
    30         *  ======== get32 ========
    31         *  Return a 32-bit timestamp
    32         *
    33         *  @a(returns)
    34         *  Returns a 32-bit timestamp value.  
    35         *  Use `{@link #getFreq}` to convert this value into units of real time.
    36         *
    37         *  @see #get64
    38         */
    39        Bits32 get32();
    40    
    41        /*!
    42         *  ======== get64 ========
    43         *  Return a 64-bit timestamp
    44         *
    45         *  @param(result)  pointer to 64-bit result
    46         *
    47         *      This parameter is a pointer to a structure representing a 64-bit
    48         *      wide timestamp value where the current timestamp is written.
    49         *
    50         *      If the underlying hardware does not support 64-bit resolution, the
    51         *      `hi` field of `result` is always set to 0; see
    52         *      `{@link xdc.runtime.Types#Timestamp64}`.  So, it is possible for 
    53         *      the `lo` field to wrap around without any change to the `hi` field.
    54         *      Use `{@link #getFreq}` to convert this value into units of real 
    55         *      time.
    56         *
    57         *  @see #get32
    58         */
    59        Void get64(Types.Timestamp64 *result);
    60        
    61        /*!
    62         *  ======== getFreq ========
    63         *  Get the timestamp timer's frequency (in Hz)
    64         *
    65         *  @param(freq)  pointer to a 64-bit result
    66         *
    67         *      This parameter is a pointer to a structure representing a 64-bit
    68         *      wide frequency value where the timer's frequency (in Hz)
    69         *      is written; see `{@link xdc.runtime.Types#FreqHz}`.
    70         *      This function provides a way of converting timestamp 
    71         *      values into units of real time.
    72         *
    73         *  @see #get32
    74         *  @see #get64
    75         */
    76        Void getFreq(Types.FreqHz *freq);
    77    }
    78    /*
    79     *  @(#) xdc.runtime; 2, 1, 0,0; 12-9-2015 17:36:46; /db/ztree/library/trees/xdc/xdc-B06/src/packages/
    80     */
    81