1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved.
     3     *  This program and the accompanying materials are made available under the
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*!
    14     *  ======== ILogger ========
    15     *  Interface to service Log events
    16     *
    17     *  A logger is responsible for recording, transmitting, or otherwise
    18     *  handling `{@link Log#EventDesc Log Events}` generated by clients of the
    19     *  `{@link Log}` module. The `Log` module uses modules that implement the
    20     *  `ILogger` interface to record the log events. Most application code will
    21     *  use the `Log` module instead of directly calling the specific `ILogger`
    22     *  module implementation.
    23     *
    24     *  All logger implementations must inherit from this interface. The
    25     *  derived implementations must implement the functions defined in this
    26     *  interface but may also add additional configuration parameters and
    27     *  functions.
    28     *
    29     *  Events may be defined with a detail level, but the Log interface does not
    30     *  inherently provide support for filtering of events based on detail level.
    31     *  Instead, this is left to the ILogger implementation. ILogger
    32     *  implementations which wish to support filtering based on detail level
    33     *  should implement the IFilterLogger interface, which extends the ILogger
    34     *  interface to include APIs for getting and setting the current filter level.
    35     */
    36    @DirectCall
    37    interface ILogger {
    38    
    39        /*!
    40         *  ======== getMetaArgs ========
    41         *  Returns any meta data needed to support RTA.
    42         *
    43         *  This meta data should be returned in the form of a structure which
    44         *  can be converted into XML. This data is added to the RTA XML file
    45         *  during the application's configuration, and can be accessed later
    46         *  through the xdc.rta.MetaData module.
    47         *
    48         *  The MetaData is returned per instance of the ILogger module. The
    49         *  instance object is passed to the function as the first argument.
    50         *
    51         *  The second argument is the index of the instance in the list of 
    52         *  the ILogger's static instances.
    53         */
    54        function getMetaArgs(inst, instNum);
    55         
    56    instance:
    57    
    58        /*!
    59         *  ======== enable ========
    60         *  Enable a log
    61         *
    62         *  @a(returns)
    63         *  The function returns the state of the log (`TRUE` if enabled,
    64         *  `FALSE` if disabled) before the call. This return value allows 
    65         *  clients to restore the previous state.  
    66         *  Note: not thread safe.
    67         */
    68        Bool enable();
    69        
    70       /*!
    71         *  ======== disable ========
    72         *  Disable a log
    73         *
    74         *  Events written to a disabled log are silently discarded.
    75         *
    76         *  @a(returns)
    77         *  The function returns the state of the log (`TRUE` if enabled,
    78         *  `FALSE` if disabled) before the call. This return value allows 
    79         *  clients to restore the previous state.
    80         *  Note: not thread safe.
    81         */
    82        Bool disable(); 
    83            
    84        /*! 
    85         *  ======== write0 ========
    86         *  Process a log event with 0 arguments.
    87         *
    88         *  Same as `write4` except with 0 arguments rather than 4.
    89         *
    90         *  @see ILogger#write4()
    91         */
    92        Void write0(Log.Event evt, Types.ModuleId mid);
    93         
    94        /*! 
    95         *  ======== write1 ========
    96         *  Process a log event with 1 arguments.
    97         *
    98         *  Same as `write4` except with 1 arguments rather than 4.
    99         *
   100         *  @see ILogger#write4()
   101         */
   102        Void write1(Log.Event evt, Types.ModuleId mid, IArg a1);
   103    
   104        /*! 
   105         *  ======== write2 ========
   106         *  Process a log event with 2 arguments.
   107         *
   108         *  Same as `write4` except with 2 arguments rather than 4.
   109         *
   110         *  @see ILogger#write4()
   111         */
   112        Void write2(Log.Event evt, Types.ModuleId mid, IArg a1, IArg a2);
   113    
   114        /*! 
   115         *  ======== write4 ========
   116         *  Process a log event with up to 4 arguments.
   117         *
   118         *  The `evt` argument is of type Log.Event, which encodes the 
   119         *  `{@link Log#EventId}`, the `{@link Diags#Mask}`, and the 
   120         *  `{@link Diags#EventLevel}` of the event. The event ID can be obtained
   121         *  via `{@link Types#getEventId}(evt)`, the Diags mask can be obtained via
   122         *  `{@link Diags#getMask}(evt)`, and the event level can be obtained via
   123         *  `{@link Diags#getLevel}(evt)`.
   124         *  
   125         *  The `modId` argument is the module ID of the module that logged the
   126         *  event.
   127         *  
   128         *  The event information can be used by the logger to handle different 
   129         *  events specially. For example, the event ID can be used to compare 
   130         *  against other known `Log.Event`s.
   131         *  @p(code)
   132         *      if (Log_getEventId(MY_EVENT) == Log_getEventId(evt)) {
   133         *          :
   134         *      }
   135         *  @p
   136         *  The Diags mask and event level can be used for filtering of events 
   137         *  based on event level (see {@link IFilterLogger}), or even routing 
   138         *  events to separate loggers based on diags category (see, for example, 
   139         *  {@link LoggerBuf#statusLogger}). 
   140         *
   141         *  The Diags mask and event level are useful for handling the event, but 
   142         *  are generally not recorded by the logger because they are not needed in
   143         *  decoding and displaying the event. A more suitable value to record is a
   144         *  `{@link Types#Event}`, which encodes the event ID and module ID. For
   145         *  example, the `{@link Log#EventRec}` type stores a `{@link Types#Event}`
   146         *  in its record definition. A `{@link Types#Event}` can be created using
   147         *  the `{@link Types#makeEvent}` API given the event ID and module ID.
   148         *
   149         *  The event ID value of `0` is used to indicate an event triggered by a
   150         *  call to one of the `{@link Log#print0 Log_print[0-6]}` methods. These
   151         *  methods take a format string rather than a `Log_Event` argument and,
   152         *  as a result, the event ID encoded in `evt` is `0` and the parameter 
   153         *  `a1` is the format string.
   154         *
   155         *  Non-zero event IDs can also be used to access the `msg` string
   156         *  associated with the `{@link Log#EventDesc}` that originally
   157         *  defined the `Log` event.
   158         *  @p(code)
   159         *      Log_EventId id = Log_getEventId(evt));
   160         *      if (id != 0) {
   161         *          String msg = Text_ropeText(id);
   162         *          System_aprintf(msg, a1, a2, a3, a4);
   163         *      }
   164         *  @p
   165         *  This works because an event's ID is simply an offset into a table
   166         *  of characters (maintained by the `{@link Text}` module)
   167         *  containing the event's msg string.
   168         *
   169         *  The arguments a1, a2, etc. are parameters that are to be interpreted
   170         *  according to the message format string associated with `evt`.
   171         *
   172         *  @param(evt) event to be logged
   173         *  @param(mid) module ID of the module which logged the event
   174         *  @param(a1)  arbitrary argument passed by caller
   175         *
   176         *  @see Log#Event
   177         *  @see Log#EventDesc
   178         *  @see Text#ropeText
   179         *  @see Log#getEventId
   180         */
   181        Void write4(Log.Event evt, Types.ModuleId mid, IArg a1, IArg a2,
   182                    IArg a3, IArg a4);
   183    
   184        /*! 
   185         *  ======== write8 ========
   186         *  Process a log event with up to 8 arguments.
   187         *
   188         *  Same as `write4` except with 8 arguments rather than 4.
   189         *
   190         *  @see ILogger#write4()
   191         */
   192        Void write8(Log.Event evt, Types.ModuleId mid, IArg a1, IArg a2,
   193                    IArg a3, IArg a4, IArg a5, IArg a6, IArg a7, IArg a8);
   194    }
   195    /*
   196     *  @(#) xdc.runtime; 2, 1, 0,0; 12-9-2015 17:36:46; /db/ztree/library/trees/xdc/xdc-B06/src/packages/
   197     */
   198