1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved. 
     3     *  This program and the accompanying materials are made available under the 
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at 
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*!
    14     *  ======== IFilterLogger ========
    15     *  Interface for supporting filtering of Log events by detail level.
    16     *
    17     *  Filtering of events based on detail level is not inherently supported
    18     *  by the Log APIs as is filtering of events based on the diagnostics mask.
    19     *  
    20     *  Support for this type of filtering must be done by an `ILogger` 
    21     *  implementation. Not all users are interested in this filtering support,
    22     *  however, so it is not required of all `ILogger` implementations.
    23     *
    24     *  `ILoggers` that do intend to support filtering by detail level should 
    25     *  implement this interface, which extends the `ILogger` interface.
    26     *
    27     *  The `{@link #setFilterLevel}` and `{@link #getFilterLevel}` functions
    28     *  support runtime specification of a different filtering level for each of
    29     *  the diagnostics categories.
    30     */
    31    interface IFilterLogger inherits ILogger {
    32    
    33        /*!
    34         *  ======== filterByLevel ========
    35         *  Support filtering of events by event level
    36         *
    37         *  To improve logging performance, this feature can be disabled by setting
    38         *  `filterByLevel` to false.
    39         *
    40         *  See '{@link #setFilterLevel}' for an explanation of level filtering.
    41         */
    42        config Bool filterByLevel = false;
    43    
    44    instance:
    45    
    46        /*!
    47         *  ======== setFilterLevel ========
    48         *  Set the level of detail that instances will log
    49         *
    50         *  Events with the specified level or higher will be logged, events
    51         *  below the specified level will be dropped.
    52         *
    53         *  Events are filtered first by diags category, then by level. If an 
    54         *  event's diags category is disabled in the module's diags mask, then it 
    55         *  will be filtered out regardless of level. The event will not even be
    56         *  passed to the logger.
    57         *
    58         *  This API allows for setting the filtering level for more than one
    59         *  diags category at a time. The mask parameter can be a single category 
    60         *  or multiple categories combined, and the level will be set for all of
    61         *  those categories.   
    62         *
    63         *  @param(mask) The diags categories to set the level for
    64         *  @param(filterLevel) The new filtering level for the specified 
    65         *                      categories
    66         */
    67        Void setFilterLevel(Diags.Mask mask, Diags.EventLevel filterLevel);
    68        
    69        /*!
    70         *  ======== getFilterLevel ========
    71         *  Returns the mask of diags categories currently set to the specified 
    72         *  level.
    73         *
    74         *  See '{@link #setFilterLevel}' for an explanation of level filtering.
    75         */
    76        Diags.Mask getFilterLevel(Diags.EventLevel level);
    77    
    78    }
    79    /*
    80     *  @(#) xdc.runtime; 2, 1, 0,0; 12-9-2015 17:36:46; /db/ztree/library/trees/xdc/xdc-B06/src/packages/
    81     */
    82