1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31
32
33 package ti.sysbios.rom;
34
35 /*!
36 * ======== ROM.xdc ========
37 * ROM selection and support module.
38 *
39 * @a(CC26xx Device Users)
40 *
41 * To build a TI-RTOS application utilizing the ROM in a CC26xx device,
42 * add these lines to your configuration file:
43 *
44 * @p(code)
45 * var ROM = xdc.useModule('ti.sysbios.rom.ROM');
46 * ROM.romName = ROM.CC2650;
47 * @p
48 *
49 * @a(IAR Workbench Users of CC26xx Devices)
50 *
51 * IAR Workbench users should use the CC2650.icf file provided in the
52 * the following directory relative to the BIOS installation:
53 * @p(code)
54 * ti/sysbios/rom/cortexm/cc26xx/golden/CC26xx/CC2650.icf
55 * @p
56 *
57 * If for some reason you must use your own .icf file, then you are
58 * required to copy the contiguous block of 131 lines at the end of the
59 * above referenced CC2650.icf file starting with:
60 * @p(code)
61 * place at address mem:0x0000058c {readonly section .const_xdc_runtime_Error_policy__C};
62 * place at address mem:0x00000538 {readonly section .const_xdc_runtime_IModule_Interface__BASE__C};
63 * ...
64 * @p
65 * into your .icf file. Failing to do this will result in your application
66 * getting stuck in a forever loop at startup.
67 *
68 * @p(html)
69 * <br/>
70 * <br/>
71 * @p
72 *
73 * @a(CC13xx Device Users)
74 *
75 * To build a TI-RTOS application utilizing the ROM in a CC13xx device,
76 * add these lines to your configuration file:
77 *
78 * @p(code)
79 * var ROM = xdc.useModule('ti.sysbios.rom.ROM');
80 * ROM.romName = ROM.CC1350;
81 * @p
82 *
83 * @a(IAR Workbench Users of CC13xx Devices)
84 *
85 * IAR Workbench users should use the CC1350.icf file provided in the
86 * the following directory relative to the BIOS installation:
87 * @p(code)
88 * ti/sysbios/rom/cortexm/cc13xx/golden/CC13xx/CC1350.icf
89 * @p
90 *
91 * If for some reason you must use your own .icf file, then you are
92 * required to copy the contiguous block of 131 lines at the end of the
93 * above referenced CC1350.icf file starting with:
94 * @p(code)
95 * place at address mem:0x00001490 {readonly section .const_xdc_runtime_Error_policy__C};
96 * place at address mem:0x0000143c {readonly section .const_xdc_runtime_IModule_Interface__BASE__C};
97 * ...
98 * @p
99 * into your .icf file. Failing to do this will result in your application
100 * getting stuck in a forever loop at startup.
101 */
102
103 @Template('./ROM.xdt')
104 metaonly module ROM
105 {
106 enum RomName {
107 NO_ROM, /*! Default for NOT building against a ROM */
108 CC2650, /*! Use for all CC26xx devices */
109 CC2640R2F, /*! Use for all CC26xx R2 devices */
110 CC1350, /*! Use for all CC13xx devices */
111 F28004x, /*! Use for all F28004x class devices */
112 F28004x_P2, /*! Use for all F28004x P2 class devices */
113 CC2650_FLASH /*! THIS OPTION IS NOT SUPPORTED! */
114 };
115
116 /*!
117 * The name of the device being used.
118 * Currently only 'ROM.CC2650' and
119 * 'ROM.CC1350' are supported.
120 */
121 metaonly config RomName romName = NO_ROM;
122
123 /*! @_nodoc */
124 metaonly config String configDefs[];
125
126 /*!
127 * @_nodoc
128 * Defines an array of func pointers to allow
129 * indirect access to functions accessed from within ROM code
130 * but NOT to be included in the ROM.
131 *
132 * When the ROM is built, functions labels added to the excludedFuncs
133 * are -D defined as derefenced function calls.
134 *
135 * When an application is built, the API's corresponding function ptr
136 * is populated with the named function addresses.
137 */
138 metaonly config String excludedFuncs[];
139
140 /*! @_nodoc */
141 metaonly config String generatedFuncs[];
142
143 /*! @_nodoc */
144 metaonly config String otherLibs[];
145
146 /*! @_nodoc */
147 metaonly config String otherLibIncludes[];
148
149 /*! @_nodoc */
150 metaonly config String otherLibFuncs[];
151
152 /*! @_nodoc */
153 metaonly config Bool makePatch = false;
154
155
156 /*!
157 * @_nodoc
158 * ======== getOtherLibs ========
159 * Get the list of "-l lib"
160 * to link rom with.
161 */
162 metaonly String getOtherLibs();
163
164 /*!
165 * @_nodoc
166 * ======== getLibDefs ========
167 * Get the compiler -D mappings of the
168 * library funcs into function ptrs
169 */
170 metaonly String getOtherLibDefs();
171
172 /*!
173 * @_nodoc
174 * ======== getExternDefs ========
175 * Get the compiler -D mappings of the
176 * extern funcs into function ptrs
177 */
178 metaonly String getExternDefs();
179
180 /*!
181 * @_nodoc
182 * ======== getGeneratedDefs ========
183 * Get the compiler -D mappings of the
184 * generated funcs into function ptrs
185 */
186 metaonly String getGeneratedDefs();
187
188 /*!
189 * @_nodoc
190 * ======== getConfigDefs ========
191 * Get the list of module configuration -D's
192 */
193 metaonly String getConfigDefs();
194
195 /*!
196 * @_nodoc
197 * ======== getExterns ========
198 * Get the list of externally referenced symbols
199 */
200 metaonly String getExterns();
201
202
203 /*!
204 * @_nodoc
205 * ======== makeExternsFile ========
206 * Creates a file of name 'fileName' that includes the list of funcs
207 * defined in the excludedFuncs[] array.
208 */
209 function makeExternsFile(fileName);
210 }